/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#define LOG_TAG "light_hidl_hal_test"
#include <android-base/logging.h>
#include <android/hardware/light/2.0/ILight.h>
#include <android/hardware/light/2.0/types.h>
#include <VtsHalHidlTargetTestBase.h>
#include <set>
#include <unistd.h>
using ::android::hardware::light::V2_0::Brightness;
using ::android::hardware::light::V2_0::Flash;
using ::android::hardware::light::V2_0::ILight;
using ::android::hardware::light::V2_0::LightState;
using ::android::hardware::light::V2_0::Status;
using ::android::hardware::light::V2_0::Type;
using ::android::hardware::hidl_vec;
using ::android::hardware::Return;
using ::android::hardware::Void;
using ::android::sp;
#define ASSERT_OK(ret) ASSERT_TRUE(ret.isOk())
#define EXPECT_OK(ret) EXPECT_TRUE(ret.isOk())
const static LightState kWhite = {
.color = 0xFFFFFFFF,
.flashMode = Flash::TIMED,
.flashOnMs = 100,
.flashOffMs = 50,
.brightnessMode = Brightness::USER,
};
const static LightState kLowPersistance = {
.color = 0xFF123456,
.flashMode = Flash::TIMED,
.flashOnMs = 100,
.flashOffMs = 50,
.brightnessMode = Brightness::LOW_PERSISTENCE,
};
const static LightState kOff = {
.color = 0x00000000,
.flashMode = Flash::NONE,
.flashOnMs = 0,
.flashOffMs = 0,
.brightnessMode = Brightness::USER,
};
const static std::set<Type> kAllTypes = {
Type::BACKLIGHT,
Type::KEYBOARD,
Type::BUTTONS,
Type::BATTERY,
Type::NOTIFICATIONS,
Type::ATTENTION,
Type::BLUETOOTH,
Type::WIFI
};
class LightHidlTest : public ::testing::VtsHalHidlTargetTestBase {
public:
virtual void SetUp() override {
light = ::testing::VtsHalHidlTargetTestBase::getService<ILight>();
ASSERT_NE(light, nullptr);
LOG(INFO) << "Test is remote " << light->isRemote();
ASSERT_OK(light->getSupportedTypes([this](const hidl_vec<Type> &types) {
supportedTypes = types;
}));
}
sp<ILight> light;
std::vector<Type> supportedTypes;
virtual void TearDown() override {
for (const Type& type: supportedTypes) {
Return<Status> ret = light->setLight(type, kOff);
EXPECT_OK(ret);
EXPECT_EQ(Status::SUCCESS, static_cast<Status>(ret));
}
// must leave the device in a useable condition
if (std::find(supportedTypes.begin(),
supportedTypes.end(),
Type::BACKLIGHT) != supportedTypes.end()) {
Return<Status> ret = light->setLight(Type::BACKLIGHT, kWhite);
EXPECT_OK(ret);
EXPECT_EQ(Status::SUCCESS, static_cast<Status>(ret));
}
}
};
/**
* Ensure all lights which are reported as supported work.
*/
TEST_F(LightHidlTest, TestSupported) {
for (const Type& type: supportedTypes) {
Return<Status> ret = light->setLight(type, kWhite);
EXPECT_OK(ret);
EXPECT_EQ(Status::SUCCESS, static_cast<Status>(ret));
}
}
/**
* Ensure BRIGHTNESS_NOT_SUPPORTED is returned if LOW_PERSISTANCE is not supported.
*/
TEST_F(LightHidlTest, TestLowPersistance) {
for (const Type& type: supportedTypes) {
Return<Status> ret = light->setLight(type, kLowPersistance);
EXPECT_OK(ret);
Status status = ret;
EXPECT_TRUE(Status::SUCCESS == status ||
Status::BRIGHTNESS_NOT_SUPPORTED == status);
}
}
/**
* Ensure lights which are not supported return LIGHT_NOT_SUPPORTED
*/
TEST_F(LightHidlTest, TestUnsupported) {
std::set<Type> unsupportedTypes = kAllTypes;
for (const Type& type: supportedTypes) {
unsupportedTypes.erase(type);
}
for (const Type& type: unsupportedTypes) {
Return<Status> ret = light->setLight(type, kWhite);
EXPECT_OK(ret);
EXPECT_EQ(Status::LIGHT_NOT_SUPPORTED, static_cast<Status>(ret));
}
}
int main(int argc, char **argv) {
::testing::InitGoogleTest(&argc, argv);
int status = RUN_ALL_TESTS();
LOG(INFO) << "Test result = " << status;
return status;
}