/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
package android.hardware.media.omx@1.0;
import IOmxBufferSource;
import android.hardware.media@1.0::types;
/**
* Ref: frameworks/av/include/media/IOMX.h: IOMXNode
* Ref: https://www.khronos.org/registry/omxil/specs/OpenMAX_IL_1_1_2_Specification.pdf
*/
/**
* IOmxNode is an interface for communicating with an OMX component (called
* "node" here) that has been previously obtained by calling
* IOmx::allocateNode().
*/
interface IOmxNode {
/**
* Free the node.
*
* @param[out] status will be the status of the call.
*/
freeNode(
) generates (
Status status
);
/**
* Invoke a command on the node.
*
* @param[in] cmd indicates the type of the command.
* @param[in] param is a parameter for the command.
* @param[out] status will be the status of the call.
*
* @see OMX_SendCommand() in the OpenMax IL standard.
*/
sendCommand(
uint32_t cmd,
int32_t param
) generates (
Status status
);
/**
* Retrieve a parameter setting from the node.
*
* @param[in] index indicates the type of the parameter to retrieve.
* @param[in] inParams holds some information about the retrieval.
* @param[out] status will be the status of the call.
* @param[out] outParams will be the current parameter setting.
*
* @see OMX_GetParameter() in the OpenMax IL standard.
*/
getParameter(
uint32_t index,
Bytes inParams // TODO: describe structure better or point at standard
) generates (
Status status,
Bytes outParams // TODO: describe structure better or point at standard
);
/**
* Change a parameter setting of the node.
*
* @param[in] index indicates the type of the parameter to change.
* @param[in] params holds the new parameter setting.
* @param[out] status will be the status of the call.
*
* @see OMX_SetParameter() in the OpenMax IL standard.
*/
setParameter(
uint32_t index,
Bytes params // TODO: describe structure better or point at standard
) generates (
Status status
);
/**
* Retrieve a configuration from the node.
*
* @param[in] index indicates the type of the configuration to retrieve.
* @param[in] inConfig holds some information about the retrieval.
* @param[out] status will be the status of the call.
* @param[out] outConfig will be the current configuration.
*
* @see OMX_GetConfig() in the OpenMax IL standard.
*/
getConfig(
uint32_t index,
Bytes inConfig // TODO: describe structure better or point at standard
) generates (
Status status,
Bytes outConfig // TODO: describe structure better or point at standard
);
/**
* Change a configuration of the node.
*
* @param[in] index indicates the type of the configuration to change.
* @param[in] config holds the new configuration.
* @param[out] status will be the status of the call.
*
* @see OMX_SetConfig() in the OpenMax IL standard.
*/
setConfig(
uint32_t index,
Bytes config // TODO: describe structure better or point at standard
) generates (
Status status
);
/**
* Set the mode of a port on the node.
*
* @param[in] portIndex is the index of the port.
* @param[in] mode is the target mode on the specified port.
*/
setPortMode(
uint32_t portIndex,
PortMode mode
) generates (
Status status
);
/**
* Prepare a port for adaptive playback. This is based on the extension
* "OMX.google.android.index.prepareForAdaptivePlayback".
*
* @param[in] portIndex is the index of the port.
* @param[in] enable indicates whether adaptive playback is enabled or not.
* @param[in] maxFrameWidth specifies the maximum frame width.
* @param[in] maxFrameHeight specifies the maximum frame height.
* @param[out] status status will be the status of the call.
*/
prepareForAdaptivePlayback(
uint32_t portIndex,
bool enable,
uint32_t maxFrameWidth,
uint32_t maxFrameHeight
) generates (
Status status
);
/**
* Configure a port for a tunneled playback mode. This is based on the
* extension "OMX.google.android.index.configureVideoTunnelMode".
*
* @param[in] portIndex is the index of the port.
* @param[in] tunneled indicates whether the tunneled mode is used or not.
* @param[in] audioHwSync is the HW SYNC ID of the audio HAL output stream
* to sync the video with.
* @param[out] status will be the status of the call.
* @param[out] sidebandHandle will contain the codec-allocated sideband
* window handle.
*/
configureVideoTunnelMode(
uint32_t portIndex,
bool tunneled,
uint32_t audioHwSync
) generates (
Status status,
handle sidebandHandle
);
/**
* Retrieve the buffer usage on a port. This is based on the extension
* "OMX.google.android.index.getAndroidNativeBufferUsage".
*
* @param[in] portIndex is the index of the port.
* @param[out] status will be the status of the call.
* @param[out] usage will be the usage.
*/
getGraphicBufferUsage(
uint32_t portIndex
) generates (
Status status,
uint32_t usage // TODO: Ask graphics team to define an enum.
);
/**
* Set up a listener to events related to the input surface.
*
* @param[in] bufferSource is the listener object that implements
* IOmxBufferSource.
* @param[out] status will be the status of the call.
*
* @see IOmxBufferSource.
*/
setInputSurface(
IOmxBufferSource bufferSource
) generates (
Status status
);
/**
* Allocate an opaque buffer on a port as a native handle.
*
* @param[in] portIndex is the index of the port.
* @param[in] size is the desired size of the buffer.
* @param[out] status will be the status of the call.
* @param[out] buffer will be the id of the allocated buffer, which will be
* needed in some other buffer-related function calls.
* @param[out] nativeHandle will be the native handle of the allocated
* buffer.
*
* @see OMX_AllocateBuffer() in the OpenMax IL standard.
*/
allocateSecureBuffer(
uint32_t portIndex,
uint64_t size
) generates (
Status status,
BufferId buffer,
handle nativeHandle
);
/**
* Assign a buffer to a port.
*
* @param[in] portIndex is the index of the port.
* @param[in] omxBuffer is the buffer to be assigned to the port.
* @param[out] status will be the status of the call.
* @param[out] buffer will be the id of the assigned buffer, which will be
* needed in some other buffer-related function calls.
*
* @see OMX_UseBuffer() in the OpenMax IL standard.
*/
useBuffer(
uint32_t portIndex,
CodecBuffer omxBuffer
) generates (
Status status,
BufferId buffer
);
/**
* Free a buffer previously assigned to a port by allocateSecureBuffer() or
* useBuffer().
*
* @param[in] portIndex is the index of the port.
* @param[in] buffer is the id of the buffer to be freed.
* @param[out] status will be the status of the call.
*
* @see OMX_FreeBuffer() in the OpenMax IL standard.
*/
freeBuffer(
uint32_t portIndex,
BufferId buffer
) generates (
Status status
);
/**
* Pass \p fence to the node if it supports fences. Otherwise, it waits on
* \p fence before calling OMX_FillThisBuffer(). The node will take
* ownership of the fence even if this call fails.
*
* If the port is in metadata mode, the buffer will be updated to point to
* the new buffer passed in via \p omxBuffer before OMX_FillThisBuffer() is
* called. Otherwise, \p omxBuffer is not used.
*
* @param[in] buffer is the id of the buffer to fill.
* @param[in] omxBuffer points to the new buffer in metadata mode.
* @param[in] fence is the fence to wait for (if not null).
* @param[out] status is the status of the call.
*
* @see OMX_FillThisBuffer() in the OpenMax IL standard.
*/
fillBuffer(
BufferId buffer,
CodecBuffer omxBuffer,
Fence fence
) generates (
Status status
);
/**
* Pass \p fence to the node if it supports fences. Otherwise, wait on
* \p fence before calling OMX_EmptyThisBuffer(). The node will take
* ownership of the fence even if this call fails.
*
* If the port is in metadata mode, the buffer will be updated to point to
* the new buffer passed in via \p omxBuffer before OMX_EmptyThisBuffer() is
* called. Otherwise, \p omxBuffer is not used.
*
* @param[in] buffer is the id of the buffer to fill.
* @param[in] omxBuffer points to the new buffer in metadata mode.
* @param[in] flags is put into the header information that is passed to
* OMX_EmptyBuffer().
* @param[in] timestampUs is put into the header information that is passed
* to OMX_EmptyBuffer().
* @param[in] fence is the fence to wait for (if not null).
* @param[out] status is the status of the call.
*
* @see OMX_EmptyThisBuffer() in the OpenMax IL standard.
*/
emptyBuffer(
BufferId buffer,
CodecBuffer omxBuffer,
uint32_t flags, // TODO: describe structure better or point at standard
uint64_t timestampUs,
Fence fence
) generates (
Status status
);
/**
* Request the node to translate an extension string to an index.
*
* @param[in] parameterName is the requested extension string.
* @param[out] status is the status of the call.
* @param[out] index is the translated index.
*
* @see OMX_GetExtensionIndex() in the OpenMax IL standard.
*/
getExtensionIndex(
string parameterName
) generates (
Status status,
uint32_t index
);
/**
* Add an OMX message on the node's message queue. The instance of
* IOmxObserver that was obtained during the creation of the node will
* receive the message in batches by the callback
* IOmxObserver::onMessages().
*
* @param[in] msg is the message to send.
* @param[out] status is the status of the call.
*
* @see IOmxObserver::onMessages().
*/
dispatchMessage(
Message msg
) generates (
Status status
);
};