/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
package android.hardware.memtrack@1.0;
/**
* The Memory Tracker HAL is designed to return information about
* device-specific memory usage.
* The primary goal is to be able to track memory that is not
* trackable in any other way, for example texture memory that is allocated by
* a process, but not mapped in to that process's address space.
* A secondary goal is to be able to categorize memory used by a process into
* GL, graphics, etc. All memory sizes must be in real memory usage,
* accounting for stride, bit depth, rounding up to page size, etc.
*
* Constructor for the interface should be used to perform memtrack management
* setup actions and is called once before any calls to getMemory().
*/
interface IMemtrack {
/**
* getMemory() populates MemtrackRecord vector with the sizes of memory
* plus associated flags for that memory.
*
* This function must be thread-safe, it may get called from multiple
* threads at the same time.
*
* A process collecting memory statistics will call getMemory for each
* combination of pid and memory type. For each memory type that it
* recognizes, the HAL must fill out an array of memtrack_record
* structures breaking down the statistics of that memory type as much as
* possible. For example,
* getMemory(<pid>, GL) might return:
* { { 4096, ACCOUNTED | PRIVATE | SYSTEM },
* { 40960, UNACCOUNTED | PRIVATE | SYSTEM },
* { 8192, ACCOUNTED | PRIVATE | DEDICATED },
* { 8192, UNACCOUNTED | PRIVATE | DEDICATED } }
* If the HAL cannot differentiate between SYSTEM and DEDICATED memory, it
* could return:
* { { 12288, ACCOUNTED | PRIVATE },
* { 49152, UNACCOUNTED | PRIVATE } }
*
* Memory must not overlap between types. For example, a graphics buffer
* that has been mapped into the GPU as a surface must show up when
* GRAPHICS is requested and not when GL
* is requested.
*
* @param pid process for which memory information is requested
* @param type memory type that information is being requested about
* @return records vector of MemtrackRecord containing memory information
* @return retval SUCCESS on success, TYPE_NOT_FOUND if the type is not
* supported.
*/
getMemory(int32_t pid, MemtrackType type)
generates (MemtrackStatus retval, vec<MemtrackRecord> records);
};