summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorKevin Rocard2017-12-02 00:15:39 -0600
committerKeun Soo Yim2018-01-23 16:42:18 -0600
commit5b21eaa608485ba6f898c917919fcf7df5955fff (patch)
tree5dc03592033d60e332f355676d6d63f60f84f2bc /media/omx/1.0
parent96b6fcdc4f3695e63f1a7a6a847396f4a09f4c1b (diff)
downloadplatform-hardware-interfaces-5b21eaa608485ba6f898c917919fcf7df5955fff.tar.gz
platform-hardware-interfaces-5b21eaa608485ba6f898c917919fcf7df5955fff.tar.xz
platform-hardware-interfaces-5b21eaa608485ba6f898c917919fcf7df5955fff.zip
Audio HAL: Allow setters to not be implemented
setSampleRate, setChannelMask, setFormat may not be implemented by the HAL, although this is not documented in the HAL API. Currently the VTS test requires their implementation if the respective getSupported{SampleRate,ChannelMask,Format} are supported. Relax this requirement as the framework never calls those setters. Note that the optionality of those functions will be documented in the next HAL API version. Test: vts-tradefed run commandAndExit vts --module VtsHalAudioV2_0Target -t CheckConfig.audioPolicyConfigurationValidation Bug: 69811500 Change-Id: I3a390ae925cabd99e7f1ed4a627e71ad87b1b437 Merged-In: I3a390ae925cabd99e7f1ed4a627e71ad87b1b437 Signed-off-by: Kevin Rocard <krocard@google.com> (cherry picked from commit 3bcba14c36062583372e903385fc4447fbcee394)
Diffstat (limited to 'media/omx/1.0')
0 files changed, 0 insertions, 0 deletions