summaryrefslogtreecommitdiffstats
path: root/wifi
diff options
context:
space:
mode:
authorTreeHugger Robot2018-05-21 15:43:04 -0500
committerAndroid (Google) Code Review2018-05-21 15:43:04 -0500
commit62b35058a3a1b69e683ab3f8dc53aa3f1337cdc1 (patch)
treec359aef0b5ff881cb1c8c629be0eec68d720cfea /wifi
parentcce4c95c1c4bd47ffb1c35605afc90fa288611e2 (diff)
parenta67fdff49b8964acf212cdbd342ccc0bb171e6d1 (diff)
downloadplatform-hardware-interfaces-62b35058a3a1b69e683ab3f8dc53aa3f1337cdc1.tar.gz
platform-hardware-interfaces-62b35058a3a1b69e683ab3f8dc53aa3f1337cdc1.tar.xz
platform-hardware-interfaces-62b35058a3a1b69e683ab3f8dc53aa3f1337cdc1.zip
Merge "[AWARE] Developer documentation on HAL usage" into pi-dev
Diffstat (limited to 'wifi')
-rw-r--r--wifi/1.0/README-NAN.md6
-rw-r--r--wifi/1.2/README-NAN.md231
2 files changed, 234 insertions, 3 deletions
diff --git a/wifi/1.0/README-NAN.md b/wifi/1.0/README-NAN.md
index f4b3320e..645c9f94 100644
--- a/wifi/1.0/README-NAN.md
+++ b/wifi/1.0/README-NAN.md
@@ -14,7 +14,7 @@ limitations under the License.
14 14
15# Wi-Fi Aware (NAN) HAL API Usage 15# Wi-Fi Aware (NAN) HAL API Usage
16 16
17The Wi-Fi Aware (NAN) HAL API is defined in (<i>hardware/interfaces/wifi/\<version\>/</i>): 17The Wi-Fi Aware (NAN) HAL API is defined in (<i>hardware/interfaces/wifi/1.0/</i>):
18 18
19* IWifiNanIface.hal 19* IWifiNanIface.hal
20* IWifiNanIfaceEventCallback.hal 20* IWifiNanIfaceEventCallback.hal
@@ -23,7 +23,7 @@ The Wi-Fi Aware (NAN) HAL API is defined in (<i>hardware/interfaces/wifi/\<versi
23The Wi-Fi Aware (NAN) HAL API surface is very large - only a subset is used from the framework. 23The Wi-Fi Aware (NAN) HAL API surface is very large - only a subset is used from the framework.
24 24
25Understanding of the HAL API subset which is actively used by the Android framework can be deduced 25Understanding of the HAL API subset which is actively used by the Android framework can be deduced
26by reviewing framework code, specifically (<i>frameworks/opt/net/wif/</i>): 26by reviewing framework code, specifically (<i>frameworks/opt/net/wifi/</i>):
27 27
28* WifiAwareNativeApi.java 28* WifiAwareNativeApi.java
29* WifiAwareNativeCallback.java 29* WifiAwareNativeCallback.java
@@ -41,7 +41,7 @@ the new HAL API only. To understand the mapping between new and legacy HALs plea
41 41
42Format: 42Format:
43* Hard-coded values are in <b>bold</b>, e.g. <b>true</b> or <b>5</b> 43* Hard-coded values are in <b>bold</b>, e.g. <b>true</b> or <b>5</b>
44* Assigned but not fixed value are specified using the <i>variable</i> keyword, possibly with some 44* Assigned but not fixed values are specified using the <i>variable</i> keyword, possibly with some
45details/constraints 45details/constraints
46* Unassigned values are specified using the <i>N/A</i> keyword. Unassigned usually means initialized 46* Unassigned values are specified using the <i>N/A</i> keyword. Unassigned usually means initialized
47to 0. 47to 0.
diff --git a/wifi/1.2/README-NAN.md b/wifi/1.2/README-NAN.md
new file mode 100644
index 00000000..00b91690
--- /dev/null
+++ b/wifi/1.2/README-NAN.md
@@ -0,0 +1,231 @@
1Copyright 2018 The Android Open Source Project
2
3Licensed under the Apache License, Version 2.0 (the "License");
4you may not use this file except in compliance with the License.
5You may obtain a copy of the License at
6
7 http://www.apache.org/licenses/LICENSE-2.0
8
9Unless required by applicable law or agreed to in writing, software
10distributed under the License is distributed on an "AS IS" BASIS,
11WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
12See the License for the specific language governing permissions and
13limitations under the License.
14
15# Wi-Fi Aware (NAN) HAL API Usage
16
17The Wi-Fi Aware (NAN) HAL API is defined in (<i>hardware/interfaces/wifi/1.0/</i> and
18<i>hardware/interfaces/wifi/1.2/</i>):
19
20* IWifiNanIface.hal
21* IWifiNanIfaceEventCallback.hal
22* types.hal (structure definitions)
23
24Note that the <i>1.2</i> HAL is supplemental to the <i>1.0</i> HAL - not a replacement.
25
26The Wi-Fi Aware (NAN) HAL API surface is very large - only a subset is used from the framework.
27
28Understanding of the HAL API subset which is actively used by the Android framework can be deduced
29by reviewing framework code, specifically (<i>frameworks/opt/net/wifi/</i>):
30
31* WifiAwareNativeApi.java
32* WifiAwareNativeCallback.java
33
34The above framework files determine the API usage - and should be consulted as the authoritative
35reference. Please consult the primary HAL file for documentation - they will not be replicated
36in this document. APIs which are in the HAL but are not listed in this README file are not used by
37the framework.
38
39Note: the HAL API is translated to the legacy HAL API (<i>wifi_nan.h</i>). This README file covers
40the new HAL API only. To understand the mapping between new and legacy HALs please consult
41<i>hardware/interfaces/wifi/\<version\>/default/hidl_struct_util.cpp</i>.
42
43## IWifiNanIface
44
45Format:
46* Hard-coded values are in <b>bold</b>, e.g. <b>true</b> or <b>5</b>
47* Assigned but not fixed values are specified using the <i>variable</i> keyword, possibly with some
48details/constraints
49* Unassigned values are specified using the <i>N/A</i> keyword. Unassigned usually means initialized
50to 0.
51
52APIs:
53
54* registerEventCallback_1_2(IWifiNanIfaceEventCallback_1_2 callback)
55* getCapabilitiesRequest
56* enableRequest_1_2
57 * NanEnableRequest
58 * bool[2] operateInBand
59 * Index [NanBandIndex.NAN_BAND_24GHZ] = <b>true</b>
60 * Index [NanBandIndex.NAN_BAND_5GHZ] = <i>variable</i>
61 * uint8_t hopCountMax = <b>2</b>
62 * NanConfigRequest configParams
63 * uint8_t masterPref = <i>variable</i>
64 * bool disableDiscoveryAddressChangeIndication = <i>variable</i>
65 * bool disableStartedClusterIndication = <i>variable</i>
66 * bool disableJoinedClusterIndication = <i>variable</i>
67 * bool includePublishServiceIdsInBeacon = <b>true</b>
68 * uint8_t numberOfPublishServiceIdsInBeacon = <b>0</b>
69 * bool includeSubscribeServiceIdsInBeacon = <b>true</b>
70 * uint8_t numberOfSubscribeServiceIdsInBeacon = <b>0</b>
71 * uint16_t rssiWindowSize = <b>8</b>
72 * uint32_t macAddressRandomizationIntervalSec = <i>variable</i>
73 * Normal run-time: set to <b>1800</b> (30 minutes)
74 * Tests: set to <b>120</b> (2 minutes)
75 * NanBandSpecificConfig[2] bandSpecificConfig
76 * Index [NanBandIndex.NAN_BAND_24GHZ]
77 * uint8_t rssiClose = <b>60</b>
78 * uint8_t rssiMiddle = <b>70</b>
79 * uint8_t rssiCloseProximity = <b>60</b>
80 * uint8_t dwellTimeMs = <b>200</b>
81 * uint16_t scanPeriodSec = <b>20</b>
82 * bool validDiscoveryWindowIntervalVal = <i>variable</i>
83 * uint8_t discoveryWindowIntervalVal = <i>variable</i>
84 * Index [NanBandIndex.NAN_BAND_5GHZ]
85 * uint8_t rssiClose = <b>60</b>
86 * uint8_t rssiMiddle = <b>75</b>
87 * uint8_t rssiCloseProximity = <b>60</b>
88 * uint8_t dwellTimeMs = <b>200</b>
89 * uint16_t scanPeriodSec = <b>20</b>
90 * bool validDiscoveryWindowIntervalVal = <i>variable</i>
91 * uint8_t discoveryWindowIntervalVal = <i>variable</i>
92 * NanDebugConfig debugConfigs
93 * bool validClusterIdVals = <b>true</b>
94 * uint16_t clusterIdBottomRangeVal = <i>variable</i>
95 * uint16_t clusterIdTopRangeVal = <i>variable</i>
96 * bool validIntfAddrVal = <b>false</b>
97 * MacAddress intfAddrVal = <i>N/A</i>
98 * bool validOuiVal = <b>false</b>
99 * uint32_t ouiVal = <i>N/A</i>
100 * bool validRandomFactorForceVal = <b>false</b>
101 * uint8_t randomFactorForceVal = <i>N/A</i>
102 * bool validHopCountForceVal = <b>false</b>
103 * uint8_t hopCountForceVal = <i>N/A</i>
104 * bool validDiscoveryChannelVal = <b>false</b>
105 * WifiChannelInMhz[2] discoveryChannelMhzVal = <i>N/A</i>
106 * bool validUseBeaconsInBandVal = <b>false</b>
107 * bool[2] useBeaconsInBandVal = <i>N/A</i>
108 * bool validUseSdfInBandVal = <b>false</b>
109 * bool[2] useSdfInBandVal = <i>N/A</i>
110 * NanConfigRequestSupplemental
111 * uint32_t discoveryBeaconIntervalMs = <b>0</b>
112 * uint32_t numberOfSpatialStreamsInDiscovery = <b>0</b>
113 * bool enableDiscoveryWindowEarlyTermination = <b>false</b>
114 * bool enableRanging = <b>true</b>
115* configRequest_1_2
116 * NanConfigRequest: same as for <i>enableRequest_1_2</i>
117* disableRequest
118* startPublishRequest
119 * NanPublishRequest
120 * NanDiscoveryCommonConfig baseConfigs
121 * uint8_t sessionId = <i>variable</i>
122 * uint16_t ttlSec = <i>variable</i>
123 * uint16_t discoveryWindowPeriod = <b>1</b>
124 * uint8_t discoveryCount = <b>0</b>
125 * vec<uint8_t> serviceName = <i>variable</i>
126 * NanMatchAlg discoveryMatchIndicator = <b>NanMatchAlg.MATCH_NEVER</b>
127 * vec<uint8_t> serviceSpecificInfo = <i>variable</i>
128 * vec<uint8_t> extendedServiceSpecificInfo = <i>N/A</i>
129 e vec<uint8_t> rxMatchFilter = <i>variable</i>
130 * vec<uint8_t> txMatchFilter = <i>variable</i>
131 * bool useRssiThreshold = <b>false</b>
132 * bool disableDiscoveryTerminationIndication = <i>variable</i>
133 * bool disableMatchExpirationIndication = <b>true</b>
134 * bool disableFollowupReceivedIndication = <b>false</b>
135 * NanDataPathSecurityConfig securityConfig = <b>NanDataPathSecurityType.OPEN</b>
136 * bool rangingRequired = <b>false</b>
137 * uint32_t rangingIntervalMsec = <i>N/A</i>
138 * bitfield<NanRangingIndication> configRangingIndications = <i>N/A</i>
139 * uint16_t distanceIngressCm = <i>N/A</i>
140 * uint16_t distanceEgressCm = <i>N/A</i>
141 * NanPublishType publishType = <i>variable</i>
142 * NanTxType txType = <b>NanTxType.BROADCAST</b>
143 * bool autoAcceptDataPathRequests = <b>false</b>
144* stopPublishRequest
145* startSubscribeRequest
146 * NanSubscribeRequest
147 * NanDiscoveryCommonConfig baseConfigs
148 * Mostly same as <i>publish</i> above except:
149 * NanMatchAlg discoveryMatchIndicator = <b>NanMatchAlg.MATCH_ONCE</b>
150 * NanSubscribeType subscribeType = <i>variable</i>
151 * NanSrfType srfType = <i>N/A</i>
152 * bool srfRespondIfInAddressSet = <i>N/A</i>
153 * bool shouldUseSrf = <i>N/A</i>
154 * bool isSsiRequiredForMatch = <i>N/A</i>
155 * vec<MacAddress> intfAddr = <i>N/A</i>
156* stopSubscribeRequest
157* transmitFollowupRequest
158 * NanTransmitFollowupRequest
159 * uint8_t discoverySessionId = <i>variable</i>
160 * uint32_t peerId = <i>variable</i>
161 * MacAddress addr = <i>variable</i>
162 * bool isHighPriority = <b>false</b>
163 * bool shouldUseDiscoveryWindow = <b>true</b>
164 * vec<uint8_t> serviceSpecificInfo = <i>variable</i>
165 * vec<uint8_t> extendedServiceSpecificInfo = <i>N/A</i>
166 * bool disableFollowupResultIndication = <b>false</b>
167* createDataInterfaceRequest
168* deleteDataInterfaceRequest
169* initiateDataPathRequest
170 * NanInitiateDataPathRequest
171 * uint32_t peerId = <i>variable</i>
172 * MacAddress peerDiscMacAddr = <i>variable</i>
173 * NanDataPathChannelCfg channelRequestType =
174 <i>NanDataPathChannelCfg.CHANNEL_NOT_REQUESTED</i>
175 * WifiChannelInMhz channel = <b>2437</b> (note that should be ignored though -
176 CHANNEL_NOT_REQUESTED!)
177 * string ifaceName = <i>variable</i>
178 * NanDataPathSecurityConfig securityConfig = <i>variable</i>
179 * vec<uint8_t> appInfo = <i>N/A</i>
180 * vec<uint8_t> serviceNameOutOfBand = <i>variable</i>
181* respondToDataPathIndicationRequest
182 * NanRespondToDataPathIndicationRequest
183 * bool acceptRequest = <i>variable</i>
184 * uint32_t ndpInstanceId = <i>variable</i>
185 * string ifaceName = <i>variable</i>
186 * NanDataPathSecurityConfig securityConfig = <i>variable</i>
187 * vec<uint8_t> appInfo = <i>N/A</i>
188 * vec<uint8_t> serviceNameOutOfBand = <i>variable</i>
189* terminateDataPathRequest
190
191## IWifiNanIfaceEventCallback_1_2
192
193Format:
194* Parameters whose values are <i>ignored</i> will be flagged, otherwise the parameter value is used
195by the framework.
196
197API:
198
199* notifyXxxResponse: all callbacks are used by framework
200* eventClusterEvent
201* eventDisabled
202* eventPublishTerminated
203* eventSubscribeTerminated
204* eventMatch
205 * NanMatchInd (all parameters are used except those listed below)
206 * vec<uint8_t> extendedServiceSpecificInfo: <i>ignored</i>
207 * bool matchOccuredInBeaconFlag: <i>ignored</i>
208 * bool outOfResourceFlag: <i>ignored</i>
209 * uint8_t rssiValue: <i>ignored</i>
210 * NanCipherSuiteType peerCipherType: <i>ignored</i>
211 * bool peerRequiresSecurityEnabledInNdp: <i>ignored</i>
212 * bool peerRequiresRanging: <i>ignored</i>
213 * uint32_t rangingMeasurementInCm: <i>ignored</i>
214 * bitfield<NanRangingIndication> rangingIndicationType: <i>ignored</i>
215* eventMatchExpired: <i>ignored</i>
216* eventFollowupReceived
217 * NanFollowupReceivedInd (all parameters are used except those listed below)
218 * bool receivedInFaw: <i>ignored</i>
219 * vec<uint8_t> extendedServiceSpecificInfo: <i>ignored</i>
220* eventTransmitFollowup
221* eventDataPathRequest
222 * NanDataPathRequestInd (all parameters are used except those listed below)
223 * bool securityRequired: <i>ignored</i>
224 * vec<uint8_t> appInfo: <i>ignored</i>
225* eventDataPathConfirm
226 * NanDataPathConfirmInd (all parameters are used except those listed below)
227 * vec<uint8_t> appInfo: <i>ignored</i>
228* eventDataPathScheduleUpdate
229 * NanDataPathScheduleUpdateInd
230* eventDataPathTerminated
231