summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
-rw-r--r--camera/device/1.0/ICameraDeviceCallback.hal2
-rw-r--r--camera/metadata/3.2/types.hal8
-rw-r--r--current.txt4
3 files changed, 2 insertions, 12 deletions
diff --git a/camera/device/1.0/ICameraDeviceCallback.hal b/camera/device/1.0/ICameraDeviceCallback.hal
index 1dfcd805..4e2e7192 100644
--- a/camera/device/1.0/ICameraDeviceCallback.hal
+++ b/camera/device/1.0/ICameraDeviceCallback.hal
@@ -33,8 +33,6 @@ interface ICameraDeviceCallback {
33 * Define a memory buffer from the provided handle and size, and return a 33 * Define a memory buffer from the provided handle and size, and return a
34 * unique identifier for the HAL to use to reference it with. 34 * unique identifier for the HAL to use to reference it with.
35 * 35 *
36 * TODO(b/33269977): Ensure this aligns with design and performance goals.
37 *
38 * @param descriptor A native handle that must have exactly one file 36 * @param descriptor A native handle that must have exactly one file
39 * descriptor in it; the file descriptor must be memory mappable to 37 * descriptor in it; the file descriptor must be memory mappable to
40 * bufferSize * bufferCount bytes. 38 * bufferSize * bufferCount bytes.
diff --git a/camera/metadata/3.2/types.hal b/camera/metadata/3.2/types.hal
index 2b4b2878..17d1d5e9 100644
--- a/camera/metadata/3.2/types.hal
+++ b/camera/metadata/3.2/types.hal
@@ -16,14 +16,6 @@
16 16
17package android.hardware.camera.metadata@3.2; 17package android.hardware.camera.metadata@3.2;
18 18
19/** TODO(b/33012412):
20 * - The following information should be code-generated from:
21 * system/media/camera/docs/metadata_properties.xml
22 * - Some enum below should be signed:
23 * - metadata section/key should be unsigned
24 * - matadata value enum should be signed
25 */
26
27/** 19/**
28 * Top level hierarchy definitions for camera metadata. *_INFO sections are for 20 * Top level hierarchy definitions for camera metadata. *_INFO sections are for
29 * the static metadata that can be retrived without opening the camera device. 21 * the static metadata that can be retrived without opening the camera device.
diff --git a/current.txt b/current.txt
index 82a1626c..701c11e5 100644
--- a/current.txt
+++ b/current.txt
@@ -50,14 +50,14 @@ da6ab32ee2793d2c86d3b603075d5383852b89d7eaa201861aa0473d418f3c7f android.hardwar
50bd42c8d7838cfed1998b49c39745dec116d2d6edc2c11a4c0399b8f3a1d1655a android.hardware.broadcastradio@1.0::types 50bd42c8d7838cfed1998b49c39745dec116d2d6edc2c11a4c0399b8f3a1d1655a android.hardware.broadcastradio@1.0::types
5181164323115d6588e259e8319fddf7487adfa1f49ce60f7e80ba74e0783392a4 android.hardware.camera.common@1.0::types 5181164323115d6588e259e8319fddf7487adfa1f49ce60f7e80ba74e0783392a4 android.hardware.camera.common@1.0::types
52c1705e9d62438a1d955269965af915ae28e692bd480a3b1ce67056fef992d62f android.hardware.camera.device@1.0::ICameraDevice 52c1705e9d62438a1d955269965af915ae28e692bd480a3b1ce67056fef992d62f android.hardware.camera.device@1.0::ICameraDevice
532b6f81bba23b652736184d19f76a2358e9bb5f5295133406d155f0d37c7bac40 android.hardware.camera.device@1.0::ICameraDeviceCallback 5378e9b44cf8660bdc1e98dca07451804153824efcd28db208a62f5ad728f44076 android.hardware.camera.device@1.0::ICameraDeviceCallback
5428f0386ba86ddf41e53a8117b48a0328d7a4d2574213e89f4a1062398a244566 android.hardware.camera.device@1.0::ICameraDevicePreviewCallback 5428f0386ba86ddf41e53a8117b48a0328d7a4d2574213e89f4a1062398a244566 android.hardware.camera.device@1.0::ICameraDevicePreviewCallback
554db48439ce9dde97f1cfb3d7408f6c737f621ac0f7494aeea35ed599bc2352a3 android.hardware.camera.device@1.0::types 554db48439ce9dde97f1cfb3d7408f6c737f621ac0f7494aeea35ed599bc2352a3 android.hardware.camera.device@1.0::types
56b32f9aeaf1c442195eb06ffc7600968c919d005b2718874f09c57287fae55918 android.hardware.camera.device@3.2::ICameraDevice 56b32f9aeaf1c442195eb06ffc7600968c919d005b2718874f09c57287fae55918 android.hardware.camera.device@3.2::ICameraDevice
5763bfc3da0f2d2301f7a0508c7c2b9ffc521d4d545ee03718da70e9d6273b3b21 android.hardware.camera.device@3.2::ICameraDeviceCallback 5763bfc3da0f2d2301f7a0508c7c2b9ffc521d4d545ee03718da70e9d6273b3b21 android.hardware.camera.device@3.2::ICameraDeviceCallback
580fa3e1e64819283b8737fc4e5ab759f0cb4ac1a996e8a51cc4aa8025a457208e android.hardware.camera.device@3.2::ICameraDeviceSession 580fa3e1e64819283b8737fc4e5ab759f0cb4ac1a996e8a51cc4aa8025a457208e android.hardware.camera.device@3.2::ICameraDeviceSession
59030be3d2b159cbde7920485807140f6b6064ef4a5de4a40a6c4bc8d2c72f7cd3 android.hardware.camera.device@3.2::types 59030be3d2b159cbde7920485807140f6b6064ef4a5de4a40a6c4bc8d2c72f7cd3 android.hardware.camera.device@3.2::types
60a2dc9063c950f73d72a83797412d5ed25e905225d4650baf2c674c4263160295 android.hardware.camera.metadata@3.2::types 605ba7947cee515d7a2359bfcbfb9678c1c3a768c288471919ac095b96ae6f3d40 android.hardware.camera.metadata@3.2::types
61f7e299d85033ac52d1095a35784fcfeaff43603f58c751e4153c85bbade3b330 android.hardware.camera.provider@2.4::ICameraProvider 61f7e299d85033ac52d1095a35784fcfeaff43603f58c751e4153c85bbade3b330 android.hardware.camera.provider@2.4::ICameraProvider
62a501ca1aecd09f1b9fd70a9af84205430dbd49a808e8fa395d363b9902e6f58c android.hardware.camera.provider@2.4::ICameraProviderCallback 62a501ca1aecd09f1b9fd70a9af84205430dbd49a808e8fa395d363b9902e6f58c android.hardware.camera.provider@2.4::ICameraProviderCallback
637f5fe8f4f8a24037153c504d8b4d3313c2ce33d81c8c69fe5194ddd2d4080e72 android.hardware.configstore@1.0::ISurfaceFlingerConfigs 637f5fe8f4f8a24037153c504d8b4d3313c2ce33d81c8c69fe5194ddd2d4080e72 android.hardware.configstore@1.0::ISurfaceFlingerConfigs