diff options
Diffstat (limited to 'neuralnetworks/1.0/IDevice.hal')
-rw-r--r-- | neuralnetworks/1.0/IDevice.hal | 2 |
1 files changed, 1 insertions, 1 deletions
diff --git a/neuralnetworks/1.0/IDevice.hal b/neuralnetworks/1.0/IDevice.hal index 49c29674..62fb2bae 100644 --- a/neuralnetworks/1.0/IDevice.hal +++ b/neuralnetworks/1.0/IDevice.hal | |||
@@ -36,7 +36,7 @@ interface IDevice { | |||
36 | /** | 36 | /** |
37 | * Gets the supported operations in a model. | 37 | * Gets the supported operations in a model. |
38 | * | 38 | * |
39 | * getSupportedSubgraph indicates which operations of a model are fully | 39 | * getSupportedOperations indicates which operations of a model are fully |
40 | * supported by the vendor driver. If an operation may not be supported for | 40 | * supported by the vendor driver. If an operation may not be supported for |
41 | * any reason, getSupportedOperations must return false for that operation. | 41 | * any reason, getSupportedOperations must return false for that operation. |
42 | * | 42 | * |