diff options
Diffstat (limited to 'neuralnetworks/1.0/types.hal')
-rw-r--r-- | neuralnetworks/1.0/types.hal | 2 |
1 files changed, 1 insertions, 1 deletions
diff --git a/neuralnetworks/1.0/types.hal b/neuralnetworks/1.0/types.hal index c97a00be..a9c91cd4 100644 --- a/neuralnetworks/1.0/types.hal +++ b/neuralnetworks/1.0/types.hal | |||
@@ -44,7 +44,7 @@ enum OperandType : int32_t { | |||
44 | * | 44 | * |
45 | * Attached to this tensor are two numbers that can be used to convert the | 45 | * Attached to this tensor are two numbers that can be used to convert the |
46 | * 8 bit integer to the real value and vice versa. These two numbers are: | 46 | * 8 bit integer to the real value and vice versa. These two numbers are: |
47 | * - scale: a 32 bit floating point value | 47 | * - scale: a 32 bit floating point value greater than zero |
48 | * - zero_value: a 32 bit integer | 48 | * - zero_value: a 32 bit integer |
49 | * | 49 | * |
50 | * The formula is: | 50 | * The formula is: |