diff options
Diffstat (limited to 'neuralnetworks/1.1/IDevice.hal')
-rw-r--r-- | neuralnetworks/1.1/IDevice.hal | 2 |
1 files changed, 1 insertions, 1 deletions
diff --git a/neuralnetworks/1.1/IDevice.hal b/neuralnetworks/1.1/IDevice.hal index ca225554..d2c48433 100644 --- a/neuralnetworks/1.1/IDevice.hal +++ b/neuralnetworks/1.1/IDevice.hal | |||
@@ -41,7 +41,7 @@ interface IDevice extends @1.0::IDevice { | |||
41 | /** | 41 | /** |
42 | * Gets the supported operations in a model. | 42 | * Gets the supported operations in a model. |
43 | * | 43 | * |
44 | * getSupportedSubgraph indicates which operations of a model are fully | 44 | * getSupportedOperations indicates which operations of a model are fully |
45 | * supported by the vendor driver. If an operation may not be supported for | 45 | * supported by the vendor driver. If an operation may not be supported for |
46 | * any reason, getSupportedOperations must return false for that operation. | 46 | * any reason, getSupportedOperations must return false for that operation. |
47 | * | 47 | * |