| Commit message (Collapse) | Author | Age | Files | Lines |
|\ |
|
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Added few more parameters required for IWLAN handover to
the existing data call setup/deactive APIs.
Test: Telephony sanity tests
bug: 64132030
Change-Id: I7bb04fc5f32908fa064370d5123252022a166abc
|
|\ \ |
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Bug: 64203181
Test: make vts
vts-tradefed run vts -m VtsHalSensorsV1_0Target
Change-Id: I1f7e3a8adf58bbeeb0928185a61f16610dd76223
|
|\ \ \
| |_|/
|/| |
| | |
| | |
| | | |
* changes:
Compatibility matrices: add minor revision to kernel versions
Compatibility matrices: kernel req at each FCM version
|
| | |
| | |
| | |
| | |
| | |
| | | |
Test: builds
Bug: 72388844
Change-Id: Id60cef10610f39d70eebccbeb6e625e3d93795c6
|
| |/
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
* devices with Shipping FCM version
legacy / O / O-MR1 use 3.18, 4.4, 4.9
* devices with Shipping FCM version P use 4.4 4.9
Bug: 72389707
Test: manual inspection on
$OUT/system/etc/vintf/compatibility_matrix.*.xml
Change-Id: I4f37325c0210f88e9e6d3e7136a82d50da3e93fe
|
| |
| |
| |
| |
| |
| | |
Bug: 70638175
Test: make
Change-Id: I1a4259542176cf44556131bb2b57107d51b2410e
|
| |
| |
| |
| |
| |
| |
| |
| | |
Also adds the new requisite types and an IndicationFilter for reporting.
Bug: 70638175
Test: n/a
Change-Id: I29f5fba4d1b21af3e7fda876c9a5c911936aeada
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Enables setting various reporting criteria for unsolicited signal
strength and LCE reports. Creates a new LCE report including both up and
down bandwidths. Updates documentation for various IndicationFilter bits
to add clarity.
Bug: 70638175
Test: n/a
Change-Id: If8141fbd89baf85ed5ee65d589f111907a9bf8b4
|
|\ \ |
|
| |/
| |
| |
| |
| |
| | |
Bug: 64131518
Test: Basic telephony sanity
Change-Id: I6bd6c6c46f8f70fd13b6c02ddfe399e04190133a
|
|\ \
| |/
|/| |
|
| |
| |
| |
| |
| |
| |
| |
| | |
Was accidentally copy-pasted here.
Bug: N/A
Test: setprop ctl.start blank_screen
Change-Id: I0b100b02aecd2649f2528834f431a0bc8b164c46
|
|\ \ |
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Hal interface for runtime management of USB gadget confiuguration.
Bug: 63669128
Test: Manually tested usb gadget hal for usb configurations
Change-Id: I1913dd5b99fdf4d710a2b0695c616c1d27575c53
|
|\ \ \ |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Add camera removal support to CameraProvider and CameraModule.
Change-Id: I047e486d1665ba9e0b1455f77a7bbbb5e0d66653
Signed-off-by: Guennadi Liakhovetski <guennadi.liakhovetski@intel.com>
|
|\ \ \ \
| |_|_|/
|/| | | |
|
| |/ /
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
SIM slot related APIs are not related to any radio/modem, so they need
to be migrate to a different HAL which is not related to any
radio/modem.
Bug: 64131518
Test: Basic telephony sanity
Change-Id: I626f13c5f6fb39091f6bddd5b6d373f09561af90
|
|/ /
| |
| |
| |
| |
| |
| |
| |
| |
| | |
This can be transitioned to by init to shutdown the
screen thereby preventing init from either depending
on binder or accessing halified sysnodes directly.
Bug: 70846424
Test: manual + init use
Change-Id: I86893ee5d7118547cd073297c0626e474f366b82
|
|\ \ |
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
According to the camera_module_t::get_number_of_cameras() description
in camera_common.h, it should only return the number of "fixed"
cameras, i.e. cameras, facing to the front and to the back. Any
cameras, with the facing value of "external," i.e. externally connected
cameras, should not be reported by it, instead they should later be
reported, using the
camera_module_callbacks_t::camera_device_status_change() callback.
However, this doesn't work. When a camera is reported this way, it is
ignored as unknown. Fix this by adding a new camera, when its status
change is reported.
Change-Id: I18874ed005f477e32fb723c00c16b67a81cde6ce
Signed-off-by: Guennadi Liakhovetski <guennadi.liakhovetski@intel.com>
|
|\ \ \ |
|
| | |/
| |/|
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
This dependency is imported but not used, so it should technically
go in the Android.bp file.
Bug: 71863483
Test: none
Change-Id: I3ee391bdea47182689156b3243b75a3572f7d8bf
|
|/ /
| |
| |
| |
| |
| |
| |
| | |
Some have missed being updated.
Bug: N/A
Test: N/A
Change-Id: I0925e85701f6e8b98f9b09bfafbed73469d1d185
|
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Rename Gralloc0Allocator to Gralloc0Hal and make it inherit from
AllocatorHal. Do the same to Gralloc1Allocator. Add GrallocLoader
to load either of Gralloc[01]Hal and create a IAllocator instance.
Test: boots and VTS
Change-Id: I09ae680c0086ca9e73e412a34d7cd2f3665d3bc2
|
| |
| |
| |
| |
| | |
Test: builds
Change-Id: I01cee2e7bc778f2e3e540a9856c25f1a0e390186
|
| |
| |
| |
| |
| |
| |
| |
| | |
Convert the default impl into a static library,
android.hardware.graphics.allocator@2.0-passthrough.
Test: boots and VTS
Change-Id: I8ec8b30766462ecb3fb789af7c6dbb3c088ccf57
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Add a header-only library
android.hardware.graphics.allocator@2.0-hal that can be used by
implementations. An imlpementation can
class VendorHal : public AllocatorHal { ... };
auto allocator = std::make_unique<Allocator>();
allocator->init(std::make_unique<VendorHal>(...));
Or, if vendor extensions are to be added to the IAllocator,
class AlocatorHalExt : public AllocatorHal { ... };
class VendorHal : public AllocatorHalExt { ... };
class AllocatorExt : public AllocatorImpl<IAllocatorExt, AllocatorHalExt> { ... };
auto allocator = std::make_unique<AllocatorExt>();
allocator->init(std::make_unique<VendorHal>(...));
Test: builds
Change-Id: I7cb7a4888316b871e5c49d96524b1642fc708f2d
|
| |
| |
| |
| |
| |
| |
| |
| | |
Move libgralloc1-adapter from 2.0/default/ to
2.0/utils/gralloc1-adapter/. Fix build issues after the move.
Test: builds
Change-Id: I674fe60c724a4ffc1540c796b92209a1dbf36438
|
|\ \ |
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Moved framework_compatibility_matrix.xml module definition
from target/board/Android.mk here because it depends on
compatibility_matrix.*.xml.
Test: m dist
Bug: 69636193
Change-Id: I7480b27756992b47555f6b397925170ae9d1ac22
|
|\ \ \
| |/ /
|/| | |
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
As part of the new NetworkScan API project, we need to add V1_2
cellInfoList in RadioIndication to support the V1_2 CellInfo as well.
Bug: 63984327, 69058403
Test: Basic telephony sanity
Change-Id: I53deb0d3b6ba58a86a8f734618841ff91d6dc6fa
|
|\ \ \ |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
So that init knows how to start it and to provide
an example of how to specify interfaces since there
are no lazy starting services on Pixel yet.
In order to make lights a lazy service, it would also
have to be marked as 'oneshot'.
Test: manually using Light as a lazy service
Bug: 64678982
Merged-In: I846a7e2d9545b42af9b985adb74883bda1b8c355
Change-Id: I846a7e2d9545b42af9b985adb74883bda1b8c355
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
FCM Version uses a different set of numbers than the SDK level.
This is to decouple the connection between them; it is not required
to have one FCM Version per SDK level.
Test: build test
Test: boots
Bug: 69636193
Change-Id: I62a29b702271d8a7ca8ae80e545a6d2e3b46fdcf
Merged-In: I62a29b702271d8a7ca8ae80e545a6d2e3b46fdcf
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
When a device is restarted, the UART may go away before the
packetizer. Print an error and sleep in case it isn't really
a restart.
Bug: 70855323
Test: Repeated restarts, check for Bluetooth tombstones
Change-Id: I2b4e677451e826d40dcc9d063d80dc0e17fc9aca
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Add mutex in function Send() and OnTimeout() to do mutual
exclusive access on lpm_wake_deasserted.
If lpm_wake_deasserted is out of sync with the actual
wake state, then platforms which use the lpm hint
will break.
Bug: 64299848
Test: run affected platform for a long period of time
and find that hci commands do not time out
Change-Id: I9f630d6f40f84b9c047c6488632cd44d6602bb14
|
|/ / /
| | |
| | |
| | |
| | |
| | |
| | | |
Test: lunch walleye_coverage-userdebug && make
verify configstore@1.0.policy is not generated.
Change-Id: Iad1f55fe10c2c77a3ca56418ec315e10ab71753f
|
|\ \ \ |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Add a test method to IBaz to test struct with a composed interface
Test: hidl_test_java/ internal master
Bug: 70529597
Change-Id: I73eaaf3dda6a24b88207729f31c75454c005c8cf
|
| |_|/
|/| |
| | |
| | |
| | |
| | |
| | |
| | | |
Test: Compile
Bug: 63760809
Change-Id: I582c259ca0787a701d434eea9592c9e8d7351f08
Merged-In: I582c259ca0787a701d434eea9592c9e8d7351f08
(cherry picked from commit 3ba20e6b6bef8059e0c366107e85965f5a433bdf)
|
|\ \ \
| |_|/
|/| | |
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Doesn't do anything, not part of the language.
Bug: 71545356
Test: none
Change-Id: I5fce87a9cf01ff546f2b7b177b60454b8bfbf106
|
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Discovered by the upcoming compiler update.
Test: m checkbuild
Change-Id: I03ed479a6a5c42d8dcc192e85d5268d1cd65cab8
|
|\ \ \ |
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Add below new interfaces, corresponding response interface and structures.
- getSimSlotsStatus()
- setSimSlotsMapping()
- simSlotsStatusChanged()
Bug: 68998818
Test: compliation
Change-Id: Ia532c502782ef4d08d27f18ee0321a3ceaa94dcf
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
- Add AssertionResult in gtest to display logs
- Refactor all the error checks
- Replace INTERNAL_ERR with INVALID_ARGUMENT for
requestIsimAuthentication
- Add missing SIM_ABSENT from ag/2582439/
- Fix incorrect indentation
Bug: 63760809
Bug: 65150146
Test: run vts
Change-Id: Id3d876ea515f47998e3e45be11db5edf306ffc24
Merged-In: Id3d876ea515f47998e3e45be11db5edf306ffc24
(cherry picked from commit e986b85fddeb3412606840e4cdc76051e3cc966e)
|