summaryrefslogtreecommitdiffstats
path: root/radio
Commit message (Expand)AuthorAgeFilesLines
* Update VTS tests so that more tests pass for O.Sanket Padawe2017-08-015-18/+34
* Merge "Add owners for radio vts." into oc-mr1-devTreeHugger Robot2017-08-012-0/+14
|\
| * Add owners for radio vts.Sanket Padawe2017-07-312-0/+14
* | Add EMPTY_RECORD for getDeviceIdentitysqian2017-07-312-52/+2
|/
* Merge "Add corresponding error code to fix vts test" into oc-mr1-devShuo Qian2017-07-312-15/+23
|\
| * Add corresponding error code to fix vts testsqian2017-07-282-15/+23
* | RadioV1_1 VTS Tests: startKeepalive, stopKeepaliveNathan Harold2017-07-283-6/+125
|\ \ | |/ |/|
| * RadioV1_1 VTS Tests: startKeepalive, stopKeepaliveNathan Harold2017-07-283-6/+125
* | Merge "Add vts test for setCarrierInfoForImsiEncryption" into oc-dr1-devShuo Qian2017-07-282-1/+26
|\|
| * Add vts test for setCarrierInfoForImsiEncryptionsqian2017-07-272-1/+26
* | Merge "Fix VTS errors of the network scan API" into oc-dr1-devYing Xu2017-07-261-3/+6
|\|
| * Fix VTS errors of the network scan APIyinxu2017-07-251-3/+6
* | Merge "Add Sim absent assertion in the setup" into oc-dr1-devShuo Qian2017-07-242-0/+8
|\|
| * Merge "Add Sim absent assertion in the setup" into oc-dr1-devShuo Qian2017-07-242-0/+8
| |\
| | * Add Sim absent assertion in the setupsqian2017-07-212-0/+8
| * | Update VTS tests so that more tests pass for O.Sanket Padawe2017-07-245-32/+53
| |/
* | Merge " Add VTS code for the network scan API" into oc-dr1-devYing Xu2017-07-202-2/+76
|\|
| * Merge " Add VTS code for the network scan API" into oc-dr1-devYing Xu2017-07-202-2/+76
| |\
| | * Add VTS code for the network scan APIyinxu2017-07-182-2/+76
* | | Merge changes from topic 'b/62584347' into oc-dr1-dev am: 696cb63064Shuo Qian2017-07-192-13/+8
|\| |
| * | Modified error code for OPERATION_NOT_ALLOWEDsqian2017-07-181-3/+3
| * | Change mapping of QMI errorNaina Nalluri2017-07-171-10/+5
| * | Merge "Fix some VTS for 2017 devices" into oc-dr1-devShuo Qian2017-07-171-13/+26
| |\ \ | | |/ | |/|
| | * Fix some VTS for 2017 devicessqian2017-07-131-13/+26
* | | Merge "Fix some VTS for 2017 devices"Shuo Qian2017-07-171-16/+26
|\ \ \
| * | | Fix some VTS for 2017 devicessqian2017-07-131-16/+26
* | | | Merge "Add RadioIndication for Radio VTS test" into oc-dr1-dev am: 7e26812206Shuo Qian2017-07-179-87/+1820
|\ \ \ \ | |/ / / |/| / / | |/ /
| * | Merge "Add RadioIndication for Radio VTS test" into oc-dr1-devShuo Qian2017-07-179-87/+1820
| |\ \
| | * | Add RadioIndication for Radio VTS testsqian2017-07-149-87/+1820
| | |/
* | | Merge "Add an empty 1.1 ISap interface." into oc-dr1-dev am: 48d56695ceAmit Mahajan2017-07-133-0/+70
|\| |
| * | Add an empty 1.1 ISap interface.Amit Mahajan2017-07-123-0/+70
| |/
* | Merge "Update .hal file for radio 1.0 hal" into oc-dr1-dev am: c631963d4bShuo Qian2017-06-281-0/+1
|\ \
| * | Merge "Update .hal file for radio 1.0 hal" into oc-dr1-devShuo Qian2017-06-281-0/+1
| |\|
| | * Merge "Update .hal file for radio 1.0 hal" into oc-dr1-devShuo Qian2017-06-281-0/+1
| | |\
| | | * Update .hal file for radio 1.0 halsqian2017-06-281-0/+1
| * | | Merge "Fix failure vts tests:" into oc-dr1-devShuo Qian2017-06-284-14/+23
| |\| |
| | * | Merge "Fix failure vts tests:" into oc-dr1-devShuo Qian2017-06-284-14/+23
| | |\ \
| | | * | Fix failure vts tests:sqian2017-06-284-14/+23
| | | |/
* | | | Merge "Add a new vts directory under 1.1 for radio 1.1 APIs vts tests." into ...Shuo Qian2017-06-2821-15/+292
|\| | |
| * | | Merge "Add a new vts directory under 1.1 for radio 1.1 APIs vts tests." into ...Shuo Qian2017-06-2821-15/+292
| |\| |
| | * | Merge "Add a new vts directory under 1.1 for radio 1.1 APIs vts tests." into ...Shuo Qian2017-06-2821-15/+292
| | |\ \ | | | |/ | | |/|
| | | * Add a new vts directory under 1.1 for radio 1.1 APIs vts tests.sqian2017-06-2821-15/+292
| | * | Radio Interface changes to allow the modem to query the frameworkpkanwar2017-06-273-13/+61
| | |/
| | * Merge "Radio Keepalive HAL" into oc-dr1-devTreeHugger Robot2017-06-275-1/+244
| | |\
| | | * Radio Keepalive HALNathan Harold2017-06-225-1/+244
* | | | Merge "Resolve differences in IRadio"TreeHugger Robot2017-06-281-20/+20
|\ \ \ \
| * | | | Resolve differences in IRadioSteven Moreland2017-06-281-20/+20
* | | | | Fix failure vts tests:sqian2017-06-284-14/+23
|/ / / /
* | | | Update IRadioResponse.hal documentation am: 6381ac46aasqian2017-06-211-5/+388
|\| | |
| * | | Update IRadioResponse.hal documentationsqian2017-06-211-5/+388
| |\| |