summaryrefslogtreecommitdiffstats
path: root/wifi
Commit message (Expand)AuthorAgeFilesLines
* Merge "[AWARE] Developer documentation on HAL usage" into pi-devTreeHugger Robot2018-05-212-3/+234
|\
| * [AWARE] Developer documentation on HAL usageEtan Cohen2018-05-182-3/+234
* | Merge "Update comments for doc comments." into pi-devTreeHugger Robot2018-05-181-3/+1
|\ \
| * | Update comments for doc comments.Steven Moreland2018-05-181-3/+1
| |/
* / wifi(implementation) Modify OWNERSRoshan Pius2018-05-181-1/+1
|/
* Add feature flag to disable wifi AP on the watch.Nick2018-05-116-3/+85
* wifi(implementation): Use stub for |read_packet_filter|Roshan Pius2018-04-202-4/+1
* Merge "persist ringbuffer to flash when vendor hal stops" into pi-devPankaj Kanwar2018-04-181-7/+25
|\
| * persist ringbuffer to flash when vendor hal stopsxshu2018-04-161-7/+25
* | VTS tests for IWifiStaIface@1.2.Bernie Innocenti2018-04-151-1/+54
|/
* Merge "[AWARE][VTS] Add VTS tests for the Wi-Fi 1.2 Aware HAL" into pi-devTreeHugger Robot2018-04-102-0/+553
|\
| * [AWARE][VTS] Add VTS tests for the Wi-Fi 1.2 Aware HALEtan Cohen2018-04-102-0/+553
* | Merge "[AWARE] Support a mix of 1.0 and 1.2 Callback registration" into pi-devEtan Cohen2018-04-102-10/+30
|\|
| * [AWARE] Support a mix of 1.0 and 1.2 Callback registrationEtan Cohen2018-04-102-10/+30
* | [WIFI][VTS]: Check for the Logger capability Support am: 020374e42b am: 65e95...Srinivas Dasari2018-04-101-2/+8
|\ \ | |/ |/|
| * [WIFI][VTS]: Check for the Logger capability SupportSrinivas Dasari2018-04-101-2/+8
| |\
| | * [WIFI][VTS]: Check for the Logger capability SupportSrinivas Dasari2018-04-101-2/+8
| * | wifi(vts): Skip tests if feature not supportedRoshan Pius2018-03-281-0/+10
| |\|
| | * wifi(vts): Skip tests if feature not supportedRoshan Pius2018-03-211-0/+10
| | * supplicant(vts): Remove start/stop frameworkRoshan Pius2018-01-232-16/+0
* | | Merge "SetMacAddress in Vendor HAL" into pi-devTreeHugger Robot2018-03-305-0/+104
|\ \ \
| * | | SetMacAddress in Vendor HALJong Wook Kim2018-03-275-0/+104
* | | | WiFi: Add vts tests for ISupplicantStaIface 1.1Ahmed ElArabawy2018-03-274-0/+149
* | | | WiFi: supplicant HAL: Modify onEapFailure CallbackAhmed ElArabawy2018-03-273-0/+95
|/ / /
* | | Wire readApfPacketFilterData() to the legacy halBernie Innocenti2018-03-265-4/+48
* | | Merge "Add capabilities to wifi HAL service" into pi-devTom Cherry2018-03-231-0/+1
|\ \ \
| * | | Add capabilities to wifi HAL serviceTom Cherry2018-03-231-0/+1
* | | | Merge "[RTT][AWARE] Support new legacy error codes for Aware RTT" into pi-devEtan Cohen2018-03-091-0/+4
|\ \ \ \
| * | | | [RTT][AWARE] Support new legacy error codes for Aware RTTEtan Cohen2018-03-081-0/+4
| |/ / /
* | | | Merge "supplicant/hostapd(vts): Test for terminate" into pi-devTreeHugger Robot2018-03-062-0/+16
|\ \ \ \
| * | | | supplicant/hostapd(vts): Test for terminateRoshan Pius2018-03-062-0/+16
| |/ / /
* / / / WiFi: Wait for driver to be ready before operationAhmed ElArabawy2018-03-062-1/+8
|/ / /
* | | Merge "Add a wifi hal interface to read-back the APF memory."Bernie Innocenti2018-03-042-0/+55
|\ \ \
| * | | Add a wifi hal interface to read-back the APF memory.Bernie Innocenti2018-03-022-0/+55
* | | | Merge "wifi(implementation): Remove support for STA + STA in chip combination"TreeHugger Robot2018-03-024-37/+12
|\ \ \ \ | |/ / / |/| | |
| * | | wifi(implementation): Remove support for STA + STA in chip combinationRoshan Pius2018-03-024-37/+12
* | | | WiFi: Add VTS for Wifi HAL V1.2Ahmed ElArabawy2018-03-014-0/+246
|/ / /
* | | Merge "supplicant 1.0 (vts): Add ifaces at init for 1.1 HAL service"Roshan Pius2018-02-283-2/+65
|\ \ \
| * | | supplicant 1.0 (vts): Add ifaces at init for 1.1 HAL serviceRoshan Pius2018-02-273-2/+65
* | | | wpa_supplicant(sta_network): Support encrypted imsi identity API for EAP-AKA/SIMEcco Park2018-02-264-0/+99
|/ / /
* | | Merge "Convert wifi hal test to use VtsHalHidlTargetTestEnvBase"Zhuoyao Zhang2018-02-1414-53/+173
|\ \ \
| * | | Convert wifi hal test to use VtsHalHidlTargetTestEnvBaseZhuoyao Zhang2018-02-1214-53/+173
* | | | [AWARE] Fix type of channel width to use enumerationEtan Cohen2018-02-072-2/+7
|/ / /
* | | Merge "Followup CL for ringbuffer in wifi_hal"Oscar Shu2018-02-053-99/+136
|\ \ \
| * | | Followup CL for ringbuffer in wifi_halxshu2018-01-243-99/+136
* | | | wpa/hostapd(interface): Add terminate methodRoshan Pius2018-02-012-0/+16
* | | | Wifi: Add Support for Body Proximity for SARAhmed ElArabawy2018-01-265-12/+97
* | | | HIDL changes to support Stadium Wifi.pkanwar2018-01-252-0/+101
* | | | wifi(implementation): Check if wifi_chip is null in debug()Roshan Pius2018-01-241-0/+3
* | | | Merge changes from topic "radio_mode_cbs_hidl"TreeHugger Robot2018-01-2412-8/+410
|\ \ \ \ | |/ / / |/| | |