/* * Copyright (C) 2016 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ #define LOG_TAG "StreamOutHAL" //#define LOG_NDEBUG 0 #define ATRACE_TAG ATRACE_TAG_AUDIO #include #include #include #include #include "StreamOut.h" #include "Util.h" namespace android { namespace hardware { namespace audio { namespace V2_0 { namespace implementation { using ::android::hardware::audio::common::V2_0::ThreadInfo; namespace { class WriteThread : public Thread { public: // WriteThread's lifespan never exceeds StreamOut's lifespan. WriteThread(std::atomic* stop, audio_stream_out_t* stream, StreamOut::CommandMQ* commandMQ, StreamOut::DataMQ* dataMQ, StreamOut::StatusMQ* statusMQ, EventFlag* efGroup) : Thread(false /*canCallJava*/), mStop(stop), mStream(stream), mCommandMQ(commandMQ), mDataMQ(dataMQ), mStatusMQ(statusMQ), mEfGroup(efGroup), mBuffer(nullptr) {} bool init() { mBuffer.reset(new (std::nothrow) uint8_t[mDataMQ->getQuantumCount()]); return mBuffer != nullptr; } virtual ~WriteThread() {} private: std::atomic* mStop; audio_stream_out_t* mStream; StreamOut::CommandMQ* mCommandMQ; StreamOut::DataMQ* mDataMQ; StreamOut::StatusMQ* mStatusMQ; EventFlag* mEfGroup; std::unique_ptr mBuffer; IStreamOut::WriteStatus mStatus; bool threadLoop() override; void doGetLatency(); void doGetPresentationPosition(); void doWrite(); }; void WriteThread::doWrite() { const size_t availToRead = mDataMQ->availableToRead(); mStatus.retval = Result::OK; mStatus.reply.written = 0; if (mDataMQ->read(&mBuffer[0], availToRead)) { ssize_t writeResult = mStream->write(mStream, &mBuffer[0], availToRead); if (writeResult >= 0) { mStatus.reply.written = writeResult; } else { mStatus.retval = Stream::analyzeStatus("write", writeResult); } } } void WriteThread::doGetPresentationPosition() { mStatus.retval = StreamOut::getPresentationPositionImpl( mStream, &mStatus.reply.presentationPosition.frames, &mStatus.reply.presentationPosition.timeStamp); } void WriteThread::doGetLatency() { mStatus.retval = Result::OK; mStatus.reply.latencyMs = mStream->get_latency(mStream); } bool WriteThread::threadLoop() { // This implementation doesn't return control back to the Thread until it // decides to stop, // as the Thread uses mutexes, and this can lead to priority inversion. while (!std::atomic_load_explicit(mStop, std::memory_order_acquire)) { uint32_t efState = 0; mEfGroup->wait(static_cast(MessageQueueFlagBits::NOT_EMPTY), &efState); if (!(efState & static_cast(MessageQueueFlagBits::NOT_EMPTY))) { continue; // Nothing to do. } if (!mCommandMQ->read(&mStatus.replyTo)) { continue; // Nothing to do. } switch (mStatus.replyTo) { case IStreamOut::WriteCommand::WRITE: doWrite(); break; case IStreamOut::WriteCommand::GET_PRESENTATION_POSITION: doGetPresentationPosition(); break; case IStreamOut::WriteCommand::GET_LATENCY: doGetLatency(); break; default: ALOGE("Unknown write thread command code %d", mStatus.replyTo); mStatus.retval = Result::NOT_SUPPORTED; break; } if (!mStatusMQ->write(&mStatus)) { ALOGE("status message queue write failed"); } mEfGroup->wake(static_cast(MessageQueueFlagBits::NOT_FULL)); } return false; } } // namespace StreamOut::StreamOut(const sp& device, audio_stream_out_t* stream) : mIsClosed(false), mDevice(device), mStream(stream), mStreamCommon(new Stream(&stream->common)), mStreamMmap(new StreamMmap(stream)), mEfGroup(nullptr), mStopWriteThread(false) {} StreamOut::~StreamOut() { ATRACE_CALL(); close(); if (mWriteThread.get()) { ATRACE_NAME("mWriteThread->join"); status_t status = mWriteThread->join(); ALOGE_IF(status, "write thread exit error: %s", strerror(-status)); } if (mEfGroup) { status_t status = EventFlag::deleteEventFlag(&mEfGroup); ALOGE_IF(status, "write MQ event flag deletion error: %s", strerror(-status)); } mCallback.clear(); mDevice->closeOutputStream(mStream); mStream = nullptr; } // Methods from ::android::hardware::audio::V2_0::IStream follow. Return StreamOut::getFrameSize() { return audio_stream_out_frame_size(mStream); } Return StreamOut::getFrameCount() { return mStreamCommon->getFrameCount(); } Return StreamOut::getBufferSize() { return mStreamCommon->getBufferSize(); } Return StreamOut::getSampleRate() { return mStreamCommon->getSampleRate(); } Return StreamOut::getSupportedSampleRates( getSupportedSampleRates_cb _hidl_cb) { return mStreamCommon->getSupportedSampleRates(_hidl_cb); } Return StreamOut::setSampleRate(uint32_t sampleRateHz) { return mStreamCommon->setSampleRate(sampleRateHz); } Return StreamOut::getChannelMask() { return mStreamCommon->getChannelMask(); } Return StreamOut::getSupportedChannelMasks( getSupportedChannelMasks_cb _hidl_cb) { return mStreamCommon->getSupportedChannelMasks(_hidl_cb); } Return StreamOut::setChannelMask(AudioChannelMask mask) { return mStreamCommon->setChannelMask(mask); } Return StreamOut::getFormat() { return mStreamCommon->getFormat(); } Return StreamOut::getSupportedFormats(getSupportedFormats_cb _hidl_cb) { return mStreamCommon->getSupportedFormats(_hidl_cb); } Return StreamOut::setFormat(AudioFormat format) { return mStreamCommon->setFormat(format); } Return StreamOut::getAudioProperties(getAudioProperties_cb _hidl_cb) { return mStreamCommon->getAudioProperties(_hidl_cb); } Return StreamOut::addEffect(uint64_t effectId) { return mStreamCommon->addEffect(effectId); } Return StreamOut::removeEffect(uint64_t effectId) { return mStreamCommon->removeEffect(effectId); } Return StreamOut::standby() { return mStreamCommon->standby(); } Return StreamOut::getDevice() { return mStreamCommon->getDevice(); } Return StreamOut::setDevice(const DeviceAddress& address) { return mStreamCommon->setDevice(address); } Return StreamOut::setConnectedState(const DeviceAddress& address, bool connected) { return mStreamCommon->setConnectedState(address, connected); } Return StreamOut::setHwAvSync(uint32_t hwAvSync) { return mStreamCommon->setHwAvSync(hwAvSync); } Return StreamOut::getParameters(const hidl_vec& keys, getParameters_cb _hidl_cb) { return mStreamCommon->getParameters(keys, _hidl_cb); } Return StreamOut::setParameters( const hidl_vec& parameters) { return mStreamCommon->setParameters(parameters); } Return StreamOut::debugDump(const hidl_handle& fd) { return mStreamCommon->debugDump(fd); } Return StreamOut::close() { if (mIsClosed) return Result::INVALID_STATE; mIsClosed = true; if (mWriteThread.get()) { mStopWriteThread.store(true, std::memory_order_release); } if (mEfGroup) { mEfGroup->wake(static_cast(MessageQueueFlagBits::NOT_EMPTY)); } return Result::OK; } // Methods from ::android::hardware::audio::V2_0::IStreamOut follow. Return StreamOut::getLatency() { return mStream->get_latency(mStream); } Return StreamOut::setVolume(float left, float right) { if (mStream->set_volume == NULL) { return Result::NOT_SUPPORTED; } if (!isGainNormalized(left)) { ALOGW("Can not set a stream output volume {%f, %f} outside [0,1]", left, right); return Result::INVALID_ARGUMENTS; } return Stream::analyzeStatus("set_volume", mStream->set_volume(mStream, left, right)); } Return StreamOut::prepareForWriting(uint32_t frameSize, uint32_t framesCount, prepareForWriting_cb _hidl_cb) { status_t status; ThreadInfo threadInfo = {0, 0}; // Wrap the _hidl_cb to return an error auto sendError = [this, &threadInfo, &_hidl_cb](Result result) { _hidl_cb(result, CommandMQ::Descriptor(), DataMQ::Descriptor(), StatusMQ::Descriptor(), threadInfo); }; // Create message queues. if (mDataMQ) { ALOGE("the client attempts to call prepareForWriting twice"); sendError(Result::INVALID_STATE); return Void(); } std::unique_ptr tempCommandMQ(new CommandMQ(1)); // Check frameSize and framesCount if (frameSize == 0 || framesCount == 0) { ALOGE("Null frameSize (%u) or framesCount (%u)", frameSize, framesCount); sendError(Result::INVALID_ARGUMENTS); return Void(); } if (frameSize > Stream::MAX_BUFFER_SIZE / framesCount) { ALOGE("Buffer too big: %u*%u bytes > MAX_BUFFER_SIZE (%u)", frameSize, framesCount, Stream::MAX_BUFFER_SIZE); sendError(Result::INVALID_ARGUMENTS); return Void(); } std::unique_ptr tempDataMQ( new DataMQ(frameSize * framesCount, true /* EventFlag */)); std::unique_ptr tempStatusMQ(new StatusMQ(1)); if (!tempCommandMQ->isValid() || !tempDataMQ->isValid() || !tempStatusMQ->isValid()) { ALOGE_IF(!tempCommandMQ->isValid(), "command MQ is invalid"); ALOGE_IF(!tempDataMQ->isValid(), "data MQ is invalid"); ALOGE_IF(!tempStatusMQ->isValid(), "status MQ is invalid"); sendError(Result::INVALID_ARGUMENTS); return Void(); } EventFlag* tempRawEfGroup{}; status = EventFlag::createEventFlag(tempDataMQ->getEventFlagWord(), &tempRawEfGroup); std::unique_ptr tempElfGroup( tempRawEfGroup, [](auto* ef) { EventFlag::deleteEventFlag(&ef); }); if (status != OK || !tempElfGroup) { ALOGE("failed creating event flag for data MQ: %s", strerror(-status)); sendError(Result::INVALID_ARGUMENTS); return Void(); } // Create and launch the thread. auto tempWriteThread = std::make_unique( &mStopWriteThread, mStream, tempCommandMQ.get(), tempDataMQ.get(), tempStatusMQ.get(), tempElfGroup.get()); if (!tempWriteThread->init()) { ALOGW("failed to start writer thread: %s", strerror(-status)); sendError(Result::INVALID_ARGUMENTS); return Void(); } status = tempWriteThread->run("writer", PRIORITY_URGENT_AUDIO); if (status != OK) { ALOGW("failed to start writer thread: %s", strerror(-status)); sendError(Result::INVALID_ARGUMENTS); return Void(); } mCommandMQ = std::move(tempCommandMQ); mDataMQ = std::move(tempDataMQ); mStatusMQ = std::move(tempStatusMQ); mWriteThread = tempWriteThread.release(); mEfGroup = tempElfGroup.release(); threadInfo.pid = getpid(); threadInfo.tid = mWriteThread->getTid(); _hidl_cb(Result::OK, *mCommandMQ->getDesc(), *mDataMQ->getDesc(), *mStatusMQ->getDesc(), threadInfo); return Void(); } Return StreamOut::getRenderPosition(getRenderPosition_cb _hidl_cb) { uint32_t halDspFrames; Result retval = Stream::analyzeStatus( "get_render_position", mStream->get_render_position(mStream, &halDspFrames)); _hidl_cb(retval, halDspFrames); return Void(); } Return StreamOut::getNextWriteTimestamp( getNextWriteTimestamp_cb _hidl_cb) { Result retval(Result::NOT_SUPPORTED); int64_t timestampUs = 0; if (mStream->get_next_write_timestamp != NULL) { retval = Stream::analyzeStatus( "get_next_write_timestamp", mStream->get_next_write_timestamp(mStream, ×tampUs)); } _hidl_cb(retval, timestampUs); return Void(); } Return StreamOut::setCallback(const sp& callback) { if (mStream->set_callback == NULL) return Result::NOT_SUPPORTED; int result = mStream->set_callback(mStream, StreamOut::asyncCallback, this); if (result == 0) { mCallback = callback; } return Stream::analyzeStatus("set_callback", result); } Return StreamOut::clearCallback() { if (mStream->set_callback == NULL) return Result::NOT_SUPPORTED; mCallback.clear(); return Result::OK; } // static int StreamOut::asyncCallback(stream_callback_event_t event, void*, void* cookie) { wp weakSelf(reinterpret_cast(cookie)); sp self = weakSelf.promote(); if (self == nullptr || self->mCallback == nullptr) return 0; ALOGV("asyncCallback() event %d", event); switch (event) { case STREAM_CBK_EVENT_WRITE_READY: self->mCallback->onWriteReady(); break; case STREAM_CBK_EVENT_DRAIN_READY: self->mCallback->onDrainReady(); break; case STREAM_CBK_EVENT_ERROR: self->mCallback->onError(); break; default: ALOGW("asyncCallback() unknown event %d", event); break; } return 0; } Return StreamOut::supportsPauseAndResume( supportsPauseAndResume_cb _hidl_cb) { _hidl_cb(mStream->pause != NULL, mStream->resume != NULL); return Void(); } Return StreamOut::pause() { return mStream->pause != NULL ? Stream::analyzeStatus("pause", mStream->pause(mStream)) : Result::NOT_SUPPORTED; } Return StreamOut::resume() { return mStream->resume != NULL ? Stream::analyzeStatus("resume", mStream->resume(mStream)) : Result::NOT_SUPPORTED; } Return StreamOut::supportsDrain() { return mStream->drain != NULL; } Return StreamOut::drain(AudioDrain type) { return mStream->drain != NULL ? Stream::analyzeStatus( "drain", mStream->drain(mStream, static_cast(type))) : Result::NOT_SUPPORTED; } Return StreamOut::flush() { return mStream->flush != NULL ? Stream::analyzeStatus("flush", mStream->flush(mStream)) : Result::NOT_SUPPORTED; } // static Result StreamOut::getPresentationPositionImpl(audio_stream_out_t* stream, uint64_t* frames, TimeSpec* timeStamp) { // Don't logspam on EINVAL--it's normal for get_presentation_position // to return it sometimes. EAGAIN may be returned by A2DP audio HAL // implementation. ENODATA can also be reported while the writer is // continuously querying it, but the stream has been stopped. static const std::vector ignoredErrors{EINVAL, EAGAIN, ENODATA}; Result retval(Result::NOT_SUPPORTED); if (stream->get_presentation_position == NULL) return retval; struct timespec halTimeStamp; retval = Stream::analyzeStatus("get_presentation_position", stream->get_presentation_position(stream, frames, &halTimeStamp), ignoredErrors); if (retval == Result::OK) { timeStamp->tvSec = halTimeStamp.tv_sec; timeStamp->tvNSec = halTimeStamp.tv_nsec; } return retval; } Return StreamOut::getPresentationPosition( getPresentationPosition_cb _hidl_cb) { uint64_t frames = 0; TimeSpec timeStamp = {0, 0}; Result retval = getPresentationPositionImpl(mStream, &frames, &timeStamp); _hidl_cb(retval, frames, timeStamp); return Void(); } Return StreamOut::start() { return mStreamMmap->start(); } Return StreamOut::stop() { return mStreamMmap->stop(); } Return StreamOut::createMmapBuffer(int32_t minSizeFrames, createMmapBuffer_cb _hidl_cb) { return mStreamMmap->createMmapBuffer( minSizeFrames, audio_stream_out_frame_size(mStream), _hidl_cb); } Return StreamOut::getMmapPosition(getMmapPosition_cb _hidl_cb) { return mStreamMmap->getMmapPosition(_hidl_cb); } } // namespace implementation } // namespace V2_0 } // namespace audio } // namespace hardware } // namespace android