/* * Copyright (C) 2016 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ package android.hardware.nfc@1.0; import INfcClientCallback; interface INfc { /** * Opens the NFC controller device and performs initialization. * This may include patch download and other vendor-specific initialization. * * If open completes successfully, the controller should be ready to perform * NCI initialization - ie accept CORE_RESET and subsequent commands through * the write() call. * * If open() returns NfcStatus::OK, the NCI stack will wait for a * NfcEvent.OPEN_CPLT before continuing. * * If open() returns NfcStatus::FAILED, the NCI stack will stop. * */ @entry @callflow(next={"write", "coreInitialized", "prediscover", "powerCycle", "controlGranted"}) open(INfcClientCallback clientCallback) generates (NfcStatus status); /** * Performs an NCI write. * * This method may queue writes and return immediately. The only * requirement is that the writes are executed in order. * * @return number of bytes written to the NFCC */ @callflow(next={"write", "prediscover", "coreInitialized", "close", "powerCycle", "controlGranted"}) write(NfcData data) generates (uint32_t retval); /** * coreInitialized() is called after the CORE_INIT_RSP is received from the * NFCC. At this time, the HAL can do any chip-specific configuration. * * If coreInitialized() returns NfcStatus::OK, the NCI stack will wait for a * NfcEvent.POST_INIT_CPLT before continuing. * * If coreInitialized() returns NfcStatus::FAILED, the NCI stack will * continue immediately. */ @callflow(next={"write", "prediscover", "close"}) coreInitialized(NfcData data) generates (NfcStatus status); /** * prediscover is called every time before starting RF discovery. * It is a good place to do vendor-specific configuration that must be * performed every time RF discovery is about to be started. * * If prediscover() returns NfcStatus::OK, the NCI stack will wait for a * NfcEvent.PREDISCOVER_CPLT before continuing. * * If prediscover() returns NfcStatus::FAILED, the NCI stack will start * RF discovery immediately. */ @callflow(next={"write", "close", "coreInitialized", "powerCycle", "controlGranted"}) prediscover() generates (NfcStatus status); /** * Close the NFC controller. Should free all resources. * * @return NfcStatus::OK on success and NfcStatus::FAILED on error. */ @exit close() generates (NfcStatus status); /** * Grant HAL the exclusive control to send NCI commands. * Called in response to NfcEvent.REQUEST_CONTROL. * Must only be called when there are no NCI commands pending. * NfcEvent.RELEASE_CONTROL will notify when HAL no longer needs exclusive control. * * @return NfcStatus::OK on success and NfcStatus::FAILED on error. */ @callflow(next={"write", "close", "prediscover", "coreInitialized", "powerCycle"}) controlGranted() generates (NfcStatus status); /** * Restart controller by power cyle; * NfcEvent.OPEN_CPLT will notify when operation is complete. * * @return NfcStatus::OK on success and NfcStatus::FAILED on error. */ @callflow(next={"write", "coreInitialized", "prediscover", "controlGranted", "close"}) powerCycle() generates (NfcStatus status); };