/* * Copyright 2016 The Android Open Source Project * * Licensed under the Apache License, Version 2.0 (the "License"); * you may not use this file except in compliance with the License. * You may obtain a copy of the License at * * http://www.apache.org/licenses/LICENSE-2.0 * * Unless required by applicable law or agreed to in writing, software * distributed under the License is distributed on an "AS IS" BASIS, * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. * See the License for the specific language governing permissions and * limitations under the License. */ package android.hardware.wifi.supplicant@1.0; import ISupplicantNetwork; /** * Interface exposed by the supplicant for each network interface (e.g wlan0) * it controls. */ interface ISupplicantIface { /** * Size limits for some of the params used in this interface. */ enum ParamSizeLimits : uint32_t { WPS_DEVICE_NAME_MAX_LEN = 32, WPS_MANUFACTURER_MAX_LEN = 64, WPS_MODEL_NAME_MAX_LEN = 32, WPS_MODEL_NUMBER_MAX_LEN = 32, WPS_SERIAL_NUMBER_MAX_LEN = 32 }; /** * Retrieves the name of the network interface. * * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID| * @return name Name of the network interface, e.g., wlan0 */ getName() generates (SupplicantStatus status, string name); /** * Retrieves the type of the network interface. * * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID| * @return type Type of the network interface, e.g., STA. */ getType() generates (SupplicantStatus status, IfaceType type); /** * Add a new network to the interface. * * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_UNKNOWN|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID| * @return network HIDL interface object representing the new network if * successful, null otherwise. */ addNetwork() generates (SupplicantStatus status, ISupplicantNetwork network); /** * Remove a network from the interface. * * Use |ISupplicantNetwork.getId()| on the corresponding network HIDL * interface object to retrieve the ID. * * @param id Network ID allocated to the corresponding network. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_UNKNOWN|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_NETWORK_UNKNOWN| */ removeNetwork(SupplicantNetworkId id) generates (SupplicantStatus status); /** * Gets a HIDL interface object for the network corresponding to the * |SupplicantNetworkId|. * * Use |ISupplicantNetwork.getId()| on the corresponding network HIDL * interface object to retrieve the ID. * * @param id Network ID allocated to the corresponding network. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_UNKNOWN|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_NETWORK_UNKNOWN| * @return network HIDL interface object representing the new network if * successful, null otherwise. */ getNetwork(SupplicantNetworkId id) generates (SupplicantStatus status, ISupplicantNetwork network); /** * Retrieve a list of all the network Id's controlled by the supplicant. * * The corresponding |ISupplicantNetwork| object for any network can be * retrieved using |getNetwork| method. * * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_UNKNOWN| * @return networkIds List of all network Id's controlled by the supplicant. */ listNetworks() generates (SupplicantStatus status, vec networkIds); /** * Set the device name for WPS operations. * User-friendly description of device (up to |WPS_DEVICE_NAME_MAX_LEN| * octets encoded in UTF-8). * * @parm name Name to be set. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_UNKNOWN| */ setWpsDeviceName(string name) generates (SupplicantStatus status); /** * Set the manufacturer for WPS operations. * The manufacturer of the device (up to |WPS_MANUFACTURER_MAX_LEN| ASCII * characters). * * @parm manufacturer Manufacture to be set. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_UNKNOWN| */ setWpsManufacturer(string manufacturer) generates (SupplicantStatus status); /** * Set the model name for WPS operations. * Model of the device (up to |WPS_MODEL_NAME_MAX_LEN| ASCII characters). * * @parm modelName Model name to be set. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_UNKNOWN| */ setWpsModelName(string modelName) generates (SupplicantStatus status); /** * Set the model number for WPS operations. * Additional device description (up to |WPS_MODEL_NUMBER_MAX_LEN| ASCII * characters). * * @parm modelNumber Model number to be set. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_UNKNOWN| */ setWpsModelNumber(string modelNumber) generates (SupplicantStatus status); /** * Set the serial number for WPS operations. * Serial number of the device (up to |WPS_SERIAL_NUMBER_MAX_LEN| characters) * * @parm serialNumber Serial number to be set. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_UNKNOWN| */ setWpsSerialNumber(string serialNumber) generates (SupplicantStatus status); /** * Set the list of supported config methods for WPS operations. * * @param configMethods Mask of WPS configuration methods supported by the * device. * @return status Status of the operation. * Possible status codes: * |SupplicantStatusCode.SUCCESS|, * |SupplicantStatusCode.FAILURE_IFACE_INVALID|, * |SupplicantStatusCode.FAILURE_UNKNOWN| */ setWpsConfigMethods(bitfield configMethods) generates (SupplicantStatus status); };