summaryrefslogtreecommitdiffstats
blob: 37b7124a26b084425cb85835495b7c8e64a9412a (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
/*
 * Copyright (C) 2016 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include <common/all-versions/IncludeGuard.h>

//#define LOG_NDEBUG 0

#include <memory.h>
#include <string.h>
#include <algorithm>

#include <android/log.h>

using ::android::hardware::audio::common::AUDIO_HAL_VERSION::HidlUtils;

namespace android {
namespace hardware {
namespace audio {
namespace AUDIO_HAL_VERSION {
namespace implementation {

Device::Device(audio_hw_device_t* device) : mDevice(device) {}

Device::~Device() {
    int status = audio_hw_device_close(mDevice);
    ALOGW_IF(status, "Error closing audio hw device %p: %s", mDevice, strerror(-status));
    mDevice = nullptr;
}

Result Device::analyzeStatus(const char* funcName, int status) {
    if (status != 0) {
        ALOGW("Device %p %s: %s", mDevice, funcName, strerror(-status));
    }
    switch (status) {
        case 0:
            return Result::OK;
        case -EINVAL:
            return Result::INVALID_ARGUMENTS;
        case -ENODATA:
            return Result::INVALID_STATE;
        case -ENODEV:
            return Result::NOT_INITIALIZED;
        case -ENOSYS:
            return Result::NOT_SUPPORTED;
        default:
            return Result::INVALID_STATE;
    }
}

void Device::closeInputStream(audio_stream_in_t* stream) {
    mDevice->close_input_stream(mDevice, stream);
}

void Device::closeOutputStream(audio_stream_out_t* stream) {
    mDevice->close_output_stream(mDevice, stream);
}

char* Device::halGetParameters(const char* keys) {
    return mDevice->get_parameters(mDevice, keys);
}

int Device::halSetParameters(const char* keysAndValues) {
    return mDevice->set_parameters(mDevice, keysAndValues);
}

// Methods from ::android::hardware::audio::AUDIO_HAL_VERSION::IDevice follow.
Return<Result> Device::initCheck() {
    return analyzeStatus("init_check", mDevice->init_check(mDevice));
}

Return<Result> Device::setMasterVolume(float volume) {
    if (mDevice->set_master_volume == NULL) {
        return Result::NOT_SUPPORTED;
    }
    if (!isGainNormalized(volume)) {
        ALOGW("Can not set a master volume (%f) outside [0,1]", volume);
        return Result::INVALID_ARGUMENTS;
    }
    return analyzeStatus("set_master_volume", mDevice->set_master_volume(mDevice, volume));
}

Return<void> Device::getMasterVolume(getMasterVolume_cb _hidl_cb) {
    Result retval(Result::NOT_SUPPORTED);
    float volume = 0;
    if (mDevice->get_master_volume != NULL) {
        retval = analyzeStatus("get_master_volume", mDevice->get_master_volume(mDevice, &volume));
    }
    _hidl_cb(retval, volume);
    return Void();
}

Return<Result> Device::setMicMute(bool mute) {
    return analyzeStatus("set_mic_mute", mDevice->set_mic_mute(mDevice, mute));
}

Return<void> Device::getMicMute(getMicMute_cb _hidl_cb) {
    bool mute = false;
    Result retval = analyzeStatus("get_mic_mute", mDevice->get_mic_mute(mDevice, &mute));
    _hidl_cb(retval, mute);
    return Void();
}

Return<Result> Device::setMasterMute(bool mute) {
    Result retval(Result::NOT_SUPPORTED);
    if (mDevice->set_master_mute != NULL) {
        retval = analyzeStatus("set_master_mute", mDevice->set_master_mute(mDevice, mute));
    }
    return retval;
}

Return<void> Device::getMasterMute(getMasterMute_cb _hidl_cb) {
    Result retval(Result::NOT_SUPPORTED);
    bool mute = false;
    if (mDevice->get_master_mute != NULL) {
        retval = analyzeStatus("get_master_mute", mDevice->get_master_mute(mDevice, &mute));
    }
    _hidl_cb(retval, mute);
    return Void();
}

Return<void> Device::getInputBufferSize(const AudioConfig& config, getInputBufferSize_cb _hidl_cb) {
    audio_config_t halConfig;
    HidlUtils::audioConfigToHal(config, &halConfig);
    size_t halBufferSize = mDevice->get_input_buffer_size(mDevice, &halConfig);
    Result retval(Result::INVALID_ARGUMENTS);
    uint64_t bufferSize = 0;
    if (halBufferSize != 0) {
        retval = Result::OK;
        bufferSize = halBufferSize;
    }
    _hidl_cb(retval, bufferSize);
    return Void();
}

Return<void> Device::openOutputStream(int32_t ioHandle, const DeviceAddress& device,
                                      const AudioConfig& config, AudioOutputFlagBitfield flags,
#ifdef AUDIO_HAL_VERSION_4_0
                                      const SourceMetadata& /* sourceMetadata */,
#endif
                                      openOutputStream_cb _hidl_cb) {
    audio_config_t halConfig;
    HidlUtils::audioConfigToHal(config, &halConfig);
    audio_stream_out_t* halStream;
    ALOGV(
        "open_output_stream handle: %d devices: %x flags: %#x "
        "srate: %d format %#x channels %x address %s",
        ioHandle, static_cast<audio_devices_t>(device.device),
        static_cast<audio_output_flags_t>(flags), halConfig.sample_rate, halConfig.format,
        halConfig.channel_mask, deviceAddressToHal(device).c_str());
    int status =
        mDevice->open_output_stream(mDevice, ioHandle, static_cast<audio_devices_t>(device.device),
                                    static_cast<audio_output_flags_t>(flags), &halConfig,
                                    &halStream, deviceAddressToHal(device).c_str());
    ALOGV("open_output_stream status %d stream %p", status, halStream);
    sp<IStreamOut> streamOut;
    if (status == OK) {
        streamOut = new StreamOut(this, halStream);
    }
    AudioConfig suggestedConfig;
    HidlUtils::audioConfigFromHal(halConfig, &suggestedConfig);
    _hidl_cb(analyzeStatus("open_output_stream", status), streamOut, suggestedConfig);
    return Void();
}

Return<void> Device::openInputStream(int32_t ioHandle, const DeviceAddress& device,
                                     const AudioConfig& config, AudioInputFlagBitfield flags,
                                     AudioSource source, openInputStream_cb _hidl_cb) {
    audio_config_t halConfig;
    HidlUtils::audioConfigToHal(config, &halConfig);
    audio_stream_in_t* halStream;
    ALOGV(
        "open_input_stream handle: %d devices: %x flags: %#x "
        "srate: %d format %#x channels %x address %s source %d",
        ioHandle, static_cast<audio_devices_t>(device.device),
        static_cast<audio_input_flags_t>(flags), halConfig.sample_rate, halConfig.format,
        halConfig.channel_mask, deviceAddressToHal(device).c_str(),
        static_cast<audio_source_t>(source));
    int status = mDevice->open_input_stream(
        mDevice, ioHandle, static_cast<audio_devices_t>(device.device), &halConfig, &halStream,
        static_cast<audio_input_flags_t>(flags), deviceAddressToHal(device).c_str(),
        static_cast<audio_source_t>(source));
    ALOGV("open_input_stream status %d stream %p", status, halStream);
    sp<IStreamIn> streamIn;
    if (status == OK) {
        streamIn = new StreamIn(this, halStream);
    }
    AudioConfig suggestedConfig;
    HidlUtils::audioConfigFromHal(halConfig, &suggestedConfig);
    _hidl_cb(analyzeStatus("open_input_stream", status), streamIn, suggestedConfig);
    return Void();
}

#ifdef AUDIO_HAL_VERSION_4_0
Return<void> Device::openInputStream(int32_t ioHandle, const DeviceAddress& device,
                                     const AudioConfig& config, AudioInputFlagBitfield flags,
                                     const SinkMetadata& sinkMetadata,
                                     openInputStream_cb _hidl_cb) {
    if (sinkMetadata.tracks.size() == 0) {
        // This should never happen, the framework must not create as stream
        // if there is no client
        ALOGE("openInputStream called without tracks connected");
        _hidl_cb(Result::INVALID_ARGUMENTS, nullptr, AudioConfig());
        return Void();
    }
    // Pick the first one as the main until the legacy API is update
    AudioSource source = sinkMetadata.tracks[0].source;
    return openInputStream(ioHandle, device, config, flags, source, _hidl_cb);
}
#endif

Return<bool> Device::supportsAudioPatches() {
    return version() >= AUDIO_DEVICE_API_VERSION_3_0;
}

Return<void> Device::createAudioPatch(const hidl_vec<AudioPortConfig>& sources,
                                      const hidl_vec<AudioPortConfig>& sinks,
                                      createAudioPatch_cb _hidl_cb) {
    Result retval(Result::NOT_SUPPORTED);
    AudioPatchHandle patch = 0;
    if (version() >= AUDIO_DEVICE_API_VERSION_3_0) {
        std::unique_ptr<audio_port_config[]> halSources(HidlUtils::audioPortConfigsToHal(sources));
        std::unique_ptr<audio_port_config[]> halSinks(HidlUtils::audioPortConfigsToHal(sinks));
        audio_patch_handle_t halPatch = AUDIO_PATCH_HANDLE_NONE;
        retval = analyzeStatus("create_audio_patch",
                               mDevice->create_audio_patch(mDevice, sources.size(), &halSources[0],
                                                           sinks.size(), &halSinks[0], &halPatch));
        if (retval == Result::OK) {
            patch = static_cast<AudioPatchHandle>(halPatch);
        }
    }
    _hidl_cb(retval, patch);
    return Void();
}

Return<Result> Device::releaseAudioPatch(int32_t patch) {
    if (version() >= AUDIO_DEVICE_API_VERSION_3_0) {
        return analyzeStatus(
            "release_audio_patch",
            mDevice->release_audio_patch(mDevice, static_cast<audio_patch_handle_t>(patch)));
    }
    return Result::NOT_SUPPORTED;
}

Return<void> Device::getAudioPort(const AudioPort& port, getAudioPort_cb _hidl_cb) {
    audio_port halPort;
    HidlUtils::audioPortToHal(port, &halPort);
    Result retval = analyzeStatus("get_audio_port", mDevice->get_audio_port(mDevice, &halPort));
    AudioPort resultPort = port;
    if (retval == Result::OK) {
        HidlUtils::audioPortFromHal(halPort, &resultPort);
    }
    _hidl_cb(retval, resultPort);
    return Void();
}

Return<Result> Device::setAudioPortConfig(const AudioPortConfig& config) {
    if (version() >= AUDIO_DEVICE_API_VERSION_3_0) {
        struct audio_port_config halPortConfig;
        HidlUtils::audioPortConfigToHal(config, &halPortConfig);
        return analyzeStatus("set_audio_port_config",
                             mDevice->set_audio_port_config(mDevice, &halPortConfig));
    }
    return Result::NOT_SUPPORTED;
}

#ifdef AUDIO_HAL_VERSION_2_0
Return<AudioHwSync> Device::getHwAvSync() {
    int halHwAvSync;
    Result retval = getParam(AudioParameter::keyHwAvSync, &halHwAvSync);
    return retval == Result::OK ? halHwAvSync : AUDIO_HW_SYNC_INVALID;
}
#elif defined(AUDIO_HAL_VERSION_4_0)
Return<void> Device::getHwAvSync(getHwAvSync_cb _hidl_cb) {
    int halHwAvSync;
    Result retval = getParam(AudioParameter::keyHwAvSync, &halHwAvSync);
    _hidl_cb(retval, halHwAvSync);
    return Void();
}
#endif

Return<Result> Device::setScreenState(bool turnedOn) {
    return setParam(AudioParameter::keyScreenState, turnedOn);
}

#ifdef AUDIO_HAL_VERSION_2_0
Return<void> Device::getParameters(const hidl_vec<hidl_string>& keys, getParameters_cb _hidl_cb) {
    getParametersImpl({}, keys, _hidl_cb);
    return Void();
}

Return<Result> Device::setParameters(const hidl_vec<ParameterValue>& parameters) {
    return setParametersImpl({} /* context */, parameters);
}
#elif defined(AUDIO_HAL_VERSION_4_0)
Return<void> Device::getParameters(const hidl_vec<ParameterValue>& context,
                                   const hidl_vec<hidl_string>& keys, getParameters_cb _hidl_cb) {
    getParametersImpl(context, keys, _hidl_cb);
    return Void();
}
Return<Result> Device::setParameters(const hidl_vec<ParameterValue>& context,
                                     const hidl_vec<ParameterValue>& parameters) {
    return setParametersImpl(context, parameters);
}
#endif

#ifdef AUDIO_HAL_VERSION_2_0
Return<void> Device::debugDump(const hidl_handle& fd) {
    return debug(fd, {});
}
#endif

Return<void> Device::debug(const hidl_handle& fd, const hidl_vec<hidl_string>& /* options */) {
    if (fd.getNativeHandle() != nullptr && fd->numFds == 1) {
        analyzeStatus("dump", mDevice->dump(mDevice, fd->data[0]));
    }
    return Void();
}

#ifdef AUDIO_HAL_VERSION_4_0
Return<void> Device::getMicrophones(getMicrophones_cb _hidl_cb) {
    Result retval = Result::NOT_SUPPORTED;
    size_t actual_mics = AUDIO_MICROPHONE_MAX_COUNT;
    audio_microphone_characteristic_t mic_array[AUDIO_MICROPHONE_MAX_COUNT];

    hidl_vec<MicrophoneInfo> microphones;
    if (mDevice->get_microphones != NULL &&
        mDevice->get_microphones(mDevice, &mic_array[0], &actual_mics) == 0) {
        microphones.resize(actual_mics);
        for (size_t i = 0; i < actual_mics; ++i) {
            halToMicrophoneCharacteristics(&microphones[i], mic_array[i]);
        }
        retval = Result::OK;
    }
    _hidl_cb(retval, microphones);
    return Void();
}

Return<Result> Device::setConnectedState(const DeviceAddress& address, bool connected) {
    auto key = connected ? AudioParameter::keyStreamConnect : AudioParameter::keyStreamDisconnect;
    return setParam(key, address);
}
#endif

}  // namespace implementation
}  // namespace AUDIO_HAL_VERSION
}  // namespace audio
}  // namespace hardware
}  // namespace android