summaryrefslogtreecommitdiffstats
blob: fa0ef45becc3afca2abdea5aea215c1de234da96 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
/*
 * Copyright (C) 2016 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include <common/all-versions/IncludeGuard.h>

#include <inttypes.h>

#include <android/log.h>
#include <hardware/audio.h>
#include <hardware/audio_effect.h>
#include <media/TypeConverter.h>
#include <utils/SortedVector.h>
#include <utils/Vector.h>

namespace android {
namespace hardware {
namespace audio {
namespace AUDIO_HAL_VERSION {
namespace implementation {

Stream::Stream(audio_stream_t* stream) : mStream(stream) {}

Stream::~Stream() {
    mStream = nullptr;
}

// static
Result Stream::analyzeStatus(const char* funcName, int status) {
    static const std::vector<int> empty;
    return analyzeStatus(funcName, status, empty);
}

template <typename T>
inline bool element_in(T e, const std::vector<T>& v) {
    return std::find(v.begin(), v.end(), e) != v.end();
}

// static
Result Stream::analyzeStatus(const char* funcName, int status,
                             const std::vector<int>& ignoreErrors) {
    if (status != 0 && (ignoreErrors.empty() || !element_in(-status, ignoreErrors))) {
        ALOGW("Error from HAL stream in function %s: %s", funcName, strerror(-status));
    }
    switch (status) {
        case 0:
            return Result::OK;
        case -EINVAL:
            return Result::INVALID_ARGUMENTS;
        case -ENODATA:
            return Result::INVALID_STATE;
        case -ENODEV:
            return Result::NOT_INITIALIZED;
        case -ENOSYS:
            return Result::NOT_SUPPORTED;
        default:
            return Result::INVALID_STATE;
    }
}

char* Stream::halGetParameters(const char* keys) {
    return mStream->get_parameters(mStream, keys);
}

int Stream::halSetParameters(const char* keysAndValues) {
    return mStream->set_parameters(mStream, keysAndValues);
}

// Methods from ::android::hardware::audio::AUDIO_HAL_VERSION::IStream follow.
Return<uint64_t> Stream::getFrameSize() {
    // Needs to be implemented by interface subclasses. But can't be declared as pure virtual,
    // since interface subclasses implementation do not inherit from this class.
    LOG_ALWAYS_FATAL("Stream::getFrameSize is pure abstract");
    return uint64_t{};
}

Return<uint64_t> Stream::getFrameCount() {
    int halFrameCount;
    Result retval = getParam(AudioParameter::keyFrameCount, &halFrameCount);
    return retval == Result::OK ? halFrameCount : 0;
}

Return<uint64_t> Stream::getBufferSize() {
    return mStream->get_buffer_size(mStream);
}

Return<uint32_t> Stream::getSampleRate() {
    return mStream->get_sample_rate(mStream);
}

#ifdef AUDIO_HAL_VERSION_2_0
Return<void> Stream::getSupportedSampleRates(getSupportedSampleRates_cb _hidl_cb) {
    return getSupportedSampleRates(getFormat(), _hidl_cb);
}
Return<void> Stream::getSupportedChannelMasks(getSupportedChannelMasks_cb _hidl_cb) {
    return getSupportedChannelMasks(getFormat(), _hidl_cb);
}
#endif

Return<void> Stream::getSupportedSampleRates(AudioFormat format,
                                             getSupportedSampleRates_cb _hidl_cb) {
    AudioParameter context;
    context.addInt(String8(AUDIO_PARAMETER_STREAM_FORMAT), int(format));
    String8 halListValue;
    Result result =
        getParam(AudioParameter::keyStreamSupportedSamplingRates, &halListValue, context);
    hidl_vec<uint32_t> sampleRates;
    SortedVector<uint32_t> halSampleRates;
    if (result == Result::OK) {
        halSampleRates =
            samplingRatesFromString(halListValue.string(), AudioParameter::valueListSeparator);
        sampleRates.setToExternal(halSampleRates.editArray(), halSampleRates.size());
    }
#ifdef AUDIO_HAL_VERSION_2_0
    _hidl_cb(sampleRates);
#endif
#ifdef AUDIO_HAL_VERSION_4_0
    _hidl_cb(result, sampleRates);
#endif
    return Void();
}

Return<void> Stream::getSupportedChannelMasks(AudioFormat format,
                                              getSupportedChannelMasks_cb _hidl_cb) {
    AudioParameter context;
    context.addInt(String8(AUDIO_PARAMETER_STREAM_FORMAT), int(format));
    String8 halListValue;
    Result result = getParam(AudioParameter::keyStreamSupportedChannels, &halListValue, context);
    hidl_vec<AudioChannelBitfield> channelMasks;
    SortedVector<audio_channel_mask_t> halChannelMasks;
    if (result == Result::OK) {
        halChannelMasks =
            channelMasksFromString(halListValue.string(), AudioParameter::valueListSeparator);
        channelMasks.resize(halChannelMasks.size());
        for (size_t i = 0; i < halChannelMasks.size(); ++i) {
            channelMasks[i] = AudioChannelBitfield(halChannelMasks[i]);
        }
    }
#ifdef AUDIO_HAL_VERSION_2_0
    _hidl_cb(channelMasks);
#elif defined(AUDIO_HAL_VERSION_4_0)
    _hidl_cb(result, channelMasks);
#endif
    return Void();
}

Return<Result> Stream::setSampleRate(uint32_t sampleRateHz) {
    return setParam(AudioParameter::keySamplingRate, static_cast<int>(sampleRateHz));
}

Return<AudioChannelBitfield> Stream::getChannelMask() {
    return AudioChannelBitfield(mStream->get_channels(mStream));
}

Return<Result> Stream::setChannelMask(AudioChannelBitfield mask) {
    return setParam(AudioParameter::keyChannels, static_cast<int>(mask));
}

Return<AudioFormat> Stream::getFormat() {
    return AudioFormat(mStream->get_format(mStream));
}

Return<void> Stream::getSupportedFormats(getSupportedFormats_cb _hidl_cb) {
    String8 halListValue;
    Result result = getParam(AudioParameter::keyStreamSupportedFormats, &halListValue);
    hidl_vec<AudioFormat> formats;
    Vector<audio_format_t> halFormats;
    if (result == Result::OK) {
        halFormats = formatsFromString(halListValue.string(), AudioParameter::valueListSeparator);
        formats.resize(halFormats.size());
        for (size_t i = 0; i < halFormats.size(); ++i) {
            formats[i] = AudioFormat(halFormats[i]);
        }
    }
    _hidl_cb(formats);
    return Void();
}

Return<Result> Stream::setFormat(AudioFormat format) {
    return setParam(AudioParameter::keyFormat, static_cast<int>(format));
}

Return<void> Stream::getAudioProperties(getAudioProperties_cb _hidl_cb) {
    uint32_t halSampleRate = mStream->get_sample_rate(mStream);
    audio_channel_mask_t halMask = mStream->get_channels(mStream);
    audio_format_t halFormat = mStream->get_format(mStream);
    _hidl_cb(halSampleRate, AudioChannelBitfield(halMask), AudioFormat(halFormat));
    return Void();
}

Return<Result> Stream::addEffect(uint64_t effectId) {
    effect_handle_t halEffect = EffectMap::getInstance().get(effectId);
    if (halEffect != NULL) {
        return analyzeStatus("add_audio_effect", mStream->add_audio_effect(mStream, halEffect));
    } else {
        ALOGW("Invalid effect ID passed from client: %" PRIu64, effectId);
        return Result::INVALID_ARGUMENTS;
    }
}

Return<Result> Stream::removeEffect(uint64_t effectId) {
    effect_handle_t halEffect = EffectMap::getInstance().get(effectId);
    if (halEffect != NULL) {
        return analyzeStatus("remove_audio_effect",
                             mStream->remove_audio_effect(mStream, halEffect));
    } else {
        ALOGW("Invalid effect ID passed from client: %" PRIu64, effectId);
        return Result::INVALID_ARGUMENTS;
    }
}

Return<Result> Stream::standby() {
    return analyzeStatus("standby", mStream->standby(mStream));
}

Return<Result> Stream::setHwAvSync(uint32_t hwAvSync) {
    return setParam(AudioParameter::keyStreamHwAvSync, static_cast<int>(hwAvSync));
}

#ifdef AUDIO_HAL_VERSION_2_0
Return<AudioDevice> Stream::getDevice() {
    int device = 0;
    Result retval = getParam(AudioParameter::keyRouting, &device);
    return retval == Result::OK ? static_cast<AudioDevice>(device) : AudioDevice::NONE;
}

Return<Result> Stream::setDevice(const DeviceAddress& address) {
    return setParam(AudioParameter::keyRouting, address);
}

Return<void> Stream::getParameters(const hidl_vec<hidl_string>& keys, getParameters_cb _hidl_cb) {
    getParametersImpl({} /* context */, keys, _hidl_cb);
    return Void();
}

Return<Result> Stream::setParameters(const hidl_vec<ParameterValue>& parameters) {
    return setParametersImpl({} /* context */, parameters);
}

Return<Result> Stream::setConnectedState(const DeviceAddress& address, bool connected) {
    return setParam(
        connected ? AudioParameter::keyStreamConnect : AudioParameter::keyStreamDisconnect,
        address);
}
#elif defined(AUDIO_HAL_VERSION_4_0)
Return<void> Stream::getDevices(getDevices_cb _hidl_cb) {
    int device = 0;
    Result retval = getParam(AudioParameter::keyRouting, &device);
    hidl_vec<DeviceAddress> devices;
    if (retval == Result::OK) {
        devices.resize(1);
        devices[0].device = static_cast<AudioDevice>(device);
    }
    _hidl_cb(retval, devices);
    return Void();
}

Return<Result> Stream::setDevices(const hidl_vec<DeviceAddress>& devices) {
    // FIXME: can the legacy API set multiple device with address ?
    if (devices.size() > 1) {
        return Result::NOT_SUPPORTED;
    }
    DeviceAddress address;
    if (devices.size() == 1) {
        address = devices[0];
    } else {
        address.device = AudioDevice::NONE;
    }
    return setParam(AudioParameter::keyRouting, address);
}
Return<void> Stream::getParameters(const hidl_vec<ParameterValue>& context,
                                   const hidl_vec<hidl_string>& keys, getParameters_cb _hidl_cb) {
    getParametersImpl(context, keys, _hidl_cb);
    return Void();
}

Return<Result> Stream::setParameters(const hidl_vec<ParameterValue>& context,
                                     const hidl_vec<ParameterValue>& parameters) {
    return setParametersImpl(context, parameters);
}
#endif

Return<Result> Stream::start() {
    return Result::NOT_SUPPORTED;
}

Return<Result> Stream::stop() {
    return Result::NOT_SUPPORTED;
}

Return<void> Stream::createMmapBuffer(int32_t minSizeFrames __unused,
                                      createMmapBuffer_cb _hidl_cb) {
    Result retval(Result::NOT_SUPPORTED);
    MmapBufferInfo info;
    _hidl_cb(retval, info);
    return Void();
}

Return<void> Stream::getMmapPosition(getMmapPosition_cb _hidl_cb) {
    Result retval(Result::NOT_SUPPORTED);
    MmapPosition position;
    _hidl_cb(retval, position);
    return Void();
}

Return<Result> Stream::close() {
    return Result::NOT_SUPPORTED;
}

Return<void> Stream::debug(const hidl_handle& fd, const hidl_vec<hidl_string>& /* options */) {
    if (fd.getNativeHandle() != nullptr && fd->numFds == 1) {
        analyzeStatus("dump", mStream->dump(mStream, fd->data[0]));
    }
    return Void();
}

#ifdef AUDIO_HAL_VERSION_2_0
Return<void> Stream::debugDump(const hidl_handle& fd) {
    return debug(fd, {} /* options */);
}
#endif

}  // namespace implementation
}  // namespace AUDIO_HAL_VERSION
}  // namespace audio
}  // namespace hardware
}  // namespace android