1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
|
/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#define LOG_TAG "fingerprint_hidl_hal_test"
#include <VtsHalHidlTargetTestBase.h>
#include <VtsHalHidlTargetTestEnvBase.h>
#include <android-base/logging.h>
#include <android-base/properties.h>
#include <android/hardware/biometrics/fingerprint/2.1/IBiometricsFingerprint.h>
#include <android/hardware/biometrics/fingerprint/2.1/IBiometricsFingerprintClientCallback.h>
#include <hidl/HidlSupport.h>
#include <hidl/HidlTransportSupport.h>
#include <cinttypes>
#include <future>
#include <utility>
using android::base::GetUintProperty;
using android::Condition;
using android::hardware::biometrics::fingerprint::V2_1::IBiometricsFingerprint;
using android::hardware::biometrics::fingerprint::V2_1::IBiometricsFingerprintClientCallback;
using android::hardware::biometrics::fingerprint::V2_1::FingerprintAcquiredInfo;
using android::hardware::biometrics::fingerprint::V2_1::FingerprintError;
using android::hardware::biometrics::fingerprint::V2_1::RequestStatus;
using android::hardware::hidl_vec;
using android::hardware::Return;
using android::Mutex;
using android::sp;
namespace {
static const uint32_t kTimeout = 3;
static const std::chrono::seconds kTimeoutInSeconds = std::chrono::seconds(kTimeout);
static const uint32_t kGroupId = 99;
static std::string kTmpDir = "";
static const uint32_t kIterations = 1000;
// Wait for a callback to occur (signaled by the given future) up to the
// provided timeout. If the future is invalid or the callback does not come
// within the given time, returns false.
template<class ReturnType>
bool waitForCallback(
std::future<ReturnType> future,
std::chrono::milliseconds timeout = kTimeoutInSeconds) {
auto expiration = std::chrono::system_clock::now() + timeout;
EXPECT_TRUE(future.valid());
if (future.valid()) {
std::future_status status = future.wait_until(expiration);
EXPECT_NE(std::future_status::timeout, status)
<< "Timed out waiting for callback";
if (status == std::future_status::ready) {
return true;
}
}
return false;
}
// Base callback implementation that just logs all callbacks by default
class FingerprintCallbackBase : public IBiometricsFingerprintClientCallback {
public:
// implement methods of IBiometricsFingerprintClientCallback
virtual Return<void> onEnrollResult(uint64_t, uint32_t, uint32_t, uint32_t)
override {
ALOGD("Enroll callback called.");
return Return<void>();
}
virtual Return<void> onAcquired(uint64_t, FingerprintAcquiredInfo, int32_t)
override {
ALOGD("Acquired callback called.");
return Return<void>();
}
virtual Return<void> onAuthenticated(uint64_t, uint32_t, uint32_t,
const hidl_vec<uint8_t>&) override {
ALOGD("Authenticated callback called.");
return Return<void>();
}
virtual Return<void> onError(uint64_t, FingerprintError, int32_t)
override {
ALOGD("Error callback called.");
EXPECT_TRUE(false); // fail any test that triggers an error
return Return<void>();
}
virtual Return<void> onRemoved(uint64_t, uint32_t, uint32_t, uint32_t)
override {
ALOGD("Removed callback called.");
return Return<void>();
}
virtual Return<void> onEnumerate(uint64_t, uint32_t, uint32_t, uint32_t)
override {
ALOGD("Enumerate callback called.");
return Return<void>();
}
};
class EnumerateCallback : public FingerprintCallbackBase {
public:
virtual Return<void> onEnumerate(uint64_t deviceId, uint32_t fingerId,
uint32_t groupId, uint32_t remaining) override {
this->deviceId = deviceId;
this->fingerId = fingerId;
this->groupId = groupId;
this->remaining = remaining;
if(remaining == 0UL) {
promise.set_value();
}
return Return<void>();
}
uint64_t deviceId;
uint32_t fingerId;
uint32_t groupId;
uint32_t remaining;
std::promise<void> promise;
};
class ErrorCallback : public FingerprintCallbackBase {
public:
ErrorCallback(
bool filterErrors=false,
FingerprintError errorType=FingerprintError::ERROR_NO_ERROR) {
this->filterErrors = filterErrors;
this->errorType = errorType;
}
virtual Return<void> onError(uint64_t deviceId, FingerprintError error,
int32_t vendorCode) override {
if ((this->filterErrors && this->errorType == error) || !this->filterErrors) {
this->deviceId = deviceId;
this->error = error;
this->vendorCode = vendorCode;
promise.set_value();
}
return Return<void>();
}
bool filterErrors;
FingerprintError errorType;
uint64_t deviceId;
FingerprintError error;
int32_t vendorCode;
std::promise<void> promise;
};
class RemoveCallback : public FingerprintCallbackBase {
public:
RemoveCallback(uint32_t groupId) {
this->removeGroupId = groupId;
}
virtual Return<void> onRemoved(uint64_t, uint32_t, uint32_t groupId,
uint32_t remaining) override {
EXPECT_EQ(this->removeGroupId, groupId);
if(remaining == 0UL) {
promise.set_value();
}
return Return<void>();
}
uint32_t removeGroupId;
std::promise<void> promise;
};
// Test environment for Fingerprint HIDL HAL.
class FingerprintHidlEnvironment : public ::testing::VtsHalHidlTargetTestEnvBase {
public:
// get the test environment singleton
static FingerprintHidlEnvironment* Instance() {
static FingerprintHidlEnvironment* instance = new FingerprintHidlEnvironment;
return instance;
}
virtual void registerTestServices() override { registerTestService<IBiometricsFingerprint>(); }
};
class FingerprintHidlTest : public ::testing::VtsHalHidlTargetTestBase {
public:
virtual void SetUp() override {
mService = ::testing::VtsHalHidlTargetTestBase::getService<IBiometricsFingerprint>(
FingerprintHidlEnvironment::Instance()->getServiceName<IBiometricsFingerprint>());
ASSERT_FALSE(mService == nullptr);
/*
* Devices shipped from now on will instead store
* fingerprint data under /data/vendor_de/<user-id>/fpdata.
* Support for /data/vendor_de and /data/vendor_ce has been added to vold.
*/
uint64_t api_level = GetUintProperty<uint64_t>("ro.product.first_api_level", 0);
if (api_level == 0) {
api_level = GetUintProperty<uint64_t>("ro.build.version.sdk", 0);
}
ASSERT_TRUE(api_level != 0);
// 27 is the API number for O-MR1
if (api_level <= 27) {
kTmpDir = "/data/system/users/0/fpdata/";
} else {
kTmpDir = "/data/vendor_de/0/fpdata/";
}
Return<RequestStatus> res = mService->setActiveGroup(kGroupId, kTmpDir);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
}
virtual void TearDown() override {}
sp<IBiometricsFingerprint> mService;
};
// The service should be reachable.
TEST_F(FingerprintHidlTest, ConnectTest) {
sp<FingerprintCallbackBase> cb = new FingerprintCallbackBase();
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
}
// Starting the service with null callback should succeed.
TEST_F(FingerprintHidlTest, ConnectNullTest) {
Return<uint64_t> rc = mService->setNotify(NULL);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
}
// Pre-enroll should always return unique, cryptographically secure, non-zero number
TEST_F(FingerprintHidlTest, PreEnrollTest) {
std::map<uint64_t, uint64_t> m;
for(unsigned int i = 0; i < kIterations; ++i) {
uint64_t res = static_cast<uint64_t>(mService->preEnroll());
EXPECT_NE(0UL, res);
m[res]++;
EXPECT_EQ(1UL, m[res]);
}
}
// Enroll with an invalid (all zeroes) HAT should fail.
TEST_F(FingerprintHidlTest, EnrollInvalidHatTest) {
sp<ErrorCallback> cb = new ErrorCallback();
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
uint8_t token[69];
for(int i=0; i<69; i++) {
token[i] = 0;
}
Return<RequestStatus> res = mService->enroll(token, kGroupId, kTimeout);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// At least one call to onError should occur
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
ASSERT_NE(FingerprintError::ERROR_NO_ERROR, cb->error);
}
// Enroll with an invalid (null) HAT should fail.
TEST_F(FingerprintHidlTest, EnrollNullTest) {
sp<ErrorCallback> cb = new ErrorCallback();
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
uint8_t token[69];
Return<RequestStatus> res = mService->enroll(token, kGroupId, kTimeout);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// At least one call to onError should occur
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
ASSERT_NE(FingerprintError::ERROR_NO_ERROR, cb->error);
}
// PostEnroll should always return within 3s
TEST_F(FingerprintHidlTest, PostEnrollTest) {
sp<FingerprintCallbackBase> cb = new FingerprintCallbackBase();
Return<uint64_t> rc = mService->setNotify(cb);
auto start = std::chrono::system_clock::now();
Return<RequestStatus> res = mService->postEnroll();
auto elapsed = std::chrono::system_clock::now() - start;
ASSERT_GE(kTimeoutInSeconds, elapsed);
}
// getAuthenticatorId should always return non-zero numbers
TEST_F(FingerprintHidlTest, GetAuthenticatorIdTest) {
Return<uint64_t> res = mService->getAuthenticatorId();
EXPECT_NE(0UL, static_cast<uint64_t>(res));
}
// Enumerate should always trigger onEnumerated(fid=0, rem=0) when there are no fingerprints
TEST_F(FingerprintHidlTest, EnumerateTest) {
sp<EnumerateCallback> cb = new EnumerateCallback();
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
// Callback will return when rem=0 is found
Return<RequestStatus> res = mService->enumerate();
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
EXPECT_EQ(0UL, cb->fingerId);
EXPECT_EQ(0UL, cb->remaining);
}
// Remove should succeed on any inputs
// At least one callback with "remaining=0" should occur
TEST_F(FingerprintHidlTest, RemoveFingerprintTest) {
// Register callback
sp<RemoveCallback> cb = new RemoveCallback(kGroupId);
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
// Remove a fingerprint
Return<RequestStatus> res = mService->remove(kGroupId, 1);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// At least one call to onRemove with remaining=0 should occur
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
}
// Remove should accept 0 to delete all fingerprints
// At least one callback with "remaining=0" should occur.
TEST_F(FingerprintHidlTest, RemoveAllFingerprintsTest) {
// Register callback
sp<RemoveCallback> cb = new RemoveCallback(kGroupId);
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
// Remove all fingerprints
Return<RequestStatus> res = mService->remove(kGroupId, 0);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
}
// Active group should successfully set to a writable location.
TEST_F(FingerprintHidlTest, SetActiveGroupTest) {
// Create an active group
Return<RequestStatus> res = mService->setActiveGroup(2, kTmpDir);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// Reset active group
res = mService->setActiveGroup(kGroupId, kTmpDir);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
}
// Active group should fail to set to an unwritable location.
TEST_F(FingerprintHidlTest, SetActiveGroupUnwritableTest) {
// Create an active group to an unwritable location (device root dir)
Return<RequestStatus> res = mService->setActiveGroup(3, "/");
ASSERT_NE(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// Reset active group
res = mService->setActiveGroup(kGroupId, kTmpDir);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
}
// Active group should fail to set to a null location.
TEST_F(FingerprintHidlTest, SetActiveGroupNullTest) {
// Create an active group to a null location.
Return<RequestStatus> res = mService->setActiveGroup(4, nullptr);
ASSERT_NE(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// Reset active group
res = mService->setActiveGroup(kGroupId, kTmpDir);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
}
// Cancel should always return ERROR_CANCELED from any starting state including
// the IDLE state.
TEST_F(FingerprintHidlTest, CancelTest) {
sp<ErrorCallback> cb = new ErrorCallback(true, FingerprintError::ERROR_CANCELED);
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0UL, static_cast<uint64_t>(rc));
Return<RequestStatus> res = mService->cancel();
// check that we were able to make an IPC request successfully
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// make sure callback was invoked within kTimeoutInSeconds
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
// check error should be ERROR_CANCELED
ASSERT_EQ(FingerprintError::ERROR_CANCELED, cb->error);
}
// A call to cancel should succeed during enroll.
TEST_F(FingerprintHidlTest, CancelEnrollTest) {
Return<RequestStatus> res = mService->setActiveGroup(kGroupId, kTmpDir);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
sp<ErrorCallback> cb = new ErrorCallback(true, FingerprintError::ERROR_CANCELED);
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0U, static_cast<uint64_t>(rc));
uint8_t token[69];
res = mService->enroll(token, kGroupId, kTimeout);
// check that we were able to make an IPC request successfully
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
res = mService->cancel();
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// make sure callback was invoked within kTimeoutInSeconds
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
// check error should be ERROR_CANCELED
ASSERT_EQ(FingerprintError::ERROR_CANCELED, cb->error);
}
// A call to cancel should succeed during authentication.
TEST_F(FingerprintHidlTest, CancelAuthTest) {
sp<ErrorCallback> cb = new ErrorCallback(true, FingerprintError::ERROR_CANCELED);
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0U, static_cast<uint64_t>(rc));
Return<RequestStatus> res = mService->authenticate(0, kGroupId);
// check that we were able to make an IPC request successfully
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
res = mService->cancel();
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// make sure callback was invoked within kTimeoutInSeconds
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
// check error should be ERROR_CANCELED
ASSERT_EQ(FingerprintError::ERROR_CANCELED, cb->error);
}
// A call to cancel should succeed during authentication.
TEST_F(FingerprintHidlTest, CancelRemoveTest) {
sp<ErrorCallback> cb = new ErrorCallback(true, FingerprintError::ERROR_CANCELED);
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0U, static_cast<uint64_t>(rc));
// Remove a fingerprint
Return<RequestStatus> res = mService->remove(kGroupId, 1);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
res = mService->cancel();
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// make sure callback was invoked within kTimeoutInSeconds
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
// check error should be ERROR_CANCELED
ASSERT_EQ(FingerprintError::ERROR_CANCELED, cb->error);
}
// A call to cancel should succeed during authentication.
TEST_F(FingerprintHidlTest, CancelRemoveAllTest) {
sp<ErrorCallback> cb = new ErrorCallback(true, FingerprintError::ERROR_CANCELED);
Return<uint64_t> rc = mService->setNotify(cb);
ASSERT_NE(0U, static_cast<uint64_t>(rc));
// Remove a fingerprint
Return<RequestStatus> res = mService->remove(kGroupId, 0);
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
res = mService->cancel();
ASSERT_EQ(RequestStatus::SYS_OK, static_cast<RequestStatus>(res));
// make sure callback was invoked within kTimeoutInSeconds
ASSERT_TRUE(waitForCallback(cb->promise.get_future()));
// check error should be ERROR_CANCELED
ASSERT_EQ(FingerprintError::ERROR_CANCELED, cb->error);
}
} // anonymous namespace
int main(int argc, char **argv) {
::testing::AddGlobalTestEnvironment(FingerprintHidlEnvironment::Instance());
::testing::InitGoogleTest(&argc, argv);
FingerprintHidlEnvironment::Instance()->init(&argc, argv);
int status = RUN_ALL_TESTS();
LOG(INFO) << "Test result = " << status;
return status;
}
|