1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
|
/* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
package android.hardware.broadcastradio@2.0;
interface ITunerCallback {
/**
* Method called by the HAL when a tuning operation fails asynchronously
* following a step(), scan() or tune() command.
*
* This callback is only called when the step(), scan() or tune() command
* returned OK at first.
*
* @param result TIMEOUT in case of time out.
* @param selector A ProgramSelector structure passed from tune() call;
* empty for step() and scan().
*/
oneway onTuneFailed(Result result, ProgramSelector selector);
/**
* Method called by the HAL when current program information (including
* metadata) is updated.
*
* This is also called when the radio tuned to the static (not a valid
* station), see the TUNED flag of ProgramInfoFlags.
*
* @param info Current program information.
*/
oneway onCurrentProgramInfoChanged(ProgramInfo info);
/**
* A delta update of the program list, called whenever there's a change in
* the list.
*
* If there are frequent changes, HAL implementation must throttle the rate
* of the updates.
*
* There is a hard limit on binder transaction buffer, and the list must
* not exceed it. For large lists, HAL implementation must split them to
* multiple chunks, no larger than 500kiB each.
*
* @param chunk A chunk of the program list update.
*/
oneway onProgramListUpdated(ProgramListChunk chunk);
/**
* Method called by the HAL when the antenna gets connected or disconnected.
*
* For a new tuner session, client must assume the antenna is connected.
* If it's not, then antennaStateChange must be called within
* Constants::ANTENNA_DISCONNECTED_TIMEOUT_MS to indicate that.
*
* @param connected True if the antenna is now connected, false otherwise.
*/
oneway onAntennaStateChange(bool connected);
/**
* Generic callback for passing updates to vendor-specific parameter values.
* The framework does not interpret the parameters, they are passed
* in an opaque manner between a vendor application and HAL.
*
* It's up to the HAL implementation if and how to implement this callback,
* as long as it obeys the prefix rule. In particular, only selected keys
* may be notified this way. However, setParameters must not trigger
* this callback, while an internal event can change parameters
* asynchronously.
*
* @param parameters Vendor-specific key-value pairs,
* opaque to Android framework.
*/
oneway onParametersUpdated(vec<VendorKeyValue> parameters);
};
|