1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
|
//
// Copyright (C) 2017 The Android Open Source Project
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
// http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.
//
#ifndef ANDROID_HARDWARE_CONFIGSTORE_UTILS_H
#define ANDROID_HARDWARE_CONFIGSTORE_UTILS_H
#include <android/hardware/configstore/1.0/types.h>
#include <android/hardware/configstore/1.1/types.h>
#include <hidl/Status.h>
#include <sstream>
namespace android {
namespace hardware {
namespace details {
// Templated classes can use the below method
// to avoid creating dependencies on liblog.
bool wouldLogInfo();
void logAlwaysInfo(const std::string& message);
void logAlwaysError(const std::string& message);
} // namespace details
namespace configstore {
// import types from configstore
using ::android::hardware::configstore::V1_1::DisplayOrientation;
using ::android::hardware::configstore::V1_0::OptionalBool;
using ::android::hardware::configstore::V1_0::OptionalInt32;
using ::android::hardware::configstore::V1_0::OptionalUInt32;
using ::android::hardware::configstore::V1_0::OptionalInt64;
using ::android::hardware::configstore::V1_0::OptionalUInt64;
using ::android::hardware::configstore::V1_0::OptionalString;
using ::android::hardware::configstore::V1_1::OptionalDisplayOrientation;
static inline std::ostream& operator<<(std::ostream& os, DisplayOrientation orientation) {
os << ::android::hardware::configstore::V1_1::toString(orientation);
return os;
}
// a function to retrieve and cache the service handle
// for a particular interface
template <typename I>
sp<I> getService() {
// static initializer used for synchronizations
static sp<I> configs = I::getService();
return configs;
}
// arguments V: type for the value (i.e., OptionalXXX)
// I: interface class name
// func: member function pointer
template<typename V, typename I, android::hardware::Return<void> (I::* func)
(std::function<void(const V&)>)>
decltype(V::value) get(const decltype(V::value) &defValue) {
using namespace android::hardware::details;
// static initializer used for synchronizations
auto getHelper = []()->V {
V ret;
sp<I> configs = getService<I>();
if (!configs.get()) {
// fallback to the default value
ret.specified = false;
} else {
auto status = (*configs.*func)([&ret](V v) {
ret = v;
});
if (!status.isOk()) {
std::ostringstream oss;
oss << "HIDL call failed for retrieving a config item from "
"configstore : "
<< status.description().c_str();
logAlwaysError(oss.str());
ret.specified = false;
}
}
return ret;
};
static V cachedValue = getHelper();
if (wouldLogInfo()) {
std::string iname = __PRETTY_FUNCTION__;
// func name starts with "func = " in __PRETTY_FUNCTION__
auto pos = iname.find("func = ");
if (pos != std::string::npos) {
iname = iname.substr(pos + sizeof("func = "));
iname.pop_back(); // remove trailing ']'
} else {
iname += " (unknown)";
}
std::ostringstream oss;
oss << iname << " retrieved: "
<< (cachedValue.specified ? cachedValue.value : defValue)
<< (cachedValue.specified ? "" : " (default)");
logAlwaysInfo(oss.str());
}
return cachedValue.specified ? cachedValue.value : defValue;
}
template<typename I, android::hardware::Return<void> (I::* func)
(std::function<void(const OptionalBool&)>)>
bool getBool(const bool defValue) {
return get<OptionalBool, I, func>(defValue);
}
template<typename I, android::hardware::Return<void> (I::* func)
(std::function<void(const OptionalInt32&)>)>
int32_t getInt32(const int32_t defValue) {
return get<OptionalInt32, I, func>(defValue);
}
template<typename I, android::hardware::Return<void> (I::* func)
(std::function<void(const OptionalUInt32&)>)>
uint32_t getUInt32(const uint32_t defValue) {
return get<OptionalUInt32, I, func>(defValue);
}
template<typename I, android::hardware::Return<void> (I::* func)
(std::function<void(const OptionalInt64&)>)>
int64_t getInt64(const int64_t defValue) {
return get<OptionalInt64, I, func>(defValue);
}
template<typename I, android::hardware::Return<void> (I::* func)
(std::function<void(const OptionalUInt64&)>)>
uint64_t getUInt64(const uint64_t defValue) {
return get<OptionalUInt64, I, func>(defValue);
}
template<typename I, android::hardware::Return<void> (I::* func)
(std::function<void(const OptionalString&)>)>
std::string getString(const std::string &defValue) {
return get<OptionalString, I, func>(defValue);
}
template <typename I, android::hardware::Return<void> (I::*func)(
std::function<void(const OptionalDisplayOrientation&)>)>
DisplayOrientation getDisplayOrientation(DisplayOrientation defValue) {
return get<OptionalDisplayOrientation, I, func>(defValue);
}
} // namespace configstore
} // namespace hardware
} // namespace android
#endif // ANDROID_HARDWARE_CONFIGSTORE_UTILS_H
|