1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
443
444
445
446
447
448
449
450
451
452
453
454
455
456
457
458
459
460
461
462
463
464
465
466
467
468
469
470
471
472
473
474
475
476
477
478
479
480
481
482
483
484
485
486
487
488
489
490
491
492
493
494
495
496
497
498
499
500
501
502
503
504
505
506
507
508
509
510
511
512
513
514
515
516
517
518
519
520
521
522
523
524
525
526
527
528
529
530
531
532
533
534
535
536
537
538
539
540
541
542
543
544
545
546
547
548
549
550
551
552
553
554
555
556
557
558
559
560
561
562
563
564
565
566
567
568
569
570
571
572
573
574
575
576
577
578
579
580
581
582
583
584
585
586
587
588
589
590
591
592
593
594
595
596
597
598
599
600
601
602
603
604
605
606
607
608
609
610
611
612
613
614
615
616
617
618
619
620
621
622
623
624
625
626
627
628
629
630
631
632
|
/*
* Copyright (C) 2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
package android.hardware.gnss@1.0;
/** The callback interface to report measurements from the HAL. */
interface IGnssMeasurementCallback {
/**
* Flags to indicate what fields in GnssClock are valid.
*/
@export(name="", value_prefix="GNSS_CLOCK_")
enum GnssClockFlags : uint16_t {
/** A valid 'leap second' is stored in the data structure. */
HAS_LEAP_SECOND = 1 << 0,
/** A valid 'time uncertainty' is stored in the data structure. */
HAS_TIME_UNCERTAINTY = 1 << 1,
/** A valid 'full bias' is stored in the data structure. */
HAS_FULL_BIAS = 1 << 2,
/** A valid 'bias' is stored in the data structure. */
HAS_BIAS = 1 << 3,
/** A valid 'bias uncertainty' is stored in the data structure. */
HAS_BIAS_UNCERTAINTY = 1 << 4,
/** A valid 'drift' is stored in the data structure. */
HAS_DRIFT = 1 << 5,
/** A valid 'drift uncertainty' is stored in the data structure. */
HAS_DRIFT_UNCERTAINTY = 1 << 6
};
/**
* Flags to indicate what fields in GnssMeasurement are valid.
*/
@export(name="", value_prefix="GNSS_MEASUREMENT_")
enum GnssMeasurementFlags : uint32_t {
/** A valid 'snr' is stored in the data structure. */
HAS_SNR = 1 << 0,
/** A valid 'carrier frequency' is stored in the data structure. */
HAS_CARRIER_FREQUENCY = 1 << 9,
/** A valid 'carrier cycles' is stored in the data structure. */
HAS_CARRIER_CYCLES = 1 << 10,
/** A valid 'carrier phase' is stored in the data structure. */
HAS_CARRIER_PHASE = 1 << 11,
/** A valid 'carrier phase uncertainty' is stored in the data structure. */
HAS_CARRIER_PHASE_UNCERTAINTY = 1 << 12,
/** A valid automatic gain control is stored in the data structure. */
HAS_AUTOMATIC_GAIN_CONTROL = 1 << 13
};
/**
* Enumeration of available values for the GNSS Measurement's multipath
* indicator.
*/
@export(name="", value_prefix="GNSS_MULTIPATH_")
enum GnssMultipathIndicator : uint8_t {
/** The indicator is not available or unknown. */
INDICATOR_UNKNOWN = 0,
/** The measurement is indicated to be affected by multipath. */
INDICATOR_PRESENT = 1,
/** The measurement is indicated to be not affected by multipath. */
INDICATIOR_NOT_PRESENT = 2
};
/**
* Flags indicating the GNSS measurement state.
*
* The expected behavior here is for GNSS HAL to set all the flags that applies.
* For example, if the state for a satellite is only C/A code locked and bit
* synchronized, and there is still millisecond ambiguity, the state must be
* set as:
*
* STATE_CODE_LOCK | STATE_BIT_SYNC | STATE_MSEC_AMBIGUOUS
*
* If GNSS is still searching for a satellite, the corresponding state must be
* set to STATE_UNKNOWN(0).
*/
@export(name="", value_prefix="GNSS_MEASUREMENT_")
enum GnssMeasurementState : uint32_t {
STATE_UNKNOWN = 0,
STATE_CODE_LOCK = 1 << 0,
STATE_BIT_SYNC = 1 << 1,
STATE_SUBFRAME_SYNC = 1 << 2,
STATE_TOW_DECODED = 1 << 3,
STATE_MSEC_AMBIGUOUS = 1 << 4,
STATE_SYMBOL_SYNC = 1 << 5,
STATE_GLO_STRING_SYNC = 1 << 6,
STATE_GLO_TOD_DECODED = 1 << 7,
STATE_BDS_D2_BIT_SYNC = 1 << 8,
STATE_BDS_D2_SUBFRAME_SYNC = 1 << 9,
STATE_GAL_E1BC_CODE_LOCK = 1 << 10,
STATE_GAL_E1C_2ND_CODE_LOCK = 1 << 11,
STATE_GAL_E1B_PAGE_SYNC = 1 << 12,
STATE_SBAS_SYNC = 1 << 13,
STATE_TOW_KNOWN = 1 << 14,
STATE_GLO_TOD_KNOWN = 1 << 15,
};
/**
* Flags indicating the Accumulated Delta Range's states.
*/
@export(name="", value_prefix="GNSS_")
enum GnssAccumulatedDeltaRangeState : uint16_t {
ADR_STATE_UNKNOWN = 0,
ADR_STATE_VALID = 1 << 0,
ADR_STATE_RESET = 1 << 1,
ADR_STATE_CYCLE_SLIP = 1 << 2,
};
/**
* Represents an estimate of the GNSS clock time.
*/
struct GnssClock {
/**
* A set of flags indicating the validity of the fields in this data
* structure.
*
* Fields for which there is no corresponding flag must be filled in
* with a valid value. For convenience, these are marked as mandatory.
*
* Others fields may have invalid information in them, if not marked as
* valid by the corresponding bit in gnssClockFlags.
*/
bitfield<GnssClockFlags> gnssClockFlags;
/**
* Leap second data.
* The sign of the value is defined by the following equation:
* utcTimeNs = timeNs - (fullBiasNs + biasNs) - leapSecond *
* 1,000,000,000
*
* If this data is available, gnssClockFlags must contain
* HAS_LEAP_SECOND.
*/
int16_t leapSecond;
/**
* The GNSS receiver internal clock value. This is the local hardware clock
* value.
*
* For local hardware clock, this value is expected to be monotonically
* increasing while the hardware clock remains powered on. (For the case of a
* HW clock that is not continuously on, see the
* hwClockDiscontinuityCount field). The receiver's estimate of GNSS time
* can be derived by subtracting the sum of fullBiasNs and biasNs (when
* available) from this value.
*
* This GNSS time must be the best estimate of current GNSS time
* that GNSS receiver can achieve.
*
* Sub-nanosecond accuracy can be provided by means of the 'biasNs' field.
* The value contains the timeUncertaintyNs in it.
*
* This value is mandatory.
*/
int64_t timeNs;
/**
* 1-Sigma uncertainty associated with the clock's time in nanoseconds.
* The uncertainty is represented as an absolute (single sided) value.
*
* If the data is available, gnssClockFlags must contain
* HAS_TIME_UNCERTAINTY. Ths value is ideally zero, as the time
* 'latched' by timeNs is defined as the reference clock vs. which all
* other times (and corresponding uncertainties) are measured.
*/
double timeUncertaintyNs;
/**
* The difference between hardware clock ('time' field) inside GNSS receiver
* and the true GPS time since 0000Z, January 6, 1980, in nanoseconds.
*
* The sign of the value is defined by the following equation:
* local estimate of GPS time = timeNs - (fullBiasNs + biasNs)
*
* If receiver has computed time for a non-GPS constellation, the time offset of
* that constellation versus GPS time must be applied to fill this value.
*
* The error estimate for the sum of this and the biasNs is the biasUncertaintyNs.
*
* If the data is available gnssClockFlags must contain HAS_FULL_BIAS.
*
* This value is mandatory if the receiver has estimated GPS time.
*/
int64_t fullBiasNs;
/**
* Sub-nanosecond bias - used with fullBiasNS, see fullBiasNs for details.
*
* The error estimate for the sum of this and the fullBiasNs is the
* biasUncertaintyNs.
*
* If the data is available gnssClockFlags must contain HAS_BIAS.
*
* This value is mandatory if the receiver has estimated GPS time.
*/
double biasNs;
/**
* 1-Sigma uncertainty associated with the local estimate of GNSS time (clock
* bias) in nanoseconds. The uncertainty is represented as an absolute
* (single sided) value.
*
* The caller is responsible for using this uncertainty (it can be very
* large before the GPS time has been fully resolved.)
*
* If the data is available gnssClockFlags must contain HAS_BIAS_UNCERTAINTY.
*
* This value is mandatory if the receiver has estimated GPS time.
*/
double biasUncertaintyNs;
/**
* The clock's drift in nanoseconds (per second).
*
* A positive value means that the frequency is higher than the nominal
* frequency, and that the (fullBiasNs + biasNs) is growing more positive
* over time.
*
* If the data is available gnssClockFlags must contain HAS_DRIFT.
*
* This value is mandatory if the receiver has estimated GPS time.
*/
double driftNsps;
/**
* 1-Sigma uncertainty associated with the clock's drift in nanoseconds (per
* second).
* The uncertainty is represented as an absolute (single sided) value.
*
* If the data is available gnssClockFlags must contain HAS_DRIFT_UNCERTAINTY.
*
* This value is mandatory if the receiver has estimated GPS time.
*/
double driftUncertaintyNsps;
/**
* This field must be incremented, when there are discontinuities in the
* hardware clock.
*
* A "discontinuity" is meant to cover the case of a switch from one source
* of clock to another. A single free-running crystal oscillator (XO)
* will generally not have any discontinuities, and this can be set and
* left at 0.
*
* If, however, the timeNs value (HW clock) is derived from a composite of
* sources, that is not as smooth as a typical XO, or is otherwise stopped &
* restarted, then this value shall be incremented each time a discontinuity
* occurs. (E.g. this value can start at zero at device boot-up and
* increment each time there is a change in clock continuity. In the
* unlikely event that this value reaches full scale, rollover (not
* clamping) is required, such that this value continues to change, during
* subsequent discontinuity events.)
*
* While this number stays the same, between GnssClock reports, it can be
* safely assumed that the timeNs value has been running continuously, e.g.
* derived from a single, high quality clock (XO like, or better, that is
* typically used during continuous GNSS signal sampling.)
*
* It is expected, esp. during periods where there are few GNSS signals
* available, that the HW clock be discontinuity-free as long as possible,
* as this avoids the need to use (waste) a GNSS measurement to fully
* re-solve for the GNSS clock bias and drift, when using the accompanying
* measurements, from consecutive GnssData reports.
*
* This value is mandatory.
*/
uint32_t hwClockDiscontinuityCount;
};
/**
* Represents a GNSS Measurement, it contains raw and computed information.
*
* All signal measurement information (e.g. svTime,
* pseudorangeRate, multipathIndicator) reported in this struct must be
* based on GNSS signal measurements only. You must not synthesize measurements
* by calculating or reporting expected measurements based on known or estimated
* position, velocity, or time.
*/
struct GnssMeasurement{
/**
* A set of flags indicating the validity of the fields in this data
* structure.
*
* Fields for which there is no corresponding flag must be filled in
* with a valid value. For convenience, these are marked as mandatory.
*
* Others fields may have invalid information in them, if not marked as
* valid by the corresponding bit in flags.
*/
bitfield<GnssMeasurementFlags> flags;
/**
* Satellite vehicle ID number, as defined in GnssSvInfo::svid
*
* This value is mandatory.
*/
int16_t svid;
/**
* Defines the constellation of the given SV.
*
* This value is mandatory.
*/
GnssConstellationType constellation;
/**
* Time offset at which the measurement was taken in nanoseconds.
* The reference receiver's time is specified by GnssData::clock::timeNs.
*
* The sign of timeOffsetNs is given by the following equation:
* measurement time = GnssClock::timeNs + timeOffsetNs
*
* It provides an individual time-stamp for the measurement, and allows
* sub-nanosecond accuracy. It may be zero if all measurements are
* aligned to a common time.
*
* This value is mandatory.
*/
double timeOffsetNs;
/**
* Per satellite sync state. It represents the current sync state for the
* associated satellite.
* Based on the sync state, the 'received GNSS tow' field must be interpreted
* accordingly.
*
* This value is mandatory.
*/
bitfield<GnssMeasurementState> state;
/**
* The received GNSS Time-of-Week at the measurement time, in nanoseconds.
* For GNSS & QZSS, this is the received GNSS Time-of-Week at the
* measurement time, in nanoseconds. The value is relative to the
* beginning of the current GNSS week.
*
* Given the highest sync state that can be achieved, per each satellite,
* valid range for this field can be:
* Searching : [ 0 ] : STATE_UNKNOWN
* C/A code lock : [ 0 1ms ] : STATE_CODE_LOCK set
* Bit sync : [ 0 20ms ] : STATE_BIT_SYNC set
* Subframe sync : [ 0 6s ] : STATE_SUBFRAME_SYNC set
* TOW decoded : [ 0 1week ] : STATE_TOW_DECODED set
* TOW Known : [ 0 1week ] : STATE_TOW_KNOWN set
*
* Note: TOW Known refers to the case where TOW is possibly not decoded
* over the air but has been determined from other sources. If TOW
* decoded is set then TOW Known must also be set.
*
* Note: If there is any ambiguity in integer millisecond,
* GNSS_MEASUREMENT_STATE_MSEC_AMBIGUOUS must be set accordingly, in the
* 'state' field.
*
* This value must be populated if 'state' != STATE_UNKNOWN.
*
* For Glonass, this is the received Glonass time of day, at the
* measurement time in nanoseconds.
*
* Given the highest sync state that can be achieved, per each satellite,
* valid range for this field can be:
* Searching : [ 0 ] : STATE_UNKNOWN set
* C/A code lock : [ 0 1ms ] : STATE_CODE_LOCK set
* Symbol sync : [ 0 10ms ] : STATE_SYMBOL_SYNC set
* Bit sync : [ 0 20ms ] : STATE_BIT_SYNC set
* String sync : [ 0 2s ] : STATE_GLO_STRING_SYNC set
* Time of day decoded : [ 0 1day ] : STATE_GLO_TOD_DECODED set
* Time of day known : [ 0 1day ] : STATE_GLO_TOD_KNOWN set
*
* Note: Time of day known refers to the case where it is possibly not
* decoded over the air but has been determined from other sources. If
* Time of day decoded is set then Time of day known must also be set.
*
* For Beidou, this is the received Beidou time of week,
* at the measurement time in nanoseconds.
*
* Given the highest sync state that can be achieved, per each satellite,
* valid range for this field can be:
* Searching : [ 0 ] : STATE_UNKNOWN set.
* C/A code lock : [ 0 1ms ] : STATE_CODE_LOCK set.
* Bit sync (D2) : [ 0 2ms ] : STATE_BDS_D2_BIT_SYNC set.
* Bit sync (D1) : [ 0 20ms ] : STATE_BIT_SYNC set.
* Subframe (D2) : [ 0 0.6s ] : STATE_BDS_D2_SUBFRAME_SYNC set.
* Subframe (D1) : [ 0 6s ] : STATE_SUBFRAME_SYNC set.
* Time of week decoded : [ 0 1week ] : STATE_TOW_DECODED set.
* Time of week known : [ 0 1week ] : STATE_TOW_KNOWN set
*
* Note: TOW Known refers to the case where TOW is possibly not decoded
* over the air but has been determined from other sources. If TOW
* decoded is set then TOW Known must also be set.
*
* For Galileo, this is the received Galileo time of week,
* at the measurement time in nanoseconds.
*
* E1BC code lock : [ 0 4ms ] : STATE_GAL_E1BC_CODE_LOCK set.
* E1C 2nd code lock : [ 0 100ms] : STATE_GAL_E1C_2ND_CODE_LOCK set.
* E1B page : [ 0 2s ] : STATE_GAL_E1B_PAGE_SYNC set.
* Time of week decoded : [ 0 1week] : STATE_TOW_DECODED is set.
* Time of week known : [ 0 1week] : STATE_TOW_KNOWN set
*
* Note: TOW Known refers to the case where TOW is possibly not decoded
* over the air but has been determined from other sources. If TOW
* decoded is set then TOW Known must also be set.
*
* For SBAS, this is received SBAS time, at the measurement time in
* nanoseconds.
*
* Given the highest sync state that can be achieved, per each satellite,
* valid range for this field can be:
* Searching : [ 0 ] : STATE_UNKNOWN
* C/A code lock: [ 0 1ms ] : STATE_CODE_LOCK is set
* Symbol sync : [ 0 2ms ] : STATE_SYMBOL_SYNC is set
* Message : [ 0 1s ] : STATE_SBAS_SYNC is set
*/
int64_t receivedSvTimeInNs;
/**
* 1-Sigma uncertainty of the Received GNSS Time-of-Week in nanoseconds.
*
* This value must be populated if 'state' != STATE_UNKNOWN.
*/
int64_t receivedSvTimeUncertaintyInNs;
/**
* Carrier-to-noise density in dB-Hz, typically in the range [0, 63].
* It contains the measured C/N0 value for the signal at the antenna port.
*
* This value is mandatory.
*/
double cN0DbHz;
/**
* Pseudorange rate at the timestamp in m/s. The correction of a given
* Pseudorange Rate value includes corrections for receiver and satellite
* clock frequency errors. Ensure that this field is independent (see
* comment at top of GnssMeasurement struct.)
*
* It is mandatory to provide the 'uncorrected' 'pseudorange rate', and
* provide GnssClock's 'drift' field as well. When providing the
* uncorrected pseudorange rate, do not apply the corrections described above.)
*
* The value includes the 'pseudorange rate uncertainty' in it.
* A positive 'uncorrected' value indicates that the SV is moving away from
* the receiver.
*
* The sign of the 'uncorrected' 'pseudorange rate' and its relation to the
* sign of 'doppler shift' is given by the equation:
* pseudorange rate = -k * doppler shift (where k is a constant)
*
* This must be the most accurate pseudorange rate available, based on
* fresh signal measurements from this channel.
*
* It is mandatory that this value be provided at typical carrier phase PRR
* quality (few cm/sec per second of uncertainty, or better) - when signals
* are sufficiently strong & stable, e.g. signals from a GNSS simulator at >=
* 35 dB-Hz.
*/
double pseudorangeRateMps;
/**
* 1-Sigma uncertainty of the pseudorangeRateMps.
* The uncertainty is represented as an absolute (single sided) value.
*
* This value is mandatory.
*/
double pseudorangeRateUncertaintyMps;
/**
* Accumulated delta range's state. It indicates whether ADR is reset or
* there is a cycle slip(indicating loss of lock).
*
* This value is mandatory.
*/
bitfield<GnssAccumulatedDeltaRangeState> accumulatedDeltaRangeState;
/**
* Accumulated delta range since the last channel reset in meters.
* A positive value indicates that the SV is moving away from the receiver.
*
* The sign of the 'accumulated delta range' and its relation to the sign of
* 'carrier phase' is given by the equation:
* accumulated delta range = -k * carrier phase (where k is a constant)
*
* This value must be populated if 'accumulated delta range state' !=
* ADR_STATE_UNKNOWN.
* However, it is expected that the data is only accurate when:
* 'accumulated delta range state' == ADR_STATE_VALID.
*/
double accumulatedDeltaRangeM;
/**
* 1-Sigma uncertainty of the accumulated delta range in meters.
* This value must be populated if 'accumulated delta range state' !=
* ADR_STATE_UNKNOWN.
*/
double accumulatedDeltaRangeUncertaintyM;
/**
* Carrier frequency of the signal tracked, for example it can be the
* GPS central frequency for L1 = 1575.45 MHz, or L2 = 1227.60 MHz, L5 =
* 1176.45 MHz, varying GLO channels, etc. If the field is not set, it
* is the primary common use central frequency, e.g. L1 = 1575.45 MHz
* for GPS.
*
* For an L1, L5 receiver tracking a satellite on L1 and L5 at the same
* time, two raw measurement structs must be reported for this same
* satellite, in one of the measurement structs, all the values related
* to L1 must be filled, and in the other all of the values related to
* L5 must be filled.
*
* If the data is available, gnssMeasurementFlags must contain
* HAS_CARRIER_FREQUENCY.
*/
float carrierFrequencyHz;
/**
* The number of full carrier cycles between the satellite and the
* receiver. The reference frequency is given by the field
* 'carrierFrequencyHz'. Indications of possible cycle slips and
* resets in the accumulation of this value can be inferred from the
* accumulatedDeltaRangeState flags.
*
* If the data is available, gnssMeasurementFlags must contain
* HAS_CARRIER_CYCLES.
*/
int64_t carrierCycles;
/**
* The RF phase detected by the receiver, in the range [0.0, 1.0].
* This is usually the fractional part of the complete carrier phase
* measurement.
*
* The reference frequency is given by the field 'carrierFrequencyHz'.
* The value contains the 'carrier-phase uncertainty' in it.
*
* If the data is available, gnssMeasurementFlags must contain
* HAS_CARRIER_PHASE.
*/
double carrierPhase;
/**
* 1-Sigma uncertainty of the carrier-phase.
* If the data is available, gnssMeasurementFlags must contain
* HAS_CARRIER_PHASE_UNCERTAINTY.
*/
double carrierPhaseUncertainty;
/**
* An enumeration that indicates the 'multipath' state of the event.
*
* The multipath Indicator is intended to report the presence of overlapping
* signals that manifest as distorted correlation peaks.
*
* - if there is a distorted correlation peak shape, report that multipath
* is MULTIPATH_INDICATOR_PRESENT.
* - if there is no distorted correlation peak shape, report
* MULTIPATH_INDICATOR_NOT_PRESENT
* - if signals are too weak to discern this information, report
* MULTIPATH_INDICATOR_UNKNOWN
*
* Example: when doing the standardized overlapping Multipath Performance
* test (3GPP TS 34.171) the Multipath indicator must report
* MULTIPATH_INDICATOR_PRESENT for those signals that are tracked, and
* contain multipath, and MULTIPATH_INDICATOR_NOT_PRESENT for those
* signals that are tracked and do not contain multipath.
*/
GnssMultipathIndicator multipathIndicator;
/**
* Signal-to-noise ratio at correlator output in dB.
* If the data is available, GnssMeasurementFlags must contain HAS_SNR.
* This is the power ratio of the "correlation peak height above the
* observed noise floor" to "the noise RMS".
*/
double snrDb;
/**
* Automatic gain control (AGC) level. AGC acts as a variable gain
* amplifier adjusting the power of the incoming signal. The AGC level
* may be used to indicate potential interference. When AGC is at a
* nominal level, this value must be set as 0. Higher gain (and/or lower
* input power) must be output as a positive number. Hence in cases of
* strong jamming, in the band of this signal, this value must go more
* negative.
*
* Note: Different hardware designs (e.g. antenna, pre-amplification, or
* other RF HW components) may also affect the typical output of of this
* value on any given hardware design in an open sky test - the
* important aspect of this output is that changes in this value are
* indicative of changes on input signal power in the frequency band for
* this measurement.
*/
double agcLevelDb;
};
/**
* Represents a reading of GNSS measurements. For devices where GnssSystemInfo's
* yearOfHw is set to 2016+, it is mandatory that these be provided, on
* request, when the GNSS receiver is searching/tracking signals.
*
* - Reporting of GNSS constellation measurements is mandatory.
* - Reporting of all tracked constellations are encouraged.
*/
struct GnssData {
/** Number of GnssMeasurement elements. */
uint32_t measurementCount;
/** The array of measurements. */
GnssMeasurement[GnssMax:SVS_COUNT] measurements;
/** The GNSS clock time reading. */
GnssClock clock;
};
/**
* Callback for the hal to pass a GnssData structure back to the client.
*
* @param data Contains a reading of GNSS measurements.
*/
GnssMeasurementCb(GnssData data);
};
|