1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
279
280
281
282
283
284
285
286
287
288
289
290
291
292
293
294
295
296
297
298
299
300
301
302
303
304
305
306
307
308
309
310
311
312
313
314
315
316
317
318
319
320
321
322
323
324
325
326
327
328
329
330
331
332
333
334
335
336
337
338
339
340
341
342
343
344
345
346
347
348
349
350
351
352
353
354
355
356
357
358
359
360
361
362
363
364
365
366
367
368
369
370
371
372
373
374
375
376
377
378
379
380
381
382
383
384
385
386
387
388
389
390
391
392
393
394
395
396
397
398
399
400
401
402
403
404
405
406
407
408
409
410
411
412
413
414
415
416
417
418
419
420
421
422
423
424
425
426
427
428
429
430
431
432
433
434
435
436
437
438
439
440
441
442
|
/*
* Copyright (C) 2018 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
package android.hardware.graphics.composer@2.2;
import android.hardware.graphics.common@1.1::ColorMode;
import android.hardware.graphics.common@1.1::Dataspace;
import android.hardware.graphics.common@1.1::PixelFormat;
import android.hardware.graphics.common@1.1::RenderIntent;
import @2.1::IComposerClient;
import @2.1::Display;
import @2.1::Error;
import @2.1::IComposerClient;
interface IComposerClient extends @2.1::IComposerClient {
enum PowerMode : @2.1::IComposerClient.PowerMode {
/**
* The display is configured as in ON but may stop applying display
* updates from the client. This is effectively a hint to the device
* that drawing to the display has been suspended and that the the
* device must remain on and continue displaying its current contents
* indefinitely until the power mode changes.
*
* This mode may also be used as a signal to enable hardware-based
* functionality to take over the display and manage it autonomously
* to implement a low power always-on display.
*/
ON_SUSPEND = 4
};
/**
* Following enums define keys for metadata defined by SMPTE ST 2086:2014
* and CTA 861.3.
*/
enum PerFrameMetadataKey : int32_t {
/** SMPTE ST 2084:2014.
* Coordinates defined in CIE 1931 xy chromaticity space
*/
/** SMPTE ST 2084:2014 */
DISPLAY_RED_PRIMARY_X,
/** SMPTE ST 2084:2014 */
DISPLAY_RED_PRIMARY_Y,
/** SMPTE ST 2084:2014 */
DISPLAY_GREEN_PRIMARY_X,
/** SMPTE ST 2084:2014 */
DISPLAY_GREEN_PRIMARY_Y,
/** SMPTE ST 2084:2014 */
DISPLAY_BLUE_PRIMARY_X,
/** SMPTE ST 2084:2014 */
DISPLAY_BLUE_PRIMARY_Y,
/** SMPTE ST 2084:2014 */
WHITE_POINT_X,
/** SMPTE ST 2084:2014 */
WHITE_POINT_Y,
/** SMPTE ST 2084:2014.
* Units: nits
* max as defined by ST 2048: 10,000 nits
*/
MAX_LUMINANCE,
/** SMPTE ST 2084:2014 */
MIN_LUMINANCE,
/** CTA 861.3 */
MAX_CONTENT_LIGHT_LEVEL,
/** CTA 861.3 */
MAX_FRAME_AVERAGE_LIGHT_LEVEL,
};
struct PerFrameMetadata {
PerFrameMetadataKey key;
float value;
};
struct FloatColor {
float r;
float g;
float b;
float a;
};
enum Command : @2.1::IComposerClient.Command {
/**
* SET_LAYER_PER_FRAME_METADATA has this pseudo prototype
*
* setLayerPerFrameMetadata(Display display, Layer layer,
* vec<PerFrameMetadata> data);
*
* Sets the PerFrameMetadata for the display. This metadata must be used
* by the implementation to better tone map content to that display.
*
* This is a method that may be called every frame. Thus it's
* implemented using buffered transport.
* SET_LAYER_PER_FRAME_METADATA is the command used by the buffered transport
* mechanism.
*/
SET_LAYER_PER_FRAME_METADATA = 0x303 << @2.1::IComposerClient.Command:OPCODE_SHIFT,
/**
* SET_LAYER_COLOR has this pseudo prototype
*
* setLayerColor(FloatColor color);
*
* Sets the color of the given layer. If the composition type of the layer
* is not Composition::SOLID_COLOR, this call must succeed and have no
* other effect.
*
* @param color is the new color using float type.
*/
SET_LAYER_FLOAT_COLOR = 0x40c << @2.1::IComposerClient.Command:OPCODE_SHIFT,
};
/**
* Returns the PerFrameMetadataKeys that are supported by this device.
*
* @param display is the display on which to create the layer.
* @return keys is the vector of PerFrameMetadataKey keys that are
* supported by this device.
* @return error is NONE upon success. Otherwise,
* UNSUPPORTED if not supported on underlying HAL
*/
getPerFrameMetadataKeys(Display display)
generates (Error error,
vec<PerFrameMetadataKey> keys);
/**
* getReadbackBufferAttributes
* Returns the format which should be used when allocating a buffer for use by
* device readback as well as the dataspace in which its contents should be
* interpreted.
*
* The width and height of this buffer must be those of the currently-active
* display configuration, and the usage flags must consist of the following:
* BufferUsage::CPU_READ | BufferUsage::GPU_TEXTURE |
* BufferUsage::COMPOSER_OUTPUT
*
* The format and dataspace provided must be sufficient such that if a
* correctly-configured buffer is passed into setReadbackBuffer, filled by
* the device, and then displayed by the client as a full-screen buffer, the
* output of the display remains the same (subject to the note about protected
* content in the description of setReadbackBuffer).
*
* Parameters:
* @param display - the display on which to create the layer.
*
* @return format - the format the client should use when allocating a device
* readback buffer
* @return dataspace - the dataspace to use when interpreting the
* contents of a device readback buffer
* @return error is NONE upon success. Otherwise,
* BAD_DISPLAY when an invalid display handle was passed in.
* UNSUPPORTED if not supported on underlying HAL
*
* See also:
* setReadbackBuffer
* getReadbackBufferFence
*/
getReadbackBufferAttributes(Display display)
generates (Error error,
PixelFormat format,
Dataspace dataspace);
/**
* getReadbackBufferFence
* Returns an acquire sync fence file descriptor which must signal when the
* buffer provided to setReadbackBuffer has been filled by the device and is
* safe for the client to read.
*
* If it is already safe to read from this buffer, -1 may be returned instead.
* The client takes ownership of this file descriptor and is responsible for
* closing it when it is no longer needed.
*
* This function must be called immediately after the composition cycle being
* captured into the readback buffer. The complete ordering of a readback buffer
* capture is as follows:
*
* getReadbackBufferAttributes
* // Readback buffer is allocated
* // Many frames may pass
*
* setReadbackBuffer
* validateDisplay
* presentDisplay
* getReadbackBufferFence
* // Implicitly wait on the acquire fence before accessing the buffer
*
* Parameters:
* @param display - the display on which to create the layer.
*
* @return acquireFence - a sync fence file descriptor as described above; pointer
* must be non-NULL
* @return error - is HWC2_ERROR_NONE or one of the following errors:
* BAD_DISPLAY - an invalid display handle was passed in
* UNSUPPORTED if not supported on underlying HAL
*
* See also:
* getReadbackBufferAttributes
* setReadbackBuffer
*/
getReadbackBufferFence(Display display)
generates (Error error,
handle acquireFence);
/**
* setReadbackBuffer
* Sets the readback buffer to be filled with the contents of the next
* composition performed for this display (i.e., the contents present at the
* time of the next validateDisplay/presentDisplay cycle).
*
* This buffer must have been allocated as described in
* getReadbackBufferAttributes and is in the dataspace provided by the same.
*
* If there is hardware protected content on the display at the time of the next
* composition, the area of the readback buffer covered by such content must be
* completely black. Any areas of the buffer not covered by such content may
* optionally be black as well.
*
* The release fence file descriptor provided works identically to the one
* described for setOutputBuffer.
*
* This function must not be called between any call to validateDisplay and a
* subsequent call to presentDisplay.
*
* Parameters:
* @param display - the display on which to create the layer.
* @param buffer - the new readback buffer
* @param releaseFence - a sync fence file descriptor as described in setOutputBuffer
*
* @return error - is HWC2_ERROR_NONE or one of the following errors:
* HWC2_ERROR_BAD_DISPLAY - an invalid display handle was passed in
* HWC2_ERROR_BAD_PARAMETER - the new readback buffer handle was invalid
*
* See also:
* getReadbackBufferAttributes
* getReadbackBufferFence
*/
setReadbackBuffer(Display display, handle buffer, handle releaseFence) generates (Error error);
/**
* createVirtualDisplay_2_2
* Creates a new virtual display with the given width and height. The
* format passed into this function is the default format requested by the
* consumer of the virtual display output buffers.
*
* The display must be assumed to be on from the time the first frame is
* presented until the display is destroyed.
*
* @param width is the width in pixels.
* @param height is the height in pixels.
* @param formatHint is the default output buffer format selected by
* the consumer.
* @param outputBufferSlotCount is the number of output buffer slots to be
* reserved.
* @return error is NONE upon success. Otherwise,
* UNSUPPORTED when the width or height is too large for the
* device to be able to create a virtual display.
* NO_RESOURCES when the device is unable to create a new virtual
* display at this time.
* @return display is the newly-created virtual display.
* @return format is the format of the buffer the device will produce.
*/
@callflow(next="*")
createVirtualDisplay_2_2(uint32_t width,
uint32_t height,
PixelFormat formatHint,
uint32_t outputBufferSlotCount)
generates (Error error,
Display display,
PixelFormat format);
/**
* getClientTargetSupport_2_2
* Returns whether a client target with the given properties can be
* handled by the device.
*
* This function must return true for a client target with width and
* height equal to the active display configuration dimensions,
* PixelFormat::RGBA_8888, and Dataspace::UNKNOWN. It is not required to
* return true for any other configuration.
*
* @param display is the display to query.
* @param width is the client target width in pixels.
* @param height is the client target height in pixels.
* @param format is the client target format.
* @param dataspace is the client target dataspace, as described in
* setLayerDataspace.
* @return error is NONE upon success. Otherwise,
* BAD_DISPLAY when an invalid display handle was passed in.
* UNSUPPORTED when the given configuration is not supported.
*/
@callflow(next="*")
getClientTargetSupport_2_2(Display display,
uint32_t width,
uint32_t height,
PixelFormat format,
Dataspace dataspace)
generates (Error error);
/**
* setPowerMode_2_2
* Sets the power mode of the given display. The transition must be
* complete when this function returns. It is valid to call this function
* multiple times with the same power mode.
*
* All displays must support PowerMode::ON and PowerMode::OFF. Whether a
* display supports PowerMode::DOZE or PowerMode::DOZE_SUSPEND may be
* queried using getDozeSupport.
*
* @param display is the display to which the power mode is set.
* @param mode is the new power mode.
* @return error is NONE upon success. Otherwise,
* BAD_DISPLAY when an invalid display handle was passed in.
* BAD_PARAMETER when mode was not a valid power mode.
* UNSUPPORTED when mode is not supported on this display.
*/
setPowerMode_2_2(Display display, PowerMode mode) generates (Error error);
/**
* Returns the color modes supported on this display.
*
* All devices must support at least ColorMode::NATIVE.
*
* @param display is the display to query.
* @return error is NONE upon success. Otherwise,
* BAD_DISPLAY when an invalid display handle was passed in.
* @return modes is an array of color modes.
*/
getColorModes_2_2(Display display)
generates (Error error,
vec<ColorMode> modes);
/**
* Returns the render intents supported by the specified display and color
* mode.
*
* RenderIntent::COLORIMETRIC is always supported.
*
* @param display is the display to query.
* @param mode is the color mode to query.
* @return error is NONE upon success. Otherwise,
* BAD_DISPLAY when an invalid display handle was passed in.
* BAD_PARAMETER when an invalid color mode was passed in.
* @return intents is an array of render intents.
*/
getRenderIntents(Display display, ColorMode mode)
generates (Error error,
vec<RenderIntent> intents);
/**
* Sets the color mode and render intent of the given display.
*
* The color mode and render intent change must take effect on next
* presentDisplay.
*
* All devices must support at least ColorMode::NATIVE and
* RenderIntent::COLORIMETRIC, and displays are assumed to be in this mode
* upon hotplug.
*
* @param display is the display to which the color mode is set.
* @param mode is the color mode to set to.
* @param intent is the render intent to set to.
* @return error is NONE upon success. Otherwise,
* BAD_DISPLAY when an invalid display handle was passed in.
* BAD_PARAMETER when mode or intent is invalid
* UNSUPPORTED when mode or intent is not supported on this
* display.
*/
setColorMode_2_2(Display display, ColorMode mode, RenderIntent intent)
generates (Error error);
/*
* By default, layer dataspaces are mapped to the current color mode
* colorimetrically with a few exceptions.
*
* When the layer dataspace is a legacy dataspace (see
* common@1.1::Dataspace) and the display render intent is
* RenderIntent::ENHANCE, the pixel values can go through an
* implementation-defined saturation transform before being mapped to the
* current color mode colorimetrically.
*
* Colors that are out of the gamut of the current color mode are
* hard-clipped.
*/
/**
* Returns the saturation matrix of the specified legacy dataspace.
*
* The saturation matrix can be used to approximate the legacy dataspace
* saturation transform. It is to be applied on linear pixel values like
* this:
*
* (in GLSL)
* linearSrgb = saturationMatrix * linearSrgb;
*
* @param dataspace must be Dataspace::SRGB_LINEAR.
* @return error is NONE upon success. Otherwise,
* BAD_PARAMETER when an invalid dataspace was passed in.
* @return matrix is the 4x4 column-major matrix used to approximate the
* legacy dataspace saturation operation. The last row must be
* [0.0, 0.0, 0.0, 1.0].
*/
getDataspaceSaturationMatrix(Dataspace dataspace)
generates (Error error,
float[4][4] matrix);
/**
* Executes commands from the input command message queue. Return values
* generated by the input commands are written to the output command
* message queue in the form of value commands.
*
* @param inLength is the length of input commands.
* @param inHandles is an array of handles referenced by the input
* commands.
* @return error is NONE upon success. Otherwise,
* BAD_PARAMETER when inLength is not equal to the length of
* commands in the input command message queue.
* NO_RESOURCES when the output command message queue was not
* properly drained.
* @param outQueueChanged indicates whether the output command message
* queue has changed.
* @param outLength is the length of output commands.
* @param outHandles is an array of handles referenced by the output
* commands.
*/
executeCommands_2_2(uint32_t inLength,
vec<handle> inHandles)
generates (Error error,
bool outQueueChanged,
uint32_t outLength,
vec<handle> outHandles);
};
|