summaryrefslogtreecommitdiffstats
blob: 62fb2baed56e5252b37566ee9f5dcbf8d8839285 (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

package android.hardware.neuralnetworks@1.0;

import IPreparedModelCallback;

/**
 * This interface represents a device driver.
 */
interface IDevice {
    /**
     * Gets the capabilities of a driver.
     *
     * @return status Error status of the call, must be:
     *                - NONE if successful
     *                - DEVICE_UNAVAILABLE if driver is offline or busy
     *                - GENERAL_FAILURE if there is an unspecified error
     * @return capabilities Capabilities of the driver.
     */
    getCapabilities() generates (ErrorStatus status, Capabilities capabilities);

    /**
     * Gets the supported operations in a model.
     *
     * getSupportedOperations indicates which operations of a model are fully
     * supported by the vendor driver. If an operation may not be supported for
     * any reason, getSupportedOperations must return false for that operation.
     *
     * @param model A model whose operations--and their corresponding
     *              operands--are to be verified by the driver.
     * @return status Error status of the call, must be:
     *                - NONE if successful
     *                - DEVICE_UNAVAILABLE if driver is offline or busy
     *                - GENERAL_FAILURE if there is an unspecified error
     *                - INVALID_ARGUMENT if provided model is invalid
     * @return supportedOperations A list of supported operations, where true
     *                             indicates the operation is supported and
     *                             false indicates the operation is not
     *                             supported. The index of "supported"
     *                             corresponds with the index of the operation
     *                             it is describing.
     */
    getSupportedOperations(Model model)
                generates (ErrorStatus status, vec<bool> supportedOperations);

    /**
     * Creates a prepared model for execution.
     *
     * prepareModel is used to make any necessary transformations or alternative
     * representations to a model for execution, possiblly including
     * transformations on the constant data, optimization on the model's graph,
     * or compilation into the device's native binary format. The model itself
     * is not changed.
     *
     * The model is prepared asynchronously with respect to the caller. The
     * prepareModel function must verify the inputs to the prepareModel function
     * are correct. If there is an error, prepareModel must immediately invoke
     * the callback with the appropriate ErrorStatus value and nullptr for the
     * IPreparedModel, then return with the same ErrorStatus. If the inputs to
     * the prepareModel function are valid and there is no error, prepareModel
     * must launch an asynchronous task to prepare the model in the background,
     * and immediately return from prepareModel with ErrorStatus::NONE. If the
     * asynchronous task fails to launch, prepareModel must immediately invoke
     * the callback with ErrorStatus::GENERAL_FAILURE and nullptr for the
     * IPreparedModel, then return with ErrorStatus::GENERAL_FAILURE.
     *
     * When the asynchronous task has finished preparing the model, it must
     * immediately invoke the callback function provided as an input to
     * prepareModel. If the model was prepared successfully, the callback object
     * must be invoked with an error status of ErrorStatus::NONE and the
     * produced IPreparedModel object. If an error occurred preparing the model,
     * the callback object must be invoked with the appropriate ErrorStatus
     * value and nullptr for the IPreparedModel.
     *
     * The only information that may be unknown to the model at this stage is
     * the shape of the tensors, which may only be known at execution time. As
     * such, some driver services may return partially prepared models, where
     * the prepared model can only be finished when it is paired with a set of
     * inputs to the model. Note that the same prepared model object can be
     * used with different shapes of inputs on different (possibly concurrent)
     * executions.
     *
     * Multiple threads can call prepareModel on the same model concurrently.
     *
     * @param model The model to be prepared for execution.
     * @param callback A callback object used to return the error status of
     *                 preparing the model for execution and the prepared model
     *                 if successful, nullptr otherwise. The callback object's
     *                 notify function must be called exactly once, even if the
     *                 model could not be prepared.
     * @return status Error status of launching a task which prepares the model
     *                in the background; must be:
     *                - NONE if preparation task is successfully launched
     *                - DEVICE_UNAVAILABLE if driver is offline or busy
     *                - GENERAL_FAILURE if there is an unspecified error
     *                - INVALID_ARGUMENT if one of the input arguments is
     *                  invalid
     */
    prepareModel(Model model, IPreparedModelCallback callback)
      generates (ErrorStatus status);

    /**
     * Returns the current status of a driver.
     *
     * @return status Status of the driver, one of:
     *                - DeviceStatus::AVAILABLE
     *                - DeviceStatus::BUSY
     *                - DeviceStatus::OFFLINE
     *                - DeviceStatus::UNKNOWN
     */
    getStatus() generates (DeviceStatus status);
};