diff options
Diffstat (limited to 'CleanSpec.mk')
-rw-r--r-- | CleanSpec.mk | 55 |
1 files changed, 55 insertions, 0 deletions
diff --git a/CleanSpec.mk b/CleanSpec.mk new file mode 100644 index 00000000..cf17fee6 --- /dev/null +++ b/CleanSpec.mk | |||
@@ -0,0 +1,55 @@ | |||
1 | # Copyright (C) 2016 The Android Open-Source Project | ||
2 | # | ||
3 | # Licensed under the Apache License, Version 2.0 (the "License"); | ||
4 | # you may not use this file except in compliance with the License. | ||
5 | # You may obtain a copy of the License at | ||
6 | # | ||
7 | # http://www.apache.org/licenses/LICENSE-2.0 | ||
8 | # | ||
9 | # Unless required by applicable law or agreed to in writing, software | ||
10 | # distributed under the License is distributed on an "AS IS" BASIS, | ||
11 | # WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | ||
12 | # See the License for the specific language governing permissions and | ||
13 | # limitations under the License. | ||
14 | # | ||
15 | |||
16 | # | ||
17 | # If you don't need to do a full clean build but would like to touch | ||
18 | # a file or delete some intermediate files, add a clean step to the end | ||
19 | # of the list. These steps will only be run once, if they haven't been | ||
20 | # run before. | ||
21 | # | ||
22 | # E.g.: | ||
23 | # $(call add-clean-step, touch -c external/sqlite/sqlite3.h) | ||
24 | # $(call add-clean-step, rm -rf $(PRODUCT_OUT)/obj/STATIC_LIBRARIES/libz_intermediates) | ||
25 | # | ||
26 | # Always use "touch -c" and "rm -f" or "rm -rf" to gracefully deal with | ||
27 | # files that are missing or have been moved. | ||
28 | # | ||
29 | # Use $(PRODUCT_OUT) to get to the "out/target/product/blah/" directory. | ||
30 | # Use $(OUT_DIR) to refer to the "out" directory. | ||
31 | # | ||
32 | # If you need to re-do something that's already mentioned, just copy | ||
33 | # the command and add it to the bottom of the list. E.g., if a change | ||
34 | # that you made last week required touching a file and a change you | ||
35 | # made today requires touching the same file, just copy the old | ||
36 | # touch step and add it to the end of the list. | ||
37 | # | ||
38 | # ************************************************ | ||
39 | # NEWER CLEAN STEPS MUST BE AT THE END OF THE LIST | ||
40 | # ************************************************ | ||
41 | |||
42 | # For example: | ||
43 | #$(call add-clean-step, rm -rf $(OUT_DIR)/target/common/obj/APPS/AndroidTests_intermediates) | ||
44 | #$(call add-clean-step, rm -rf $(OUT_DIR)/target/common/obj/JAVA_LIBRARIES/core_intermediates) | ||
45 | #$(call add-clean-step, find $(OUT_DIR) -type f -name "IGTalkSession*" -print0 | xargs -0 rm -f) | ||
46 | #$(call add-clean-step, rm -rf $(PRODUCT_OUT)/data/*) | ||
47 | |||
48 | $(call add-clean-step, rm -rf $(OUT_DIR)/target/common/obj/JAVA_LIBRARIES/android.car*) | ||
49 | $(call add-clean-step, rm -rf $(OUT_DIR)/target/common/obj/PACKAGING/android.car*) | ||
50 | $(call add-clean-step, rm -rf $(OUT_DIR)/target/common/obj/JAVA_LIBRARIES/android.support.car*) | ||
51 | $(call add-clean-step, rm -rf $(OUT_DIR)/target/common/obj/PACKAGING/android.support.car*) | ||
52 | |||
53 | # ************************************************ | ||
54 | # NEWER CLEAN STEPS MUST BE AT THE END OF THE LIST | ||
55 | # ************************************************ | ||