summaryrefslogtreecommitdiffstats
Commit message (Expand)AuthorAgeFilesLines
* Create fake CarPropertyValue for an error eventKai2019-06-063-9/+39
* Fix operators priority to prevent NullPointerExceptionOleh Cherpak2019-02-151-1/+1
* DO NOT MERGE - Merge pie-platform-release (PPRL.181205.001) into masterXin Li2018-12-112-13/+7
|\
| * Merge "Cache CarPropertyConfigs in CarPropertyService" into pi-devTreeHugger Robot2018-07-301-8/+7
| |\
| | * Cache CarPropertyConfigs in CarPropertyServiceKai2018-07-201-8/+7
| * | Merge "Remove ADJUST_CAR_CABIN permission" into pi-devTreeHugger Robot2018-07-231-5/+0
| |\ \
| | * | Remove ADJUST_CAR_CABIN permissionKai2018-07-231-5/+0
| | |/
* | | Convert sysui to bpJason Monk2018-09-051-2/+2
* | | Merge "Provide an option to disable UxR change broadcast." into pi-devRam Periathiruvadi2018-07-192-1/+64
|\| |
| * | Merge "Provide an option to disable UxR change broadcast." into pi-devpie-dr1-devTreeHugger Robot2018-07-192-1/+64
| |\ \
| | * | Provide an option to disable UxR change broadcast.Ram Periathiruvadi2018-07-192-1/+64
* | | | Merge "Change default name of first admin user in headless model." into pi-devYing Zheng2018-07-131-1/+1
|\| | |
| * | | Merge "Change default name of first admin user in headless model." into pi-devTreeHugger Robot2018-07-131-1/+1
| |\ \ \
| | * | | Change default name of first admin user in headless model.Ying Zheng2018-07-111-1/+1
| | | |/ | | |/|
* | | | Merge "Fix CarPackageManager reading blacklisted packages." into pi-devRam Periathiruvadi2018-07-111-3/+11
|\| | |
| * | | Merge "Fix CarPackageManager reading blacklisted packages." into pi-devRam Periathiruvadi2018-07-111-3/+11
| |\ \ \ | | |_|/ | |/| |
| | * | Fix CarPackageManager reading blacklisted packages.Ram Periathiruvadi2018-07-111-3/+11
| | |/
* | | Update default fallback idling state UX restrictions.Ram Periathiruvadi2018-07-112-1/+5
|\| |
| * | Update default fallback idling state UX restrictions.Ram Periathiruvadi2018-07-112-1/+5
| |/
* | Merge "Send global type property event in register" into pi-devKai Wang2018-07-101-3/+13
|\|
| * Merge "Send global type property event in register" into pi-devKai Wang2018-07-101-3/+13
| |\
| | * Send global type property event in registerKai2018-07-021-3/+13
* | | Merge "Init DayNightMode after booting" into pi-devKai Wang2018-07-101-13/+26
|\| |
| * | Merge "Init DayNightMode after booting" into pi-devKai Wang2018-07-101-13/+26
| |\ \
| | * | Init DayNightMode after bootingKai2018-06-251-13/+26
* | | | Merge "Adding car specific default guest restrictions." into pi-devJovana Knezevic2018-06-301-0/+1
|\| | |
| * | | Merge "Adding car specific default guest restrictions." into pi-devJovana Knezevic2018-06-301-0/+1
| |\ \ \
| | * | | Adding car specific default guest restrictions.jovanak2018-06-301-0/+1
| | | |/ | | |/|
* | | | Merge "Invoke Assistant via VoiceInteractionSession." into pi-devNicholas Sauer2018-06-281-7/+35
|\| | |
| * | | Invoke Assistant via VoiceInteractionSession.Nicholas Sauer2018-06-281-7/+35
| |/ /
* | | Disable location for headless system user.Ying Zheng2018-06-261-3/+14
|\| |
| * | Disable location for headless system user.Ying Zheng2018-06-261-3/+14
* | | Merge "Update last active user." into pi-devYing Zheng2018-06-251-7/+8
|\| |
| * | Merge "Update last active user." into pi-devYing Zheng2018-06-251-7/+8
| |\ \
| | * | Update last active user.Ying Zheng2018-06-251-7/+8
* | | | Fix bug in CarPropertyUtils.toCarPropertyValue which returns an Integer when ...Xin Wei Chow2018-06-221-9/+25
|\| | |
| * | | Fix bug in CarPropertyUtils.toCarPropertyValue which returns an Integer when ...Xin Wei Chow2018-06-221-9/+25
| |/ /
* | | Merge "Update set last active user to exclude ephemeral users." into pi-devYing Zheng2018-06-211-2/+1
|\| |
| * | Merge "Update set last active user to exclude ephemeral users." into pi-devYing Zheng2018-06-211-2/+1
| |\ \
| | * | Update set last active user to exclude ephemeral users.Ying Zheng2018-06-211-2/+1
* | | | resolve merge conflicts of de7be61a2dfb41c54550a4edcde65721f38d5422 to pi-dev...Steve Paik2018-06-212-29/+21
|\| | |
| * | | Merge "Fix display brightness scaling" into pi-devSteve Paik2018-06-212-29/+21
| |\ \ \ | | |/ / | |/| |
| | * | Fix display brightness scalingSteve Paik2018-06-212-29/+21
| | |/
* | | Complete the logic around last active user, including:Ying Zheng2018-06-201-2/+14
|\| |
| * | Complete the logic around last active user, including:Ying Zheng2018-06-201-2/+14
| |/
* | Merge "Update the CarLocationService to work when the system user is headless...Gregory Clark2018-06-202-67/+127
|\|
| * Merge "Update the CarLocationService to work when the system user is headless...Gregory Clark2018-06-202-67/+127
| |\
| | * Update the CarLocationService to work when the system user is headless.Gregory Clark2018-06-192-67/+127
* | | Merge "Ensure the initial volume when creating audio patch" into pi-devHongwei Wang2018-06-191-0/+5
|\| |
| * | Merge "Ensure the initial volume when creating audio patch" into pi-devHongwei Wang2018-06-191-0/+5
| |\ \ | | |/ | |/|