summaryrefslogtreecommitdiffstats
path: root/tests
Commit message (Expand)AuthorAgeFilesLines
* Remove references to non-existant directoriesDan Willemsen2019-05-281-1/+0
* Merge "Schematize Car system properties"Treehugger Robot2018-12-131-6/+7
|\
| * Schematize Car system propertiesInseob Kim2018-12-071-6/+7
* | DO NOT MERGE - Merge pie-platform-release (PPRL.181205.001) into masterXin Li2018-12-1112-2/+926
|\ \
| * | Adds CarTrustAgentClientApp as test app for trust agentandroid-9.0.0_r47android-9.0.0_r46android-9.0.0_r45android-9.0.0_r44android-9.0.0_r43android-9.0.0_r42android-9.0.0_r41android-9.0.0_r40android-9.0.0_r37android-9.0.0_r36pie-qpr3-s1-releasepie-qpr3-releasepie-qpr3-b-releasepie-b4s4-devHongwei Wang2018-08-0910-0/+921
| * | Fixed package name in mocked car serviceChao Yan2018-07-241-1/+1
| * | Remove ADJUST_CAR_CABIN permissionKai2018-07-231-1/+4
* | | Add cleanup upon disconnect of CarServicerleix2018-11-281-0/+8
| |/ |/|
* | Use public APIs not internal APIspie-tempNeil Fuller2018-10-101-6/+5
|\ \
| * | Use public APIs not internal APIsandroid-o-mr1-iot-release-smart-display-r3oreo-mr1-1.2-iot-releaseNeil Fuller2018-10-101-6/+5
* | | Migrate to androidx namespace for support library.Anthony Chen2018-08-2925-34/+56
| |/ |/|
* | Merge "Add connectivity test fragment to KitchenSink" into pi-devTreeHugger Robot2018-07-095-0/+235
|\ \
| * | Add connectivity test fragment to KitchenSinkPavel Maltsev2018-06-295-0/+235
* | | Merge "Adding car specific default guest restrictions." into pi-devJovana Knezevic2018-06-302-40/+55
|\ \ \
| * | | Adding car specific default guest restrictions.jovanak2018-06-302-40/+55
| |/ /
* | | Merge "Fix setting night mode and change test crashes EKS" into pi-devKai Wang2018-06-295-107/+165
|\ \ \
| * | | Fix setting night mode and change test crashes EKSKai2018-06-295-107/+165
* | | | Fixing a bug in maximum users allowed logic on the device.jovanak2018-06-291-0/+19
| |/ / |/| |
* | | Adding methods for keeping track of user limits on the device.jovanak2018-06-282-41/+117
|/ /
* | Disable location for headless system user.Ying Zheng2018-06-261-10/+57
* | Merge "Enables registering/unregistering multiple update listeners." into pi-devJovana Knezevic2018-06-251-5/+104
|\ \
| * | Enables registering/unregistering multiple update listeners.jovanak2018-06-251-5/+104
* | | Update last active user.Ying Zheng2018-06-251-3/+3
|/ /
* | Merge "Update set last active user to exclude ephemeral users." into pi-devYing Zheng2018-06-212-7/+36
|\ \
| * | Update set last active user to exclude ephemeral users.Ying Zheng2018-06-212-7/+36
* | | Return mocked AudioManager in car unit testsHongwei Wang2018-06-211-0/+2
|/ /
* | Complete the logic around last active user, including:Ying Zheng2018-06-202-98/+215
* | Removes the test that fails when running it in user 0.jovanak2018-06-201-4/+0
* | Update the CarLocationService to work when the system user is headless.Gregory Clark2018-06-191-6/+46
* | Merge "Adjusting restrictions applied to non-admins." into pi-devJovana Knezevic2018-06-191-13/+37
|\ \
| * | Adjusting restrictions applied to non-admins.jovanak2018-06-181-13/+37
* | | Merge "Fix CarUserManagerHelperTest." into pi-devYing Zheng2018-06-151-1/+1
|\ \ \
| * | | Fix CarUserManagerHelperTest.Ying Zheng2018-06-151-1/+1
* | | | Merge "Only admins or system user car create other admins." into pi-devJovana Knezevic2018-06-151-0/+41
|\ \ \ \ | |/ / / |/| | |
| * | | Only admins or system user car create other admins.jovanak2018-06-151-0/+41
| |/ /
* | | [Garage Mode: Refactoring] Scoped out GarageModePolicy into separateSerik Beketayev2018-06-141-74/+69
* | | Merge "Disable add accounts for user 0." into pi-devYing Zheng2018-06-142-1/+22
|\ \ \
| * | | Disable add accounts for user 0.Ying Zheng2018-06-142-1/+22
* | | | Merge "Clean up for ENV_OUTSIDE_TEMPERATURE" into pi-devKai Wang2018-06-142-7/+11
|\ \ \ \ | |/ / / |/| | |
| * | | Clean up for ENV_OUTSIDE_TEMPERATUREKai2018-06-132-7/+11
| |/ /
* / / Fixing tests in CarUserManagerHelperTest.jovanak2018-06-131-34/+12
|/ /
* | Merge "Adding default user restrictions for non-admin users." into pi-devTreeHugger Robot2018-06-121-0/+45
|\ \
| * | Adding default user restrictions for non-admin users.jovanak2018-06-121-0/+45
* | | Merge "Adding API for assigning admin privileges to CarUserManagerHelper." in...Jovana Knezevic2018-06-121-0/+26
|\| |
| * | Adding API for assigning admin privileges to CarUserManagerHelper.jovanak2018-06-111-0/+26
* | | Merge "Fixing failing tests in CarUserManagerHelperTest." into pi-devJovana Knezevic2018-06-111-61/+41
|\| | | |/ |/|
| * Fixing failing tests in CarUserManagerHelperTest.jovanak2018-06-081-61/+41
* | Merge "Fix Sensor test fragment" into pi-devTreeHugger Robot2018-06-072-160/+40
|\ \
| * | Fix Sensor test fragmentSteve Paik2018-06-072-160/+40
| |/
* | Merge "Add a mic button to use Activity#showAssist." into pi-devTreeHugger Robot2018-06-062-5/+21
|\ \