summaryrefslogtreecommitdiffstats
path: root/tests
Commit message (Expand)AuthorAgeFilesLines
* Adds CarTrustAgentClientApp as test app for trust agentandroid-9.0.0_r47android-9.0.0_r46android-9.0.0_r45android-9.0.0_r44android-9.0.0_r43android-9.0.0_r42android-9.0.0_r41android-9.0.0_r40android-9.0.0_r37android-9.0.0_r36pie-qpr3-s1-releasepie-qpr3-releasepie-qpr3-b-releasepie-b4s4-devHongwei Wang2018-08-0910-0/+921
* Fixed package name in mocked car serviceChao Yan2018-07-241-1/+1
* Remove ADJUST_CAR_CABIN permissionKai2018-07-231-1/+4
* Merge "Add connectivity test fragment to KitchenSink" into pi-devTreeHugger Robot2018-07-095-0/+235
|\
| * Add connectivity test fragment to KitchenSinkPavel Maltsev2018-06-295-0/+235
* | Merge "Adding car specific default guest restrictions." into pi-devJovana Knezevic2018-06-302-40/+55
|\ \
| * | Adding car specific default guest restrictions.jovanak2018-06-302-40/+55
| |/
* | Merge "Fix setting night mode and change test crashes EKS" into pi-devKai Wang2018-06-295-107/+165
|\ \
| * | Fix setting night mode and change test crashes EKSKai2018-06-295-107/+165
* | | Fixing a bug in maximum users allowed logic on the device.jovanak2018-06-291-0/+19
| |/ |/|
* | Adding methods for keeping track of user limits on the device.jovanak2018-06-282-41/+117
|/
* Disable location for headless system user.Ying Zheng2018-06-261-10/+57
* Merge "Enables registering/unregistering multiple update listeners." into pi-devJovana Knezevic2018-06-251-5/+104
|\
| * Enables registering/unregistering multiple update listeners.jovanak2018-06-251-5/+104
* | Update last active user.Ying Zheng2018-06-251-3/+3
|/
* Merge "Update set last active user to exclude ephemeral users." into pi-devYing Zheng2018-06-212-7/+36
|\
| * Update set last active user to exclude ephemeral users.Ying Zheng2018-06-212-7/+36
* | Return mocked AudioManager in car unit testsHongwei Wang2018-06-211-0/+2
|/
* Complete the logic around last active user, including:Ying Zheng2018-06-202-98/+215
* Removes the test that fails when running it in user 0.jovanak2018-06-201-4/+0
* Update the CarLocationService to work when the system user is headless.Gregory Clark2018-06-191-6/+46
* Merge "Adjusting restrictions applied to non-admins." into pi-devJovana Knezevic2018-06-191-13/+37
|\
| * Adjusting restrictions applied to non-admins.jovanak2018-06-181-13/+37
* | Merge "Fix CarUserManagerHelperTest." into pi-devYing Zheng2018-06-151-1/+1
|\ \
| * | Fix CarUserManagerHelperTest.Ying Zheng2018-06-151-1/+1
* | | Merge "Only admins or system user car create other admins." into pi-devJovana Knezevic2018-06-151-0/+41
|\ \ \ | |/ / |/| |
| * | Only admins or system user car create other admins.jovanak2018-06-151-0/+41
| |/
* | [Garage Mode: Refactoring] Scoped out GarageModePolicy into separateSerik Beketayev2018-06-141-74/+69
* | Merge "Disable add accounts for user 0." into pi-devYing Zheng2018-06-142-1/+22
|\ \
| * | Disable add accounts for user 0.Ying Zheng2018-06-142-1/+22
* | | Merge "Clean up for ENV_OUTSIDE_TEMPERATURE" into pi-devKai Wang2018-06-142-7/+11
|\ \ \ | |/ / |/| |
| * | Clean up for ENV_OUTSIDE_TEMPERATUREKai2018-06-132-7/+11
| |/
* / Fixing tests in CarUserManagerHelperTest.jovanak2018-06-131-34/+12
|/
* Merge "Adding default user restrictions for non-admin users." into pi-devTreeHugger Robot2018-06-121-0/+45
|\
| * Adding default user restrictions for non-admin users.jovanak2018-06-121-0/+45
* | Merge "Adding API for assigning admin privileges to CarUserManagerHelper." in...Jovana Knezevic2018-06-121-0/+26
|\|
| * Adding API for assigning admin privileges to CarUserManagerHelper.jovanak2018-06-111-0/+26
* | Merge "Fixing failing tests in CarUserManagerHelperTest." into pi-devJovana Knezevic2018-06-111-61/+41
|\|
| * Fixing failing tests in CarUserManagerHelperTest.jovanak2018-06-081-61/+41
* | Merge "Fix Sensor test fragment" into pi-devTreeHugger Robot2018-06-072-160/+40
|\ \
| * | Fix Sensor test fragmentSteve Paik2018-06-072-160/+40
| |/
* | Merge "Add a mic button to use Activity#showAssist." into pi-devTreeHugger Robot2018-06-062-5/+21
|\ \
| * | Add a mic button to use Activity#showAssist.Nicholas Sauer2018-06-062-5/+21
| |/
* / Fix driving state for manual transmission.Ram Periathiruvadi2018-06-061-6/+89
|/
* Merge "Rename VEHICLE_AREA_TYPE_NONE --> VEHICLE_AREA_TYPE_GLOBAL" into pi-devTreeHugger Robot2018-06-055-21/+23
|\
| * Rename VEHICLE_AREA_TYPE_NONE --> VEHICLE_AREA_TYPE_GLOBALSteve Paik2018-06-045-21/+23
* | Update Car UxR Manager API name.Ram Periathiruvadi2018-06-042-2/+2
|/
* Create CarPropertyService and CarPropertyManagerSteve Paik2018-06-0115-77/+685
* DO NOT MERGE - Create a car user service. Protected by flag.Ying Zheng2018-06-013-2/+126
* Merge "Add a flag to protect headless user 0 multi-user model." into pi-devYing Zheng2018-05-312-10/+40
|\