/*
* Copyright (C) 2005-2016 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef _LIBS_LOG_EVENT_LIST_H
#define _LIBS_LOG_EVENT_LIST_H
#include <stdint.h>
#if (defined(__cplusplus) && defined(_USING_LIBCXX))
extern "C++" {
#include <string>
}
#endif
#include <log/log.h>
#ifdef __cplusplus
extern "C" {
#endif
#ifndef __ANDROID_USE_LIBLOG_EVENT_INTERFACE
#ifndef __ANDROID_API__
#define __ANDROID_USE_LIBLOG_EVENT_INTERFACE 1
#elif __ANDROID_API__ > 23 /* > Marshmallow */
#define __ANDROID_USE_LIBLOG_EVENT_INTERFACE 1
#else
#define __ANDROID_USE_LIBLOG_EVENT_INTERFACE 0
#endif
#endif
#if __ANDROID_USE_LIBLOG_EVENT_INTERFACE
/* For manipulating lists of events. */
#define ANDROID_MAX_LIST_NEST_DEPTH 8
/*
* The opaque context used to manipulate lists of events.
*/
#ifndef __android_log_context_defined
#define __android_log_context_defined
typedef struct android_log_context_internal* android_log_context;
#endif
/*
* Elements returned when reading a list of events.
*/
#ifndef __android_log_list_element_defined
#define __android_log_list_element_defined
typedef struct {
AndroidEventLogType type;
uint16_t complete;
uint16_t len;
union {
int32_t int32;
int64_t int64;
char* string;
float float32;
} data;
} android_log_list_element;
#endif
/*
* Creates a context associated with an event tag to write elements to
* the list of events.
*/
android_log_context create_android_logger(uint32_t tag);
/* All lists must be braced by a begin and end call */
/*
* NB: If the first level braces are missing when specifying multiple
* elements, we will manufacturer a list to embrace it for your API
* convenience. For a single element, it will remain solitary.
*/
int android_log_write_list_begin(android_log_context ctx);
int android_log_write_list_end(android_log_context ctx);
int android_log_write_int32(android_log_context ctx, int32_t value);
int android_log_write_int64(android_log_context ctx, int64_t value);
int android_log_write_string8(android_log_context ctx, const char* value);
int android_log_write_string8_len(android_log_context ctx,
const char* value, size_t maxlen);
int android_log_write_float32(android_log_context ctx, float value);
/* Submit the composed list context to the specified logger id */
/* NB: LOG_ID_EVENTS and LOG_ID_SECURITY only valid binary buffers */
int android_log_write_list(android_log_context ctx, log_id_t id);
/*
* Creates a context from a raw buffer representing a list of events to be read.
*/
android_log_context create_android_log_parser(const char* msg, size_t len);
android_log_list_element android_log_read_next(android_log_context ctx);
android_log_list_element android_log_peek_next(android_log_context ctx);
/* Finished with reader or writer context */
int android_log_destroy(android_log_context* ctx);
#ifdef __cplusplus
#ifndef __class_android_log_event_list_defined
#define __class_android_log_event_list_defined
/* android_log_list C++ helpers */
extern "C++" {
class android_log_event_list {
friend class __android_log_event_list;
private:
android_log_context ctx;
int ret;
android_log_event_list(const android_log_event_list&) = delete;
void operator =(const android_log_event_list&) = delete;
public:
explicit android_log_event_list(int tag) : ret(0) {
ctx = create_android_logger(static_cast<uint32_t>(tag));
}
explicit android_log_event_list(log_msg& log_msg) : ret(0) {
ctx = create_android_log_parser(log_msg.msg() + sizeof(uint32_t),
log_msg.entry.len - sizeof(uint32_t));
}
~android_log_event_list() { android_log_destroy(&ctx); }
int close() {
int retval = android_log_destroy(&ctx);
if (retval < 0) ret = retval;
return retval;
}
/* To allow above C calls to use this class as parameter */
operator android_log_context() const { return ctx; }
int status() const { return ret; }
int begin() {
int retval = android_log_write_list_begin(ctx);
if (retval < 0) ret = retval;
return ret;
}
int end() {
int retval = android_log_write_list_end(ctx);
if (retval < 0) ret = retval;
return ret;
}
android_log_event_list& operator <<(int32_t value) {
int retval = android_log_write_int32(ctx, value);
if (retval < 0) ret = retval;
return *this;
}
android_log_event_list& operator <<(uint32_t value) {
int retval = android_log_write_int32(ctx, static_cast<int32_t>(value));
if (retval < 0) ret = retval;
return *this;
}
android_log_event_list& operator <<(int64_t value) {
int retval = android_log_write_int64(ctx, value);
if (retval < 0) ret = retval;
return *this;
}
android_log_event_list& operator <<(uint64_t value) {
int retval = android_log_write_int64(ctx, static_cast<int64_t>(value));
if (retval < 0) ret = retval;
return *this;
}
android_log_event_list& operator <<(const char* value) {
int retval = android_log_write_string8(ctx, value);
if (retval < 0) ret = retval;
return *this;
}
#if defined(_USING_LIBCXX)
android_log_event_list& operator <<(const std::string& value) {
int retval = android_log_write_string8_len(ctx,
value.data(),
value.length());
if (retval < 0) ret = retval;
return *this;
}
#endif
android_log_event_list& operator <<(float value) {
int retval = android_log_write_float32(ctx, value);
if (retval < 0) ret = retval;
return *this;
}
int write(log_id_t id = LOG_ID_EVENTS) {
int retval = android_log_write_list(ctx, id);
if (retval < 0) ret = retval;
return ret;
}
int operator <<(log_id_t id) {
int retval = android_log_write_list(ctx, id);
if (retval < 0) ret = retval;
android_log_destroy(&ctx);
return ret;
}
/*
* Append<Type> methods removes any integer promotion
* confusion, and adds access to string with length.
* Append methods are also added for all types for
* convenience.
*/
bool AppendInt(int32_t value) {
int retval = android_log_write_int32(ctx, value);
if (retval < 0) ret = retval;
return ret >= 0;
}
bool AppendLong(int64_t value) {
int retval = android_log_write_int64(ctx, value);
if (retval < 0) ret = retval;
return ret >= 0;
}
bool AppendString(const char* value) {
int retval = android_log_write_string8(ctx, value);
if (retval < 0) ret = retval;
return ret >= 0;
}
bool AppendString(const char* value, size_t len) {
int retval = android_log_write_string8_len(ctx, value, len);
if (retval < 0) ret = retval;
return ret >= 0;
}
#if defined(_USING_LIBCXX)
bool AppendString(const std::string& value) {
int retval = android_log_write_string8_len(ctx,
value.data(),
value.length());
if (retval < 0) ret = retval;
return ret;
}
bool Append(const std::string& value) {
int retval = android_log_write_string8_len(ctx,
value.data(),
value.length());
if (retval < 0) ret = retval;
return ret;
}
#endif
bool AppendFloat(float value) {
int retval = android_log_write_float32(ctx, value);
if (retval < 0) ret = retval;
return ret >= 0;
}
template <typename Tvalue>
bool Append(Tvalue value) { *this << value; return ret >= 0; }
bool Append(const char* value, size_t len) {
int retval = android_log_write_string8_len(ctx, value, len);
if (retval < 0) ret = retval;
return ret >= 0;
}
android_log_list_element read() { return android_log_read_next(ctx); }
android_log_list_element peek() { return android_log_peek_next(ctx); }
};
}
#endif
#endif
#endif /* __ANDROID_USE_LIBLOG_EVENT_INTERFACE */
#ifdef __cplusplus
}
#endif
#endif /* _LIBS_LOG_EVENT_LIST_H */