// Copyright (C) 2016 The Android Open Source Project
//
// Licensed under the Apache License, Version 2.0 (the "License");
// you may not use this file except in compliance with the License.
// You may obtain a copy of the License at
//
// http://www.apache.org/licenses/LICENSE-2.0
//
// Unless required by applicable law or agreed to in writing, software
// distributed under the License is distributed on an "AS IS" BASIS,
// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
// See the License for the specific language governing permissions and
// limitations under the License.
#include "capabilities.h"
#include <sys/capability.h>
#include <sys/prctl.h>
#include <map>
#include <memory>
#include <android-base/logging.h>
#include <android-base/macros.h>
#define CAP_MAP_ENTRY(cap) { #cap, CAP_##cap }
namespace android {
namespace init {
static const std::map<std::string, int> cap_map = {
CAP_MAP_ENTRY(CHOWN),
CAP_MAP_ENTRY(DAC_OVERRIDE),
CAP_MAP_ENTRY(DAC_READ_SEARCH),
CAP_MAP_ENTRY(FOWNER),
CAP_MAP_ENTRY(FSETID),
CAP_MAP_ENTRY(KILL),
CAP_MAP_ENTRY(SETGID),
CAP_MAP_ENTRY(SETUID),
CAP_MAP_ENTRY(SETPCAP),
CAP_MAP_ENTRY(LINUX_IMMUTABLE),
CAP_MAP_ENTRY(NET_BIND_SERVICE),
CAP_MAP_ENTRY(NET_BROADCAST),
CAP_MAP_ENTRY(NET_ADMIN),
CAP_MAP_ENTRY(NET_RAW),
CAP_MAP_ENTRY(IPC_LOCK),
CAP_MAP_ENTRY(IPC_OWNER),
CAP_MAP_ENTRY(SYS_MODULE),
CAP_MAP_ENTRY(SYS_RAWIO),
CAP_MAP_ENTRY(SYS_CHROOT),
CAP_MAP_ENTRY(SYS_PTRACE),
CAP_MAP_ENTRY(SYS_PACCT),
CAP_MAP_ENTRY(SYS_ADMIN),
CAP_MAP_ENTRY(SYS_BOOT),
CAP_MAP_ENTRY(SYS_NICE),
CAP_MAP_ENTRY(SYS_RESOURCE),
CAP_MAP_ENTRY(SYS_TIME),
CAP_MAP_ENTRY(SYS_TTY_CONFIG),
CAP_MAP_ENTRY(MKNOD),
CAP_MAP_ENTRY(LEASE),
CAP_MAP_ENTRY(AUDIT_WRITE),
CAP_MAP_ENTRY(AUDIT_CONTROL),
CAP_MAP_ENTRY(SETFCAP),
CAP_MAP_ENTRY(MAC_OVERRIDE),
CAP_MAP_ENTRY(MAC_ADMIN),
CAP_MAP_ENTRY(SYSLOG),
CAP_MAP_ENTRY(WAKE_ALARM),
CAP_MAP_ENTRY(BLOCK_SUSPEND),
CAP_MAP_ENTRY(AUDIT_READ),
};
static_assert(CAP_LAST_CAP == CAP_AUDIT_READ, "CAP_LAST_CAP is not CAP_AUDIT_READ");
static bool ComputeCapAmbientSupported() {
return prctl(PR_CAP_AMBIENT, PR_CAP_AMBIENT_IS_SET, CAP_CHOWN, 0, 0) >= 0;
}
static unsigned int ComputeLastValidCap() {
// Android does not support kernels < 3.8. 'CAP_WAKE_ALARM' has been present since 3.0, see
// http://lxr.free-electrons.com/source/include/linux/capability.h?v=3.0#L360.
unsigned int last_valid_cap = CAP_WAKE_ALARM;
for (; prctl(PR_CAPBSET_READ, last_valid_cap, 0, 0, 0) >= 0; ++last_valid_cap);
// |last_valid_cap| will be the first failing value.
return last_valid_cap - 1;
}
static bool DropBoundingSet(const CapSet& to_keep) {
unsigned int last_valid_cap = GetLastValidCap();
// When dropping the bounding set, attempt to drop capabilities reported at
// run-time, not at compile-time.
// If the run-time kernel is older than the compile-time headers, this
// avoids dropping an invalid capability. If the run-time kernel is newer
// than the headers, this guarantees all capabilities (even those unknown at
// compile time) will be dropped.
for (size_t cap = 0; cap <= last_valid_cap; ++cap) {
if (cap < to_keep.size() && to_keep.test(cap)) {
// No need to drop this capability.
continue;
}
if (cap_drop_bound(cap) == -1) {
PLOG(ERROR) << "cap_drop_bound(" << cap << ") failed";
return false;
}
}
return true;
}
static bool SetProcCaps(const CapSet& to_keep, bool add_setpcap) {
ScopedCaps caps(cap_init());
cap_clear(caps.get());
cap_value_t value[1];
for (size_t cap = 0; cap < to_keep.size(); ++cap) {
if (to_keep.test(cap)) {
value[0] = cap;
if (cap_set_flag(caps.get(), CAP_INHERITABLE, arraysize(value), value, CAP_SET) != 0 ||
cap_set_flag(caps.get(), CAP_PERMITTED, arraysize(value), value, CAP_SET) != 0) {
PLOG(ERROR) << "cap_set_flag(INHERITABLE|PERMITTED, " << cap << ") failed";
return false;
}
}
}
if (add_setpcap) {
value[0] = CAP_SETPCAP;
if (cap_set_flag(caps.get(), CAP_PERMITTED, arraysize(value), value, CAP_SET) != 0 ||
cap_set_flag(caps.get(), CAP_EFFECTIVE, arraysize(value), value, CAP_SET) != 0) {
PLOG(ERROR) << "cap_set_flag(PERMITTED|EFFECTIVE, " << CAP_SETPCAP << ") failed";
return false;
}
}
if (cap_set_proc(caps.get()) != 0) {
PLOG(ERROR) << "cap_set_proc(" << to_keep.to_ulong() << ") failed";
return false;
}
return true;
}
static bool SetAmbientCaps(const CapSet& to_raise) {
for (size_t cap = 0; cap < to_raise.size(); ++cap) {
if (to_raise.test(cap)) {
if (prctl(PR_CAP_AMBIENT, PR_CAP_AMBIENT_RAISE, cap, 0, 0) != 0) {
PLOG(ERROR) << "prctl(PR_CAP_AMBIENT, PR_CAP_AMBIENT_RAISE, " << cap << ") failed";
return false;
}
}
}
return true;
}
int LookupCap(const std::string& cap_name) {
auto e = cap_map.find(cap_name);
if (e != cap_map.end()) {
return e->second;
} else {
return -1;
}
}
bool CapAmbientSupported() {
static bool cap_ambient_supported = ComputeCapAmbientSupported();
return cap_ambient_supported;
}
unsigned int GetLastValidCap() {
static unsigned int last_valid_cap = ComputeLastValidCap();
return last_valid_cap;
}
bool SetCapsForExec(const CapSet& to_keep) {
// Need to keep SETPCAP to drop bounding set below.
bool add_setpcap = true;
if (!SetProcCaps(to_keep, add_setpcap)) {
LOG(ERROR) << "failed to apply initial capset";
return false;
}
if (!DropBoundingSet(to_keep)) {
return false;
}
// If SETPCAP wasn't specifically requested, drop it now.
add_setpcap = false;
if (!SetProcCaps(to_keep, add_setpcap)) {
LOG(ERROR) << "failed to apply final capset";
return false;
}
// Add the capabilities to the ambient set so that they are preserved across
// execve(2).
// See http://man7.org/linux/man-pages/man7/capabilities.7.html.
return SetAmbientCaps(to_keep);
}
bool DropInheritableCaps() {
ScopedCaps caps(cap_get_proc());
if (cap_clear_flag(caps.get(), CAP_INHERITABLE) == -1) {
PLOG(ERROR) << "cap_clear_flag(INHERITABLE) failed";
return false;
}
if (cap_set_proc(caps.get()) != 0) {
PLOG(ERROR) << "cap_set_proc() failed";
return false;
}
return true;
}
} // namespace init
} // namespace android