/*
* Copyright (C) 2017 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#include "init_first_stage.h"
#include <stdlib.h>
#include <unistd.h>
#include <chrono>
#include <memory>
#include <set>
#include <string>
#include <vector>
#include <android-base/chrono_utils.h>
#include <android-base/file.h>
#include <android-base/logging.h>
#include <android-base/strings.h>
#include <liblp/metadata_format.h>
#include "devices.h"
#include "fs_mgr.h"
#include "fs_mgr_avb.h"
#include "fs_mgr_dm_linear.h"
#include "uevent.h"
#include "uevent_listener.h"
#include "util.h"
using android::base::Timer;
using android::fs_mgr::LogicalPartitionTable;
namespace android {
namespace init {
// Class Declarations
// ------------------
class FirstStageMount {
public:
FirstStageMount();
virtual ~FirstStageMount() = default;
// The factory method to create either FirstStageMountVBootV1 or FirstStageMountVBootV2
// based on device tree configurations.
static std::unique_ptr<FirstStageMount> Create();
bool DoFirstStageMount(); // Mounts fstab entries read from device tree.
bool InitDevices();
protected:
ListenerAction HandleBlockDevice(const std::string& name, const Uevent&);
bool InitRequiredDevices();
bool InitMappedDevice(const std::string& verity_device);
bool CreateLogicalPartitions();
bool MountPartitions();
bool GetBackingDmLinearDevices();
virtual ListenerAction UeventCallback(const Uevent& uevent);
// Pure virtual functions.
virtual bool GetDmVerityDevices() = 0;
virtual bool SetUpDmVerity(fstab_rec* fstab_rec) = 0;
bool need_dm_verity_;
std::unique_ptr<fstab, decltype(&fs_mgr_free_fstab)> device_tree_fstab_;
std::unique_ptr<LogicalPartitionTable> dm_linear_table_;
std::string lp_metadata_partition_;
std::vector<fstab_rec*> mount_fstab_recs_;
std::set<std::string> required_devices_partition_names_;
std::unique_ptr<DeviceHandler> device_handler_;
UeventListener uevent_listener_;
};
class FirstStageMountVBootV1 : public FirstStageMount {
public:
FirstStageMountVBootV1() = default;
~FirstStageMountVBootV1() override = default;
protected:
bool GetDmVerityDevices() override;
bool SetUpDmVerity(fstab_rec* fstab_rec) override;
};
class FirstStageMountVBootV2 : public FirstStageMount {
public:
friend void SetInitAvbVersionInRecovery();
FirstStageMountVBootV2();
~FirstStageMountVBootV2() override = default;
protected:
ListenerAction UeventCallback(const Uevent& uevent) override;
bool GetDmVerityDevices() override;
bool SetUpDmVerity(fstab_rec* fstab_rec) override;
bool InitAvbHandle();
std::string device_tree_vbmeta_parts_;
FsManagerAvbUniquePtr avb_handle_;
ByNameSymlinkMap by_name_symlink_map_;
};
// Static Functions
// ----------------
static inline bool IsDtVbmetaCompatible() {
return is_android_dt_value_expected("vbmeta/compatible", "android,vbmeta");
}
static bool inline IsRecoveryMode() {
return access("/sbin/recovery", F_OK) == 0;
}
static inline bool IsDmLinearEnabled() {
static bool checked = false;
static bool enabled = false;
if (checked) {
return enabled;
}
import_kernel_cmdline(false, [](const std::string& key, const std::string& value, bool in_qemu) {
if (key == "androidboot.logical_partitions" && value == "1") {
enabled = true;
}
});
checked = true;
return enabled;
}
// Class Definitions
// -----------------
FirstStageMount::FirstStageMount()
: need_dm_verity_(false), device_tree_fstab_(fs_mgr_read_fstab_dt(), fs_mgr_free_fstab) {
if (device_tree_fstab_) {
// Stores device_tree_fstab_->recs[] into mount_fstab_recs_ (vector<fstab_rec*>)
// for easier manipulation later, e.g., range-base for loop.
for (int i = 0; i < device_tree_fstab_->num_entries; i++) {
mount_fstab_recs_.push_back(&device_tree_fstab_->recs[i]);
}
} else {
LOG(INFO) << "Failed to read fstab from device tree";
}
if (IsDmLinearEnabled()) {
dm_linear_table_ = android::fs_mgr::LoadPartitionsFromDeviceTree();
}
auto boot_devices = fs_mgr_get_boot_devices();
device_handler_ =
std::make_unique<DeviceHandler>(std::vector<Permissions>{}, std::vector<SysfsPermissions>{},
std::vector<Subsystem>{}, std::move(boot_devices), false);
}
std::unique_ptr<FirstStageMount> FirstStageMount::Create() {
if (IsDtVbmetaCompatible()) {
return std::make_unique<FirstStageMountVBootV2>();
} else {
return std::make_unique<FirstStageMountVBootV1>();
}
}
bool FirstStageMount::DoFirstStageMount() {
if (!IsDmLinearEnabled() && mount_fstab_recs_.empty()) {
// Nothing to mount.
LOG(INFO) << "First stage mount skipped (missing/incompatible/empty fstab in device tree)";
return true;
}
if (!InitDevices()) return false;
if (!CreateLogicalPartitions()) return false;
if (!MountPartitions()) return false;
return true;
}
bool FirstStageMount::InitDevices() {
return GetBackingDmLinearDevices() && GetDmVerityDevices() && InitRequiredDevices();
}
bool FirstStageMount::GetBackingDmLinearDevices() {
// Add any additional devices required for dm-linear mappings.
if (!IsDmLinearEnabled()) {
return true;
}
required_devices_partition_names_.emplace(LP_METADATA_PARTITION_NAME);
if (dm_linear_table_) {
for (const auto& partition : dm_linear_table_->partitions) {
for (const auto& extent : partition.extents) {
const std::string& partition_name = android::base::Basename(extent.block_device());
required_devices_partition_names_.emplace(partition_name);
}
}
}
return true;
}
// Creates devices with uevent->partition_name matching one in the member variable
// required_devices_partition_names_. Found partitions will then be removed from it
// for the subsequent member function to check which devices are NOT created.
bool FirstStageMount::InitRequiredDevices() {
if (required_devices_partition_names_.empty()) {
return true;
}
if (IsDmLinearEnabled() || need_dm_verity_) {
const std::string dm_path = "/devices/virtual/misc/device-mapper";
bool found = false;
auto dm_callback = [this, &dm_path, &found](const Uevent& uevent) {
if (uevent.path == dm_path) {
device_handler_->HandleDeviceEvent(uevent);
found = true;
return ListenerAction::kStop;
}
return ListenerAction::kContinue;
};
uevent_listener_.RegenerateUeventsForPath("/sys" + dm_path, dm_callback);
if (!found) {
LOG(INFO) << "device-mapper device not found in /sys, waiting for its uevent";
Timer t;
uevent_listener_.Poll(dm_callback, 10s);
LOG(INFO) << "Wait for device-mapper returned after " << t;
}
if (!found) {
LOG(ERROR) << "device-mapper device not found after polling timeout";
return false;
}
}
auto uevent_callback = [this](const Uevent& uevent) { return UeventCallback(uevent); };
uevent_listener_.RegenerateUevents(uevent_callback);
// UeventCallback() will remove found partitions from required_devices_partition_names_.
// So if it isn't empty here, it means some partitions are not found.
if (!required_devices_partition_names_.empty()) {
LOG(INFO) << __PRETTY_FUNCTION__
<< ": partition(s) not found in /sys, waiting for their uevent(s): "
<< android::base::Join(required_devices_partition_names_, ", ");
Timer t;
uevent_listener_.Poll(uevent_callback, 10s);
LOG(INFO) << "Wait for partitions returned after " << t;
}
if (!required_devices_partition_names_.empty()) {
LOG(ERROR) << __PRETTY_FUNCTION__ << ": partition(s) not found after polling timeout: "
<< android::base::Join(required_devices_partition_names_, ", ");
return false;
}
return true;
}
bool FirstStageMount::CreateLogicalPartitions() {
if (!IsDmLinearEnabled()) {
return true;
}
if (lp_metadata_partition_.empty()) {
LOG(ERROR) << "Could not locate logical partition tables in partition "
<< LP_METADATA_PARTITION_NAME;
return false;
}
if (dm_linear_table_) {
if (!android::fs_mgr::CreateLogicalPartitions(*dm_linear_table_.get())) {
return false;
}
}
return android::fs_mgr::CreateLogicalPartitions(lp_metadata_partition_);
}
ListenerAction FirstStageMount::HandleBlockDevice(const std::string& name, const Uevent& uevent) {
// Matches partition name to create device nodes.
// Both required_devices_partition_names_ and uevent->partition_name have A/B
// suffix when A/B is used.
auto iter = required_devices_partition_names_.find(name);
if (iter != required_devices_partition_names_.end()) {
LOG(VERBOSE) << __PRETTY_FUNCTION__ << ": found partition: " << *iter;
if (IsDmLinearEnabled() && name == LP_METADATA_PARTITION_NAME) {
std::vector<std::string> links = device_handler_->GetBlockDeviceSymlinks(uevent);
lp_metadata_partition_ = links[0];
}
required_devices_partition_names_.erase(iter);
device_handler_->HandleDeviceEvent(uevent);
if (required_devices_partition_names_.empty()) {
return ListenerAction::kStop;
} else {
return ListenerAction::kContinue;
}
}
return ListenerAction::kContinue;
}
ListenerAction FirstStageMount::UeventCallback(const Uevent& uevent) {
// Ignores everything that is not a block device.
if (uevent.subsystem != "block") {
return ListenerAction::kContinue;
}
if (!uevent.partition_name.empty()) {
return HandleBlockDevice(uevent.partition_name, uevent);
} else {
size_t base_idx = uevent.path.rfind('/');
if (base_idx != std::string::npos) {
return HandleBlockDevice(uevent.path.substr(base_idx + 1), uevent);
}
}
// Not found a partition or find an unneeded partition, continue to find others.
return ListenerAction::kContinue;
}
// Creates "/dev/block/dm-XX" for dm-verity by running coldboot on /sys/block/dm-XX.
bool FirstStageMount::InitMappedDevice(const std::string& dm_device) {
const std::string device_name(basename(dm_device.c_str()));
const std::string syspath = "/sys/block/" + device_name;
bool found = false;
auto verity_callback = [&device_name, &dm_device, this, &found](const Uevent& uevent) {
if (uevent.device_name == device_name) {
LOG(VERBOSE) << "Creating device-mapper device : " << dm_device;
device_handler_->HandleDeviceEvent(uevent);
found = true;
return ListenerAction::kStop;
}
return ListenerAction::kContinue;
};
uevent_listener_.RegenerateUeventsForPath(syspath, verity_callback);
if (!found) {
LOG(INFO) << "dm-verity device not found in /sys, waiting for its uevent";
Timer t;
uevent_listener_.Poll(verity_callback, 10s);
LOG(INFO) << "wait for dm-verity device returned after " << t;
}
if (!found) {
LOG(ERROR) << "dm-verity device not found after polling timeout";
return false;
}
return true;
}
bool FirstStageMount::MountPartitions() {
for (auto fstab_rec : mount_fstab_recs_) {
if (fs_mgr_is_logical(fstab_rec)) {
if (!fs_mgr_update_logical_partition(fstab_rec)) {
return false;
}
if (!InitMappedDevice(fstab_rec->blk_device)) {
return false;
}
}
if (!SetUpDmVerity(fstab_rec)) {
PLOG(ERROR) << "Failed to setup verity for '" << fstab_rec->mount_point << "'";
return false;
}
if (fs_mgr_do_mount_one(fstab_rec)) {
PLOG(ERROR) << "Failed to mount '" << fstab_rec->mount_point << "'";
return false;
}
}
return true;
}
bool FirstStageMountVBootV1::GetDmVerityDevices() {
std::string verity_loc_device;
need_dm_verity_ = false;
for (auto fstab_rec : mount_fstab_recs_) {
// Don't allow verifyatboot in the first stage.
if (fs_mgr_is_verifyatboot(fstab_rec)) {
LOG(ERROR) << "Partitions can't be verified at boot";
return false;
}
// Checks for verified partitions.
if (fs_mgr_is_verified(fstab_rec)) {
need_dm_verity_ = true;
}
// Checks if verity metadata is on a separate partition. Note that it is
// not partition specific, so there must be only one additional partition
// that carries verity state.
if (fstab_rec->verity_loc) {
if (verity_loc_device.empty()) {
verity_loc_device = fstab_rec->verity_loc;
} else if (verity_loc_device != fstab_rec->verity_loc) {
LOG(ERROR) << "More than one verity_loc found: " << verity_loc_device << ", "
<< fstab_rec->verity_loc;
return false;
}
}
}
// Includes the partition names of fstab records and verity_loc_device (if any).
// Notes that fstab_rec->blk_device has A/B suffix updated by fs_mgr when A/B is used.
for (auto fstab_rec : mount_fstab_recs_) {
required_devices_partition_names_.emplace(basename(fstab_rec->blk_device));
}
if (!verity_loc_device.empty()) {
required_devices_partition_names_.emplace(basename(verity_loc_device.c_str()));
}
return true;
}
bool FirstStageMountVBootV1::SetUpDmVerity(fstab_rec* fstab_rec) {
if (fs_mgr_is_verified(fstab_rec)) {
int ret = fs_mgr_setup_verity(fstab_rec, false /* wait_for_verity_dev */);
switch (ret) {
case FS_MGR_SETUP_VERITY_SKIPPED:
case FS_MGR_SETUP_VERITY_DISABLED:
LOG(INFO) << "Verity disabled/skipped for '" << fstab_rec->mount_point << "'";
return true;
case FS_MGR_SETUP_VERITY_SUCCESS:
// The exact block device name (fstab_rec->blk_device) is changed to
// "/dev/block/dm-XX". Needs to create it because ueventd isn't started in init
// first stage.
return InitMappedDevice(fstab_rec->blk_device);
default:
return false;
}
}
return true; // Returns true to mount the partition.
}
// FirstStageMountVBootV2 constructor.
// Gets the vbmeta partitions from device tree.
// /{
// firmware {
// android {
// vbmeta {
// compatible = "android,vbmeta";
// parts = "vbmeta,boot,system,vendor"
// };
// };
// };
// }
FirstStageMountVBootV2::FirstStageMountVBootV2() : avb_handle_(nullptr) {
if (!read_android_dt_file("vbmeta/parts", &device_tree_vbmeta_parts_)) {
PLOG(ERROR) << "Failed to read vbmeta/parts from device tree";
return;
}
}
bool FirstStageMountVBootV2::GetDmVerityDevices() {
need_dm_verity_ = false;
// fstab_rec->blk_device has A/B suffix.
for (auto fstab_rec : mount_fstab_recs_) {
if (fs_mgr_is_avb(fstab_rec)) {
need_dm_verity_ = true;
}
required_devices_partition_names_.emplace(basename(fstab_rec->blk_device));
}
// libavb verifies AVB metadata on all verified partitions at once.
// e.g., The device_tree_vbmeta_parts_ will be "vbmeta,boot,system,vendor"
// for libavb to verify metadata, even if there is only /vendor in the
// above mount_fstab_recs_.
if (need_dm_verity_) {
if (device_tree_vbmeta_parts_.empty()) {
LOG(ERROR) << "Missing vbmeta parts in device tree";
return false;
}
std::vector<std::string> partitions = android::base::Split(device_tree_vbmeta_parts_, ",");
std::string ab_suffix = fs_mgr_get_slot_suffix();
for (const auto& partition : partitions) {
// required_devices_partition_names_ is of type std::set so it's not an issue
// to emplace a partition twice. e.g., /vendor might be in both places:
// - device_tree_vbmeta_parts_ = "vbmeta,boot,system,vendor"
// - mount_fstab_recs_: /vendor_a
required_devices_partition_names_.emplace(partition + ab_suffix);
}
}
return true;
}
ListenerAction FirstStageMountVBootV2::UeventCallback(const Uevent& uevent) {
// Check if this uevent corresponds to one of the required partitions and store its symlinks if
// so, in order to create FsManagerAvbHandle later.
// Note that the parent callback removes partitions from the list of required partitions
// as it finds them, so this must happen first.
if (!uevent.partition_name.empty() &&
required_devices_partition_names_.find(uevent.partition_name) !=
required_devices_partition_names_.end()) {
// GetBlockDeviceSymlinks() will return three symlinks at most, depending on
// the content of uevent. by-name symlink will be at [0] if uevent->partition_name
// is not empty. e.g.,
// - /dev/block/platform/soc.0/f9824900.sdhci/by-name/modem
// - /dev/block/platform/soc.0/f9824900.sdhci/mmcblk0p1
std::vector<std::string> links = device_handler_->GetBlockDeviceSymlinks(uevent);
if (!links.empty()) {
auto[it, inserted] = by_name_symlink_map_.emplace(uevent.partition_name, links[0]);
if (!inserted) {
LOG(ERROR) << "Partition '" << uevent.partition_name
<< "' already existed in the by-name symlink map with a value of '"
<< it->second << "', new value '" << links[0] << "' will be ignored.";
}
}
}
return FirstStageMount::UeventCallback(uevent);
}
bool FirstStageMountVBootV2::SetUpDmVerity(fstab_rec* fstab_rec) {
if (fs_mgr_is_avb(fstab_rec)) {
if (!InitAvbHandle()) return false;
SetUpAvbHashtreeResult hashtree_result =
avb_handle_->SetUpAvbHashtree(fstab_rec, false /* wait_for_verity_dev */);
switch (hashtree_result) {
case SetUpAvbHashtreeResult::kDisabled:
return true; // Returns true to mount the partition.
case SetUpAvbHashtreeResult::kSuccess:
// The exact block device name (fstab_rec->blk_device) is changed to
// "/dev/block/dm-XX". Needs to create it because ueventd isn't started in init
// first stage.
return InitMappedDevice(fstab_rec->blk_device);
default:
return false;
}
}
return true; // Returns true to mount the partition.
}
bool FirstStageMountVBootV2::InitAvbHandle() {
if (avb_handle_) return true; // Returns true if the handle is already initialized.
if (by_name_symlink_map_.empty()) {
LOG(ERROR) << "by_name_symlink_map_ is empty";
return false;
}
avb_handle_ = FsManagerAvbHandle::Open(std::move(by_name_symlink_map_));
by_name_symlink_map_.clear(); // Removes all elements after the above std::move().
if (!avb_handle_) {
PLOG(ERROR) << "Failed to open FsManagerAvbHandle";
return false;
}
// Sets INIT_AVB_VERSION here for init to set ro.boot.avb_version in the second stage.
setenv("INIT_AVB_VERSION", avb_handle_->avb_version().c_str(), 1);
return true;
}
// Public functions
// ----------------
// Mounts partitions specified by fstab in device tree.
bool DoFirstStageMount() {
// Skips first stage mount if we're in recovery mode.
if (IsRecoveryMode()) {
LOG(INFO) << "First stage mount skipped (recovery mode)";
return true;
}
std::unique_ptr<FirstStageMount> handle = FirstStageMount::Create();
if (!handle) {
LOG(ERROR) << "Failed to create FirstStageMount";
return false;
}
return handle->DoFirstStageMount();
}
void SetInitAvbVersionInRecovery() {
if (!IsRecoveryMode()) {
LOG(INFO) << "Skipped setting INIT_AVB_VERSION (not in recovery mode)";
return;
}
if (!IsDtVbmetaCompatible()) {
LOG(INFO) << "Skipped setting INIT_AVB_VERSION (not vbmeta compatible)";
return;
}
// Initializes required devices for the subsequent FsManagerAvbHandle::Open()
// to verify AVB metadata on all partitions in the verified chain.
// We only set INIT_AVB_VERSION when the AVB verification succeeds, i.e., the
// Open() function returns a valid handle.
// We don't need to mount partitions here in recovery mode.
FirstStageMountVBootV2 avb_first_mount;
if (!avb_first_mount.InitDevices()) {
LOG(ERROR) << "Failed to init devices for INIT_AVB_VERSION";
return;
}
FsManagerAvbUniquePtr avb_handle =
FsManagerAvbHandle::Open(std::move(avb_first_mount.by_name_symlink_map_));
if (!avb_handle) {
PLOG(ERROR) << "Failed to open FsManagerAvbHandle for INIT_AVB_VERSION";
return;
}
setenv("INIT_AVB_VERSION", avb_handle->avb_version().c_str(), 1);
}
} // namespace init
} // namespace android