summaryrefslogblamecommitdiffstats
blob: 327b4444f1a91341eaf06cc778e3b60e8759b1d4 (plain) (tree)











































































                                                                                                   

                                                 






                                     

                                         












                                                                                                  

                                                                  









                                                            

































































                                                                               



































































































                                                                                                










































                                                                                                 






                                                 
                                            



                       
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "result.h"

#include "errno.h"

#include <string>

#include <gtest/gtest.h>

using namespace std::string_literals;

namespace android {
namespace init {

TEST(result, result_accessors) {
    Result<std::string> result = "success";
    ASSERT_TRUE(result);
    ASSERT_TRUE(result.has_value());

    EXPECT_EQ("success", *result);
    EXPECT_EQ("success", result.value());

    EXPECT_EQ('s', result->data()[0]);
}

TEST(result, result_accessors_rvalue) {
    ASSERT_TRUE(Result<std::string>("success"));
    ASSERT_TRUE(Result<std::string>("success").has_value());

    EXPECT_EQ("success", *Result<std::string>("success"));
    EXPECT_EQ("success", Result<std::string>("success").value());

    EXPECT_EQ('s', Result<std::string>("success")->data()[0]);
}

TEST(result, result_success) {
    Result<Success> result = Success();
    ASSERT_TRUE(result);
    ASSERT_TRUE(result.has_value());

    EXPECT_EQ(Success(), *result);
    EXPECT_EQ(Success(), result.value());
}

TEST(result, result_success_rvalue) {
    // Success() doesn't actually create a Result<Success> object, but rather an object that can be
    // implicitly constructed into a Result<Success> object.

    auto MakeRvalueSuccessResult = []() -> Result<Success> { return Success(); };
    ASSERT_TRUE(MakeRvalueSuccessResult());
    ASSERT_TRUE(MakeRvalueSuccessResult().has_value());

    EXPECT_EQ(Success(), *MakeRvalueSuccessResult());
    EXPECT_EQ(Success(), MakeRvalueSuccessResult().value());
}

TEST(result, result_error) {
    Result<Success> result = Error() << "failure" << 1;
    ASSERT_FALSE(result);
    ASSERT_FALSE(result.has_value());

    EXPECT_EQ(0, result.error_errno());
    EXPECT_EQ("failure1", result.error_string());
}

TEST(result, result_error_empty) {
    Result<Success> result = Error();
    ASSERT_FALSE(result);
    ASSERT_FALSE(result.has_value());

    EXPECT_EQ(0, result.error_errno());
    EXPECT_EQ("", result.error_string());
}

TEST(result, result_error_rvalue) {
    // Error() and ErrnoError() aren't actually used to create a Result<T> object.
    // Under the hood, they are an intermediate class that can be implicitly constructed into a
    // Result<T>.  This is needed both to create the ostream and because Error() itself, by
    // definition will not know what the type, T, of the underlying Result<T> object that it would
    // create is.

    auto MakeRvalueErrorResult = []() -> Result<Success> { return Error() << "failure" << 1; };
    ASSERT_FALSE(MakeRvalueErrorResult());
    ASSERT_FALSE(MakeRvalueErrorResult().has_value());

    EXPECT_EQ(0, MakeRvalueErrorResult().error_errno());
    EXPECT_EQ("failure1", MakeRvalueErrorResult().error_string());
}

TEST(result, result_errno_error) {
    constexpr int test_errno = 6;
    errno = test_errno;
    Result<Success> result = ErrnoError() << "failure" << 1;

    ASSERT_FALSE(result);
    ASSERT_FALSE(result.has_value());

    EXPECT_EQ(test_errno, result.error_errno());
    EXPECT_EQ("failure1: "s + strerror(test_errno), result.error_string());
}

TEST(result, result_errno_error_no_text) {
    constexpr int test_errno = 6;
    errno = test_errno;
    Result<Success> result = ErrnoError();

    ASSERT_FALSE(result);
    ASSERT_FALSE(result.has_value());

    EXPECT_EQ(test_errno, result.error_errno());
    EXPECT_EQ(strerror(test_errno), result.error_string());
}

TEST(result, result_error_from_other_result) {
    auto error_text = "test error"s;
    Result<Success> result = Error() << error_text;

    ASSERT_FALSE(result);
    ASSERT_FALSE(result.has_value());

    Result<std::string> result2 = result.error();

    ASSERT_FALSE(result2);
    ASSERT_FALSE(result2.has_value());

    EXPECT_EQ(0, result.error_errno());
    EXPECT_EQ(error_text, result.error_string());
}

TEST(result, result_error_through_ostream) {
    auto error_text = "test error"s;
    Result<Success> result = Error() << error_text;

    ASSERT_FALSE(result);
    ASSERT_FALSE(result.has_value());

    Result<std::string> result2 = Error() << result.error();

    ASSERT_FALSE(result2);
    ASSERT_FALSE(result2.has_value());

    EXPECT_EQ(0, result.error_errno());
    EXPECT_EQ(error_text, result.error_string());
}

TEST(result, result_errno_error_through_ostream) {
    auto error_text = "test error"s;
    constexpr int test_errno = 6;
    errno = 6;
    Result<Success> result = ErrnoError() << error_text;

    errno = 0;

    ASSERT_FALSE(result);
    ASSERT_FALSE(result.has_value());

    Result<std::string> result2 = Error() << result.error();

    ASSERT_FALSE(result2);
    ASSERT_FALSE(result2.has_value());

    EXPECT_EQ(test_errno, result.error_errno());
    EXPECT_EQ(error_text + ": " + strerror(test_errno), result.error_string());
}

TEST(result, constructor_forwarding) {
    auto result = Result<std::string>(5, 'a');

    ASSERT_TRUE(result);
    ASSERT_TRUE(result.has_value());

    EXPECT_EQ("aaaaa", *result);
}

struct ConstructorTracker {
    static size_t constructor_called;
    static size_t copy_constructor_called;
    static size_t move_constructor_called;
    static size_t copy_assignment_called;
    static size_t move_assignment_called;

    template <typename T>
    ConstructorTracker(T&& string) : string(string) {
        ++constructor_called;
    }

    ConstructorTracker(const ConstructorTracker& ct) {
        ++copy_constructor_called;
        string = ct.string;
    }
    ConstructorTracker(ConstructorTracker&& ct) noexcept {
        ++move_constructor_called;
        string = std::move(ct.string);
    }
    ConstructorTracker& operator=(const ConstructorTracker& ct) {
        ++copy_assignment_called;
        string = ct.string;
        return *this;
    }
    ConstructorTracker& operator=(ConstructorTracker&& ct) noexcept {
        ++move_assignment_called;
        string = std::move(ct.string);
        return *this;
    }

    std::string string;
};

size_t ConstructorTracker::constructor_called = 0;
size_t ConstructorTracker::copy_constructor_called = 0;
size_t ConstructorTracker::move_constructor_called = 0;
size_t ConstructorTracker::copy_assignment_called = 0;
size_t ConstructorTracker::move_assignment_called = 0;

Result<ConstructorTracker> ReturnConstructorTracker(const std::string& in) {
    if (in.empty()) {
        return "literal string";
    }
    if (in == "test2") {
        return ConstructorTracker(in + in + "2");
    }
    ConstructorTracker result(in + " " + in);
    return result;
};

TEST(result, no_copy_on_return) {
    // If returning parameters that may be used to implicitly construct the type T of Result<T>,
    // then those parameters are forwarded to the construction of Result<T>.

    // If returning an prvalue or xvalue, it will be move constructed during the construction of
    // Result<T>.

    // This check ensures that that is the case, and particularly that no copy constructors
    // are called.

    auto result1 = ReturnConstructorTracker("");
    ASSERT_TRUE(result1);
    EXPECT_EQ("literal string", result1->string);
    EXPECT_EQ(1U, ConstructorTracker::constructor_called);
    EXPECT_EQ(0U, ConstructorTracker::copy_constructor_called);
    EXPECT_EQ(0U, ConstructorTracker::move_constructor_called);
    EXPECT_EQ(0U, ConstructorTracker::copy_assignment_called);
    EXPECT_EQ(0U, ConstructorTracker::move_assignment_called);

    auto result2 = ReturnConstructorTracker("test2");
    ASSERT_TRUE(result2);
    EXPECT_EQ("test2test22", result2->string);
    EXPECT_EQ(2U, ConstructorTracker::constructor_called);
    EXPECT_EQ(0U, ConstructorTracker::copy_constructor_called);
    EXPECT_EQ(1U, ConstructorTracker::move_constructor_called);
    EXPECT_EQ(0U, ConstructorTracker::copy_assignment_called);
    EXPECT_EQ(0U, ConstructorTracker::move_assignment_called);

    auto result3 = ReturnConstructorTracker("test3");
    ASSERT_TRUE(result3);
    EXPECT_EQ("test3 test3", result3->string);
    EXPECT_EQ(3U, ConstructorTracker::constructor_called);
    EXPECT_EQ(0U, ConstructorTracker::copy_constructor_called);
    EXPECT_EQ(2U, ConstructorTracker::move_constructor_called);
    EXPECT_EQ(0U, ConstructorTracker::copy_assignment_called);
    EXPECT_EQ(0U, ConstructorTracker::move_assignment_called);
}

// Below two tests require that we do not hide the move constructor with our forwarding reference
// constructor.  This is done with by disabling the forwarding reference constructor if its first
// and only type is Result<T>.
TEST(result, result_result_with_success) {
    auto return_result_result_with_success = []() -> Result<Result<Success>> {
        return Result<Success>();
    };
    auto result = return_result_result_with_success();
    ASSERT_TRUE(result);
    ASSERT_TRUE(*result);

    auto inner_result = result.value();
    ASSERT_TRUE(inner_result);
}

TEST(result, result_result_with_failure) {
    auto return_result_result_with_error = []() -> Result<Result<Success>> {
        return Result<Success>(ResultError("failure string", 6));
    };
    auto result = return_result_result_with_error();
    ASSERT_TRUE(result);
    ASSERT_FALSE(*result);
    EXPECT_EQ("failure string", result->error_string());
    EXPECT_EQ(6, result->error_errno());
}

// This test requires that we disable the forwarding reference constructor if Result<T> is the
// *only* type that we are forwarding.  In otherwords, if we are forwarding Result<T>, int to
// construct a Result<T>, then we still need the constructor.
TEST(result, result_two_parameter_constructor_same_type) {
    struct TestStruct {
        TestStruct(int value) : value_(value) {}
        TestStruct(Result<TestStruct> result, int value) : value_(result->value_ * value) {}
        int value_;
    };

    auto return_test_struct = []() -> Result<TestStruct> { return {Result<TestStruct>(6), 6}; };

    auto result = return_test_struct();
    ASSERT_TRUE(result);
    EXPECT_EQ(36, result->value_);
}

TEST(result, die_on_access_failed_result) {
    Result<std::string> result = Error();
    ASSERT_DEATH(*result, "");
}

TEST(result, die_on_get_error_succesful_result) {
    Result<std::string> result = "success";
    ASSERT_DEATH(result.error_string(), "");
}

}  // namespace init
}  // namespace android