summaryrefslogblamecommitdiffstats
blob: a3494a280bdfd6ab96df1e0cdf2ef39e19e6e64c (plain) (tree)


























                                                                           

















                                                                             
                                                                     





                                                                                       
                             
         
                                                               




                                                                                     
                                                             







                                                                                          
                                                                        
                                     
                                                                        



                                                                            
                                                                     




                                                                                                   
                     

































































                                                                                              
                                                               


                                         
                     


                                                                              
                         



                                                                              
                         





                                                          
                         


                                              
                     



                                         
                                                               
                   








                                                           
                                                                


                                                                                                
                                                                    
                       
     
                     



                       
/*
 * Copyright (C) 2017 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "security.h"

#include <errno.h>
#include <fcntl.h>
#include <unistd.h>

#include <fstream>

#include <android-base/logging.h>
#include <android-base/unique_fd.h>

using android::base::unique_fd;

namespace android {
namespace init {

// Writes 512 bytes of output from Hardware RNG (/dev/hw_random, backed
// by Linux kernel's hw_random framework) into Linux RNG's via /dev/urandom.
// Does nothing if Hardware RNG is not present.
//
// Since we don't yet trust the quality of Hardware RNG, these bytes are not
// mixed into the primary pool of Linux RNG and the entropy estimate is left
// unmodified.
//
// If the HW RNG device /dev/hw_random is present, we require that at least
// 512 bytes read from it are written into Linux RNG. QA is expected to catch
// devices/configurations where these I/O operations are blocking for a long
// time. We do not reboot or halt on failures, as this is a best-effort
// attempt.
Result<Success> MixHwrngIntoLinuxRngAction(const BuiltinArguments&) {
    unique_fd hwrandom_fd(
        TEMP_FAILURE_RETRY(open("/dev/hw_random", O_RDONLY | O_NOFOLLOW | O_CLOEXEC)));
    if (hwrandom_fd == -1) {
        if (errno == ENOENT) {
            LOG(INFO) << "/dev/hw_random not found";
            // It's not an error to not have a Hardware RNG.
            return Success();
        }
        return ErrnoError() << "Failed to open /dev/hw_random";
    }

    unique_fd urandom_fd(
        TEMP_FAILURE_RETRY(open("/dev/urandom", O_WRONLY | O_NOFOLLOW | O_CLOEXEC)));
    if (urandom_fd == -1) {
        return ErrnoError() << "Failed to open /dev/urandom";
    }

    char buf[512];
    size_t total_bytes_written = 0;
    while (total_bytes_written < sizeof(buf)) {
        ssize_t chunk_size =
            TEMP_FAILURE_RETRY(read(hwrandom_fd, buf, sizeof(buf) - total_bytes_written));
        if (chunk_size == -1) {
            return ErrnoError() << "Failed to read from /dev/hw_random";
        } else if (chunk_size == 0) {
            return Error() << "Failed to read from /dev/hw_random: EOF";
        }

        chunk_size = TEMP_FAILURE_RETRY(write(urandom_fd, buf, chunk_size));
        if (chunk_size == -1) {
            return ErrnoError() << "Failed to write to /dev/urandom";
        }
        total_bytes_written += chunk_size;
    }

    LOG(INFO) << "Mixed " << total_bytes_written << " bytes from /dev/hw_random into /dev/urandom";
    return Success();
}

static bool SetHighestAvailableOptionValue(std::string path, int min, int max) {
    std::ifstream inf(path, std::fstream::in);
    if (!inf) {
        LOG(ERROR) << "Cannot open for reading: " << path;
        return false;
    }

    int current = max;
    while (current >= min) {
        // try to write out new value
        std::string str_val = std::to_string(current);
        std::ofstream of(path, std::fstream::out);
        if (!of) {
            LOG(ERROR) << "Cannot open for writing: " << path;
            return false;
        }
        of << str_val << std::endl;
        of.close();

        // check to make sure it was recorded
        inf.seekg(0);
        std::string str_rec;
        inf >> str_rec;
        if (str_val.compare(str_rec) == 0) {
            break;
        }
        current--;
    }
    inf.close();

    if (current < min) {
        LOG(ERROR) << "Unable to set minimum option value " << min << " in " << path;
        return false;
    }
    return true;
}

#define MMAP_RND_PATH "/proc/sys/vm/mmap_rnd_bits"
#define MMAP_RND_COMPAT_PATH "/proc/sys/vm/mmap_rnd_compat_bits"

// __attribute__((unused)) due to lack of mips support: see mips block in SetMmapRndBitsAction
static bool __attribute__((unused)) SetMmapRndBitsMin(int start, int min, bool compat) {
    std::string path;
    if (compat) {
        path = MMAP_RND_COMPAT_PATH;
    } else {
        path = MMAP_RND_PATH;
    }

    return SetHighestAvailableOptionValue(path, min, start);
}

// Set /proc/sys/vm/mmap_rnd_bits and potentially
// /proc/sys/vm/mmap_rnd_compat_bits to the maximum supported values.
// Returns -1 if unable to set these to an acceptable value.
//
// To support this sysctl, the following upstream commits are needed:
//
// d07e22597d1d mm: mmap: add new /proc tunable for mmap_base ASLR
// e0c25d958f78 arm: mm: support ARCH_MMAP_RND_BITS
// 8f0d3aa9de57 arm64: mm: support ARCH_MMAP_RND_BITS
// 9e08f57d684a x86: mm: support ARCH_MMAP_RND_BITS
// ec9ee4acd97c drivers: char: random: add get_random_long()
// 5ef11c35ce86 mm: ASLR: use get_random_long()
Result<Success> SetMmapRndBitsAction(const BuiltinArguments&) {
// values are arch-dependent
#if defined(USER_MODE_LINUX)
    // uml does not support mmap_rnd_bits
    return Success();
#elif defined(__aarch64__)
    // arm64 supports 18 - 33 bits depending on pagesize and VA_SIZE
    if (SetMmapRndBitsMin(33, 24, false) && SetMmapRndBitsMin(16, 16, true)) {
        return Success();
    }
#elif defined(__x86_64__)
    // x86_64 supports 28 - 32 bits
    if (SetMmapRndBitsMin(32, 32, false) && SetMmapRndBitsMin(16, 16, true)) {
        return Success();
    }
#elif defined(__arm__) || defined(__i386__)
    // check to see if we're running on 64-bit kernel
    bool h64 = !access(MMAP_RND_COMPAT_PATH, F_OK);
    // supported 32-bit architecture must have 16 bits set
    if (SetMmapRndBitsMin(16, 16, h64)) {
        return Success();
    }
#elif defined(__mips__) || defined(__mips64__)
    // TODO: add mips support b/27788820
    return Success();
#else
    LOG(ERROR) << "Unknown architecture";
#endif

    LOG(FATAL) << "Unable to set adequate mmap entropy value!";
    return Error();
}

#define KPTR_RESTRICT_PATH "/proc/sys/kernel/kptr_restrict"
#define KPTR_RESTRICT_MINVALUE 2
#define KPTR_RESTRICT_MAXVALUE 4

// Set kptr_restrict to the highest available level.
//
// Aborts if unable to set this to an acceptable value.
Result<Success> SetKptrRestrictAction(const BuiltinArguments&) {
    std::string path = KPTR_RESTRICT_PATH;

    if (!SetHighestAvailableOptionValue(path, KPTR_RESTRICT_MINVALUE, KPTR_RESTRICT_MAXVALUE)) {
        LOG(FATAL) << "Unable to set adequate kptr_restrict value!";
        return Error();
    }
    return Success();
}

}  // namespace init
}  // namespace android