summaryrefslogblamecommitdiffstats
blob: 0b0332429152e4c8b4d5d3646cbac057dec93127 (plain) (tree)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16















                                                                           
                            
 
                   
                   
                       
                      
                     

                   
                                      
                                 

                                      

                 
                             
                    
 



                                      


                   

















                                                                                                  

                            





                                          
            












                                                                                                   

     



                                                                                        



                              
                           

                                           
                                                           




                




                                   

                       
/*
 * Copyright (C) 2010 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#include "sigchld_handler.h"

#include <signal.h>
#include <string.h>
#include <sys/socket.h>
#include <sys/types.h>
#include <sys/wait.h>
#include <unistd.h>

#include <android-base/chrono_utils.h>
#include <android-base/logging.h>
#include <android-base/scopeguard.h>
#include <android-base/stringprintf.h>

#include "init.h"
#include "property_service.h"
#include "service.h"

using android::base::StringPrintf;
using android::base::boot_clock;
using android::base::make_scope_guard;

namespace android {
namespace init {

static bool ReapOneProcess() {
    siginfo_t siginfo = {};
    // This returns a zombie pid or informs us that there are no zombies left to be reaped.
    // It does NOT reap the pid; that is done below.
    if (TEMP_FAILURE_RETRY(waitid(P_ALL, 0, &siginfo, WEXITED | WNOHANG | WNOWAIT)) != 0) {
        PLOG(ERROR) << "waitid failed";
        return false;
    }

    auto pid = siginfo.si_pid;
    if (pid == 0) return false;

    // At this point we know we have a zombie pid, so we use this scopeguard to reap the pid
    // whenever the function returns from this point forward.
    // We do NOT want to reap the zombie earlier as in Service::Reap(), we kill(-pid, ...) and we
    // want the pid to remain valid throughout that (and potentially future) usages.
    auto reaper = make_scope_guard([pid] { TEMP_FAILURE_RETRY(waitpid(pid, nullptr, WNOHANG)); });

    std::string name;
    std::string wait_string;
    Service* service = nullptr;

    if (PropertyChildReap(pid)) {
        name = "Async property child";
    } else if (SubcontextChildReap(pid)) {
        name = "Subcontext";
    } else {
        service = ServiceList::GetInstance().FindService(pid, &Service::pid);

        if (service) {
            name = StringPrintf("Service '%s' (pid %d)", service->name().c_str(), pid);
            if (service->flags() & SVC_EXEC) {
                auto exec_duration = boot_clock::now() - service->time_started();
                auto exec_duration_ms =
                    std::chrono::duration_cast<std::chrono::milliseconds>(exec_duration).count();
                wait_string = StringPrintf(" waiting took %f seconds", exec_duration_ms / 1000.0f);
            }
        } else {
            name = StringPrintf("Untracked pid %d", pid);
        }
    }

    if (siginfo.si_code == CLD_EXITED) {
        LOG(INFO) << name << " exited with status " << siginfo.si_status << wait_string;
    } else {
        LOG(INFO) << name << " received signal " << siginfo.si_status << wait_string;
    }

    if (!service) return true;

    service->Reap(siginfo);

    if (service->flags() & SVC_TEMPORARY) {
        ServiceList::GetInstance().RemoveService(*service);
    }

    return true;
}

void ReapAnyOutstandingChildren() {
    while (ReapOneProcess()) {
    }
}

}  // namespace init
}  // namespace android