/*
* Copyright (C) 2010 The Android Open Source Project
*
* Licensed under the Apache License, Version 2.0 (the "License");
* you may not use this file except in compliance with the License.
* You may obtain a copy of the License at
*
* http://www.apache.org/licenses/LICENSE-2.0
*
* Unless required by applicable law or agreed to in writing, software
* distributed under the License is distributed on an "AS IS" BASIS,
* WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
* See the License for the specific language governing permissions and
* limitations under the License.
*/
#ifndef _INIT_UTIL_H_
#define _INIT_UTIL_H_
#include <sys/stat.h>
#include <sys/types.h>
#include <chrono>
#include <functional>
#include <ostream>
#include <string>
#include <android-base/chrono_utils.h>
#include <selinux/label.h>
#include "result.h"
#define COLDBOOT_DONE "/dev/.coldboot_done"
using android::base::boot_clock;
using namespace std::chrono_literals;
namespace android {
namespace init {
int CreateSocket(const char* name, int type, bool passcred, mode_t perm, uid_t uid, gid_t gid,
const char* socketcon);
Result<std::string> ReadFile(const std::string& path);
Result<Success> WriteFile(const std::string& path, const std::string& content);
Result<uid_t> DecodeUid(const std::string& name);
bool mkdir_recursive(const std::string& pathname, mode_t mode);
int wait_for_file(const char *filename, std::chrono::nanoseconds timeout);
void import_kernel_cmdline(bool in_qemu,
const std::function<void(const std::string&, const std::string&, bool)>&);
bool make_dir(const std::string& path, mode_t mode);
std::string bytes_to_hex(const uint8_t *bytes, size_t bytes_len);
bool is_dir(const char* pathname);
bool expand_props(const std::string& src, std::string* dst);
// Returns the platform's Android DT directory as specified in the kernel cmdline.
// If the platform does not configure a custom DT path, returns the standard one (based in procfs).
const std::string& get_android_dt_dir();
// Reads or compares the content of device tree file under the platform's Android DT directory.
bool read_android_dt_file(const std::string& sub_path, std::string* dt_content);
bool is_android_dt_value_expected(const std::string& sub_path, const std::string& expected_content);
bool IsLegalPropertyName(const std::string& name);
} // namespace init
} // namespace android
#endif