summaryrefslogblamecommitdiffstats
blob: ae7a33412b7c99e18e37361adfc05845d8fbbbd0 (plain) (tree)
1
2
  
                                                          


















                                                                           


                  


                    

                   

                   
                 
 
                        
                    
 
                            
                            
 
                                                            
 
                                      








                                                          








                    

            



                         

                                           
 

                                              
 

                                       
 

                               
 

                         
 




                           

           
                    







                                                                     





                                                                            

 

                                           
 
 
                          
 

                          
 
                           
 



                              

                                            




                                                                






                                                                          
     

              




                                 




                                                                




                                                            

                                  
 
         
 



                                                                         
 
           














                                                                            


















































                                                                             
                                          




























                                            
         
 

















                                                                          
     




























                                                  





                                                                         










                                                                          

 
                   
  
                                

                                   







                                                                         
     


                




                          




                                                             

                                                                  
                    
                  
      




                                      
                    
                 
     
                    
      
 














                                                                     
                    
                                   
     
                         
      

                                                                  
 



                                                                  
 
                                
                    




                                                                            
                        



                                                                           
                       




                                                                        
                    




                              
                     




                                                                              
                           





                                                                           
                     





                                                                            
            







































                                                                      
     













                                   
     


                                   
     




                                 
     





                              
     

































                                                                            
 

                                                       

 






                                                                           








































                                                                                 
     
   
 




                                                        

     





                               
 
      

            




                                                   


                             




                                                 


                                                              
 
         
 








                                              
 

            






                                                                    
                                                                   
                                           




















                                                                           

 




                                                                

 










                                                                              


                                            

 



                                                                       
 
 


                                                                

 
                                                         



                                                                         
 

                                                             
                                                                             
                                                                        


                                                              
 
 

                                                      
 
/*
 * Copyright (C) 2008-2014 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */
/*
 * Intercepts log messages intended for the Android log device.
 * When running in the context of the simulator, the messages are
 * passed on to the underlying (fake) log device.  When not in the
 * simulator, messages are printed to stderr.
 */
#include <ctype.h>
#include <errno.h>
#include <fcntl.h>
#if !defined(_WIN32)
#include <pthread.h>
#endif
#include <stdint.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <time.h>

#include <android/log.h>
#include <log/uio.h>

#include "fake_log_device.h"
#include "log_portability.h"

#define kMaxTagLen 16 /* from the long-dead utils/Log.cpp */

#define kTagSetSize 16 /* arbitrary */

#if 0
#define TRACE(...) printf("fake_log_device: " __VA_ARGS__)
#else
#define TRACE(...) ((void)0)
#endif

/* from the long-dead utils/Log.cpp */
typedef enum {
  FORMAT_OFF = 0,
  FORMAT_BRIEF,
  FORMAT_PROCESS,
  FORMAT_TAG,
  FORMAT_THREAD,
  FORMAT_RAW,
  FORMAT_TIME,
  FORMAT_THREADTIME,
  FORMAT_LONG
} LogFormat;

/*
 * Log driver state.
 */
typedef struct LogState {
  /* the fake fd that's seen by the user */
  int fakeFd;

  /* a printable name for this fake device */
  char debugName[sizeof("/dev/log/security")];

  /* nonzero if this is a binary log */
  int isBinary;

  /* global minimum priority */
  int globalMinPriority;

  /* output format */
  LogFormat outputFormat;

  /* tags and priorities */
  struct {
    char tag[kMaxTagLen];
    int minPriority;
  } tagSet[kTagSetSize];
} LogState;

#if !defined(_WIN32)
/*
 * Locking.  Since we're emulating a device, we need to be prepared
 * to have multiple callers at the same time.  This lock is used
 * to both protect the fd list and to prevent LogStates from being
 * freed out from under a user.
 */
static pthread_mutex_t fakeLogDeviceLock = PTHREAD_MUTEX_INITIALIZER;

static void lock() {
  /*
   * If we trigger a signal handler in the middle of locked activity and the
   * signal handler logs a message, we could get into a deadlock state.
   */
  pthread_mutex_lock(&fakeLogDeviceLock);
}

static void unlock() {
  pthread_mutex_unlock(&fakeLogDeviceLock);
}

#else  // !defined(_WIN32)

#define lock() ((void)0)
#define unlock() ((void)0)

#endif  // !defined(_WIN32)

/*
 * File descriptor management.
 */
#define FAKE_FD_BASE 10000
#define MAX_OPEN_LOGS 8
static LogState openLogTable[MAX_OPEN_LOGS];

/*
 * Allocate an fd and associate a new LogState with it.
 * The fd is available via the fakeFd field of the return value.
 */
static LogState* createLogState() {
  size_t i;

  for (i = 0; i < (sizeof(openLogTable) / sizeof(openLogTable[0])); i++) {
    if (openLogTable[i].fakeFd == 0) {
      openLogTable[i].fakeFd = FAKE_FD_BASE + i;
      return &openLogTable[i];
    }
  }
  return NULL;
}

/*
 * Translate an fd to a LogState.
 */
static LogState* fdToLogState(int fd) {
  if (fd >= FAKE_FD_BASE && fd < FAKE_FD_BASE + MAX_OPEN_LOGS) {
    return &openLogTable[fd - FAKE_FD_BASE];
  }
  return NULL;
}

/*
 * Unregister the fake fd and free the memory it pointed to.
 */
static void deleteFakeFd(int fd) {
  LogState* ls;

  lock();

  ls = fdToLogState(fd);
  if (ls != NULL) {
    memset(&openLogTable[fd - FAKE_FD_BASE], 0, sizeof(openLogTable[0]));
  }

  unlock();
}

/*
 * Configure logging based on ANDROID_LOG_TAGS environment variable.  We
 * need to parse a string that looks like
 *
 *   *:v jdwp:d dalvikvm:d dalvikvm-gc:i dalvikvmi:i
 *
 * The tag (or '*' for the global level) comes first, followed by a colon
 * and a letter indicating the minimum priority level we're expected to log.
 * This can be used to reveal or conceal logs with specific tags.
 *
 * We also want to check ANDROID_PRINTF_LOG to determine how the output
 * will look.
 */
static void configureInitialState(const char* pathName, LogState* logState) {
  static const int kDevLogLen = sizeof("/dev/log/") - 1;

  strncpy(logState->debugName, pathName, sizeof(logState->debugName));
  logState->debugName[sizeof(logState->debugName) - 1] = '\0';

  /* identify binary logs */
  if (!strcmp(pathName + kDevLogLen, "events") ||
      !strcmp(pathName + kDevLogLen, "security")) {
    logState->isBinary = 1;
  }

  /* global min priority defaults to "info" level */
  logState->globalMinPriority = ANDROID_LOG_INFO;

  /*
   * This is based on the the long-dead utils/Log.cpp code.
   */
  const char* tags = getenv("ANDROID_LOG_TAGS");
  TRACE("Found ANDROID_LOG_TAGS='%s'\n", tags);
  if (tags != NULL) {
    int entry = 0;

    while (*tags != '\0') {
      char tagName[kMaxTagLen];
      int i, minPrio;

      while (isspace(*tags)) tags++;

      i = 0;
      while (*tags != '\0' && !isspace(*tags) && *tags != ':' &&
             i < kMaxTagLen) {
        tagName[i++] = *tags++;
      }
      if (i == kMaxTagLen) {
        TRACE("ERROR: env tag too long (%d chars max)\n", kMaxTagLen - 1);
        return;
      }
      tagName[i] = '\0';

      /* default priority, if there's no ":" part; also zero out '*' */
      minPrio = ANDROID_LOG_VERBOSE;
      if (tagName[0] == '*' && tagName[1] == '\0') {
        minPrio = ANDROID_LOG_DEBUG;
        tagName[0] = '\0';
      }

      if (*tags == ':') {
        tags++;
        if (*tags >= '0' && *tags <= '9') {
          if (*tags >= ('0' + ANDROID_LOG_SILENT))
            minPrio = ANDROID_LOG_VERBOSE;
          else
            minPrio = *tags - '\0';
        } else {
          switch (*tags) {
            case 'v':
              minPrio = ANDROID_LOG_VERBOSE;
              break;
            case 'd':
              minPrio = ANDROID_LOG_DEBUG;
              break;
            case 'i':
              minPrio = ANDROID_LOG_INFO;
              break;
            case 'w':
              minPrio = ANDROID_LOG_WARN;
              break;
            case 'e':
              minPrio = ANDROID_LOG_ERROR;
              break;
            case 'f':
              minPrio = ANDROID_LOG_FATAL;
              break;
            case 's':
              minPrio = ANDROID_LOG_SILENT;
              break;
            default:
              minPrio = ANDROID_LOG_DEFAULT;
              break;
          }
        }

        tags++;
        if (*tags != '\0' && !isspace(*tags)) {
          TRACE("ERROR: garbage in tag env; expected whitespace\n");
          TRACE("       env='%s'\n", tags);
          return;
        }
      }

      if (tagName[0] == 0) {
        logState->globalMinPriority = minPrio;
        TRACE("+++ global min prio %d\n", logState->globalMinPriority);
      } else {
        logState->tagSet[entry].minPriority = minPrio;
        strcpy(logState->tagSet[entry].tag, tagName);
        TRACE("+++ entry %d: %s:%d\n", entry, logState->tagSet[entry].tag,
              logState->tagSet[entry].minPriority);
        entry++;
      }
    }
  }

  /*
   * Taken from the long-dead utils/Log.cpp
   */
  const char* fstr = getenv("ANDROID_PRINTF_LOG");
  LogFormat format;
  if (fstr == NULL) {
    format = FORMAT_BRIEF;
  } else {
    if (strcmp(fstr, "brief") == 0)
      format = FORMAT_BRIEF;
    else if (strcmp(fstr, "process") == 0)
      format = FORMAT_PROCESS;
    else if (strcmp(fstr, "tag") == 0)
      format = FORMAT_PROCESS;
    else if (strcmp(fstr, "thread") == 0)
      format = FORMAT_PROCESS;
    else if (strcmp(fstr, "raw") == 0)
      format = FORMAT_PROCESS;
    else if (strcmp(fstr, "time") == 0)
      format = FORMAT_PROCESS;
    else if (strcmp(fstr, "long") == 0)
      format = FORMAT_PROCESS;
    else
      format = (LogFormat)atoi(fstr);  // really?!
  }

  logState->outputFormat = format;
}

/*
 * Return a human-readable string for the priority level.  Always returns
 * a valid string.
 */
static const char* getPriorityString(int priority) {
  /* the first character of each string should be unique */
  static const char* priorityStrings[] = { "Verbose", "Debug", "Info",
                                           "Warn",    "Error", "Assert" };
  int idx;

  idx = (int)priority - (int)ANDROID_LOG_VERBOSE;
  if (idx < 0 ||
      idx >= (int)(sizeof(priorityStrings) / sizeof(priorityStrings[0])))
    return "?unknown?";
  return priorityStrings[idx];
}

#if defined(_WIN32)
/*
 * WIN32 does not have writev().
 * Make up something to replace it.
 */
static ssize_t fake_writev(int fd, const struct iovec* iov, int iovcnt) {
  ssize_t result = 0;
  const struct iovec* end = iov + iovcnt;
  for (; iov < end; iov++) {
    ssize_t w = write(fd, iov->iov_base, iov->iov_len);
    if (w != (ssize_t)iov->iov_len) {
      if (w < 0) return w;
      return result + w;
    }
    result += w;
  }
  return result;
}

#define writev fake_writev
#endif

/*
 * Write a filtered log message to stderr.
 *
 * Log format parsing taken from the long-dead utils/Log.cpp.
 */
static void showLog(LogState* state, int logPrio, const char* tag,
                    const char* msg) {
#if !defined(_WIN32)
  struct tm tmBuf;
#endif
  struct tm* ptm;
  char timeBuf[32];
  char prefixBuf[128], suffixBuf[128];
  char priChar;
  time_t when;
#if !defined(_WIN32)
  pid_t pid, tid;
#else
  uint32_t pid, tid;
#endif

  TRACE("LOG %d: %s %s", logPrio, tag, msg);

  priChar = getPriorityString(logPrio)[0];
  when = time(NULL);
  pid = tid = getpid();  // find gettid()?

/*
 * Get the current date/time in pretty form
 *
 * It's often useful when examining a log with "less" to jump to
 * a specific point in the file by searching for the date/time stamp.
 * For this reason it's very annoying to have regexp meta characters
 * in the time stamp.  Don't use forward slashes, parenthesis,
 * brackets, asterisks, or other special chars here.
 */
#if !defined(_WIN32)
  ptm = localtime_r(&when, &tmBuf);
#else
  ptm = localtime(&when);
#endif
  // strftime(timeBuf, sizeof(timeBuf), "%Y-%m-%d %H:%M:%S", ptm);
  strftime(timeBuf, sizeof(timeBuf), "%m-%d %H:%M:%S", ptm);

  /*
   * Construct a buffer containing the log header and log message.
   */
  size_t prefixLen, suffixLen;

  switch (state->outputFormat) {
    case FORMAT_TAG:
      prefixLen =
          snprintf(prefixBuf, sizeof(prefixBuf), "%c/%-8s: ", priChar, tag);
      strcpy(suffixBuf, "\n");
      suffixLen = 1;
      break;
    case FORMAT_PROCESS:
      prefixLen =
          snprintf(prefixBuf, sizeof(prefixBuf), "%c(%5d) ", priChar, pid);
      suffixLen = snprintf(suffixBuf, sizeof(suffixBuf), "  (%s)\n", tag);
      break;
    case FORMAT_THREAD:
      prefixLen = snprintf(prefixBuf, sizeof(prefixBuf), "%c(%5d:%5d) ",
                           priChar, pid, tid);
      strcpy(suffixBuf, "\n");
      suffixLen = 1;
      break;
    case FORMAT_RAW:
      prefixBuf[0] = 0;
      prefixLen = 0;
      strcpy(suffixBuf, "\n");
      suffixLen = 1;
      break;
    case FORMAT_TIME:
      prefixLen =
          snprintf(prefixBuf, sizeof(prefixBuf), "%s %-8s\n\t", timeBuf, tag);
      strcpy(suffixBuf, "\n");
      suffixLen = 1;
      break;
    case FORMAT_THREADTIME:
      prefixLen =
          snprintf(prefixBuf, sizeof(prefixBuf), "%s %5d %5d %c %-8s \n\t",
                   timeBuf, pid, tid, priChar, tag);
      strcpy(suffixBuf, "\n");
      suffixLen = 1;
      break;
    case FORMAT_LONG:
      prefixLen =
          snprintf(prefixBuf, sizeof(prefixBuf), "[ %s %5d:%5d %c/%-8s ]\n",
                   timeBuf, pid, tid, priChar, tag);
      strcpy(suffixBuf, "\n\n");
      suffixLen = 2;
      break;
    default:
      prefixLen = snprintf(prefixBuf, sizeof(prefixBuf),
                           "%c/%-8s(%5d): ", priChar, tag, pid);
      strcpy(suffixBuf, "\n");
      suffixLen = 1;
      break;
  }

  /*
   * Figure out how many lines there will be.
   */
  const char* end = msg + strlen(msg);
  size_t numLines = 0;
  const char* p = msg;
  while (p < end) {
    if (*p++ == '\n') numLines++;
  }
  if (p > msg && *(p - 1) != '\n') {
    numLines++;
  }

  /*
   * Create an array of iovecs large enough to write all of
   * the lines with a prefix and a suffix.
   */
  const size_t INLINE_VECS = 64;
  const size_t MAX_LINES = ((size_t)~0) / (3 * sizeof(struct iovec*));
  struct iovec stackVec[INLINE_VECS];
  struct iovec* vec = stackVec;
  size_t numVecs;

  if (numLines > MAX_LINES) numLines = MAX_LINES;

  numVecs = numLines * 3;  // 3 iovecs per line.
  if (numVecs > INLINE_VECS) {
    vec = (struct iovec*)malloc(sizeof(struct iovec) * numVecs);
    if (vec == NULL) {
      msg = "LOG: write failed, no memory";
      numVecs = INLINE_VECS;
      numLines = numVecs / 3;
      vec = stackVec;
    }
  }

  /*
   * Fill in the iovec pointers.
   */
  p = msg;
  struct iovec* v = vec;
  int totalLen = 0;
  while (numLines > 0 && p < end) {
    if (prefixLen > 0) {
      v->iov_base = prefixBuf;
      v->iov_len = prefixLen;
      totalLen += prefixLen;
      v++;
    }
    const char* start = p;
    while (p < end && *p != '\n') {
      p++;
    }
    if ((p - start) > 0) {
      v->iov_base = (void*)start;
      v->iov_len = p - start;
      totalLen += p - start;
      v++;
    }
    if (*p == '\n') p++;
    if (suffixLen > 0) {
      v->iov_base = suffixBuf;
      v->iov_len = suffixLen;
      totalLen += suffixLen;
      v++;
    }
    numLines -= 1;
  }

  /*
   * Write the entire message to the log file with a single writev() call.
   * We need to use this rather than a collection of printf()s on a FILE*
   * because of multi-threading and multi-process issues.
   *
   * If the file was not opened with O_APPEND, this will produce interleaved
   * output when called on the same file from multiple processes.
   *
   * If the file descriptor is actually a network socket, the writev()
   * call may return with a partial write.  Putting the writev() call in
   * a loop can result in interleaved data.  This can be alleviated
   * somewhat by wrapping the writev call in the Mutex.
   */

  for (;;) {
    int cc = writev(fileno(stderr), vec, v - vec);

    if (cc == totalLen) break;

    if (cc < 0) {
      if (errno == EINTR) continue;

      /* can't really log the failure; for now, throw out a stderr */
      fprintf(stderr, "+++ LOG: write failed (errno=%d)\n", errno);
      break;
    } else {
      /* shouldn't happen when writing to file or tty */
      fprintf(stderr, "+++ LOG: write partial (%d of %d)\n", cc, totalLen);
      break;
    }
  }

  /* if we allocated storage for the iovecs, free it */
  if (vec != stackVec) free(vec);
}

/*
 * Receive a log message.  We happen to know that "vector" has three parts:
 *
 *  priority (1 byte)
 *  tag (N bytes -- null-terminated ASCII string)
 *  message (N bytes -- null-terminated ASCII string)
 */
static ssize_t logWritev(int fd, const struct iovec* vector, int count) {
  LogState* state;

  /* Make sure that no-one frees the LogState while we're using it.
   * Also guarantees that only one thread is in showLog() at a given
   * time (if it matters).
   */
  lock();

  state = fdToLogState(fd);
  if (state == NULL) {
    errno = EBADF;
    goto error;
  }

  if (state->isBinary) {
    TRACE("%s: ignoring binary log\n", state->debugName);
    goto bail;
  }

  if (count != 3) {
    TRACE("%s: writevLog with count=%d not expected\n", state->debugName, count);
    goto error;
  }

  /* pull out the three fields */
  int logPrio = *(const char*)vector[0].iov_base;
  const char* tag = (const char*)vector[1].iov_base;
  const char* msg = (const char*)vector[2].iov_base;

  /* see if this log tag is configured */
  int i;
  int minPrio = state->globalMinPriority;
  for (i = 0; i < kTagSetSize; i++) {
    if (state->tagSet[i].minPriority == ANDROID_LOG_UNKNOWN)
      break; /* reached end of configured values */

    if (strcmp(state->tagSet[i].tag, tag) == 0) {
      // TRACE("MATCH tag '%s'\n", tag);
      minPrio = state->tagSet[i].minPriority;
      break;
    }
  }

  if (logPrio >= minPrio) {
    showLog(state, logPrio, tag, msg);
  } else {
    // TRACE("+++ NOLOG(%d): %s %s", logPrio, tag, msg);
  }

bail:
  unlock();
  int len = 0;
  for (i = 0; i < count; ++i) {
    len += vector[i].iov_len;
  }
  return len;

error:
  unlock();
  return -1;
}

/*
 * Free up our state and close the fake descriptor.
 */
static int logClose(int fd) {
  deleteFakeFd(fd);
  return 0;
}

/*
 * Open a log output device and return a fake fd.
 */
static int logOpen(const char* pathName, int flags __unused) {
  LogState* logState;
  int fd = -1;

  lock();

  logState = createLogState();
  if (logState != NULL) {
    configureInitialState(pathName, logState);
    fd = logState->fakeFd;
  } else {
    errno = ENFILE;
  }

  unlock();

  return fd;
}

/*
 * Runtime redirection.  If this binary is running in the simulator,
 * just pass log messages to the emulated device.  If it's running
 * outside of the simulator, write the log messages to stderr.
 */

static int (*redirectOpen)(const char* pathName, int flags) = NULL;
static int (*redirectClose)(int fd) = NULL;
static ssize_t (*redirectWritev)(int fd, const struct iovec* vector,
                                 int count) = NULL;

static void setRedirects() {
  const char* ws;

  /* Wrapsim sets this environment variable on children that it's
   * created using its LD_PRELOAD wrapper.
   */
  ws = getenv("ANDROID_WRAPSIM");
  if (ws != NULL && strcmp(ws, "1") == 0) {
    /* We're running inside wrapsim, so we can just write to the device. */
    redirectOpen = (int (*)(const char* pathName, int flags))open;
    redirectClose = close;
    redirectWritev = writev;
  } else {
    /* There's no device to delegate to; handle the logging ourselves. */
    redirectOpen = logOpen;
    redirectClose = logClose;
    redirectWritev = logWritev;
  }
}

LIBLOG_HIDDEN int fakeLogOpen(const char* pathName, int flags) {
  if (redirectOpen == NULL) {
    setRedirects();
  }
  return redirectOpen(pathName, flags);
}

/*
 * The logger API has no means or need to 'stop' or 'close' using the logs,
 * and as such, there is no way for that 'stop' or 'close' to translate into
 * a close operation to the fake log handler. fakeLogClose is provided for
 * completeness only.
 *
 * We have no intention of adding a log close operation as it would complicate
 * every user of the logging API with no gain since the only valid place to
 * call is in the exit handler. Logging can continue in the exit handler to
 * help debug HOST tools ...
 */
LIBLOG_HIDDEN int fakeLogClose(int fd) {
  /* Assume that open() was called first. */
  return redirectClose(fd);
}

LIBLOG_HIDDEN ssize_t fakeLogWritev(int fd, const struct iovec* vector,
                                    int count) {
  /* Assume that open() was called first. */
  return redirectWritev(fd, vector, count);
}

LIBLOG_HIDDEN ssize_t __send_log_msg(char* buf __unused,
                                     size_t buf_size __unused) {
  return -ENODEV;
}

LIBLOG_ABI_PUBLIC int __android_log_is_loggable(int prio,
                                                const char* tag __unused,
                                                int def) {
  int logLevel = def;
  return logLevel >= 0 && prio >= logLevel;
}

LIBLOG_ABI_PUBLIC int __android_log_is_loggable_len(int prio,
                                                    const char* tag __unused,
                                                    size_t len __unused,
                                                    int def) {
  int logLevel = def;
  return logLevel >= 0 && prio >= logLevel;
}

LIBLOG_ABI_PRIVATE int __android_log_is_debuggable() {
  return 1;
}