summaryrefslogblamecommitdiffstats
blob: 76d016c13be50c7edb7e036eabbdafe723ee0c92 (plain) (tree)



















                                                                           
                      
                 


               
                    
                                  
 

                                
                
                       






                                     
                        
                                            
                      


                                       
                              
                     
                                       
                               



                         

                                                                        
                                                                   
                                                   
 
                          
                    
                             
                         
                                                       

                                 



                                       




                                         


                                  
                                           

                                                                



                                                       


                                                             
                                
 






                                                                              
                               
                        
                                                       







                                                     



                             
                 


                       
 


                                     


                                                                      


                              
 


                                   
 
                              





                                                                       




                                                       
     
                               

                                                                           

  
                                              
 
                              
/*
 * Copyright (C) 2012-2013 The Android Open Source Project
 *
 * Licensed under the Apache License, Version 2.0 (the "License");
 * you may not use this file except in compliance with the License.
 * You may obtain a copy of the License at
 *
 *      http://www.apache.org/licenses/LICENSE-2.0
 *
 * Unless required by applicable law or agreed to in writing, software
 * distributed under the License is distributed on an "AS IS" BASIS,
 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
 * See the License for the specific language governing permissions and
 * limitations under the License.
 */

#ifndef _LOGD_LOG_TIMES_H__
#define _LOGD_LOG_TIMES_H__

#include <pthread.h>
#include <sys/types.h>
#include <time.h>

#include <list>

#include <log/log.h>
#include <sysutils/SocketClient.h>

typedef unsigned int log_mask_t;

class LogReader;
class LogBufferElement;

class LogTimeEntry {
    static pthread_mutex_t timesLock;
    unsigned int mRefCount;
    bool mRelease;
    bool mError;
    bool threadRunning;
    bool leadingDropped;
    pthread_cond_t threadTriggeredCondition;
    pthread_t mThread;
    LogReader& mReader;
    static void* threadStart(void* me);
    static void threadStop(void* me);
    const log_mask_t mLogMask;
    const pid_t mPid;
    unsigned int skipAhead[LOG_ID_MAX];
    pid_t mLastTid[LOG_ID_MAX];
    unsigned long mCount;
    unsigned long mTail;
    unsigned long mIndex;

   public:
    LogTimeEntry(LogReader& reader, SocketClient* client, bool nonBlock,
                 unsigned long tail, log_mask_t logMask, pid_t pid,
                 log_time start, uint64_t timeout);

    SocketClient* mClient;
    log_time mStart;
    struct timespec mTimeout;
    const bool mNonBlock;
    const log_time mEnd;  // only relevant if mNonBlock

    // Protect List manipulations
    static void wrlock(void) {
        pthread_mutex_lock(&timesLock);
    }
    static void rdlock(void) {
        pthread_mutex_lock(&timesLock);
    }
    static void unlock(void) {
        pthread_mutex_unlock(&timesLock);
    }

    void startReader_Locked(void);

    bool runningReader_Locked(void) const {
        return threadRunning || mRelease || mError || mNonBlock;
    }
    void triggerReader_Locked(void) {
        pthread_cond_signal(&threadTriggeredCondition);
    }

    void triggerSkip_Locked(log_id_t id, unsigned int skip) {
        skipAhead[id] = skip;
    }
    void cleanSkip_Locked(void);

    // These called after LogTimeEntry removed from list, lock implicitly held
    void release_nodelete_Locked(void) {
        mRelease = true;
        pthread_cond_signal(&threadTriggeredCondition);
        // assumes caller code path will call decRef_Locked()
    }

    void release_Locked(void) {
        mRelease = true;
        pthread_cond_signal(&threadTriggeredCondition);
        if (mRefCount || threadRunning) {
            return;
        }
        // No one else is holding a reference to this
        delete this;
    }

    // Called to mark socket in jeopardy
    void error_Locked(void) {
        mError = true;
    }
    void error(void) {
        wrlock();
        error_Locked();
        unlock();
    }

    bool isError_Locked(void) const {
        return mRelease || mError;
    }

    // Mark Used
    //  Locking implied, grabbed when protection around loop iteration
    void incRef_Locked(void) {
        ++mRefCount;
    }

    bool owned_Locked(void) const {
        return mRefCount != 0;
    }

    void decRef_Locked(void) {
        if ((mRefCount && --mRefCount) || !mRelease || threadRunning) {
            return;
        }
        // No one else is holding a reference to this
        delete this;
    }
    bool isWatching(log_id_t id) const {
        return mLogMask & (1 << id);
    }
    bool isWatchingMultiple(log_mask_t logMask) const {
        return mLogMask & logMask;
    }
    // flushTo filter callbacks
    static int FilterFirstPass(const LogBufferElement* element, void* me);
    static int FilterSecondPass(const LogBufferElement* element, void* me);
};

typedef std::list<LogTimeEntry*> LastLogTimes;

#endif  // _LOGD_LOG_TIMES_H__