diff options
author | Doug Zongker | 2009-10-07 17:06:02 -0500 |
---|---|---|
committer | Doug Zongker | 2009-10-07 17:06:02 -0500 |
commit | 46ef2b87d01a2df67074351d0078bf900550f343 (patch) | |
tree | b4d7f3072dc8182297d549473746474ca27bb311 | |
parent | b084929f5dd57b878f6debe6567a6c8888061fa0 (diff) | |
download | platform-system-core-46ef2b87d01a2df67074351d0078bf900550f343.tar.gz platform-system-core-46ef2b87d01a2df67074351d0078bf900550f343.tar.xz platform-system-core-46ef2b87d01a2df67074351d0078bf900550f343.zip |
add free space on system and cache to free_storage_left log eventandroid-1.6_r2
-rw-r--r-- | logcat/event-log-tags | 26 |
1 files changed, 13 insertions, 13 deletions
diff --git a/logcat/event-log-tags b/logcat/event-log-tags index 6df379230..b5e535cf7 100644 --- a/logcat/event-log-tags +++ b/logcat/event-log-tags | |||
@@ -21,7 +21,7 @@ | |||
21 | # 2: long | 21 | # 2: long |
22 | # 3: string | 22 | # 3: string |
23 | # 4: list | 23 | # 4: list |
24 | # | 24 | # |
25 | # The data unit is a number taken from the following list: | 25 | # The data unit is a number taken from the following list: |
26 | # 1: Number of objects | 26 | # 1: Number of objects |
27 | # 2: Number of bytes | 27 | # 2: Number of bytes |
@@ -58,11 +58,11 @@ | |||
58 | # This is logged when the partial wake lock (keeping the device awake | 58 | # This is logged when the partial wake lock (keeping the device awake |
59 | # regardless of whether the screen is off) is acquired or released. | 59 | # regardless of whether the screen is off) is acquired or released. |
60 | 2729 power_partial_wake_state (releasedorAcquired|1|5),(tag|3) | 60 | 2729 power_partial_wake_state (releasedorAcquired|1|5),(tag|3) |
61 | # This is logged when battery goes from discharging to charging. | 61 | # This is logged when battery goes from discharging to charging. |
62 | # It lets us count the total amount of time between charges and the discharge level | 62 | # It lets us count the total amount of time between charges and the discharge level |
63 | 2730 battery_discharge (duration|2|3),(minLevel|1|6),(maxLevel|1|6) | 63 | 2730 battery_discharge (duration|2|3),(minLevel|1|6),(maxLevel|1|6) |
64 | # | 64 | # |
65 | # Leave IDs through 2739 for more power logs | 65 | # Leave IDs through 2739 for more power logs |
66 | # | 66 | # |
67 | 67 | ||
68 | # This event is logged when the location service uploads location data. | 68 | # This event is logged when the location service uploads location data. |
@@ -79,8 +79,8 @@ | |||
79 | 2744 free_storage_changed (data|2|2) | 79 | 2744 free_storage_changed (data|2|2) |
80 | # Device low memory notification and disk space free on the /data partition, in bytes at that time | 80 | # Device low memory notification and disk space free on the /data partition, in bytes at that time |
81 | 2745 low_storage (data|2|2) | 81 | 2745 low_storage (data|2|2) |
82 | # disk space free on the /data partition in bytes | 82 | # disk space free on the /data, /system, and /cache partitions in bytes |
83 | 2746 free_storage_left (data|2|2) | 83 | 2746 free_storage_left (data|2|2),(system|2|2),(cache|2|2) |
84 | 84 | ||
85 | # when a NotificationManager.notify is called | 85 | # when a NotificationManager.notify is called |
86 | 2750 notification_enqueue (pkg|3),(id|1|5),(notification|3) | 86 | 2750 notification_enqueue (pkg|3),(id|1|5),(notification|3) |
@@ -160,9 +160,9 @@ | |||
160 | 30010 am_proc_bound (PID|1|5),(Process Name|3) | 160 | 30010 am_proc_bound (PID|1|5),(Process Name|3) |
161 | # Application process died | 161 | # Application process died |
162 | 30011 am_proc_died (PID|1|5),(Process Name|3) | 162 | 30011 am_proc_died (PID|1|5),(Process Name|3) |
163 | # The Activity Manager failed to pause the given activity. | 163 | # The Activity Manager failed to pause the given activity. |
164 | 30012 am_failed_to_pause (Token|1|5),(Wanting to pause|3),(Currently pausing|3) | 164 | 30012 am_failed_to_pause (Token|1|5),(Wanting to pause|3),(Currently pausing|3) |
165 | # Attempting to pause the current activity | 165 | # Attempting to pause the current activity |
166 | 30013 am_pause_activity (Token|1|5),(Component Name|3) | 166 | 30013 am_pause_activity (Token|1|5),(Component Name|3) |
167 | # Application process has been started | 167 | # Application process has been started |
168 | 30014 am_proc_start (PID|1|5),(UID|1|5),(Process Name|3),(Type|3),(Component|3) | 168 | 30014 am_proc_start (PID|1|5),(UID|1|5),(Process Name|3),(Type|3),(Component|3) |
@@ -262,28 +262,28 @@ | |||
262 | # Connectivity state changed: | 262 | # Connectivity state changed: |
263 | # [31-13] Reserved for future use | 263 | # [31-13] Reserved for future use |
264 | # [12- 9] Network subtype (for mobile network, as defined by TelephonyManager) | 264 | # [12- 9] Network subtype (for mobile network, as defined by TelephonyManager) |
265 | # [ 8- 3] Detailed state ordinal (as defined by NetworkInfo.DetailedState) | 265 | # [ 8- 3] Detailed state ordinal (as defined by NetworkInfo.DetailedState) |
266 | # [ 2- 0] Network type (as defined by ConnectivityManager) | 266 | # [ 2- 0] Network type (as defined by ConnectivityManager) |
267 | 50020 connectivity_state_changed (custom|1|5) | 267 | 50020 connectivity_state_changed (custom|1|5) |
268 | 268 | ||
269 | # Wi-Fi network state changed: | 269 | # Wi-Fi network state changed: |
270 | # [31- 6] Reserved for future use | 270 | # [31- 6] Reserved for future use |
271 | # [ 5- 0] Detailed state ordinal (as defined by NetworkInfo.DetailedState) | 271 | # [ 5- 0] Detailed state ordinal (as defined by NetworkInfo.DetailedState) |
272 | 50021 wifi_network_state_changed (network_state|1|5) | 272 | 50021 wifi_network_state_changed (network_state|1|5) |
273 | 273 | ||
274 | # Wi-Fi supplicant state changed: | 274 | # Wi-Fi supplicant state changed: |
275 | # [31- 6] Reserved for future use | 275 | # [31- 6] Reserved for future use |
276 | # [ 5- 0] Supplicant state ordinal (as defined by SupplicantState) | 276 | # [ 5- 0] Supplicant state ordinal (as defined by SupplicantState) |
277 | 50022 wifi_supplicant_state_changed (supplicant_state|1|5) | 277 | 50022 wifi_supplicant_state_changed (supplicant_state|1|5) |
278 | 278 | ||
279 | # Wi-Fi driver state changed: | 279 | # Wi-Fi driver state changed: |
280 | # [31- 1] Reserved for future use | 280 | # [31- 1] Reserved for future use |
281 | # [ 0- 0] Driver start (1) or stopped (0) | 281 | # [ 0- 0] Driver start (1) or stopped (0) |
282 | 50023 wifi_driver_state_changed (driver_state|1|5) | 282 | 50023 wifi_driver_state_changed (driver_state|1|5) |
283 | 283 | ||
284 | # Wi-Fi interface configuration state changed: | 284 | # Wi-Fi interface configuration state changed: |
285 | # [31- 1] Reserved for future use | 285 | # [31- 1] Reserved for future use |
286 | # [ 0- 0] Interface configuration succeeded (1) or failed (0) | 286 | # [ 0- 0] Interface configuration succeeded (1) or failed (0) |
287 | 50024 wifi_interface_configuration_state_changed (IP_configuration|1|5) | 287 | 50024 wifi_interface_configuration_state_changed (IP_configuration|1|5) |
288 | 288 | ||
289 | # Wi-Fi supplicant connection state changed: | 289 | # Wi-Fi supplicant connection state changed: |
@@ -333,7 +333,7 @@ | |||
333 | #//device/dalvik/libcore/luni/src/main/native/org_apache_harmony_luni_platform_OSNetworkSystem.c | 333 | #//device/dalvik/libcore/luni/src/main/native/org_apache_harmony_luni_platform_OSNetworkSystem.c |
334 | 51000 socket_stats (send|1|2),(recv|1|2),(ip|1|5),(port|1|5),(close|1|5) | 334 | 51000 socket_stats (send|1|2),(recv|1|2),(ip|1|5),(port|1|5),(close|1|5) |
335 | 335 | ||
336 | # db stats. 0 is query, 1 is write (may become more fine grained in the | 336 | # db stats. 0 is query, 1 is write (may become more fine grained in the |
337 | # future) | 337 | # future) |
338 | 52000 db_operation (name|3),(op_type|1|5),(time|2|3) | 338 | 52000 db_operation (name|3),(op_type|1|5),(time|2|3) |
339 | 339 | ||