summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorTreehugger Robot2018-04-20 15:46:41 -0500
committerGerrit Code Review2018-04-20 15:46:41 -0500
commit656bc2463023ec6a223138131a8f8fc0bf739dd4 (patch)
treec7e80dbb61de53e84bb426708d88b95327a54522
parent395131df7baa7b5a141cd2c48f22dd2a4dfb7091 (diff)
parentf089e1403baa70864869aea4eb680c82f7debbb1 (diff)
downloadplatform-system-core-656bc2463023ec6a223138131a8f8fc0bf739dd4.tar.gz
platform-system-core-656bc2463023ec6a223138131a8f8fc0bf739dd4.tar.xz
platform-system-core-656bc2463023ec6a223138131a8f8fc0bf739dd4.zip
Merge "llkd: add live-lock daemon"
-rw-r--r--libcutils/include/private/android_filesystem_config.h1
-rw-r--r--llkd/Android.bp42
-rw-r--r--llkd/OWNERS2
-rw-r--r--llkd/README.md116
-rw-r--r--llkd/include/llkd.h76
-rw-r--r--llkd/libllkd.cpp1159
-rw-r--r--llkd/llkd.cpp50
-rw-r--r--llkd/llkd.rc18
-rw-r--r--llkd/tests/Android.bp41
-rw-r--r--llkd/tests/llkd_test.cpp243
10 files changed, 1748 insertions, 0 deletions
diff --git a/libcutils/include/private/android_filesystem_config.h b/libcutils/include/private/android_filesystem_config.h
index 8209167e3..3be8ad0ea 100644
--- a/libcutils/include/private/android_filesystem_config.h
+++ b/libcutils/include/private/android_filesystem_config.h
@@ -130,6 +130,7 @@
130#define AID_INCIDENTD 1067 /* incidentd daemon */ 130#define AID_INCIDENTD 1067 /* incidentd daemon */
131#define AID_SECURE_ELEMENT 1068 /* secure element subsystem */ 131#define AID_SECURE_ELEMENT 1068 /* secure element subsystem */
132#define AID_LMKD 1069 /* low memory killer daemon */ 132#define AID_LMKD 1069 /* low memory killer daemon */
133#define AID_LLKD 1070 /* live lock daemon */
133/* Changes to this file must be made in AOSP, *not* in internal branches. */ 134/* Changes to this file must be made in AOSP, *not* in internal branches. */
134 135
135#define AID_SHELL 2000 /* adb and debug shell user */ 136#define AID_SHELL 2000 /* adb and debug shell user */
diff --git a/llkd/Android.bp b/llkd/Android.bp
new file mode 100644
index 000000000..a6edd26ce
--- /dev/null
+++ b/llkd/Android.bp
@@ -0,0 +1,42 @@
1cc_library_headers {
2 name: "llkd_headers",
3
4 export_include_dirs: ["include"],
5}
6
7cc_library_static {
8 name: "libllkd",
9
10 srcs: [
11 "libllkd.cpp",
12 ],
13
14 shared_libs: [
15 "libbase",
16 "libcutils",
17 "liblog",
18 ],
19
20 export_include_dirs: ["include"],
21
22 cflags: ["-Werror"],
23}
24
25cc_binary {
26 name: "llkd",
27
28 srcs: [
29 "llkd.cpp",
30 ],
31 shared_libs: [
32 "libbase",
33 "libcutils",
34 "liblog",
35 ],
36 static_libs: [
37 "libllkd",
38 ],
39 cflags: ["-Werror"],
40
41 init_rc: ["llkd.rc"],
42}
diff --git a/llkd/OWNERS b/llkd/OWNERS
new file mode 100644
index 000000000..b6af537ef
--- /dev/null
+++ b/llkd/OWNERS
@@ -0,0 +1,2 @@
1salyzyn@google.com
2surenb@google.com
diff --git a/llkd/README.md b/llkd/README.md
new file mode 100644
index 000000000..146a99895
--- /dev/null
+++ b/llkd/README.md
@@ -0,0 +1,116 @@
1Android Live-LocK Daemon
2========================
3
4Introduction
5------------
6
7Android Live-LocK Daemon (llkd) is used to catch kernel deadlocks and mitigate.
8
9Code is structured to allow integration into another service as either as part
10of the main loop, or spun off as a thread should that be necessary. A default
11standalone implementation is provided by llkd component.
12
13The 'C' interface from libllkd component is thus:
14
15 #include "llkd.h"
16 bool llkInit(const char* threadname) /* return true if enabled */
17 unsigned llkCheckMillseconds(void) /* ms to sleep for next check */
18
19If a threadname is provided, a thread will be automatically spawned, otherwise
20caller must call llkCheckMilliseconds in its main loop. Function will return
21the period of time before the next expected call to this handler.
22
23Operations
24----------
25
26If a thread is in D or Z state with no forward progress for longer than
27ro.llk.timeout_ms, or ro.llk.[D|Z].timeout_ms, kill the process or parent
28process respectively. If another scan shows the same process continues to
29exist, then have a confirmed live-lock condition and need to panic. Panic
30the kernel in a manner to provide the greatest bugreporting details as to the
31condition. Add a alarm self watchdog should llkd ever get locked up that is
32double the expected time to flow through the mainloop. Sampling is every
33ro.llk_sample_ms.
34
35Default will not monitor init, or [kthreadd] and all that [kthreadd] spawns.
36This reduces the effectiveness of llkd by limiting its coverage. If there is
37value in covering [kthreadd] spawned threads, the requirement will be that
38the drivers not remain in a persistent 'D' state, or that they have mechanisms
39to recover the thread should it be killed externally (this is good driver
40coding hygiene, a common request to add such to publicly reviewed kernel.org
41maintained drivers). For instance use wait_event_interruptible() instead of
42wait_event(). The blacklists can be adjusted accordingly if these
43conditions are met to cover kernel components.
44
45An accompanying gTest set have been added, and will setup a persistent D or Z
46process, with and without forward progress, but not in a live-lock state
47because that would require a buggy kernel, or a module or kernel modification
48to stimulate. The test will check that llkd will mitigate first by killing
49the appropriate process. D state is setup by vfork() waiting for exec() in
50child process. Z state is setup by fork() and an un-waited for child process.
51Should be noted that both of these conditions should never happen on Android
52on purpose, and llkd effectively sweeps up processes that create these
53conditions. If the test can, it will reconfigure llkd to expedite the test
54duration by adjusting the ro.llk.* Android properties. Tests run the D state
55with some scheduling progress to ensure that ABA checking prevents false
56triggers.
57
58Android Properties
59------------------
60
61Android Properties llkd respond to (<prop>_ms parms are in milliseconds):
62
63#### ro.config.low_ram
64default false, if true do not sysrq t (dump all threads).
65
66#### ro.llk.enable
67default false, allow live-lock daemon to be enabled.
68
69#### ro.khungtask.enable
70default false, allow [khungtask] daemon to be enabled.
71
72#### ro.llk.mlockall
73default false, enable call to mlockall().
74
75#### ro.khungtask.timeout
76default value 12 minutes, [khungtask] maximum timelimit.
77
78#### ro.llk.timeout_ms
79default 10 minutes, D or Z maximum timelimit, double this value and it sets
80the alarm watchdog for llkd.
81
82#### ro.llk.D.timeout_ms
83default ro.llk.timeout_ms, D maximum timelimit.
84
85#### ro.llk.Z.timeout_ms
86default ro.llk.timeout_ms, Z maximum timelimit.
87
88#### ro.llk.check_ms
89default 2 minutes samples of threads for D or Z.
90
91#### ro.llk.blacklist.process
92default 0,1,2 (kernel, init and [kthreadd]) plus process names
93init,[kthreadd],[khungtaskd],lmkd,lmkd.llkd,llkd,watchdogd,
94[watchdogd],[watchdogd/0],...,[watchdogd/<get_nprocs-1>].
95
96#### ro.llk.blacklist.parent
97default 0,2 (kernel and [kthreadd]).
98
99#### ro.llk.blacklist.uid
100default <empty>, comma separated list of uid numbers or names.
101
102Architectural Concerns
103----------------------
104
105- Figure out how to communicate the kernel panic better to bootstat canonical
106 boot reason determination. This may require an alteration to bootstat, or
107 some logging from llkd. Would like to see boot reason to be
108 watchdog,livelock as a minimum requirement. Or more specifically would want
109 watchdog,livelock,device or watchdog,livelock,zombie be reported.
110 Currently reports panic,sysrq (user requested panic) or panic depending on
111 system support of pstore.
112- Create kernel module and associated gTest to actually test panic.
113- Create gTest to test out blacklist (ro.llk.blacklist.<properties> generally
114 not be inputs). Could require more test-only interfaces to libllkd.
115- Speed up gTest using something else than ro.llk.<properties>, which should
116 not be inputs.
diff --git a/llkd/include/llkd.h b/llkd/include/llkd.h
new file mode 100644
index 000000000..2ae28ed77
--- /dev/null
+++ b/llkd/include/llkd.h
@@ -0,0 +1,76 @@
1/*
2 * Copyright (C) 2018 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#ifndef _LLKD_H_
18#define _LLKD_H_
19
20#ifndef LOG_TAG
21#define LOG_TAG "livelock"
22#endif
23
24#include <stdbool.h>
25#include <sys/cdefs.h>
26
27__BEGIN_DECLS
28
29bool llkInit(const char* threadname); /* threadname NULL, not spawned */
30unsigned llkCheckMilliseconds(void);
31
32/* clang-format off */
33#define LLK_ENABLE_PROPERTY "ro.llk.enable"
34#define LLK_ENABLE_DEFAULT false
35#define KHT_ENABLE_PROPERTY "ro.khungtask.enable"
36#define LLK_MLOCKALL_PROPERTY "ro.llk.mlockall"
37#define LLK_MLOCKALL_DEFAULT true
38#define LLK_TIMEOUT_MS_PROPERTY "ro.llk.timeout_ms"
39#define KHT_TIMEOUT_PROPERTY "ro.khungtask.timeout"
40#define LLK_D_TIMEOUT_MS_PROPERTY "ro.llk.D.timeout_ms"
41#define LLK_Z_TIMEOUT_MS_PROPERTY "ro.llk.Z.timeout_ms"
42#define LLK_CHECK_MS_PROPERTY "ro.llk.check_ms"
43/* LLK_CHECK_MS_DEFAULT = actual timeout_ms / LLK_CHECKS_PER_TIMEOUT_DEFAULT */
44#define LLK_CHECKS_PER_TIMEOUT_DEFAULT 5
45#define LLK_BLACKLIST_PROCESS_PROPERTY "ro.llk.blacklist.process"
46#define LLK_BLACKLIST_PROCESS_DEFAULT \
47 "0,1,2,init,[kthreadd],[khungtaskd],lmkd,lmkd.llkd,llkd,watchdogd,[watchdogd],[watchdogd/0]"
48#define LLK_BLACKLIST_PARENT_PROPERTY "ro.llk.blacklist.parent"
49#define LLK_BLACKLIST_PARENT_DEFAULT "0,2,[kthreadd]"
50#define LLK_BLACKLIST_UID_PROPERTY "ro.llk.blacklist.uid"
51#define LLK_BLACKLIST_UID_DEFAULT ""
52/* clang-format on */
53
54__END_DECLS
55
56#ifdef __cplusplus
57extern "C++" { /* In case this included wrapped with __BEGIN_DECLS */
58
59#include <chrono>
60
61__BEGIN_DECLS
62/* C++ code allowed to not specify threadname argument for this C linkage */
63bool llkInit(const char* threadname = nullptr);
64__END_DECLS
65std::chrono::milliseconds llkCheck(bool checkRunning = false);
66
67/* clang-format off */
68#define LLK_TIMEOUT_MS_DEFAULT std::chrono::duration_cast<milliseconds>(std::chrono::minutes(10))
69#define LLK_TIMEOUT_MS_MINIMUM std::chrono::duration_cast<std::chrono::milliseconds>(std::chrono::seconds(10))
70#define LLK_CHECK_MS_MINIMUM std::chrono::duration_cast<std::chrono::milliseconds>(std::chrono::seconds(1))
71/* clang-format on */
72
73} /* extern "C++" */
74#endif /* __cplusplus */
75
76#endif /* _LLKD_H_ */
diff --git a/llkd/libllkd.cpp b/llkd/libllkd.cpp
new file mode 100644
index 000000000..b25eb06c0
--- /dev/null
+++ b/llkd/libllkd.cpp
@@ -0,0 +1,1159 @@
1/*
2 * Copyright (C) 2018 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#include "llkd.h"
18
19#include <ctype.h>
20#include <dirent.h> // opendir() and readdir()
21#include <errno.h>
22#include <fcntl.h>
23#include <pthread.h>
24#include <pwd.h> // getpwuid()
25#include <signal.h>
26#include <stdint.h>
27#include <sys/cdefs.h> // ___STRING, __predict_true() and _predict_false()
28#include <sys/mman.h> // mlockall()
29#include <sys/prctl.h>
30#include <sys/stat.h> // lstat()
31#include <sys/syscall.h> // __NR_getdents64
32#include <sys/sysinfo.h> // get_nprocs_conf()
33#include <sys/types.h>
34#include <time.h>
35#include <unistd.h>
36
37#include <chrono>
38#include <ios>
39#include <sstream>
40#include <string>
41#include <unordered_map>
42#include <unordered_set>
43
44#include <android-base/file.h>
45#include <android-base/logging.h>
46#include <android-base/parseint.h>
47#include <android-base/properties.h>
48#include <android-base/strings.h>
49#include <cutils/android_get_control_file.h>
50#include <log/log_main.h>
51
52#define ARRAY_SIZE(x) (sizeof(x) / sizeof(*(x)))
53
54#define TASK_COMM_LEN 16 // internal kernel, not uapi, from .../linux/include/linux/sched.h
55
56using namespace std::chrono_literals;
57using namespace std::chrono;
58
59namespace {
60
61constexpr pid_t kernelPid = 0;
62constexpr pid_t initPid = 1;
63constexpr pid_t kthreaddPid = 2;
64
65constexpr char procdir[] = "/proc/";
66
67// Configuration
68milliseconds llkUpdate; // last check ms signature
69milliseconds llkCycle; // ms to next thread check
70bool llkEnable = LLK_ENABLE_DEFAULT; // llk daemon enabled
71bool llkRunning = false; // thread is running
72bool llkMlockall = LLK_MLOCKALL_DEFAULT; // run mlocked
73milliseconds llkTimeoutMs = LLK_TIMEOUT_MS_DEFAULT; // default timeout
74enum { llkStateD, llkStateZ, llkNumStates }; // state indexes
75milliseconds llkStateTimeoutMs[llkNumStates]; // timeout override for each detection state
76milliseconds llkCheckMs; // checking interval to inspect any
77 // persistent live-locked states
78bool llkLowRam; // ro.config.low_ram
79bool khtEnable = LLK_ENABLE_DEFAULT; // [khungtaskd] panic
80// [khungtaskd] should have a timeout beyond the granularity of llkTimeoutMs.
81// Provides a wide angle of margin b/c khtTimeout is also its granularity.
82seconds khtTimeout = duration_cast<seconds>(llkTimeoutMs * (1 + LLK_CHECKS_PER_TIMEOUT_DEFAULT) /
83 LLK_CHECKS_PER_TIMEOUT_DEFAULT);
84
85// Blacklist variables, initialized with comma separated lists of high false
86// positive and/or dangerous references, e.g. without self restart, for pid,
87// ppid, name and uid:
88
89// list of pids, or tids or names to skip. kernel pid (0), init pid (1),
90// [kthreadd] pid (2), ourselves, "init", "[kthreadd]", "lmkd", "llkd" or
91// combinations of watchdogd in kernel and user space.
92std::unordered_set<std::string> llkBlacklistProcess;
93// list of parent pids, comm or cmdline names to skip. default:
94// kernel pid (0), [kthreadd] (2), or ourselves, enforced and implied
95std::unordered_set<std::string> llkBlacklistParent;
96// list of uids, and uid names, to skip, default nothing
97std::unordered_set<std::string> llkBlacklistUid;
98
99class dir {
100 public:
101 enum level { proc, task, numLevels };
102
103 private:
104 int fd;
105 size_t available_bytes;
106 dirent* next;
107 // each directory level picked to be just north of 4K in size
108 static constexpr size_t buffEntries = 15;
109 static dirent buff[numLevels][buffEntries];
110
111 bool fill(enum level index) {
112 if (index >= numLevels) return false;
113 if (available_bytes != 0) return true;
114 if (__predict_false(fd < 0)) return false;
115 // getdents64 has no libc wrapper
116 auto rc = TEMP_FAILURE_RETRY(syscall(__NR_getdents64, fd, buff[index], sizeof(buff[0]), 0));
117 if (rc <= 0) return false;
118 available_bytes = rc;
119 next = buff[index];
120 return true;
121 }
122
123 public:
124 dir() : fd(-1), available_bytes(0), next(nullptr) {}
125
126 explicit dir(const char* directory)
127 : fd(__predict_true(directory != nullptr)
128 ? ::open(directory, O_CLOEXEC | O_DIRECTORY | O_RDONLY)
129 : -1),
130 available_bytes(0),
131 next(nullptr) {}
132
133 explicit dir(const std::string&& directory)
134 : fd(::open(directory.c_str(), O_CLOEXEC | O_DIRECTORY | O_RDONLY)),
135 available_bytes(0),
136 next(nullptr) {}
137
138 explicit dir(const std::string& directory)
139 : fd(::open(directory.c_str(), O_CLOEXEC | O_DIRECTORY | O_RDONLY)),
140 available_bytes(0),
141 next(nullptr) {}
142
143 // Don't need any copy or move constructors.
144 explicit dir(const dir& c) = delete;
145 explicit dir(dir& c) = delete;
146 explicit dir(dir&& c) = delete;
147
148 ~dir() {
149 if (fd >= 0) {
150 ::close(fd);
151 }
152 }
153
154 operator bool() const { return fd >= 0; }
155
156 void reset(void) {
157 if (fd >= 0) {
158 ::close(fd);
159 fd = -1;
160 available_bytes = 0;
161 next = nullptr;
162 }
163 }
164
165 dir& reset(const char* directory) {
166 reset();
167 // available_bytes will _always_ be zero here as its value is
168 // intimately tied to fd < 0 or not.
169 fd = ::open(directory, O_CLOEXEC | O_DIRECTORY | O_RDONLY);
170 return *this;
171 }
172
173 void rewind(void) {
174 if (fd >= 0) {
175 ::lseek(fd, off_t(0), SEEK_SET);
176 available_bytes = 0;
177 next = nullptr;
178 }
179 }
180
181 dirent* read(enum level index = proc, dirent* def = nullptr) {
182 if (!fill(index)) return def;
183 auto ret = next;
184 available_bytes -= next->d_reclen;
185 next = reinterpret_cast<dirent*>(reinterpret_cast<char*>(next) + next->d_reclen);
186 return ret;
187 }
188} llkTopDirectory;
189
190dirent dir::buff[dir::numLevels][dir::buffEntries];
191
192// helper functions
193
194bool llkIsMissingExeLink(pid_t tid) {
195 char c;
196 // CAP_SYS_PTRACE is required to prevent ret == -1, but ENOENT is signal
197 auto ret = ::readlink((procdir + std::to_string(tid) + "/exe").c_str(), &c, sizeof(c));
198 return (ret == -1) && (errno == ENOENT);
199}
200
201// Common routine where caller accepts empty content as error/passthrough.
202// Reduces the churn of reporting read errors in the callers.
203std::string ReadFile(std::string&& path) {
204 std::string content;
205 if (!android::base::ReadFileToString(path, &content)) {
206 PLOG(DEBUG) << "Read " << path << " failed";
207 content = "";
208 }
209 return content;
210}
211
212std::string llkProcGetName(pid_t tid, const char* node = "/cmdline") {
213 std::string content = ReadFile(procdir + std::to_string(tid) + node);
214 static constexpr char needles[] = " \t\r\n"; // including trailing nul
215 auto pos = content.find_first_of(needles, 0, sizeof(needles));
216 if (pos != std::string::npos) {
217 content.erase(pos);
218 }
219 return content;
220}
221
222uid_t llkProcGetUid(pid_t tid) {
223 // Get the process' uid. The following read from /status is admittedly
224 // racy, prone to corruption due to shape-changes. The consequences are
225 // not catastrophic as we sample a few times before taking action.
226 //
227 // If /loginuid worked on reliably, or on Android (all tasks report -1)...
228 // Android lmkd causes /cgroup to contain memory:/<dom>/uid_<uid>/pid_<pid>
229 // which is tighter, but also not reliable.
230 std::string content = ReadFile(procdir + std::to_string(tid) + "/status");
231 static constexpr char Uid[] = "\nUid:";
232 auto pos = content.find(Uid);
233 if (pos == std::string::npos) {
234 return -1;
235 }
236 pos += ::strlen(Uid);
237 while ((pos < content.size()) && ::isblank(content[pos])) {
238 ++pos;
239 }
240 content.erase(0, pos);
241 for (pos = 0; (pos < content.size()) && ::isdigit(content[pos]); ++pos) {
242 ;
243 }
244 // Content of form 'Uid: 0 0 0 0', newline is error
245 if ((pos >= content.size()) || !::isblank(content[pos])) {
246 return -1;
247 }
248 content.erase(pos);
249 uid_t ret;
250 if (!android::base::ParseInt(content, &ret, uid_t(0))) {
251 return -1;
252 }
253 return ret;
254}
255
256struct proc {
257 pid_t tid; // monitored thread id (in Z or D state).
258 nanoseconds schedUpdate; // /proc/<tid>/sched "se.avg.lastUpdateTime",
259 uint64_t nrSwitches; // /proc/<tid>/sched "nr_switches" for
260 // refined ABA problem detection, determine
261 // forward scheduling progress.
262 milliseconds update; // llkUpdate millisecond signature of last.
263 milliseconds count; // duration in state.
264 pid_t pid; // /proc/<pid> before iterating through
265 // /proc/<pid>/task/<tid> for threads.
266 pid_t ppid; // /proc/<tid>/stat field 4 parent pid.
267 uid_t uid; // /proc/<tid>/status Uid: field.
268 unsigned time; // sum of /proc/<tid>/stat field 14 utime &
269 // 15 stime for coarse ABA problem detection.
270 std::string cmdline; // cached /cmdline content
271 char state; // /proc/<tid>/stat field 3: Z or D
272 // (others we do not monitor: S, R, T or ?)
273 char comm[TASK_COMM_LEN + 3]; // space for adding '[' and ']'
274 bool exeMissingValid; // exeMissing has been cached
275 bool cmdlineValid; // cmdline has been cached
276 bool updated; // cleared before monitoring pass.
277 bool killed; // sent a kill to this thread, next panic...
278
279 void setComm(const char* _comm) { strncpy(comm + 1, _comm, sizeof(comm) - 2); }
280
281 proc(pid_t tid, pid_t pid, pid_t ppid, const char* _comm, int time, char state)
282 : tid(tid),
283 schedUpdate(0),
284 nrSwitches(0),
285 update(llkUpdate),
286 count(0),
287 pid(pid),
288 ppid(ppid),
289 uid(-1),
290 time(time),
291 state(state),
292 exeMissingValid(false),
293 cmdlineValid(false),
294 updated(true),
295 killed(false) {
296 memset(comm, '\0', sizeof(comm));
297 setComm(_comm);
298 }
299
300 const char* getComm(void) {
301 if (comm[1] == '\0') { // comm Valid?
302 strncpy(comm + 1, llkProcGetName(tid, "/comm").c_str(), sizeof(comm) - 2);
303 }
304 if (!exeMissingValid) {
305 if (llkIsMissingExeLink(tid)) {
306 comm[0] = '[';
307 }
308 exeMissingValid = true;
309 }
310 size_t len = strlen(comm + 1);
311 if (__predict_true(len < (sizeof(comm) - 1))) {
312 if (comm[0] == '[') {
313 if ((comm[len] != ']') && __predict_true(len < (sizeof(comm) - 2))) {
314 comm[++len] = ']';
315 comm[++len] = '\0';
316 }
317 } else {
318 if (comm[len] == ']') {
319 comm[len] = '\0';
320 }
321 }
322 }
323 return &comm[comm[0] != '['];
324 }
325
326 const char* getCmdline(void) {
327 if (!cmdlineValid) {
328 cmdline = llkProcGetName(tid);
329 cmdlineValid = true;
330 }
331 return cmdline.c_str();
332 }
333
334 uid_t getUid(void) {
335 if (uid <= 0) { // Churn on root user, because most likely to setuid()
336 uid = llkProcGetUid(tid);
337 }
338 return uid;
339 }
340
341 void reset(void) { // reset cache, if we detected pid rollover
342 uid = -1;
343 state = '?';
344 cmdline = "";
345 comm[0] = '\0';
346 exeMissingValid = false;
347 cmdlineValid = false;
348 }
349};
350
351std::unordered_map<pid_t, proc> tids;
352
353// Check range and setup defaults, in order of propagation:
354// llkTimeoutMs
355// llkCheckMs
356// ...
357// KISS to keep it all self-contained, and called multiple times as parameters
358// are interpreted so that defaults, llkCheckMs and llkCycle make sense.
359void llkValidate() {
360 if (llkTimeoutMs == 0ms) {
361 llkTimeoutMs = LLK_TIMEOUT_MS_DEFAULT;
362 }
363 llkTimeoutMs = std::max(llkTimeoutMs, LLK_TIMEOUT_MS_MINIMUM);
364 if (llkCheckMs == 0ms) {
365 llkCheckMs = llkTimeoutMs / LLK_CHECKS_PER_TIMEOUT_DEFAULT;
366 }
367 llkCheckMs = std::min(llkCheckMs, llkTimeoutMs);
368
369 for (size_t state = 0; state < ARRAY_SIZE(llkStateTimeoutMs); ++state) {
370 if (llkStateTimeoutMs[state] == 0ms) {
371 llkStateTimeoutMs[state] = llkTimeoutMs;
372 }
373 llkStateTimeoutMs[state] =
374 std::min(std::max(llkStateTimeoutMs[state], LLK_TIMEOUT_MS_MINIMUM), llkTimeoutMs);
375 llkCheckMs = std::min(llkCheckMs, llkStateTimeoutMs[state]);
376 }
377
378 llkCheckMs = std::max(llkCheckMs, LLK_CHECK_MS_MINIMUM);
379 if (llkCycle == 0ms) {
380 llkCycle = llkCheckMs;
381 }
382 llkCycle = std::min(llkCycle, llkCheckMs);
383}
384
385milliseconds llkGetTimespecDiffMs(timespec* from, timespec* to) {
386 return duration_cast<milliseconds>(seconds(to->tv_sec - from->tv_sec)) +
387 duration_cast<milliseconds>(nanoseconds(to->tv_nsec - from->tv_nsec));
388}
389
390std::string llkProcGetName(pid_t tid, const char* comm, const char* cmdline) {
391 if ((cmdline != nullptr) && (*cmdline != '\0')) {
392 return cmdline;
393 }
394 if ((comm != nullptr) && (*comm != '\0')) {
395 return comm;
396 }
397
398 // UNLIKELY! Here because killed before we kill it?
399 // Assume change is afoot, do not call llkTidAlloc
400
401 // cmdline ?
402 std::string content = llkProcGetName(tid);
403 if (content.size() != 0) {
404 return content;
405 }
406 // Comm instead?
407 content = llkProcGetName(tid, "/comm");
408 if (llkIsMissingExeLink(tid) && (content.size() != 0)) {
409 return '[' + content + ']';
410 }
411 return content;
412}
413
414int llkKillOneProcess(pid_t pid, char state, pid_t tid, const char* tcomm = nullptr,
415 const char* tcmdline = nullptr, const char* pcomm = nullptr,
416 const char* pcmdline = nullptr) {
417 std::string forTid;
418 if (tid != pid) {
419 forTid = " for '" + llkProcGetName(tid, tcomm, tcmdline) + "' (" + std::to_string(tid) + ")";
420 }
421 LOG(INFO) << "Killing '" << llkProcGetName(pid, pcomm, pcmdline) << "' (" << pid
422 << ") to check forward scheduling progress in " << state << " state" << forTid;
423 // CAP_KILL required
424 errno = 0;
425 auto r = ::kill(pid, SIGKILL);
426 if (r) {
427 PLOG(ERROR) << "kill(" << pid << ")=" << r << ' ';
428 }
429
430 return r;
431}
432
433// Kill one process
434int llkKillOneProcess(pid_t pid, proc* tprocp) {
435 return llkKillOneProcess(pid, tprocp->state, tprocp->tid, tprocp->getComm(),
436 tprocp->getCmdline());
437}
438
439// Kill one process specified by kprocp
440int llkKillOneProcess(proc* kprocp, proc* tprocp) {
441 if (kprocp == nullptr) {
442 return -2;
443 }
444
445 return llkKillOneProcess(kprocp->tid, tprocp->state, tprocp->tid, tprocp->getComm(),
446 tprocp->getCmdline(), kprocp->getComm(), kprocp->getCmdline());
447}
448
449// Acquire file descriptor from environment, or open and cache it.
450// NB: cache is unnecessary in our current context, pedantically
451// required to prevent leakage of file descriptors in the future.
452int llkFileToWriteFd(const std::string& file) {
453 static std::unordered_map<std::string, int> cache;
454 auto search = cache.find(file);
455 if (search != cache.end()) return search->second;
456 auto fd = android_get_control_file(file.c_str());
457 if (fd >= 0) return fd;
458 fd = TEMP_FAILURE_RETRY(::open(file.c_str(), O_WRONLY | O_CLOEXEC));
459 if (fd >= 0) cache.emplace(std::make_pair(file, fd));
460 return fd;
461}
462
463// Wrap android::base::WriteStringToFile to use android_get_control_file.
464bool llkWriteStringToFile(const std::string& string, const std::string& file) {
465 auto fd = llkFileToWriteFd(file);
466 if (fd < 0) return false;
467 return android::base::WriteStringToFd(string, fd);
468}
469
470bool llkWriteStringToFileConfirm(const std::string& string, const std::string& file) {
471 auto fd = llkFileToWriteFd(file);
472 auto ret = (fd < 0) ? false : android::base::WriteStringToFd(string, fd);
473 std::string content;
474 if (!android::base::ReadFileToString(file, &content)) return ret;
475 return android::base::Trim(content) == string;
476}
477
478void llkPanicKernel(bool dump, pid_t tid) __noreturn;
479void llkPanicKernel(bool dump, pid_t tid) {
480 auto sysrqTriggerFd = llkFileToWriteFd("/proc/sysrq-trigger");
481 if (sysrqTriggerFd < 0) {
482 // DYB
483 llkKillOneProcess(initPid, 'R', tid);
484 // The answer to life, the universe and everything
485 ::exit(42);
486 // NOTREACHED
487 }
488 ::sync();
489 if (dump) {
490 // Show all locks that are held
491 android::base::WriteStringToFd("d", sysrqTriggerFd);
492 // This can trigger hardware watchdog, that is somewhat _ok_.
493 // But useless if pstore configured for <256KB, low ram devices ...
494 if (!llkLowRam) {
495 android::base::WriteStringToFd("t", sysrqTriggerFd);
496 }
497 ::usleep(200000); // let everything settle
498 }
499 android::base::WriteStringToFd("c", sysrqTriggerFd);
500 // NOTREACHED
501 // DYB
502 llkKillOneProcess(initPid, 'R', tid);
503 // I sat at my desk, stared into the garden and thought '42 will do'.
504 // I typed it out. End of story
505 ::exit(42);
506 // NOTREACHED
507}
508
509void llkAlarmHandler(int) {
510 llkPanicKernel(false, ::getpid());
511}
512
513milliseconds GetUintProperty(const std::string& key, milliseconds def) {
514 return milliseconds(android::base::GetUintProperty(key, static_cast<uint64_t>(def.count()),
515 static_cast<uint64_t>(def.max().count())));
516}
517
518seconds GetUintProperty(const std::string& key, seconds def) {
519 return seconds(android::base::GetUintProperty(key, static_cast<uint64_t>(def.count()),
520 static_cast<uint64_t>(def.max().count())));
521}
522
523proc* llkTidLookup(pid_t tid) {
524 auto search = tids.find(tid);
525 if (search == tids.end()) {
526 return nullptr;
527 }
528 return &search->second;
529}
530
531void llkTidRemove(pid_t tid) {
532 tids.erase(tid);
533}
534
535proc* llkTidAlloc(pid_t tid, pid_t pid, pid_t ppid, const char* comm, int time, char state) {
536 auto it = tids.emplace(std::make_pair(tid, proc(tid, pid, ppid, comm, time, state)));
537 return &it.first->second;
538}
539
540std::string llkFormat(milliseconds ms) {
541 auto sec = duration_cast<seconds>(ms);
542 std::ostringstream s;
543 s << sec.count() << '.';
544 auto f = s.fill('0');
545 auto w = s.width(3);
546 s << std::right << (ms - sec).count();
547 s.width(w);
548 s.fill(f);
549 s << 's';
550 return s.str();
551}
552
553std::string llkFormat(seconds s) {
554 return std::to_string(s.count()) + 's';
555}
556
557std::string llkFormat(bool flag) {
558 return flag ? "true" : "false";
559}
560
561std::string llkFormat(const std::unordered_set<std::string>& blacklist) {
562 std::string ret;
563 for (auto entry : blacklist) {
564 if (ret.size()) {
565 ret += ",";
566 }
567 ret += entry;
568 }
569 return ret;
570}
571
572// We only officially support comma separators, but wetware being what they
573// are will take some liberty and I do not believe they should be punished.
574std::unordered_set<std::string> llkSplit(const std::string& s,
575 const std::string& delimiters = ", \t:") {
576 std::unordered_set<std::string> result;
577
578 size_t base = 0;
579 size_t found;
580 while (true) {
581 found = s.find_first_of(delimiters, base);
582 result.emplace(s.substr(base, found - base));
583 if (found == s.npos) break;
584 base = found + 1;
585 }
586 return result;
587}
588
589bool llkSkipName(const std::string& name,
590 const std::unordered_set<std::string>& blacklist = llkBlacklistProcess) {
591 if ((name.size() == 0) || (blacklist.size() == 0)) {
592 return false;
593 }
594
595 return blacklist.find(name) != blacklist.end();
596}
597
598bool llkSkipPid(pid_t pid) {
599 return llkSkipName(std::to_string(pid), llkBlacklistProcess);
600}
601
602bool llkSkipPpid(pid_t ppid) {
603 return llkSkipName(std::to_string(ppid), llkBlacklistParent);
604}
605
606bool llkSkipUid(uid_t uid) {
607 // Match by number?
608 if (llkSkipName(std::to_string(uid), llkBlacklistUid)) {
609 return true;
610 }
611
612 // Match by name?
613 auto pwd = ::getpwuid(uid);
614 return (pwd != nullptr) && __predict_true(pwd->pw_name != nullptr) &&
615 __predict_true(pwd->pw_name[0] != '\0') && llkSkipName(pwd->pw_name, llkBlacklistUid);
616}
617
618bool getValidTidDir(dirent* dp, std::string* piddir) {
619 if (!::isdigit(dp->d_name[0])) {
620 return false;
621 }
622
623 // Corner case can not happen in reality b/c of above ::isdigit check
624 if (__predict_false(dp->d_type != DT_DIR)) {
625 if (__predict_false(dp->d_type == DT_UNKNOWN)) { // can't b/c procfs
626 struct stat st;
627 *piddir = procdir;
628 *piddir += dp->d_name;
629 return (lstat(piddir->c_str(), &st) == 0) && (st.st_mode & S_IFDIR);
630 }
631 return false;
632 }
633
634 *piddir = procdir;
635 *piddir += dp->d_name;
636 return true;
637}
638
639bool llkIsMonitorState(char state) {
640 return (state == 'Z') || (state == 'D');
641}
642
643// returns -1 if not found
644long long getSchedValue(const std::string& schedString, const char* key) {
645 auto pos = schedString.find(key);
646 if (pos == std::string::npos) {
647 return -1;
648 }
649 pos = schedString.find(':', pos);
650 if (__predict_false(pos == std::string::npos)) {
651 return -1;
652 }
653 while ((++pos < schedString.size()) && ::isblank(schedString[pos])) {
654 ;
655 }
656 long long ret;
657 if (!android::base::ParseInt(schedString.substr(pos), &ret, static_cast<long long>(0))) {
658 return -1;
659 }
660 return ret;
661}
662
663// Primary ABA mitigation watching last time schedule activity happened
664void llkCheckSchedUpdate(proc* procp, const std::string& piddir) {
665 // Audit finds /proc/<tid>/sched is just over 1K, and
666 // is rarely larger than 2K, even less on Android.
667 // For example, the "se.avg.lastUpdateTime" field we are
668 // interested in typically within the primary set in
669 // the first 1K.
670 //
671 // Proc entries can not be read >1K atomically via libbase,
672 // but if there are problems we assume at least a few
673 // samples of reads occur before we take any real action.
674 std::string schedString = ReadFile(piddir + "/sched");
675 if (schedString.size() == 0) {
676 // /schedstat is not as standardized, but in 3.1+
677 // Android devices, the third field is nr_switches
678 // from /sched:
679 schedString = ReadFile(piddir + "/schedstat");
680 if (schedString.size() == 0) {
681 return;
682 }
683 auto val = static_cast<unsigned long long>(-1);
684 if (((::sscanf(schedString.c_str(), "%*d %*d %llu", &val)) == 1) &&
685 (val != static_cast<unsigned long long>(-1)) && (val != 0) &&
686 (val != procp->nrSwitches)) {
687 procp->nrSwitches = val;
688 procp->count = 0ms;
689 procp->killed = false;
690 }
691 return;
692 }
693
694 auto val = getSchedValue(schedString, "\nse.avg.lastUpdateTime");
695 if (val == -1) {
696 val = getSchedValue(schedString, "\nse.svg.last_update_time");
697 }
698 if (val != -1) {
699 auto schedUpdate = nanoseconds(val);
700 if (schedUpdate != procp->schedUpdate) {
701 procp->schedUpdate = schedUpdate;
702 procp->count = 0ms;
703 procp->killed = false;
704 }
705 }
706
707 val = getSchedValue(schedString, "\nnr_switches");
708 if (val != -1) {
709 if (static_cast<uint64_t>(val) != procp->nrSwitches) {
710 procp->nrSwitches = val;
711 procp->count = 0ms;
712 procp->killed = false;
713 }
714 }
715}
716
717void llkLogConfig(void) {
718 LOG(INFO) << "ro.config.low_ram=" << llkFormat(llkLowRam) << "\n"
719 << LLK_ENABLE_PROPERTY "=" << llkFormat(llkEnable) << "\n"
720 << KHT_ENABLE_PROPERTY "=" << llkFormat(khtEnable) << "\n"
721 << LLK_MLOCKALL_PROPERTY "=" << llkFormat(llkMlockall) << "\n"
722 << KHT_TIMEOUT_PROPERTY "=" << llkFormat(khtTimeout) << "\n"
723 << LLK_TIMEOUT_MS_PROPERTY "=" << llkFormat(llkTimeoutMs) << "\n"
724 << LLK_D_TIMEOUT_MS_PROPERTY "=" << llkFormat(llkStateTimeoutMs[llkStateD]) << "\n"
725 << LLK_Z_TIMEOUT_MS_PROPERTY "=" << llkFormat(llkStateTimeoutMs[llkStateZ]) << "\n"
726 << LLK_CHECK_MS_PROPERTY "=" << llkFormat(llkCheckMs) << "\n"
727 << LLK_BLACKLIST_PROCESS_PROPERTY "=" << llkFormat(llkBlacklistProcess) << "\n"
728 << LLK_BLACKLIST_PARENT_PROPERTY "=" << llkFormat(llkBlacklistParent) << "\n"
729 << LLK_BLACKLIST_UID_PROPERTY "=" << llkFormat(llkBlacklistUid);
730}
731
732void* llkThread(void* obj) {
733 LOG(INFO) << "started";
734
735 std::string name = std::to_string(::gettid());
736 if (!llkSkipName(name)) {
737 llkBlacklistProcess.emplace(name);
738 }
739 name = static_cast<const char*>(obj);
740 prctl(PR_SET_NAME, name.c_str());
741 if (__predict_false(!llkSkipName(name))) {
742 llkBlacklistProcess.insert(name);
743 }
744 // No longer modifying llkBlacklistProcess.
745 llkRunning = true;
746 llkLogConfig();
747 while (llkRunning) {
748 ::usleep(duration_cast<microseconds>(llkCheck(true)).count());
749 }
750 // NOTREACHED
751 LOG(INFO) << "exiting";
752 return nullptr;
753}
754
755} // namespace
756
757milliseconds llkCheck(bool checkRunning) {
758 if (!llkEnable || (checkRunning != llkRunning)) {
759 return milliseconds::max();
760 }
761
762 // Reset internal watchdog, which is a healthy engineering margin of
763 // double the maximum wait or cycle time for the mainloop that calls us.
764 //
765 // This alarm is effectively the live lock detection of llkd, as
766 // we understandably can not monitor ourselves otherwise.
767 ::alarm(duration_cast<seconds>(llkTimeoutMs * 2).count());
768
769 // kernel jiffy precision fastest acquisition
770 static timespec last;
771 timespec now;
772 ::clock_gettime(CLOCK_MONOTONIC_COARSE, &now);
773 auto ms = llkGetTimespecDiffMs(&last, &now);
774 if (ms < llkCycle) {
775 return llkCycle - ms;
776 }
777 last = now;
778
779 LOG(VERBOSE) << "opendir(\"" << procdir << "\")";
780 if (__predict_false(!llkTopDirectory)) {
781 // gid containing AID_READPROC required
782 llkTopDirectory.reset(procdir);
783 if (__predict_false(!llkTopDirectory)) {
784 // Most likely reason we could be here is a resource limit.
785 // Keep our processing down to a minimum, but not so low that
786 // we do not recover in a timely manner should the issue be
787 // transitory.
788 LOG(DEBUG) << "opendir(\"" << procdir << "\") failed";
789 return llkTimeoutMs;
790 }
791 }
792
793 for (auto& it : tids) {
794 it.second.updated = false;
795 }
796
797 auto prevUpdate = llkUpdate;
798 llkUpdate += ms;
799 ms -= llkCycle;
800 auto myPid = ::getpid();
801 auto myTid = ::gettid();
802 for (auto dp = llkTopDirectory.read(); dp != nullptr; dp = llkTopDirectory.read()) {
803 std::string piddir;
804
805 if (!getValidTidDir(dp, &piddir)) {
806 continue;
807 }
808
809 // Get the process tasks
810 std::string taskdir = piddir + "/task/";
811 int pid = -1;
812 LOG(VERBOSE) << "+opendir(\"" << taskdir << "\")";
813 dir taskDirectory(taskdir);
814 if (__predict_false(!taskDirectory)) {
815 LOG(DEBUG) << "+opendir(\"" << taskdir << "\") failed";
816 }
817 for (auto tp = taskDirectory.read(dir::task, dp); tp != nullptr;
818 tp = taskDirectory.read(dir::task)) {
819 if (!getValidTidDir(tp, &piddir)) {
820 continue;
821 }
822
823 // Get the process stat
824 std::string stat = ReadFile(piddir + "/stat");
825 if (stat.size() == 0) {
826 continue;
827 }
828 unsigned tid = -1;
829 char pdir[TASK_COMM_LEN + 1];
830 char state = '?';
831 unsigned ppid = -1;
832 unsigned utime = -1;
833 unsigned stime = -1;
834 int dummy;
835 pdir[0] = '\0';
836 // tid should not change value
837 auto match = ::sscanf(
838 stat.c_str(),
839 "%u (%" ___STRING(
840 TASK_COMM_LEN) "[^)]) %c %u %*d %*d %*d %*d %*d %*d %*d %*d %*d %u %u %d",
841 &tid, pdir, &state, &ppid, &utime, &stime, &dummy);
842 if (pid == -1) {
843 pid = tid;
844 }
845 LOG(VERBOSE) << "match " << match << ' ' << tid << " (" << pdir << ") " << state << ' '
846 << ppid << " ... " << utime << ' ' << stime << ' ' << dummy;
847 if (match != 7) {
848 continue;
849 }
850
851 auto procp = llkTidLookup(tid);
852 if (procp == nullptr) {
853 procp = llkTidAlloc(tid, pid, ppid, pdir, utime + stime, state);
854 } else {
855 // comm can change ...
856 procp->setComm(pdir);
857 procp->updated = true;
858 // pid/ppid/tid wrap?
859 if (((procp->update != prevUpdate) && (procp->update != llkUpdate)) ||
860 (procp->ppid != ppid) || (procp->pid != pid)) {
861 procp->reset();
862 } else if (procp->time != (utime + stime)) { // secondary ABA.
863 // watching utime+stime granularity jiffy
864 procp->state = '?';
865 }
866 procp->update = llkUpdate;
867 procp->pid = pid;
868 procp->ppid = ppid;
869 procp->time = utime + stime;
870 if (procp->state != state) {
871 procp->count = 0ms;
872 procp->killed = false;
873 procp->state = state;
874 } else {
875 procp->count += llkCycle;
876 }
877 }
878
879 // Filter checks in intuitive order of CPU cost to evaluate
880 // If tid unique continue, if ppid or pid unique break
881
882 if (pid == myPid) {
883 break;
884 }
885 if (!llkIsMonitorState(state)) {
886 continue;
887 }
888 if ((tid == myTid) || llkSkipPid(tid)) {
889 continue;
890 }
891 if (llkSkipPpid(ppid)) {
892 break;
893 }
894
895 if (llkSkipName(procp->getComm())) {
896 continue;
897 }
898 if (llkSkipName(procp->getCmdline())) {
899 break;
900 }
901
902 auto pprocp = llkTidLookup(ppid);
903 if (pprocp == nullptr) {
904 pprocp = llkTidAlloc(ppid, ppid, 0, "", 0, '?');
905 }
906 if ((pprocp != nullptr) && (llkSkipName(pprocp->getComm(), llkBlacklistParent) ||
907 llkSkipName(pprocp->getCmdline(), llkBlacklistParent))) {
908 break;
909 }
910
911 if ((llkBlacklistUid.size() != 0) && llkSkipUid(procp->getUid())) {
912 continue;
913 }
914
915 // ABA mitigation watching last time schedule activity happened
916 llkCheckSchedUpdate(procp, piddir);
917
918 // Can only fall through to here if registered D or Z state !!!
919 if (procp->count < llkStateTimeoutMs[(state == 'Z') ? llkStateZ : llkStateD]) {
920 LOG(VERBOSE) << state << ' ' << llkFormat(procp->count) << ' ' << ppid << "->"
921 << pid << "->" << tid << ' ' << procp->getComm();
922 continue;
923 }
924
925 // We have to kill it to determine difference between live lock
926 // and persistent state blocked on a resource. Is there something
927 // wrong with a process that has no forward scheduling progress in
928 // Z or D? Yes, generally means improper accounting in the
929 // process, but not always ...
930 //
931 // Whomever we hit with a test kill must accept the Android
932 // Aphorism that everything can be burned to the ground and
933 // must survive.
934 if (procp->killed == false) {
935 procp->killed = true;
936 // confirm: re-read uid before committing to a panic.
937 procp->uid = -1;
938 switch (state) {
939 case 'Z': // kill ppid to free up a Zombie
940 // Killing init will kernel panic without diagnostics
941 // so skip right to controlled kernel panic with
942 // diagnostics.
943 if (ppid == initPid) {
944 break;
945 }
946 LOG(WARNING) << "Z " << llkFormat(procp->count) << ' ' << ppid << "->"
947 << pid << "->" << tid << ' ' << procp->getComm() << " [kill]";
948 if ((llkKillOneProcess(pprocp, procp) >= 0) ||
949 (llkKillOneProcess(ppid, procp) >= 0)) {
950 continue;
951 }
952 break;
953
954 case 'D': // kill tid to free up an uninterruptible D
955 // If ABA is doing its job, we would not need or
956 // want the following. Test kill is a Hail Mary
957 // to make absolutely sure there is no forward
958 // scheduling progress. The cost when ABA is
959 // not working is we kill a process that likes to
960 // stay in 'D' state, instead of panicing the
961 // kernel (worse).
962 LOG(WARNING) << "D " << llkFormat(procp->count) << ' ' << pid << "->" << tid
963 << ' ' << procp->getComm() << " [kill]";
964 if ((llkKillOneProcess(llkTidLookup(pid), procp) >= 0) ||
965 (llkKillOneProcess(pid, 'D', tid) >= 0) ||
966 (llkKillOneProcess(procp, procp) >= 0) ||
967 (llkKillOneProcess(tid, 'D', tid) >= 0)) {
968 continue;
969 }
970 break;
971 }
972 }
973 // We are here because we have confirmed kernel live-lock
974 LOG(ERROR) << state << ' ' << llkFormat(procp->count) << ' ' << ppid << "->" << pid
975 << "->" << tid << ' ' << procp->getComm() << " [panic]";
976 llkPanicKernel(true, tid);
977 }
978 LOG(VERBOSE) << "+closedir()";
979 }
980 llkTopDirectory.rewind();
981 LOG(VERBOSE) << "closedir()";
982
983 // garbage collection of old process references
984 for (auto p = tids.begin(); p != tids.end();) {
985 if (!p->second.updated) {
986 IF_ALOG(LOG_VERBOSE, LOG_TAG) {
987 std::string ppidCmdline = llkProcGetName(p->second.ppid, nullptr, nullptr);
988 if (ppidCmdline.size()) {
989 ppidCmdline = "(" + ppidCmdline + ")";
990 }
991 std::string pidCmdline;
992 if (p->second.pid != p->second.tid) {
993 pidCmdline = llkProcGetName(p->second.pid, nullptr, p->second.getCmdline());
994 if (pidCmdline.size()) {
995 pidCmdline = "(" + pidCmdline + ")";
996 }
997 }
998 std::string tidCmdline =
999 llkProcGetName(p->second.tid, p->second.getComm(), p->second.getCmdline());
1000 if (tidCmdline.size()) {
1001 tidCmdline = "(" + tidCmdline + ")";
1002 }
1003 LOG(VERBOSE) << "thread " << p->second.ppid << ppidCmdline << "->" << p->second.pid
1004 << pidCmdline << "->" << p->second.tid << tidCmdline << " removed";
1005 }
1006 p = tids.erase(p);
1007 } else {
1008 ++p;
1009 }
1010 }
1011 if (__predict_false(tids.empty())) {
1012 llkTopDirectory.reset();
1013 }
1014
1015 llkCycle = llkCheckMs;
1016
1017 timespec end;
1018 ::clock_gettime(CLOCK_MONOTONIC_COARSE, &end);
1019 auto milli = llkGetTimespecDiffMs(&now, &end);
1020 LOG((milli > 10s) ? ERROR : (milli > 1s) ? WARNING : VERBOSE) << "sample " << llkFormat(milli);
1021
1022 // cap to minimum sleep for 1 second since last cycle
1023 if (llkCycle < (ms + 1s)) {
1024 return 1s;
1025 }
1026 return llkCycle - ms;
1027}
1028
1029unsigned llkCheckMilliseconds() {
1030 return duration_cast<milliseconds>(llkCheck()).count();
1031}
1032
1033bool llkInit(const char* threadname) {
1034 llkLowRam = android::base::GetBoolProperty("ro.config.low_ram", false);
1035 llkEnable = android::base::GetBoolProperty(LLK_ENABLE_PROPERTY, llkEnable);
1036 if (llkEnable && !llkTopDirectory.reset(procdir)) {
1037 // Most likely reason we could be here is llkd was started
1038 // incorrectly without the readproc permissions. Keep our
1039 // processing down to a minimum.
1040 llkEnable = false;
1041 }
1042 khtEnable = android::base::GetBoolProperty(KHT_ENABLE_PROPERTY, khtEnable);
1043 llkMlockall = android::base::GetBoolProperty(LLK_MLOCKALL_PROPERTY, llkMlockall);
1044 // if LLK_TIMOUT_MS_PROPERTY was not set, we will use a set
1045 // KHT_TIMEOUT_PROPERTY as co-operative guidance for the default value.
1046 khtTimeout = GetUintProperty(KHT_TIMEOUT_PROPERTY, khtTimeout);
1047 if (khtTimeout == 0s) {
1048 khtTimeout = duration_cast<seconds>(llkTimeoutMs * (1 + LLK_CHECKS_PER_TIMEOUT_DEFAULT) /
1049 LLK_CHECKS_PER_TIMEOUT_DEFAULT);
1050 }
1051 llkTimeoutMs =
1052 khtTimeout * LLK_CHECKS_PER_TIMEOUT_DEFAULT / (1 + LLK_CHECKS_PER_TIMEOUT_DEFAULT);
1053 llkTimeoutMs = GetUintProperty(LLK_TIMEOUT_MS_PROPERTY, llkTimeoutMs);
1054 llkValidate(); // validate llkTimeoutMs, llkCheckMs and llkCycle
1055 llkStateTimeoutMs[llkStateD] = GetUintProperty(LLK_D_TIMEOUT_MS_PROPERTY, llkTimeoutMs);
1056 llkStateTimeoutMs[llkStateZ] = GetUintProperty(LLK_Z_TIMEOUT_MS_PROPERTY, llkTimeoutMs);
1057 llkCheckMs = GetUintProperty(LLK_CHECK_MS_PROPERTY, llkCheckMs);
1058 llkValidate(); // validate all (effectively minus llkTimeoutMs)
1059 std::string defaultBlacklistProcess(
1060 std::to_string(kernelPid) + "," + std::to_string(initPid) + "," +
1061 std::to_string(kthreaddPid) + "," + std::to_string(::getpid()) + "," +
1062 std::to_string(::gettid()) + "," LLK_BLACKLIST_PROCESS_DEFAULT);
1063 if (threadname) {
1064 defaultBlacklistProcess += std::string(",") + threadname;
1065 }
1066 for (int cpu = 1; cpu < get_nprocs_conf(); ++cpu) {
1067 defaultBlacklistProcess += ",[watchdog/" + std::to_string(cpu) + "]";
1068 }
1069 defaultBlacklistProcess =
1070 android::base::GetProperty(LLK_BLACKLIST_PROCESS_PROPERTY, defaultBlacklistProcess);
1071 llkBlacklistProcess = llkSplit(defaultBlacklistProcess);
1072 if (!llkSkipName("[khungtaskd]")) { // ALWAYS ignore as special
1073 llkBlacklistProcess.emplace("[khungtaskd]");
1074 }
1075 llkBlacklistParent = llkSplit(android::base::GetProperty(
1076 LLK_BLACKLIST_PARENT_PROPERTY, std::to_string(kernelPid) + "," + std::to_string(kthreaddPid) +
1077 "," LLK_BLACKLIST_PARENT_DEFAULT));
1078 llkBlacklistUid =
1079 llkSplit(android::base::GetProperty(LLK_BLACKLIST_UID_PROPERTY, LLK_BLACKLIST_UID_DEFAULT));
1080
1081 // internal watchdog
1082 ::signal(SIGALRM, llkAlarmHandler);
1083
1084 // kernel hung task configuration? Otherwise leave it as-is
1085 if (khtEnable) {
1086 // EUID must be AID_ROOT to write to /proc/sys/kernel/ nodes, there
1087 // are no capability overrides. For security reasons we do not want
1088 // to run as AID_ROOT. We may not be able to write them successfully,
1089 // we will try, but the least we can do is read the values back to
1090 // confirm expectations and report whether configured or not.
1091 auto configured = llkWriteStringToFileConfirm(std::to_string(khtTimeout.count()),
1092 "/proc/sys/kernel/hung_task_timeout_secs");
1093 if (configured) {
1094 llkWriteStringToFile("65535", "/proc/sys/kernel/hung_task_warnings");
1095 llkWriteStringToFile("65535", "/proc/sys/kernel/hung_task_check_count");
1096 configured = llkWriteStringToFileConfirm("1", "/proc/sys/kernel/hung_task_panic");
1097 }
1098 if (configured) {
1099 LOG(INFO) << "[khungtaskd] configured";
1100 } else {
1101 LOG(WARNING) << "[khungtaskd] not configurable";
1102 }
1103 }
1104
1105 bool logConfig = true;
1106 if (llkEnable) {
1107 if (llkMlockall &&
1108 // MCL_ONFAULT pins pages as they fault instead of loading
1109 // everything immediately all at once. (Which would be bad,
1110 // because as of this writing, we have a lot of mapped pages we
1111 // never use.) Old kernels will see MCL_ONFAULT and fail with
1112 // EINVAL; we ignore this failure.
1113 //
1114 // N.B. read the man page for mlockall. MCL_CURRENT | MCL_ONFAULT
1115 // pins ⊆ MCL_CURRENT, converging to just MCL_CURRENT as we fault
1116 // in pages.
1117
1118 // CAP_IPC_LOCK required
1119 mlockall(MCL_CURRENT | MCL_FUTURE | MCL_ONFAULT) && (errno != EINVAL)) {
1120 PLOG(WARNING) << "mlockall failed ";
1121 }
1122
1123 if (threadname) {
1124 pthread_attr_t attr;
1125
1126 if (!pthread_attr_init(&attr)) {
1127 sched_param param;
1128
1129 memset(&param, 0, sizeof(param));
1130 pthread_attr_setschedparam(&attr, &param);
1131 pthread_attr_setschedpolicy(&attr, SCHED_BATCH);
1132 if (!pthread_attr_setdetachstate(&attr, PTHREAD_CREATE_DETACHED)) {
1133 pthread_t thread;
1134 if (!pthread_create(&thread, &attr, llkThread, const_cast<char*>(threadname))) {
1135 // wait a second for thread to start
1136 for (auto retry = 50; retry && !llkRunning; --retry) {
1137 ::usleep(20000);
1138 }
1139 logConfig = !llkRunning; // printed in llkd context?
1140 } else {
1141 LOG(ERROR) << "failed to spawn llkd thread";
1142 }
1143 } else {
1144 LOG(ERROR) << "failed to detach llkd thread";
1145 }
1146 pthread_attr_destroy(&attr);
1147 } else {
1148 LOG(ERROR) << "failed to allocate attibutes for llkd thread";
1149 }
1150 }
1151 } else {
1152 LOG(DEBUG) << "[khungtaskd] left unconfigured";
1153 }
1154 if (logConfig) {
1155 llkLogConfig();
1156 }
1157
1158 return llkEnable;
1159}
diff --git a/llkd/llkd.cpp b/llkd/llkd.cpp
new file mode 100644
index 000000000..f10253d45
--- /dev/null
+++ b/llkd/llkd.cpp
@@ -0,0 +1,50 @@
1/*
2 * Copyright (C) 2018 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#include "llkd.h"
18
19#include <sched.h>
20#include <unistd.h>
21
22#include <chrono>
23
24#include <android-base/logging.h>
25
26using namespace std::chrono;
27
28int main(int, char**) {
29 LOG(INFO) << "started";
30
31 bool enabled = llkInit();
32
33 // Would like this policy to be automatic as part of libllkd,
34 // but that would be presumptuous and bad side-effect.
35 struct sched_param param;
36 memset(&param, 0, sizeof(param));
37 sched_setscheduler(0, SCHED_BATCH, &param);
38
39 while (true) {
40 if (enabled) {
41 ::usleep(duration_cast<microseconds>(llkCheck()).count());
42 } else {
43 ::pause();
44 }
45 }
46 // NOTREACHED
47
48 LOG(INFO) << "exiting";
49 return 0;
50}
diff --git a/llkd/llkd.rc b/llkd/llkd.rc
new file mode 100644
index 000000000..a257e76e1
--- /dev/null
+++ b/llkd/llkd.rc
@@ -0,0 +1,18 @@
1# Configure [khungtaskd]
2on property:ro.khungtask.enable=true
3 write /proc/sys/kernel/hung_task_timeout_secs ${ro.khungtask.timeout:-720}
4 write /proc/sys/kernel/hung_task_warnings 65535
5 write /proc/sys/kernel/hung_task_check_count 65535
6 write /proc/sys/kernel/hung_task_panic 1
7
8on property:ro.llk.enable=true
9 start llkd
10
11service llkd /system/bin/llkd
12 class late_start
13 disabled
14 user llkd
15 group llkd readproc
16 capabilities KILL IPC_LOCK
17 file /proc/sysrq-trigger w
18 writepid /dev/cpuset/system-background/tasks
diff --git a/llkd/tests/Android.bp b/llkd/tests/Android.bp
new file mode 100644
index 000000000..6dd5938e3
--- /dev/null
+++ b/llkd/tests/Android.bp
@@ -0,0 +1,41 @@
1// Copyright (C) 2018 The Android Open Source Project
2//
3// Licensed under the Apache License, Version 2.0 (the "License");
4// you may not use this file except in compliance with the License.
5// You may obtain a copy of the License at
6//
7// http://www.apache.org/licenses/LICENSE-2.0
8//
9// Unless required by applicable law or agreed to in writing, software
10// distributed under the License is distributed on an "AS IS" BASIS,
11// WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
12// See the License for the specific language governing permissions and
13// limitations under the License.
14
15cc_test {
16 name: "llkd_unit_test",
17
18 shared_libs: [
19 "libbase",
20 "liblog",
21 ],
22 header_libs: [
23 "llkd_headers",
24 ],
25
26 target: {
27 android: {
28 srcs: [
29 "llkd_test.cpp",
30 ],
31 },
32 },
33
34 cflags: [
35 "-Wall",
36 "-Wextra",
37 "-Werror",
38 ],
39
40 compile_multilib: "first",
41}
diff --git a/llkd/tests/llkd_test.cpp b/llkd/tests/llkd_test.cpp
new file mode 100644
index 000000000..e3c95eba3
--- /dev/null
+++ b/llkd/tests/llkd_test.cpp
@@ -0,0 +1,243 @@
1/*
2 * Copyright (C) 2018 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#include <signal.h>
18#include <stdint.h>
19#include <sys/types.h>
20#include <sys/wait.h>
21#include <unistd.h>
22
23#include <chrono>
24#include <iostream>
25#include <string>
26
27#include <android-base/properties.h>
28#include <gtest/gtest.h>
29#include <log/log_time.h> // for MS_PER_SEC and US_PER_SEC
30
31#include "llkd.h"
32
33using namespace std::chrono;
34using namespace std::chrono_literals;
35
36namespace {
37
38milliseconds GetUintProperty(const std::string& key, milliseconds def) {
39 return milliseconds(android::base::GetUintProperty(key, static_cast<uint64_t>(def.count()),
40 static_cast<uint64_t>(def.max().count())));
41}
42
43seconds GetUintProperty(const std::string& key, seconds def) {
44 return seconds(android::base::GetUintProperty(key, static_cast<uint64_t>(def.count()),
45 static_cast<uint64_t>(def.max().count())));
46}
47
48// GTEST_LOG_(WARNING) output is fugly, this has much less noise
49// ToDo: look into fixing googletest to produce output that matches style of
50// all the other status messages, and can switch off __line__ and
51// __function__ noise
52#define GTEST_LOG_WARNING std::cerr << "[ WARNING ] "
53#define GTEST_LOG_INFO std::cerr << "[ INFO ] "
54
55// Properties is _not_ a high performance ABI!
56void rest() {
57 usleep(200000);
58}
59
60void execute(const char* command) {
61 if (getuid() || system(command)) {
62 system((std::string("su root ") + command).c_str());
63 }
64}
65
66seconds llkdSleepPeriod(char state) {
67 auto default_enable = android::base::GetBoolProperty(LLK_ENABLE_PROPERTY, LLK_ENABLE_DEFAULT);
68 if (android::base::GetProperty(LLK_ENABLE_PROPERTY, "nothing") == "nothing") {
69 GTEST_LOG_INFO << LLK_ENABLE_PROPERTY " defaults to " << (default_enable ? "true" : "false")
70 << "\n";
71 }
72 // Hail Mary hope is unconfigured.
73 if ((GetUintProperty(LLK_TIMEOUT_MS_PROPERTY, LLK_TIMEOUT_MS_DEFAULT) !=
74 duration_cast<milliseconds>(120s)) ||
75 (GetUintProperty(LLK_CHECK_MS_PROPERTY,
76 LLK_TIMEOUT_MS_DEFAULT / LLK_CHECKS_PER_TIMEOUT_DEFAULT) !=
77 duration_cast<milliseconds>(10s))) {
78 execute("stop llkd");
79 rest();
80 std::string setprop("setprop ");
81 execute((setprop + LLK_TIMEOUT_MS_PROPERTY + " 120000").c_str());
82 rest();
83 execute((setprop + KHT_TIMEOUT_PROPERTY + " 130").c_str());
84 rest();
85 execute((setprop + LLK_CHECK_MS_PROPERTY + " 10000").c_str());
86 rest();
87 execute((setprop + LLK_ENABLE_PROPERTY + " true").c_str());
88 rest();
89 }
90 default_enable = android::base::GetBoolProperty(LLK_ENABLE_PROPERTY, false);
91 if (default_enable) {
92 execute("start llkd");
93 rest();
94 GTEST_LOG_INFO << "llkd enabled\n";
95 } else {
96 GTEST_LOG_WARNING << "llkd disabled\n";
97 }
98
99 /* KISS follows llk_init() */
100 milliseconds llkTimeoutMs = LLK_TIMEOUT_MS_DEFAULT;
101 seconds khtTimeout = duration_cast<seconds>(
102 llkTimeoutMs * (1 + LLK_CHECKS_PER_TIMEOUT_DEFAULT) / LLK_CHECKS_PER_TIMEOUT_DEFAULT);
103 khtTimeout = GetUintProperty(KHT_TIMEOUT_PROPERTY, khtTimeout);
104 llkTimeoutMs =
105 khtTimeout * LLK_CHECKS_PER_TIMEOUT_DEFAULT / (1 + LLK_CHECKS_PER_TIMEOUT_DEFAULT);
106 llkTimeoutMs = GetUintProperty(LLK_TIMEOUT_MS_PROPERTY, llkTimeoutMs);
107 if (llkTimeoutMs < LLK_TIMEOUT_MS_MINIMUM) {
108 llkTimeoutMs = LLK_TIMEOUT_MS_MINIMUM;
109 }
110 milliseconds llkCheckMs = llkTimeoutMs / LLK_CHECKS_PER_TIMEOUT_DEFAULT;
111 auto timeout = GetUintProperty(
112 (state == 'Z') ? LLK_Z_TIMEOUT_MS_PROPERTY : LLK_D_TIMEOUT_MS_PROPERTY, llkTimeoutMs);
113 if (timeout < LLK_TIMEOUT_MS_MINIMUM) {
114 timeout = LLK_TIMEOUT_MS_MINIMUM;
115 }
116
117 if (llkCheckMs > timeout) {
118 llkCheckMs = timeout;
119 }
120 llkCheckMs = GetUintProperty(LLK_CHECK_MS_PROPERTY, llkCheckMs);
121 timeout += llkCheckMs;
122 auto sec = duration_cast<seconds>(timeout);
123 if (sec == 0s) {
124 ++sec;
125 } else if (sec > 59s) {
126 GTEST_LOG_WARNING << "llkd is configured for about " << duration_cast<minutes>(sec).count()
127 << " minutes to react\n";
128 }
129
130 // 33% margin for the test to naturally timeout waiting for llkd to respond
131 return (sec * 4 + 2s) / 3;
132}
133
134inline void waitForPid(pid_t child_pid) {
135 int wstatus;
136 ASSERT_LE(0, waitpid(child_pid, &wstatus, 0));
137 EXPECT_FALSE(WIFEXITED(wstatus)) << "[ INFO ] exit=" << WEXITSTATUS(wstatus);
138 ASSERT_TRUE(WIFSIGNALED(wstatus));
139 ASSERT_EQ(WTERMSIG(wstatus), SIGKILL);
140}
141
142} // namespace
143
144// The tests that use this helper are to simulate processes stuck in 'D'
145// state that are experiencing forward scheduled progress. As such the
146// expectation is that llkd will _not_ perform any mitigations. The sleepfor
147// argument helps us set the amount of forward scheduler progress.
148static void llkd_driver_ABA(const microseconds sleepfor) {
149 const auto period = llkdSleepPeriod('D');
150 if (period <= sleepfor) {
151 GTEST_LOG_WARNING << "llkd configuration too short for "
152 << duration_cast<milliseconds>(sleepfor).count() << "ms work cycle\n";
153 return;
154 }
155
156 auto child_pid = fork();
157 ASSERT_LE(0, child_pid);
158 int wstatus;
159 if (!child_pid) {
160 auto ratio = period / sleepfor;
161 ASSERT_LT(0, ratio);
162 // vfork() parent is uninterruptable D state waiting for child to exec()
163 while (--ratio > 0) {
164 auto driver_pid = vfork();
165 ASSERT_LE(0, driver_pid);
166 if (driver_pid) { // parent
167 waitpid(driver_pid, &wstatus, 0);
168 if (!WIFEXITED(wstatus)) {
169 exit(42);
170 }
171 if (WEXITSTATUS(wstatus) != 42) {
172 exit(42);
173 }
174 } else {
175 usleep(sleepfor.count());
176 exit(42);
177 }
178 }
179 exit(0);
180 }
181 ASSERT_LE(0, waitpid(child_pid, &wstatus, 0));
182 EXPECT_TRUE(WIFEXITED(wstatus));
183 if (WIFEXITED(wstatus)) {
184 EXPECT_EQ(0, WEXITSTATUS(wstatus));
185 }
186 ASSERT_FALSE(WIFSIGNALED(wstatus)) << "[ INFO ] signo=" << WTERMSIG(wstatus);
187}
188
189TEST(llkd, driver_ABA_fast) {
190 llkd_driver_ABA(5ms);
191}
192
193TEST(llkd, driver_ABA_slow) {
194 llkd_driver_ABA(1s);
195}
196
197TEST(llkd, driver_ABA_glacial) {
198 llkd_driver_ABA(1min);
199}
200
201// Following tests must be last in this file to capture possible errant
202// kernel_panic mitigation failure.
203
204// The following tests simulate processes stick in 'Z' or 'D' state with
205// no forward scheduling progress, but interruptible. As such the expectation
206// is that llkd will perform kill mitigation and not progress to kernel_panic.
207
208TEST(llkd, zombie) {
209 const auto period = llkdSleepPeriod('Z');
210
211 /* Create a Persistent Zombie Process */
212 pid_t child_pid = fork();
213 ASSERT_LE(0, child_pid);
214 if (!child_pid) {
215 auto zombie_pid = fork();
216 ASSERT_LE(0, zombie_pid);
217 if (!zombie_pid) {
218 sleep(1);
219 exit(0);
220 }
221 sleep(period.count());
222 exit(42);
223 }
224
225 waitForPid(child_pid);
226}
227
228TEST(llkd, driver) {
229 const auto period = llkdSleepPeriod('D');
230
231 /* Create a Persistent Device Process */
232 auto child_pid = fork();
233 ASSERT_LE(0, child_pid);
234 if (!child_pid) {
235 // vfork() parent is uninterruptable D state waiting for child to exec()
236 auto driver_pid = vfork();
237 ASSERT_LE(0, driver_pid);
238 sleep(period.count());
239 exit(driver_pid ? 42 : 0);
240 }
241
242 waitForPid(child_pid);
243}