diff options
author | David Anderson | 2018-07-31 18:43:26 -0500 |
---|---|---|
committer | David Anderson | 2018-08-02 11:14:47 -0500 |
commit | de1daa72aaa25de8b61f004457a60b8f4527dec6 (patch) | |
tree | 7e2859ae3b6d522f4850dcdfb26263f0ba9ddb65 | |
parent | ddcee93c0138fc68dbc6320962a53cd4761ab94b (diff) | |
download | platform-system-core-de1daa72aaa25de8b61f004457a60b8f4527dec6.tar.gz platform-system-core-de1daa72aaa25de8b61f004457a60b8f4527dec6.tar.xz platform-system-core-de1daa72aaa25de8b61f004457a60b8f4527dec6.zip |
liblp: Simplify GrowPartition().
The partition resize algorithm duplicates a lot of logic because it
handles the final free interval separately from other free intervals.
This is unnecessary and makes it harder to change the actual algorithm.
This change makes GrowPartition() treat the final free space region the
same as free gaps in between partitions. It does this by converting the
extent list into a gap list, and then adds a final gap for the remainder
of the free space. The resize function no longer has to treat the end of
the disk separately.
This patch does not change the way partitions are allocated, it is
purely a refactoring.
Bug: 79173901
Test: liblp_test gtest
Change-Id: I4780f20b23fe021eac62de874b061857712c04fe
-rw-r--r-- | fs_mgr/liblp/builder.cpp | 86 |
1 files changed, 38 insertions, 48 deletions
diff --git a/fs_mgr/liblp/builder.cpp b/fs_mgr/liblp/builder.cpp index d6eee6b32..d3c785d33 100644 --- a/fs_mgr/liblp/builder.cpp +++ b/fs_mgr/liblp/builder.cpp | |||
@@ -299,49 +299,59 @@ bool MetadataBuilder::GrowPartition(Partition* partition, uint64_t aligned_size) | |||
299 | Interval(uint64_t start, uint64_t end) : start(start), end(end) {} | 299 | Interval(uint64_t start, uint64_t end) : start(start), end(end) {} |
300 | bool operator<(const Interval& other) const { return start < other.start; } | 300 | bool operator<(const Interval& other) const { return start < other.start; } |
301 | }; | 301 | }; |
302 | std::vector<Interval> intervals; | ||
303 | 302 | ||
304 | // Collect all extents in the partition table. | 303 | // Collect all extents in the partition table, then sort them by starting |
304 | // sector. | ||
305 | std::vector<Interval> extents; | ||
305 | for (const auto& partition : partitions_) { | 306 | for (const auto& partition : partitions_) { |
306 | for (const auto& extent : partition->extents()) { | 307 | for (const auto& extent : partition->extents()) { |
307 | LinearExtent* linear = extent->AsLinearExtent(); | 308 | LinearExtent* linear = extent->AsLinearExtent(); |
308 | if (!linear) { | 309 | if (!linear) { |
309 | continue; | 310 | continue; |
310 | } | 311 | } |
311 | intervals.emplace_back(linear->physical_sector(), | 312 | extents.emplace_back(linear->physical_sector(), |
312 | linear->physical_sector() + extent->num_sectors()); | 313 | linear->physical_sector() + extent->num_sectors()); |
313 | } | 314 | } |
314 | } | 315 | } |
316 | std::sort(extents.begin(), extents.end()); | ||
315 | 317 | ||
316 | // Sort extents by starting sector. | 318 | // Convert the extent list into a list of gaps between the extents; i.e., |
317 | std::sort(intervals.begin(), intervals.end()); | 319 | // the list of ranges that are free on the disk. |
318 | 320 | std::vector<Interval> free_regions; | |
319 | // Find gaps that we can use for new extents. Note we store new extents in a | 321 | for (size_t i = 1; i < extents.size(); i++) { |
320 | // temporary vector, and only commit them if we are guaranteed enough free | 322 | const Interval& previous = extents[i - 1]; |
321 | // space. | 323 | const Interval& current = extents[i]; |
322 | std::vector<std::unique_ptr<LinearExtent>> new_extents; | ||
323 | for (size_t i = 1; i < intervals.size(); i++) { | ||
324 | const Interval& previous = intervals[i - 1]; | ||
325 | const Interval& current = intervals[i]; | ||
326 | |||
327 | if (previous.end >= current.start) { | ||
328 | // There is no gap between these two extents, try the next one. Note that | ||
329 | // extents may never overlap, but just for safety, we ignore them if they | ||
330 | // do. | ||
331 | DCHECK(previous.end == current.start); | ||
332 | continue; | ||
333 | } | ||
334 | 324 | ||
335 | uint64_t aligned = AlignSector(previous.end); | 325 | uint64_t aligned = AlignSector(previous.end); |
336 | if (aligned >= current.start) { | 326 | if (aligned >= current.start) { |
337 | // After alignment, this extent is not usable. | 327 | // There is no gap between these two extents, try the next one. |
328 | // Note that we check with >= instead of >, since alignment may | ||
329 | // bump the ending sector past the beginning of the next extent. | ||
338 | continue; | 330 | continue; |
339 | } | 331 | } |
340 | 332 | ||
333 | // The new interval represents the free space starting at the end of | ||
334 | // the previous interval, and ending at the start of the next interval. | ||
335 | free_regions.emplace_back(aligned, current.start); | ||
336 | } | ||
337 | |||
338 | // Add a final interval representing the remainder of the free space. | ||
339 | uint64_t last_free_extent_start = | ||
340 | extents.empty() ? geometry_.first_logical_sector : extents.back().end; | ||
341 | last_free_extent_start = AlignSector(last_free_extent_start); | ||
342 | if (last_free_extent_start <= geometry_.last_logical_sector) { | ||
343 | free_regions.emplace_back(last_free_extent_start, geometry_.last_logical_sector + 1); | ||
344 | } | ||
345 | |||
346 | // Find gaps that we can use for new extents. Note we store new extents in a | ||
347 | // temporary vector, and only commit them if we are guaranteed enough free | ||
348 | // space. | ||
349 | std::vector<std::unique_ptr<LinearExtent>> new_extents; | ||
350 | for (const auto& region : free_regions) { | ||
341 | // This gap is enough to hold the remainder of the space requested, so we | 351 | // This gap is enough to hold the remainder of the space requested, so we |
342 | // can allocate what we need and return. | 352 | // can allocate what we need and return. |
343 | if (current.start - aligned >= sectors_needed) { | 353 | if (region.end - region.start >= sectors_needed) { |
344 | auto extent = std::make_unique<LinearExtent>(sectors_needed, aligned); | 354 | auto extent = std::make_unique<LinearExtent>(sectors_needed, region.start); |
345 | sectors_needed -= extent->num_sectors(); | 355 | sectors_needed -= extent->num_sectors(); |
346 | new_extents.push_back(std::move(extent)); | 356 | new_extents.push_back(std::move(extent)); |
347 | break; | 357 | break; |
@@ -349,33 +359,13 @@ bool MetadataBuilder::GrowPartition(Partition* partition, uint64_t aligned_size) | |||
349 | 359 | ||
350 | // This gap is not big enough to fit the remainder of the space requested, | 360 | // This gap is not big enough to fit the remainder of the space requested, |
351 | // so consume the whole thing and keep looking for more. | 361 | // so consume the whole thing and keep looking for more. |
352 | auto extent = std::make_unique<LinearExtent>(current.start - aligned, aligned); | 362 | auto extent = std::make_unique<LinearExtent>(region.end - region.start, region.start); |
353 | sectors_needed -= extent->num_sectors(); | 363 | sectors_needed -= extent->num_sectors(); |
354 | new_extents.push_back(std::move(extent)); | 364 | new_extents.push_back(std::move(extent)); |
355 | } | 365 | } |
356 | |||
357 | // If we still have more to allocate, take it from the remaining free space | ||
358 | // in the allocatable region. | ||
359 | if (sectors_needed) { | 366 | if (sectors_needed) { |
360 | uint64_t first_sector; | 367 | LERROR << "Not enough free space to expand partition: " << partition->name(); |
361 | if (intervals.empty()) { | 368 | return false; |
362 | first_sector = geometry_.first_logical_sector; | ||
363 | } else { | ||
364 | first_sector = intervals.back().end; | ||
365 | } | ||
366 | DCHECK(first_sector <= geometry_.last_logical_sector); | ||
367 | |||
368 | // Note: After alignment, |first_sector| may be > the last usable sector. | ||
369 | first_sector = AlignSector(first_sector); | ||
370 | |||
371 | // Note: the last usable sector is inclusive. | ||
372 | if (first_sector > geometry_.last_logical_sector || | ||
373 | geometry_.last_logical_sector + 1 - first_sector < sectors_needed) { | ||
374 | LERROR << "Not enough free space to expand partition: " << partition->name(); | ||
375 | return false; | ||
376 | } | ||
377 | auto extent = std::make_unique<LinearExtent>(sectors_needed, first_sector); | ||
378 | new_extents.push_back(std::move(extent)); | ||
379 | } | 369 | } |
380 | 370 | ||
381 | for (auto& extent : new_extents) { | 371 | for (auto& extent : new_extents) { |