diff options
author | Jesse Hall | 2018-05-04 17:17:39 -0500 |
---|---|---|
committer | Jesse Hall | 2018-05-23 18:45:48 -0500 |
commit | 798ba95bda14f9f28561a2a27ba406537f8bb8a8 (patch) | |
tree | cc40d34a10ca49f5e8bb7dc5034eb6f383a0205d /libsync | |
parent | 2576a439e6c4a750e001e70d73a33d9519bb7660 (diff) | |
download | platform-system-core-798ba95bda14f9f28561a2a27ba406537f8bb8a8.tar.gz platform-system-core-798ba95bda14f9f28561a2a27ba406537f8bb8a8.tar.xz platform-system-core-798ba95bda14f9f28561a2a27ba406537f8bb8a8.zip |
sync: remove legacy sync info API
The legacy fence/pt info API has been deprecated for a while. This
change removes it from headers, so remaining users will have to switch
to the modern API when they're re-compiled. The functions are still
provided by libsync.so and tests remain, so existing binaries should
continue to work. Eventually these will be removed too, though, once
it's reasonable to expect those binaries to have been recompiled.
Bug: 35326015
Test: make checkbuild
Test: adb shell dumpsys SurfaceFlinger --latency
Change-Id: Id086fafe37c2bc1cfdca4a21107bc9208ed61f89
Diffstat (limited to 'libsync')
-rw-r--r-- | libsync/include/android/sync.h | 20 | ||||
-rw-r--r-- | libsync/sync.c | 23 | ||||
-rw-r--r-- | libsync/tests/sync_test.cpp | 29 |
3 files changed, 52 insertions, 20 deletions
diff --git a/libsync/include/android/sync.h b/libsync/include/android/sync.h index 68f74a0b2..32bb878ba 100644 --- a/libsync/include/android/sync.h +++ b/libsync/include/android/sync.h | |||
@@ -41,28 +41,8 @@ | |||
41 | 41 | ||
42 | __BEGIN_DECLS | 42 | __BEGIN_DECLS |
43 | 43 | ||
44 | struct sync_fence_info_data { | ||
45 | uint32_t len; | ||
46 | char name[32]; | ||
47 | int32_t status; | ||
48 | uint8_t pt_info[0]; | ||
49 | }; | ||
50 | |||
51 | struct sync_pt_info { | ||
52 | uint32_t len; | ||
53 | char obj_name[32]; | ||
54 | char driver_name[32]; | ||
55 | int32_t status; | ||
56 | uint64_t timestamp_ns; | ||
57 | uint8_t driver_data[0]; | ||
58 | }; | ||
59 | |||
60 | /* timeout in msecs */ | 44 | /* timeout in msecs */ |
61 | int sync_wait(int fd, int timeout); | 45 | int sync_wait(int fd, int timeout); |
62 | struct sync_fence_info_data *sync_fence_info(int fd); | ||
63 | struct sync_pt_info *sync_pt_info(struct sync_fence_info_data *info, | ||
64 | struct sync_pt_info *itr); | ||
65 | void sync_fence_info_free(struct sync_fence_info_data *info); | ||
66 | 46 | ||
67 | __END_DECLS | 47 | __END_DECLS |
68 | 48 | ||
diff --git a/libsync/sync.c b/libsync/sync.c index 6b187faed..b8c48c7f7 100644 --- a/libsync/sync.c +++ b/libsync/sync.c | |||
@@ -30,6 +30,29 @@ | |||
30 | 30 | ||
31 | #include <android/sync.h> | 31 | #include <android/sync.h> |
32 | 32 | ||
33 | /* Prototypes for deprecated functions that used to be declared in the legacy | ||
34 | * android/sync.h. They've been moved here to make sure new code does not use | ||
35 | * them, but the functions are still defined to avoid breaking existing | ||
36 | * binaries. Eventually they can be removed altogether. | ||
37 | */ | ||
38 | struct sync_fence_info_data { | ||
39 | uint32_t len; | ||
40 | char name[32]; | ||
41 | int32_t status; | ||
42 | uint8_t pt_info[0]; | ||
43 | }; | ||
44 | struct sync_pt_info { | ||
45 | uint32_t len; | ||
46 | char obj_name[32]; | ||
47 | char driver_name[32]; | ||
48 | int32_t status; | ||
49 | uint64_t timestamp_ns; | ||
50 | uint8_t driver_data[0]; | ||
51 | }; | ||
52 | struct sync_fence_info_data* sync_fence_info(int fd); | ||
53 | struct sync_pt_info* sync_pt_info(struct sync_fence_info_data* info, struct sync_pt_info* itr); | ||
54 | void sync_fence_info_free(struct sync_fence_info_data* info); | ||
55 | |||
33 | /* Legacy Sync API */ | 56 | /* Legacy Sync API */ |
34 | 57 | ||
35 | struct sync_legacy_merge_data { | 58 | struct sync_legacy_merge_data { |
diff --git a/libsync/tests/sync_test.cpp b/libsync/tests/sync_test.cpp index 0fb86d6fc..011b09d00 100644 --- a/libsync/tests/sync_test.cpp +++ b/libsync/tests/sync_test.cpp | |||
@@ -15,6 +15,35 @@ | |||
15 | #include <random> | 15 | #include <random> |
16 | #include <unordered_map> | 16 | #include <unordered_map> |
17 | 17 | ||
18 | /* These deprecated declarations were in the legacy android/sync.h. They've been removed to | ||
19 | * encourage code to move to the modern equivalents. But they are still implemented in libsync.so | ||
20 | * to avoid breaking existing binaries; as long as that's true we should keep testing them here. | ||
21 | * That means making local copies of the declarations. | ||
22 | */ | ||
23 | extern "C" { | ||
24 | |||
25 | struct sync_fence_info_data { | ||
26 | uint32_t len; | ||
27 | char name[32]; | ||
28 | int32_t status; | ||
29 | uint8_t pt_info[0]; | ||
30 | }; | ||
31 | |||
32 | struct sync_pt_info { | ||
33 | uint32_t len; | ||
34 | char obj_name[32]; | ||
35 | char driver_name[32]; | ||
36 | int32_t status; | ||
37 | uint64_t timestamp_ns; | ||
38 | uint8_t driver_data[0]; | ||
39 | }; | ||
40 | |||
41 | struct sync_fence_info_data* sync_fence_info(int fd); | ||
42 | struct sync_pt_info* sync_pt_info(struct sync_fence_info_data* info, struct sync_pt_info* itr); | ||
43 | void sync_fence_info_free(struct sync_fence_info_data* info); | ||
44 | |||
45 | } // extern "C" | ||
46 | |||
18 | // TODO: better stress tests? | 47 | // TODO: better stress tests? |
19 | // Handle more than 64 fd's simultaneously, i.e. fix sync_fence_info's 4k limit. | 48 | // Handle more than 64 fd's simultaneously, i.e. fix sync_fence_info's 4k limit. |
20 | // Handle wraparound in timelines like nvidia. | 49 | // Handle wraparound in timelines like nvidia. |