diff options
author | Badhri Jagan Sridharan | 2015-06-02 16:47:57 -0500 |
---|---|---|
committer | Elliott Hughes | 2015-06-04 15:26:29 -0500 |
commit | 71aebefe49d8126f522287bd35d17c432a4e6383 (patch) | |
tree | 62d17ad6061b67794b02c0e32a0c76798d8f2b56 /libziparchive/zip_archive.cc | |
parent | 67ab5d95058d6fe1bab71b3f69e1934728902995 (diff) | |
download | platform-system-core-71aebefe49d8126f522287bd35d17c432a4e6383.tar.gz platform-system-core-71aebefe49d8126f522287bd35d17c432a4e6383.tar.xz platform-system-core-71aebefe49d8126f522287bd35d17c432a4e6383.zip |
libziparchive: fix fallocate failures
The objective of fallocate call seems to be to
make sure that we have enough enough space left
in the disk to house the uncompressed file.
But, fallocate is only supported in the following
file systems:
btrfs, ext4, ocfs2, and xfs
Return error only when fallocate fails due to
lack of space. The immediate ftruncate call is
going to take of the majority of other errors.
Bug: http://b/21558406
Bug: 21561449
Change-Id: I7083f3c7e5d745bd6e8a190ac9020297d638d9d4
(cherry picked from commit a68d0d1fe48afc7a7a7fd0ee42df1607f21fa996)
Diffstat (limited to 'libziparchive/zip_archive.cc')
-rw-r--r-- | libziparchive/zip_archive.cc | 7 |
1 files changed, 6 insertions, 1 deletions
diff --git a/libziparchive/zip_archive.cc b/libziparchive/zip_archive.cc index 79c4c53c7..b2a9f88c5 100644 --- a/libziparchive/zip_archive.cc +++ b/libziparchive/zip_archive.cc | |||
@@ -1008,8 +1008,13 @@ class FileWriter : public Writer { | |||
1008 | // entry. Note that the call to ftruncate below will change the file size but | 1008 | // entry. Note that the call to ftruncate below will change the file size but |
1009 | // will not allocate space on disk and this call to fallocate will not | 1009 | // will not allocate space on disk and this call to fallocate will not |
1010 | // change the file size. | 1010 | // change the file size. |
1011 | // Note: fallocate is only supported by the following filesystems - | ||
1012 | // btrfs, ext4, ocfs2, and xfs. Therefore fallocate might fail with | ||
1013 | // EOPNOTSUPP error when issued in other filesystems. | ||
1014 | // Hence, check for the return error code before concluding that the | ||
1015 | // disk does not have enough space. | ||
1011 | result = TEMP_FAILURE_RETRY(fallocate(fd, 0, current_offset, declared_length)); | 1016 | result = TEMP_FAILURE_RETRY(fallocate(fd, 0, current_offset, declared_length)); |
1012 | if (result == -1) { | 1017 | if (result == -1 && errno == ENOSPC) { |
1013 | ALOGW("Zip: unable to allocate space for file to %" PRId64 ": %s", | 1018 | ALOGW("Zip: unable to allocate space for file to %" PRId64 ": %s", |
1014 | static_cast<int64_t>(declared_length + current_offset), strerror(errno)); | 1019 | static_cast<int64_t>(declared_length + current_offset), strerror(errno)); |
1015 | return std::unique_ptr<FileWriter>(nullptr); | 1020 | return std::unique_ptr<FileWriter>(nullptr); |