diff options
-rw-r--r-- | liblog/Android.bp | 1 | ||||
-rw-r--r-- | liblog/config_write.c | 23 | ||||
-rw-r--r-- | liblog/include/log/log_frontend.h | 11 | ||||
-rw-r--r-- | liblog/logger_write.c | 6 | ||||
-rw-r--r-- | liblog/stderr_write.c | 219 | ||||
-rw-r--r-- | liblog/tests/Android.mk | 2 | ||||
-rw-r--r-- | liblog/tests/liblog_test.cpp | 215 | ||||
-rw-r--r-- | liblog/tests/liblog_test_stderr.cpp | 5 | ||||
-rw-r--r-- | liblog/tests/liblog_test_stderr_local.cpp | 4 |
9 files changed, 428 insertions, 58 deletions
diff --git a/liblog/Android.bp b/liblog/Android.bp index 310dbf4c3..bb8c3af2b 100644 --- a/liblog/Android.bp +++ b/liblog/Android.bp | |||
@@ -26,6 +26,7 @@ liblog_sources = [ | |||
26 | "logger_read.c", | 26 | "logger_read.c", |
27 | "logger_write.c", | 27 | "logger_write.c", |
28 | "logprint.c", | 28 | "logprint.c", |
29 | "stderr_write.c", | ||
29 | ] | 30 | ] |
30 | liblog_host_sources = [ | 31 | liblog_host_sources = [ |
31 | "fake_log_device.c", | 32 | "fake_log_device.c", |
diff --git a/liblog/config_write.c b/liblog/config_write.c index 583dcff3a..6a6c2205d 100644 --- a/liblog/config_write.c +++ b/liblog/config_write.c | |||
@@ -78,6 +78,29 @@ LIBLOG_HIDDEN void __android_log_config_write() { | |||
78 | &fakeLoggerWrite); | 78 | &fakeLoggerWrite); |
79 | #endif | 79 | #endif |
80 | } | 80 | } |
81 | |||
82 | if (__android_log_frontend & LOGGER_STDERR) { | ||
83 | extern struct android_log_transport_write stderrLoggerWrite; | ||
84 | |||
85 | /* | ||
86 | * stderr logger should be primary if we can be the only one, or if | ||
87 | * already in the primary list. Otherwise land in the persist list. | ||
88 | * Remember we can be called here if we are already initialized. | ||
89 | */ | ||
90 | if (list_empty(&__android_log_transport_write)) { | ||
91 | __android_log_add_transport(&__android_log_transport_write, | ||
92 | &stderrLoggerWrite); | ||
93 | } else { | ||
94 | struct android_log_transport_write *transp; | ||
95 | write_transport_for_each(transp, &__android_log_transport_write) { | ||
96 | if (transp == &stderrLoggerWrite) { | ||
97 | return; | ||
98 | } | ||
99 | } | ||
100 | __android_log_add_transport(&__android_log_persist_write, | ||
101 | &stderrLoggerWrite); | ||
102 | } | ||
103 | } | ||
81 | } | 104 | } |
82 | 105 | ||
83 | LIBLOG_HIDDEN void __android_log_config_write_close() { | 106 | LIBLOG_HIDDEN void __android_log_config_write_close() { |
diff --git a/liblog/include/log/log_frontend.h b/liblog/include/log/log_frontend.h index 952777971..5efa548af 100644 --- a/liblog/include/log/log_frontend.h +++ b/liblog/include/log/log_frontend.h | |||
@@ -17,11 +17,12 @@ extern "C" { | |||
17 | /* | 17 | /* |
18 | * Logging frontends, bit mask to select features. Function returns selection. | 18 | * Logging frontends, bit mask to select features. Function returns selection. |
19 | */ | 19 | */ |
20 | #define LOGGER_DEFAULT 0x0 | 20 | #define LOGGER_DEFAULT 0x00 |
21 | #define LOGGER_LOGD 0x1 | 21 | #define LOGGER_LOGD 0x01 |
22 | #define LOGGER_KERNEL 0x2 /* Reserved/Deprecated */ | 22 | #define LOGGER_KERNEL 0x02 /* Reserved/Deprecated */ |
23 | #define LOGGER_NULL 0x4 /* Does not release resources of other selections */ | 23 | #define LOGGER_NULL 0x04 /* Does not release resources of other selections */ |
24 | #define LOGGER_LOCAL 0x8 /* logs sent to local memory */ | 24 | #define LOGGER_LOCAL 0x08 /* logs sent to local memory */ |
25 | #define LOGGER_STDERR 0x10 /* logs sent to stderr */ | ||
25 | 26 | ||
26 | /* Both return the selected frontend flag mask, or negative errno */ | 27 | /* Both return the selected frontend flag mask, or negative errno */ |
27 | int android_set_log_frontend(int frontend_flag); | 28 | int android_set_log_frontend(int frontend_flag); |
diff --git a/liblog/logger_write.c b/liblog/logger_write.c index e149e682f..2a9710164 100644 --- a/liblog/logger_write.c +++ b/liblog/logger_write.c | |||
@@ -664,9 +664,9 @@ LIBLOG_ABI_PUBLIC int android_set_log_frontend(int frontend_flag) | |||
664 | return retval; | 664 | return retval; |
665 | } | 665 | } |
666 | 666 | ||
667 | __android_log_frontend &= LOGGER_LOCAL | LOGGER_LOGD; | 667 | __android_log_frontend &= LOGGER_LOCAL | LOGGER_LOGD | LOGGER_STDERR; |
668 | 668 | ||
669 | frontend_flag &= LOGGER_LOCAL | LOGGER_LOGD; | 669 | frontend_flag &= LOGGER_LOCAL | LOGGER_LOGD | LOGGER_STDERR; |
670 | 670 | ||
671 | if (__android_log_frontend != frontend_flag) { | 671 | if (__android_log_frontend != frontend_flag) { |
672 | __android_log_frontend = frontend_flag; | 672 | __android_log_frontend = frontend_flag; |
@@ -695,7 +695,7 @@ LIBLOG_ABI_PUBLIC int android_get_log_frontend() | |||
695 | if (write_to_log == __write_to_log_null) { | 695 | if (write_to_log == __write_to_log_null) { |
696 | ret = LOGGER_NULL; | 696 | ret = LOGGER_NULL; |
697 | } else { | 697 | } else { |
698 | __android_log_frontend &= LOGGER_LOCAL | LOGGER_LOGD; | 698 | __android_log_frontend &= LOGGER_LOCAL | LOGGER_LOGD | LOGGER_STDERR; |
699 | ret = __android_log_frontend; | 699 | ret = __android_log_frontend; |
700 | if ((write_to_log != __write_to_log_init) && | 700 | if ((write_to_log != __write_to_log_init) && |
701 | (write_to_log != __write_to_log_daemon)) { | 701 | (write_to_log != __write_to_log_daemon)) { |
diff --git a/liblog/stderr_write.c b/liblog/stderr_write.c new file mode 100644 index 000000000..b73929923 --- /dev/null +++ b/liblog/stderr_write.c | |||
@@ -0,0 +1,219 @@ | |||
1 | /* | ||
2 | * Copyright (C) 2017 The Android Open Source Project | ||
3 | * | ||
4 | * Licensed under the Apache License, Version 2.0 (the "License"); | ||
5 | * you may not use this file except in compliance with the License. | ||
6 | * You may obtain a copy of the License at | ||
7 | * | ||
8 | * http://www.apache.org/licenses/LICENSE-2.0 | ||
9 | * | ||
10 | * Unless required by applicable law or agreed to in writing, software | ||
11 | * distributed under the License is distributed on an "AS IS" BASIS, | ||
12 | * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | ||
13 | * See the License for the specific language governing permissions and | ||
14 | * limitations under the License. | ||
15 | */ | ||
16 | |||
17 | /* | ||
18 | * stderr write handler. Output is logcat-like, and responds to | ||
19 | * logcat's environment variables ANDROID_PRINTF_LOG and | ||
20 | * ANDROID_LOG_TAGS to filter output. | ||
21 | * | ||
22 | * This transport only provides a writer, that means that it does not | ||
23 | * provide an End-To-End capability as the logs are effectively _lost_ | ||
24 | * to the stderr file stream. The purpose of this transport is to | ||
25 | * supply a means for command line tools to report their logging | ||
26 | * to the stderr stream, in line with all other activities. | ||
27 | */ | ||
28 | |||
29 | #include <errno.h> | ||
30 | #include <stdbool.h> | ||
31 | #include <stdio.h> | ||
32 | #include <stdlib.h> | ||
33 | #include <string.h> | ||
34 | #include <sys/types.h> | ||
35 | #include <unistd.h> | ||
36 | |||
37 | #include <log/event_tag_map.h> | ||
38 | #include <log/log.h> | ||
39 | #include <log/logprint.h> | ||
40 | #include <log/uio.h> | ||
41 | |||
42 | #include "log_portability.h" | ||
43 | #include "logger.h" | ||
44 | |||
45 | static int stderrOpen(); | ||
46 | static void stderrClose(); | ||
47 | static int stderrAvailable(log_id_t logId); | ||
48 | static int stderrWrite(log_id_t logId, struct timespec* ts, | ||
49 | struct iovec* vec, size_t nr); | ||
50 | |||
51 | struct stderrContext { | ||
52 | AndroidLogFormat* logformat; | ||
53 | #if defined(__ANDROID__) | ||
54 | EventTagMap* eventTagMap; | ||
55 | #endif | ||
56 | }; | ||
57 | |||
58 | LIBLOG_HIDDEN struct android_log_transport_write stderrLoggerWrite = { | ||
59 | .node = { &stderrLoggerWrite.node, &stderrLoggerWrite.node }, | ||
60 | .context.private = NULL, | ||
61 | .name = "stderr", | ||
62 | .available = stderrAvailable, | ||
63 | .open = stderrOpen, | ||
64 | .close = stderrClose, | ||
65 | .write = stderrWrite, | ||
66 | }; | ||
67 | |||
68 | static int stderrOpen() | ||
69 | { | ||
70 | struct stderrContext* ctx; | ||
71 | const char* envStr; | ||
72 | bool setFormat; | ||
73 | |||
74 | if (!stderr || (fileno(stderr) < 0)) { | ||
75 | return -EBADF; | ||
76 | } | ||
77 | |||
78 | if (stderrLoggerWrite.context.private) { | ||
79 | return fileno(stderr); | ||
80 | } | ||
81 | |||
82 | ctx = calloc(1, sizeof(struct stderrContext)); | ||
83 | if (!ctx) { | ||
84 | return -ENOMEM; | ||
85 | } | ||
86 | |||
87 | ctx->logformat = android_log_format_new(); | ||
88 | if (!ctx->logformat) { | ||
89 | free(ctx); | ||
90 | return -ENOMEM; | ||
91 | } | ||
92 | |||
93 | envStr = getenv("ANDROID_PRINTF_LOG"); | ||
94 | setFormat = false; | ||
95 | |||
96 | if (envStr) { | ||
97 | char* formats = strdup(envStr); | ||
98 | char* sv = NULL; | ||
99 | char* arg = formats; | ||
100 | while (!!(arg = strtok_r(arg, ",:; \t\n\r\f", &sv))) { | ||
101 | AndroidLogPrintFormat format = android_log_formatFromString(arg); | ||
102 | arg = NULL; | ||
103 | if (format == FORMAT_OFF) { | ||
104 | continue; | ||
105 | } | ||
106 | if (android_log_setPrintFormat(ctx->logformat, format) <= 0) { | ||
107 | continue; | ||
108 | } | ||
109 | setFormat = true; | ||
110 | } | ||
111 | free(formats); | ||
112 | } | ||
113 | if (!setFormat) { | ||
114 | AndroidLogPrintFormat format = android_log_formatFromString( | ||
115 | "threadtime"); | ||
116 | android_log_setPrintFormat(ctx->logformat, format); | ||
117 | } | ||
118 | envStr = getenv("ANDROID_LOG_TAGS"); | ||
119 | if (envStr) { | ||
120 | android_log_addFilterString(ctx->logformat, envStr); | ||
121 | } | ||
122 | stderrLoggerWrite.context.private = ctx; | ||
123 | |||
124 | return fileno(stderr); | ||
125 | } | ||
126 | |||
127 | static void stderrClose() | ||
128 | { | ||
129 | struct stderrContext* ctx = stderrLoggerWrite.context.private; | ||
130 | |||
131 | if (ctx) { | ||
132 | stderrLoggerWrite.context.private = NULL; | ||
133 | if (ctx->logformat) { | ||
134 | android_log_format_free(ctx->logformat); | ||
135 | ctx->logformat = NULL; | ||
136 | } | ||
137 | #if defined(__ANDROID__) | ||
138 | if (ctx->eventTagMap) { | ||
139 | android_closeEventTagMap(ctx->eventTagMap); | ||
140 | ctx->eventTagMap = NULL; | ||
141 | } | ||
142 | #endif | ||
143 | } | ||
144 | } | ||
145 | |||
146 | static int stderrAvailable(log_id_t logId) | ||
147 | { | ||
148 | if ((logId >= LOG_ID_MAX) || (logId == LOG_ID_KERNEL)) { | ||
149 | return -EINVAL; | ||
150 | } | ||
151 | return 1; | ||
152 | } | ||
153 | |||
154 | static int stderrWrite(log_id_t logId, struct timespec* ts, | ||
155 | struct iovec* vec, size_t nr) | ||
156 | { | ||
157 | struct log_msg log_msg; | ||
158 | AndroidLogEntry entry; | ||
159 | char binaryMsgBuf[1024]; | ||
160 | int err; | ||
161 | size_t i; | ||
162 | struct stderrContext* ctx = stderrLoggerWrite.context.private; | ||
163 | |||
164 | if (!ctx) return -EBADF; | ||
165 | if (!vec || !nr) return -EINVAL; | ||
166 | |||
167 | log_msg.entry.len = 0; | ||
168 | log_msg.entry.hdr_size = sizeof(log_msg.entry); | ||
169 | log_msg.entry.pid = getpid(); | ||
170 | #ifdef __BIONIC__ | ||
171 | log_msg.entry.tid = gettid(); | ||
172 | #else | ||
173 | log_msg.entry.tid = getpid(); | ||
174 | #endif | ||
175 | log_msg.entry.sec = ts->tv_sec; | ||
176 | log_msg.entry.nsec = ts->tv_nsec; | ||
177 | log_msg.entry.lid = logId; | ||
178 | log_msg.entry.uid = __android_log_uid(); | ||
179 | |||
180 | for (i = 0; i < nr; ++i) { | ||
181 | size_t len = vec[i].iov_len; | ||
182 | if ((log_msg.entry.len + len) > LOGGER_ENTRY_MAX_PAYLOAD) { | ||
183 | len = LOGGER_ENTRY_MAX_PAYLOAD - log_msg.entry.len; | ||
184 | } | ||
185 | if (!len) continue; | ||
186 | memcpy(log_msg.entry.msg + log_msg.entry.len, vec[i].iov_base, len); | ||
187 | log_msg.entry.len += len; | ||
188 | } | ||
189 | |||
190 | if ((logId == LOG_ID_EVENTS) || (logId == LOG_ID_SECURITY)) { | ||
191 | #if defined(__ANDROID__) | ||
192 | if (!ctx->eventTagMap) { | ||
193 | ctx->eventTagMap = android_openEventTagMap(NULL); | ||
194 | } | ||
195 | #endif | ||
196 | err = android_log_processBinaryLogBuffer(&log_msg.entry_v1, | ||
197 | &entry, | ||
198 | #if defined(__ANDROID__) | ||
199 | ctx->eventTagMap, | ||
200 | #else | ||
201 | NULL, | ||
202 | #endif | ||
203 | binaryMsgBuf, | ||
204 | sizeof(binaryMsgBuf)); | ||
205 | } else { | ||
206 | err = android_log_processLogBuffer(&log_msg.entry_v1, &entry); | ||
207 | } | ||
208 | |||
209 | /* print known truncated data, in essence logcat --debug */ | ||
210 | if ((err < 0) && !entry.message) return -EINVAL; | ||
211 | |||
212 | if (!android_log_shouldPrintLine(ctx->logformat, entry.tag, entry.priority)) { | ||
213 | return log_msg.entry.len; | ||
214 | } | ||
215 | |||
216 | err = android_log_printLogLine(ctx->logformat, fileno(stderr), &entry); | ||
217 | if (err < 0) return errno ? -errno : -EINVAL; | ||
218 | return log_msg.entry.len; | ||
219 | } | ||
diff --git a/liblog/tests/Android.mk b/liblog/tests/Android.mk index cfea45202..0e6432ced 100644 --- a/liblog/tests/Android.mk +++ b/liblog/tests/Android.mk | |||
@@ -57,6 +57,8 @@ test_c_flags := \ | |||
57 | test_src_files := \ | 57 | test_src_files := \ |
58 | liblog_test_default.cpp \ | 58 | liblog_test_default.cpp \ |
59 | liblog_test_local.cpp \ | 59 | liblog_test_local.cpp \ |
60 | liblog_test_stderr.cpp \ | ||
61 | liblog_test_stderr_local.cpp \ | ||
60 | log_id_test.cpp \ | 62 | log_id_test.cpp \ |
61 | log_radio_test.cpp \ | 63 | log_radio_test.cpp \ |
62 | log_read_test.cpp \ | 64 | log_read_test.cpp \ |
diff --git a/liblog/tests/liblog_test.cpp b/liblog/tests/liblog_test.cpp index bc0ea4c25..2537fac23 100644 --- a/liblog/tests/liblog_test.cpp +++ b/liblog/tests/liblog_test.cpp | |||
@@ -47,7 +47,7 @@ | |||
47 | #endif | 47 | #endif |
48 | #endif | 48 | #endif |
49 | 49 | ||
50 | #if (!defined(USING_LOGGER_DEFAULT) || !defined(USING_LOGGER_LOCAL)) | 50 | #if (!defined(USING_LOGGER_DEFAULT) || !defined(USING_LOGGER_LOCAL) || !defined(USING_LOGGER_STDERR)) |
51 | #ifdef liblog // a binary clue that we are overriding the test names | 51 | #ifdef liblog // a binary clue that we are overriding the test names |
52 | // Does not support log reading blocking feature yet | 52 | // Does not support log reading blocking feature yet |
53 | // Does not support LOG_ID_SECURITY (unless we set LOGGER_LOCAL | LOGGER_LOGD) | 53 | // Does not support LOG_ID_SECURITY (unless we set LOGGER_LOCAL | LOGGER_LOGD) |
@@ -62,6 +62,11 @@ | |||
62 | #define USING_LOGGER_DEFAULT | 62 | #define USING_LOGGER_DEFAULT |
63 | #endif | 63 | #endif |
64 | #endif | 64 | #endif |
65 | #ifdef USING_LOGGER_STDERR | ||
66 | # define SUPPORTS_END_TO_END 0 | ||
67 | #else | ||
68 | # define SUPPORTS_END_TO_END 1 | ||
69 | #endif | ||
65 | 70 | ||
66 | // enhanced version of LOG_FAILURE_RETRY to add support for EAGAIN and | 71 | // enhanced version of LOG_FAILURE_RETRY to add support for EAGAIN and |
67 | // non-syscall libs. Since we are only using this in the emergency of | 72 | // non-syscall libs. Since we are only using this in the emergency of |
@@ -98,7 +103,7 @@ TEST(liblog, __android_log_btwrite) { | |||
98 | usleep(1000); | 103 | usleep(1000); |
99 | } | 104 | } |
100 | 105 | ||
101 | #if (defined(__ANDROID__) && !defined(USING_LOGGER_LOCAL)) | 106 | #if (defined(__ANDROID__) && defined(USING_LOGGER_DEFAULT)) |
102 | static std::string popenToString(std::string command) { | 107 | static std::string popenToString(std::string command) { |
103 | std::string ret; | 108 | std::string ret; |
104 | 109 | ||
@@ -176,8 +181,8 @@ TEST(liblog, __android_log_btwrite__android_logger_list_read) { | |||
176 | LOG_ID_EVENTS, ANDROID_LOG_RDONLY | ANDROID_LOG_NONBLOCK, 1000, pid))); | 181 | LOG_ID_EVENTS, ANDROID_LOG_RDONLY | ANDROID_LOG_NONBLOCK, 1000, pid))); |
177 | 182 | ||
178 | log_time ts(CLOCK_MONOTONIC); | 183 | log_time ts(CLOCK_MONOTONIC); |
179 | ASSERT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); | 184 | EXPECT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); |
180 | #ifndef USING_LOGGER_LOCAL | 185 | #ifdef USING_LOGGER_DEFAULT |
181 | // Check that we can close and reopen the logger | 186 | // Check that we can close and reopen the logger |
182 | bool pmsgActiveAfter__android_log_btwrite; | 187 | bool pmsgActiveAfter__android_log_btwrite; |
183 | bool logdwActiveAfter__android_log_btwrite; | 188 | bool logdwActiveAfter__android_log_btwrite; |
@@ -200,8 +205,8 @@ TEST(liblog, __android_log_btwrite__android_logger_list_read) { | |||
200 | #endif | 205 | #endif |
201 | 206 | ||
202 | log_time ts1(CLOCK_MONOTONIC); | 207 | log_time ts1(CLOCK_MONOTONIC); |
203 | ASSERT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts1, sizeof(ts1))); | 208 | EXPECT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts1, sizeof(ts1))); |
204 | #ifndef USING_LOGGER_LOCAL | 209 | #ifdef USING_LOGGER_DEFAULT |
205 | if (getuid() == AID_ROOT) { | 210 | if (getuid() == AID_ROOT) { |
206 | pmsgActiveAfter__android_log_btwrite = isPmsgActive(); | 211 | pmsgActiveAfter__android_log_btwrite = isPmsgActive(); |
207 | logdwActiveAfter__android_log_btwrite = isLogdwActive(); | 212 | logdwActiveAfter__android_log_btwrite = isLogdwActive(); |
@@ -220,7 +225,7 @@ TEST(liblog, __android_log_btwrite__android_logger_list_read) { | |||
220 | break; | 225 | break; |
221 | } | 226 | } |
222 | 227 | ||
223 | ASSERT_EQ(log_msg.entry.pid, pid); | 228 | EXPECT_EQ(log_msg.entry.pid, pid); |
224 | 229 | ||
225 | if ((log_msg.entry.len != sizeof(android_log_event_long_t)) | 230 | if ((log_msg.entry.len != sizeof(android_log_event_long_t)) |
226 | || (log_msg.id() != LOG_ID_EVENTS)) { | 231 | || (log_msg.id() != LOG_ID_EVENTS)) { |
@@ -242,8 +247,8 @@ TEST(liblog, __android_log_btwrite__android_logger_list_read) { | |||
242 | } | 247 | } |
243 | } | 248 | } |
244 | 249 | ||
245 | EXPECT_EQ(1, count); | 250 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
246 | EXPECT_EQ(1, second_count); | 251 | EXPECT_EQ(SUPPORTS_END_TO_END, second_count); |
247 | 252 | ||
248 | android_logger_list_close(logger_list); | 253 | android_logger_list_close(logger_list); |
249 | #else | 254 | #else |
@@ -251,6 +256,54 @@ TEST(liblog, __android_log_btwrite__android_logger_list_read) { | |||
251 | #endif | 256 | #endif |
252 | } | 257 | } |
253 | 258 | ||
259 | #if (defined(__ANDROID__) || defined(USING_LOGGER_LOCAL)) | ||
260 | static void print_frontend(const char* prefix, int logger) { | ||
261 | static const char orstr[] = " | "; | ||
262 | |||
263 | if (!prefix) { | ||
264 | prefix = ""; | ||
265 | } | ||
266 | if (logger < 0) { | ||
267 | fprintf(stderr, "%s%s\n", prefix, strerror(-logger)); | ||
268 | return; | ||
269 | } | ||
270 | |||
271 | if (logger == LOGGER_DEFAULT) { | ||
272 | fprintf(stderr, "%sLOGGER_DEFAULT", prefix); | ||
273 | prefix = orstr; | ||
274 | } | ||
275 | if (logger & LOGGER_LOGD) { | ||
276 | fprintf(stderr, "%sLOGGER_LOGD", prefix); | ||
277 | prefix = orstr; | ||
278 | } | ||
279 | if (logger & LOGGER_KERNEL) { | ||
280 | fprintf(stderr, "%sLOGGER_KERNEL", prefix); | ||
281 | prefix = orstr; | ||
282 | } | ||
283 | if (logger & LOGGER_NULL) { | ||
284 | fprintf(stderr, "%sLOGGER_NULL", prefix); | ||
285 | prefix = orstr; | ||
286 | } | ||
287 | if (logger & LOGGER_LOCAL) { | ||
288 | fprintf(stderr, "%sLOGGER_LOCAL", prefix); | ||
289 | prefix = orstr; | ||
290 | } | ||
291 | if (logger & LOGGER_STDERR) { | ||
292 | fprintf(stderr, "%sLOGGER_STDERR", prefix); | ||
293 | prefix = orstr; | ||
294 | } | ||
295 | logger &= ~(LOGGER_LOGD | LOGGER_KERNEL | LOGGER_NULL | LOGGER_LOCAL | | ||
296 | LOGGER_STDERR); | ||
297 | if (logger) { | ||
298 | fprintf(stderr, "%s0x%x", prefix, logger); | ||
299 | prefix = orstr; | ||
300 | } | ||
301 | if (prefix == orstr) { | ||
302 | fprintf(stderr, "\n"); | ||
303 | } | ||
304 | } | ||
305 | #endif | ||
306 | |||
254 | // This test makes little sense standalone, and requires the tests ahead | 307 | // This test makes little sense standalone, and requires the tests ahead |
255 | // and behind us, to make us whole. We could incorporate a prefix and | 308 | // and behind us, to make us whole. We could incorporate a prefix and |
256 | // suffix test to make this standalone, but opted to not complicate this. | 309 | // suffix test to make this standalone, but opted to not complicate this. |
@@ -261,10 +314,14 @@ TEST(liblog, android_set_log_frontend) { | |||
261 | #endif | 314 | #endif |
262 | 315 | ||
263 | int logger = android_get_log_frontend(); | 316 | int logger = android_get_log_frontend(); |
317 | print_frontend("android_get_log_frontend = ", logger); | ||
264 | EXPECT_NE(LOGGER_NULL, logger); | 318 | EXPECT_NE(LOGGER_NULL, logger); |
265 | 319 | ||
266 | EXPECT_EQ(LOGGER_NULL, android_set_log_frontend(LOGGER_NULL)); | 320 | int ret; |
267 | EXPECT_EQ(LOGGER_NULL, android_get_log_frontend()); | 321 | EXPECT_EQ(LOGGER_NULL, ret = android_set_log_frontend(LOGGER_NULL)); |
322 | print_frontend("android_set_log_frontend = ", ret); | ||
323 | EXPECT_EQ(LOGGER_NULL, ret = android_get_log_frontend()); | ||
324 | print_frontend("android_get_log_frontend = ", ret); | ||
268 | 325 | ||
269 | pid_t pid = getpid(); | 326 | pid_t pid = getpid(); |
270 | 327 | ||
@@ -273,7 +330,7 @@ TEST(liblog, android_set_log_frontend) { | |||
273 | LOG_ID_EVENTS, ANDROID_LOG_RDONLY | ANDROID_LOG_NONBLOCK, 1000, pid))); | 330 | LOG_ID_EVENTS, ANDROID_LOG_RDONLY | ANDROID_LOG_NONBLOCK, 1000, pid))); |
274 | 331 | ||
275 | log_time ts(CLOCK_MONOTONIC); | 332 | log_time ts(CLOCK_MONOTONIC); |
276 | ASSERT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); | 333 | EXPECT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); |
277 | 334 | ||
278 | usleep(1000000); | 335 | usleep(1000000); |
279 | 336 | ||
@@ -285,7 +342,7 @@ TEST(liblog, android_set_log_frontend) { | |||
285 | break; | 342 | break; |
286 | } | 343 | } |
287 | 344 | ||
288 | ASSERT_EQ(log_msg.entry.pid, pid); | 345 | EXPECT_EQ(log_msg.entry.pid, pid); |
289 | 346 | ||
290 | if ((log_msg.entry.len != sizeof(android_log_event_long_t)) | 347 | if ((log_msg.entry.len != sizeof(android_log_event_long_t)) |
291 | || (log_msg.id() != LOG_ID_EVENTS)) { | 348 | || (log_msg.id() != LOG_ID_EVENTS)) { |
@@ -307,8 +364,10 @@ TEST(liblog, android_set_log_frontend) { | |||
307 | 364 | ||
308 | android_logger_list_close(logger_list); | 365 | android_logger_list_close(logger_list); |
309 | 366 | ||
310 | EXPECT_EQ(logger, android_set_log_frontend(logger)); | 367 | EXPECT_EQ(logger, ret = android_set_log_frontend(logger)); |
311 | EXPECT_EQ(logger, android_get_log_frontend()); | 368 | print_frontend("android_set_log_frontend = ", ret); |
369 | EXPECT_EQ(logger, ret = android_get_log_frontend()); | ||
370 | print_frontend("android_get_log_frontend = ", ret); | ||
312 | 371 | ||
313 | // False negative if liblog.__android_log_btwrite__android_logger_list_read | 372 | // False negative if liblog.__android_log_btwrite__android_logger_list_read |
314 | // fails above, so we will likely succeed. But we will have so many | 373 | // fails above, so we will likely succeed. But we will have so many |
@@ -350,7 +409,7 @@ static void bswrite_test(const char *message) { | |||
350 | log_time ts(CLOCK_REALTIME); | 409 | log_time ts(CLOCK_REALTIME); |
351 | #endif | 410 | #endif |
352 | 411 | ||
353 | ASSERT_LT(0, __android_log_bswrite(0, message)); | 412 | EXPECT_LT(0, __android_log_bswrite(0, message)); |
354 | size_t num_lines = 1, size = 0, length = 0, total = 0; | 413 | size_t num_lines = 1, size = 0, length = 0, total = 0; |
355 | const char *cp = message; | 414 | const char *cp = message; |
356 | while (*cp) { | 415 | while (*cp) { |
@@ -382,7 +441,7 @@ static void bswrite_test(const char *message) { | |||
382 | break; | 441 | break; |
383 | } | 442 | } |
384 | 443 | ||
385 | ASSERT_EQ(log_msg.entry.pid, pid); | 444 | EXPECT_EQ(log_msg.entry.pid, pid); |
386 | 445 | ||
387 | if ((log_msg.entry.sec < (ts.tv_sec - 1)) | 446 | if ((log_msg.entry.sec < (ts.tv_sec - 1)) |
388 | || ((ts.tv_sec + 1) < log_msg.entry.sec) | 447 | || ((ts.tv_sec + 1) < log_msg.entry.sec) |
@@ -413,19 +472,26 @@ static void bswrite_test(const char *message) { | |||
413 | int processBinaryLogBuffer = android_log_processBinaryLogBuffer( | 472 | int processBinaryLogBuffer = android_log_processBinaryLogBuffer( |
414 | &log_msg.entry_v1, &entry, NULL, msgBuf, sizeof(msgBuf)); | 473 | &log_msg.entry_v1, &entry, NULL, msgBuf, sizeof(msgBuf)); |
415 | EXPECT_EQ((length == total) ? 0 : -1, processBinaryLogBuffer); | 474 | EXPECT_EQ((length == total) ? 0 : -1, processBinaryLogBuffer); |
416 | if (processBinaryLogBuffer == 0) { | 475 | if ((processBinaryLogBuffer == 0) || entry.message) { |
417 | size_t line_overhead = 20; | 476 | size_t line_overhead = 20; |
418 | if (pid > 99999) ++line_overhead; | 477 | if (pid > 99999) ++line_overhead; |
419 | if (pid > 999999) ++line_overhead; | 478 | if (pid > 999999) ++line_overhead; |
420 | fflush(stderr); | 479 | fflush(stderr); |
421 | EXPECT_EQ((int)((line_overhead * num_lines) + size), | 480 | if (processBinaryLogBuffer) { |
422 | android_log_printLogLine(logformat, fileno(stderr), &entry)); | 481 | EXPECT_GT((int)((line_overhead * num_lines) + size), |
482 | android_log_printLogLine(logformat, | ||
483 | fileno(stderr), &entry)); | ||
484 | } else { | ||
485 | EXPECT_EQ((int)((line_overhead * num_lines) + size), | ||
486 | android_log_printLogLine(logformat, | ||
487 | fileno(stderr), &entry)); | ||
488 | } | ||
423 | } | 489 | } |
424 | android_log_format_free(logformat); | 490 | android_log_format_free(logformat); |
425 | } | 491 | } |
426 | } | 492 | } |
427 | 493 | ||
428 | EXPECT_EQ(1, count); | 494 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
429 | 495 | ||
430 | android_logger_list_close(logger_list); | 496 | android_logger_list_close(logger_list); |
431 | #else | 497 | #else |
@@ -527,7 +593,7 @@ static void buf_write_test(const char *message) { | |||
527 | android_log_format_free(logformat); | 593 | android_log_format_free(logformat); |
528 | } | 594 | } |
529 | 595 | ||
530 | EXPECT_EQ(1, count); | 596 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
531 | 597 | ||
532 | android_logger_list_close(logger_list); | 598 | android_logger_list_close(logger_list); |
533 | #else | 599 | #else |
@@ -1058,10 +1124,14 @@ TEST(liblog, max_payload) { | |||
1058 | 1124 | ||
1059 | android_logger_list_close(logger_list); | 1125 | android_logger_list_close(logger_list); |
1060 | 1126 | ||
1127 | #if SUPPORTS_END_TO_END | ||
1061 | EXPECT_EQ(true, matches); | 1128 | EXPECT_EQ(true, matches); |
1062 | 1129 | ||
1063 | EXPECT_LE(SIZEOF_MAX_PAYLOAD_BUF, static_cast<size_t>(max_len)); | 1130 | EXPECT_LE(SIZEOF_MAX_PAYLOAD_BUF, static_cast<size_t>(max_len)); |
1064 | #else | 1131 | #else |
1132 | EXPECT_EQ(false, matches); | ||
1133 | #endif | ||
1134 | #else | ||
1065 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 1135 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
1066 | #endif | 1136 | #endif |
1067 | } | 1137 | } |
@@ -1123,7 +1193,7 @@ TEST(liblog, __android_log_buf_print__maxtag) { | |||
1123 | android_log_format_free(logformat); | 1193 | android_log_format_free(logformat); |
1124 | } | 1194 | } |
1125 | 1195 | ||
1126 | EXPECT_EQ(1, count); | 1196 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
1127 | 1197 | ||
1128 | android_logger_list_close(logger_list); | 1198 | android_logger_list_close(logger_list); |
1129 | #else | 1199 | #else |
@@ -1184,6 +1254,11 @@ TEST(liblog, too_big_payload) { | |||
1184 | 1254 | ||
1185 | android_logger_list_close(logger_list); | 1255 | android_logger_list_close(logger_list); |
1186 | 1256 | ||
1257 | #if !SUPPORTS_END_TO_END | ||
1258 | max_len = max_len ? | ||
1259 | max_len : | ||
1260 | LOGGER_ENTRY_MAX_PAYLOAD - sizeof(big_payload_tag); | ||
1261 | #endif | ||
1187 | EXPECT_LE(LOGGER_ENTRY_MAX_PAYLOAD - sizeof(big_payload_tag), | 1262 | EXPECT_LE(LOGGER_ENTRY_MAX_PAYLOAD - sizeof(big_payload_tag), |
1188 | static_cast<size_t>(max_len)); | 1263 | static_cast<size_t>(max_len)); |
1189 | 1264 | ||
@@ -1255,14 +1330,14 @@ TEST(liblog, dual_reader) { | |||
1255 | android_logger_list_close(logger_list1); | 1330 | android_logger_list_close(logger_list1); |
1256 | android_logger_list_close(logger_list2); | 1331 | android_logger_list_close(logger_list2); |
1257 | 1332 | ||
1258 | EXPECT_EQ(num, count1); | 1333 | EXPECT_EQ(num * SUPPORTS_END_TO_END, count1); |
1259 | EXPECT_EQ(num - 10, count2); | 1334 | EXPECT_EQ((num - 10) * SUPPORTS_END_TO_END, count2); |
1260 | #else | 1335 | #else |
1261 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 1336 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
1262 | #endif | 1337 | #endif |
1263 | } | 1338 | } |
1264 | 1339 | ||
1265 | #ifndef USING_LOGGER_LOCAL // Do not retest logprint | 1340 | #ifdef USING_LOGGER_DEFAULT // Do not retest logprint |
1266 | static bool checkPriForTag(AndroidLogFormat *p_format, const char *tag, android_LogPriority pri) { | 1341 | static bool checkPriForTag(AndroidLogFormat *p_format, const char *tag, android_LogPriority pri) { |
1267 | return android_log_shouldPrintLine(p_format, tag, pri) | 1342 | return android_log_shouldPrintLine(p_format, tag, pri) |
1268 | && !android_log_shouldPrintLine(p_format, tag, (android_LogPriority)(pri - 1)); | 1343 | && !android_log_shouldPrintLine(p_format, tag, (android_LogPriority)(pri - 1)); |
@@ -1331,9 +1406,9 @@ TEST(liblog, filterRule) { | |||
1331 | 1406 | ||
1332 | android_log_format_free(p_format); | 1407 | android_log_format_free(p_format); |
1333 | } | 1408 | } |
1334 | #endif // !USING_LOGGER_LOCAL | 1409 | #endif // USING_LOGGER_DEFAULT |
1335 | 1410 | ||
1336 | #ifndef USING_LOGGER_LOCAL // Do not retest property handling | 1411 | #ifdef USING_LOGGER_DEFAULT // Do not retest property handling |
1337 | TEST(liblog, is_loggable) { | 1412 | TEST(liblog, is_loggable) { |
1338 | #ifdef __ANDROID__ | 1413 | #ifdef __ANDROID__ |
1339 | static const char tag[] = "is_loggable"; | 1414 | static const char tag[] = "is_loggable"; |
@@ -1632,12 +1707,12 @@ TEST(liblog, is_loggable) { | |||
1632 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 1707 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
1633 | #endif | 1708 | #endif |
1634 | } | 1709 | } |
1635 | #endif // !USING_LOGGER_LOCAL | 1710 | #endif // USING_LOGGER_DEFAULT |
1636 | 1711 | ||
1637 | // Following tests the specific issues surrounding error handling wrt logd. | 1712 | // Following tests the specific issues surrounding error handling wrt logd. |
1638 | // Kills logd and toss all collected data, equivalent to logcat -b all -c, | 1713 | // Kills logd and toss all collected data, equivalent to logcat -b all -c, |
1639 | // except we also return errors to the logging callers. | 1714 | // except we also return errors to the logging callers. |
1640 | #ifndef USING_LOGGER_LOCAL | 1715 | #ifdef USING_LOGGER_DEFAULT |
1641 | #ifdef TEST_PREFIX | 1716 | #ifdef TEST_PREFIX |
1642 | // helper to liblog.enoent to count end-to-end matching logging messages. | 1717 | // helper to liblog.enoent to count end-to-end matching logging messages. |
1643 | static int count_matching_ts(log_time ts) { | 1718 | static int count_matching_ts(log_time ts) { |
@@ -1687,7 +1762,7 @@ TEST(liblog, enoent) { | |||
1687 | TEST_PREFIX | 1762 | TEST_PREFIX |
1688 | log_time ts(CLOCK_MONOTONIC); | 1763 | log_time ts(CLOCK_MONOTONIC); |
1689 | EXPECT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); | 1764 | EXPECT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); |
1690 | EXPECT_EQ(1, count_matching_ts(ts)); | 1765 | EXPECT_EQ(SUPPORTS_END_TO_END, count_matching_ts(ts)); |
1691 | 1766 | ||
1692 | // This call will fail if we are setuid(AID_SYSTEM), beware of any | 1767 | // This call will fail if we are setuid(AID_SYSTEM), beware of any |
1693 | // test prior to this one playing with setuid and causing interference. | 1768 | // test prior to this one playing with setuid and causing interference. |
@@ -1732,18 +1807,18 @@ TEST(liblog, enoent) { | |||
1732 | 1807 | ||
1733 | ts = log_time(CLOCK_MONOTONIC); | 1808 | ts = log_time(CLOCK_MONOTONIC); |
1734 | EXPECT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); | 1809 | EXPECT_LT(0, __android_log_btwrite(0, EVENT_TYPE_LONG, &ts, sizeof(ts))); |
1735 | EXPECT_EQ(1, count_matching_ts(ts)); | 1810 | EXPECT_EQ(SUPPORTS_END_TO_END, count_matching_ts(ts)); |
1736 | 1811 | ||
1737 | #else | 1812 | #else |
1738 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 1813 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
1739 | #endif | 1814 | #endif |
1740 | } | 1815 | } |
1741 | #endif // !USING_LOCAL_LOGGER | 1816 | #endif // USING_LOCAL_LOGD |
1742 | 1817 | ||
1743 | // Below this point we run risks of setuid(AID_SYSTEM) which may affect others. | 1818 | // Below this point we run risks of setuid(AID_SYSTEM) which may affect others. |
1744 | 1819 | ||
1745 | // Do not retest properties, and cannot log into LOG_ID_SECURITY | 1820 | // Do not retest properties, and cannot log into LOG_ID_SECURITY |
1746 | #ifndef USING_LOGGER_LOCAL | 1821 | #ifdef USING_LOGGER_DEFAULT |
1747 | TEST(liblog, __security) { | 1822 | TEST(liblog, __security) { |
1748 | #ifdef __ANDROID__ | 1823 | #ifdef __ANDROID__ |
1749 | static const char persist_key[] = "persist.logd.security"; | 1824 | static const char persist_key[] = "persist.logd.security"; |
@@ -1929,7 +2004,7 @@ TEST(liblog, __security_buffer) { | |||
1929 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 2004 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
1930 | #endif | 2005 | #endif |
1931 | } | 2006 | } |
1932 | #endif // !USING_LOGGER_LOCAL | 2007 | #endif // USING_LOGGER_DEFAULT |
1933 | 2008 | ||
1934 | #ifdef TEST_PREFIX | 2009 | #ifdef TEST_PREFIX |
1935 | static void android_errorWriteWithInfoLog_helper(int TAG, const char* SUBTAG, | 2010 | static void android_errorWriteWithInfoLog_helper(int TAG, const char* SUBTAG, |
@@ -2047,7 +2122,7 @@ TEST(liblog, android_errorWriteWithInfoLog__android_logger_list_read__typical) { | |||
2047 | max_payload_buf, | 2122 | max_payload_buf, |
2048 | 200, | 2123 | 200, |
2049 | count); | 2124 | count); |
2050 | EXPECT_EQ(1, count); | 2125 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
2051 | #else | 2126 | #else |
2052 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 2127 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
2053 | #endif | 2128 | #endif |
@@ -2063,7 +2138,7 @@ TEST(liblog, android_errorWriteWithInfoLog__android_logger_list_read__data_too_l | |||
2063 | max_payload_buf, | 2138 | max_payload_buf, |
2064 | sizeof(max_payload_buf), | 2139 | sizeof(max_payload_buf), |
2065 | count); | 2140 | count); |
2066 | EXPECT_EQ(1, count); | 2141 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
2067 | #else | 2142 | #else |
2068 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 2143 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
2069 | #endif | 2144 | #endif |
@@ -2095,7 +2170,7 @@ TEST(liblog, android_errorWriteWithInfoLog__android_logger_list_read__subtag_too | |||
2095 | max_payload_buf, | 2170 | max_payload_buf, |
2096 | 200, | 2171 | 200, |
2097 | count); | 2172 | count); |
2098 | EXPECT_EQ(1, count); | 2173 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
2099 | #else | 2174 | #else |
2100 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 2175 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
2101 | #endif | 2176 | #endif |
@@ -2118,6 +2193,46 @@ static void android_errorWriteLog_helper(int TAG, const char *SUBTAG, int& count | |||
2118 | 2193 | ||
2119 | count = 0; | 2194 | count = 0; |
2120 | 2195 | ||
2196 | // Do a Before and After on the count to measure the effect. Decrement | ||
2197 | // what we find in Before to set the stage. | ||
2198 | ASSERT_TRUE(NULL != (logger_list = android_logger_list_open( | ||
2199 | LOG_ID_EVENTS, ANDROID_LOG_RDONLY | ANDROID_LOG_NONBLOCK, 1000, pid))); | ||
2200 | |||
2201 | for (;;) { | ||
2202 | log_msg log_msg; | ||
2203 | if (android_logger_list_read(logger_list, &log_msg) <= 0) break; | ||
2204 | |||
2205 | char *eventData = log_msg.msg(); | ||
2206 | if (!eventData) continue; | ||
2207 | |||
2208 | // Tag | ||
2209 | int tag = get4LE(eventData); | ||
2210 | eventData += 4; | ||
2211 | |||
2212 | if (tag != TAG) continue; | ||
2213 | |||
2214 | if (!SUBTAG) { | ||
2215 | // This tag should not have been written because the data was null | ||
2216 | --count; | ||
2217 | break; | ||
2218 | } | ||
2219 | |||
2220 | // List type | ||
2221 | eventData++; | ||
2222 | // Number of elements in list | ||
2223 | eventData++; | ||
2224 | // Element #1: string type for subtag | ||
2225 | eventData++; | ||
2226 | |||
2227 | eventData +=4; | ||
2228 | |||
2229 | if (memcmp(SUBTAG, eventData, strlen(SUBTAG))) continue; | ||
2230 | --count; | ||
2231 | } | ||
2232 | |||
2233 | android_logger_list_close(logger_list); | ||
2234 | |||
2235 | // Do an After on the count to measure the effect. | ||
2121 | ASSERT_TRUE(NULL != (logger_list = android_logger_list_open( | 2236 | ASSERT_TRUE(NULL != (logger_list = android_logger_list_open( |
2122 | LOG_ID_EVENTS, ANDROID_LOG_RDONLY | ANDROID_LOG_NONBLOCK, 1000, pid))); | 2237 | LOG_ID_EVENTS, ANDROID_LOG_RDONLY | ANDROID_LOG_NONBLOCK, 1000, pid))); |
2123 | 2238 | ||
@@ -2184,7 +2299,7 @@ TEST(liblog, android_errorWriteLog__android_logger_list_read__success) { | |||
2184 | #ifdef TEST_PREFIX | 2299 | #ifdef TEST_PREFIX |
2185 | int count; | 2300 | int count; |
2186 | android_errorWriteLog_helper(123456785, "test-subtag", count); | 2301 | android_errorWriteLog_helper(123456785, "test-subtag", count); |
2187 | EXPECT_EQ(1, count); | 2302 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
2188 | #else | 2303 | #else |
2189 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 2304 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
2190 | #endif | 2305 | #endif |
@@ -2703,7 +2818,7 @@ static void create_android_logger(const char *(*fn)(uint32_t tag, size_t &expect | |||
2703 | EXPECT_EQ(0, strcmp(expected_string, msgBuf)); | 2818 | EXPECT_EQ(0, strcmp(expected_string, msgBuf)); |
2704 | } | 2819 | } |
2705 | 2820 | ||
2706 | EXPECT_EQ(1, count); | 2821 | EXPECT_EQ(SUPPORTS_END_TO_END, count); |
2707 | 2822 | ||
2708 | android_logger_list_close(logger_list); | 2823 | android_logger_list_close(logger_list); |
2709 | } | 2824 | } |
@@ -2789,7 +2904,7 @@ TEST(liblog, create_android_logger_android_log_error_write_null) { | |||
2789 | #endif | 2904 | #endif |
2790 | } | 2905 | } |
2791 | 2906 | ||
2792 | #ifndef USING_LOGGER_LOCAL // Do not retest logger list handling | 2907 | #ifdef USING_LOGGER_DEFAULT // Do not retest logger list handling |
2793 | TEST(liblog, create_android_logger_overflow) { | 2908 | TEST(liblog, create_android_logger_overflow) { |
2794 | android_log_context ctx; | 2909 | android_log_context ctx; |
2795 | 2910 | ||
@@ -2829,9 +2944,9 @@ TEST(liblog, android_log_write_list_buffer) { | |||
2829 | msgBuf, sizeof(msgBuf)), 0); | 2944 | msgBuf, sizeof(msgBuf)), 0); |
2830 | EXPECT_STREQ(msgBuf, "[1005,tag_def,(tag|1),(name|3),(format|3)]"); | 2945 | EXPECT_STREQ(msgBuf, "[1005,tag_def,(tag|1),(name|3),(format|3)]"); |
2831 | } | 2946 | } |
2832 | #endif // !USING_LOGGER_LOCAL | 2947 | #endif // USING_LOGGER_DEFAULT |
2833 | 2948 | ||
2834 | #ifndef USING_LOGGER_LOCAL // Do not retest pmsg functionality | 2949 | #ifdef USING_LOGGER_DEFAULT // Do not retest pmsg functionality |
2835 | #ifdef __ANDROID__ | 2950 | #ifdef __ANDROID__ |
2836 | static const char __pmsg_file[] = | 2951 | static const char __pmsg_file[] = |
2837 | "/data/william-shakespeare/MuchAdoAboutNothing.txt"; | 2952 | "/data/william-shakespeare/MuchAdoAboutNothing.txt"; |
@@ -2957,9 +3072,9 @@ TEST(liblog, __android_log_pmsg_file_read) { | |||
2957 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 3072 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
2958 | #endif | 3073 | #endif |
2959 | } | 3074 | } |
2960 | #endif // !USING_LOGGER_LOCAL | 3075 | #endif // USING_LOGGER_DEFAULT |
2961 | 3076 | ||
2962 | #ifndef USING_LOGGER_LOCAL // Do not retest event mapping functionality | 3077 | #ifdef USING_LOGGER_DEFAULT // Do not retest event mapping functionality |
2963 | #ifdef __ANDROID__ | 3078 | #ifdef __ANDROID__ |
2964 | // must be: '<needle:> 0 kB' | 3079 | // must be: '<needle:> 0 kB' |
2965 | static bool isZero(const std::string &content, std::string::size_type pos, | 3080 | static bool isZero(const std::string &content, std::string::size_type pos, |
@@ -3063,9 +3178,9 @@ TEST(liblog, event_log_tags) { | |||
3063 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 3178 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
3064 | #endif | 3179 | #endif |
3065 | } | 3180 | } |
3066 | #endif // !USING_LOGGER_LOCAL | 3181 | #endif // USING_LOGGER_DEFAULT |
3067 | 3182 | ||
3068 | #ifndef USING_LOGGER_LOCAL // Do not retest ratelimit | 3183 | #ifdef USING_LOGGER_DEFAULT // Do not retest ratelimit |
3069 | TEST(liblog, __android_log_ratelimit) { | 3184 | TEST(liblog, __android_log_ratelimit) { |
3070 | time_t state = 0; | 3185 | time_t state = 0; |
3071 | 3186 | ||
@@ -3097,9 +3212,9 @@ TEST(liblog, __android_log_ratelimit) { | |||
3097 | } | 3212 | } |
3098 | // Do not test default seconds, to allow liblog to tune freely | 3213 | // Do not test default seconds, to allow liblog to tune freely |
3099 | } | 3214 | } |
3100 | #endif // !USING_LOGGER_LOCAL | 3215 | #endif // USING_LOGGER_DEFAULT |
3101 | 3216 | ||
3102 | #ifndef USING_LOGGER_LOCAL // Do not retest event mapping functionality | 3217 | #ifdef USING_LOGGER_DEFAULT // Do not retest event mapping functionality |
3103 | TEST(liblog, android_lookupEventTagNum) { | 3218 | TEST(liblog, android_lookupEventTagNum) { |
3104 | #ifdef __ANDROID__ | 3219 | #ifdef __ANDROID__ |
3105 | EventTagMap* map = android_openEventTagMap(NULL); | 3220 | EventTagMap* map = android_openEventTagMap(NULL); |
@@ -3115,4 +3230,4 @@ TEST(liblog, android_lookupEventTagNum) { | |||
3115 | GTEST_LOG_(INFO) << "This test does nothing.\n"; | 3230 | GTEST_LOG_(INFO) << "This test does nothing.\n"; |
3116 | #endif | 3231 | #endif |
3117 | } | 3232 | } |
3118 | #endif // !USING_LOGGER_LOCAL | 3233 | #endif // USING_LOGGER_DEFAULT |
diff --git a/liblog/tests/liblog_test_stderr.cpp b/liblog/tests/liblog_test_stderr.cpp new file mode 100644 index 000000000..f0cb192d7 --- /dev/null +++ b/liblog/tests/liblog_test_stderr.cpp | |||
@@ -0,0 +1,5 @@ | |||
1 | #include <log/log_frontend.h> | ||
2 | #define liblog liblog_stderr | ||
3 | #define TEST_PREFIX android_set_log_frontend(LOGGER_STDERR); | ||
4 | #define USING_LOGGER_STDERR | ||
5 | #include "liblog_test.cpp" | ||
diff --git a/liblog/tests/liblog_test_stderr_local.cpp b/liblog/tests/liblog_test_stderr_local.cpp new file mode 100644 index 000000000..1555b4e00 --- /dev/null +++ b/liblog/tests/liblog_test_stderr_local.cpp | |||
@@ -0,0 +1,4 @@ | |||
1 | #include <log/log_frontend.h> | ||
2 | #define liblog liblog_stderr_local | ||
3 | #define TEST_PREFIX android_set_log_frontend(LOGGER_LOCAL | LOGGER_STDERR); | ||
4 | #include "liblog_test.cpp" | ||