diff options
Diffstat (limited to 'base/include/android-base/logging.h')
-rw-r--r-- | base/include/android-base/logging.h | 3 |
1 files changed, 3 insertions, 0 deletions
diff --git a/base/include/android-base/logging.h b/base/include/android-base/logging.h index afff2c951..cc7aaf68c 100644 --- a/base/include/android-base/logging.h +++ b/base/include/android-base/logging.h | |||
@@ -105,6 +105,9 @@ void StderrLogger(LogId, LogSeverity, const char*, const char*, unsigned int, co | |||
105 | 105 | ||
106 | void DefaultAborter(const char* abort_message); | 106 | void DefaultAborter(const char* abort_message); |
107 | 107 | ||
108 | std::string GetDefaultTag(); | ||
109 | void SetDefaultTag(const std::string& tag); | ||
110 | |||
108 | #ifdef __ANDROID__ | 111 | #ifdef __ANDROID__ |
109 | // We expose this even though it is the default because a user that wants to | 112 | // We expose this even though it is the default because a user that wants to |
110 | // override the default log buffer will have to construct this themselves. | 113 | // override the default log buffer will have to construct this themselves. |