diff options
Diffstat (limited to 'init/init_parser.h')
-rw-r--r-- | init/init_parser.h | 6 |
1 files changed, 6 insertions, 0 deletions
diff --git a/init/init_parser.h b/init/init_parser.h index 722ebb26a..c07a69967 100644 --- a/init/init_parser.h +++ b/init/init_parser.h | |||
@@ -45,6 +45,9 @@ | |||
45 | // This function is called at the end of the file. | 45 | // This function is called at the end of the file. |
46 | // It indicates that the parsing has completed and any relevant objects should be committed. | 46 | // It indicates that the parsing has completed and any relevant objects should be committed. |
47 | 47 | ||
48 | namespace android { | ||
49 | namespace init { | ||
50 | |||
48 | class SectionParser { | 51 | class SectionParser { |
49 | public: | 52 | public: |
50 | virtual ~SectionParser() {} | 53 | virtual ~SectionParser() {} |
@@ -93,4 +96,7 @@ class Parser { | |||
93 | bool is_odm_etc_init_loaded_ = false; | 96 | bool is_odm_etc_init_loaded_ = false; |
94 | }; | 97 | }; |
95 | 98 | ||
99 | } // namespace init | ||
100 | } // namespace android | ||
101 | |||
96 | #endif | 102 | #endif |