diff options
Diffstat (limited to 'liblog/README')
-rw-r--r-- | liblog/README | 6 |
1 files changed, 5 insertions, 1 deletions
diff --git a/liblog/README b/liblog/README index 0676aecb8..461dfbe98 100644 --- a/liblog/README +++ b/liblog/README | |||
@@ -116,6 +116,10 @@ DESCRIPTION | |||
116 | code, otherwise the android_logger_list_read call will block for new | 116 | code, otherwise the android_logger_list_read call will block for new |
117 | entries. | 117 | entries. |
118 | 118 | ||
119 | The ANDROID_LOG_PSTORE mode flag to the android_logger_open is used to | ||
120 | switch from the active logs to the persistent logs from before the last | ||
121 | reboot. | ||
122 | |||
119 | The value returned by android_logger_open can be used as a parameter to | 123 | The value returned by android_logger_open can be used as a parameter to |
120 | the android_logger_clear function to empty the sub-log. It is recom‐ | 124 | the android_logger_clear function to empty the sub-log. It is recom‐ |
121 | mended to only open log ANDROID_LOG_WRONLY in that case. | 125 | mended to only open log ANDROID_LOG_WRONLY in that case. |
@@ -132,4 +136,4 @@ SEE ALSO | |||
132 | 136 | ||
133 | 137 | ||
134 | 138 | ||
135 | 17 Dec 2013 LIBLOG(3) | 139 | 24 Jan 2014 LIBLOG(3) |