diff options
Diffstat (limited to 'libnetutils')
-rw-r--r-- | libnetutils/Android.mk | 3 | ||||
-rw-r--r-- | libnetutils/include/netutils/dhcp.h | 44 | ||||
-rw-r--r-- | libnetutils/include/netutils/ifc.h | 66 |
3 files changed, 113 insertions, 0 deletions
diff --git a/libnetutils/Android.mk b/libnetutils/Android.mk index 2060df499..281b6c8e1 100644 --- a/libnetutils/Android.mk +++ b/libnetutils/Android.mk | |||
@@ -16,6 +16,9 @@ LOCAL_MODULE := libnetutils | |||
16 | 16 | ||
17 | LOCAL_CFLAGS := -Werror | 17 | LOCAL_CFLAGS := -Werror |
18 | 18 | ||
19 | LOCAL_EXPORT_C_INCLUDE_DIRS := $(LOCAL_PATH)/include | ||
20 | LOCAL_C_INCLUDES := $(LOCAL_PATH)/include | ||
21 | |||
19 | include $(BUILD_SHARED_LIBRARY) | 22 | include $(BUILD_SHARED_LIBRARY) |
20 | 23 | ||
21 | include $(CLEAR_VARS) | 24 | include $(CLEAR_VARS) |
diff --git a/libnetutils/include/netutils/dhcp.h b/libnetutils/include/netutils/dhcp.h new file mode 100644 index 000000000..008dbd887 --- /dev/null +++ b/libnetutils/include/netutils/dhcp.h | |||
@@ -0,0 +1,44 @@ | |||
1 | /* | ||
2 | * Copyright 2010, The Android Open Source Project | ||
3 | * | ||
4 | * Licensed under the Apache License, Version 2.0 (the "License"); | ||
5 | * you may not use this file except in compliance with the License. | ||
6 | * You may obtain a copy of the License at | ||
7 | * | ||
8 | * http://www.apache.org/licenses/LICENSE-2.0 | ||
9 | * | ||
10 | * Unless required by applicable law or agreed to in writing, software | ||
11 | * distributed under the License is distributed on an "AS IS" BASIS, | ||
12 | * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | ||
13 | * See the License for the specific language governing permissions and | ||
14 | * limitations under the License. | ||
15 | */ | ||
16 | |||
17 | #ifndef _NETUTILS_DHCP_H_ | ||
18 | #define _NETUTILS_DHCP_H_ | ||
19 | |||
20 | #include <sys/cdefs.h> | ||
21 | #include <arpa/inet.h> | ||
22 | |||
23 | __BEGIN_DECLS | ||
24 | |||
25 | extern int do_dhcp(char *iname); | ||
26 | extern int dhcp_start(const char *ifname); | ||
27 | extern int dhcp_start_renew(const char *ifname); | ||
28 | extern int dhcp_get_results(const char *ifname, | ||
29 | char *ipaddr, | ||
30 | char *gateway, | ||
31 | uint32_t *prefixLength, | ||
32 | char *dns[], | ||
33 | char *server, | ||
34 | uint32_t *lease, | ||
35 | char *vendorInfo, | ||
36 | char *domain, | ||
37 | char *mtu); | ||
38 | extern int dhcp_stop(const char *ifname); | ||
39 | extern int dhcp_release_lease(const char *ifname); | ||
40 | extern char *dhcp_get_errmsg(); | ||
41 | |||
42 | __END_DECLS | ||
43 | |||
44 | #endif /* _NETUTILS_DHCP_H_ */ | ||
diff --git a/libnetutils/include/netutils/ifc.h b/libnetutils/include/netutils/ifc.h new file mode 100644 index 000000000..3b272343d --- /dev/null +++ b/libnetutils/include/netutils/ifc.h | |||
@@ -0,0 +1,66 @@ | |||
1 | /* | ||
2 | * Copyright 2008, The Android Open Source Project | ||
3 | * | ||
4 | * Licensed under the Apache License, Version 2.0 (the "License"); | ||
5 | * you may not use this file except in compliance with the License. | ||
6 | * You may obtain a copy of the License at | ||
7 | * | ||
8 | * http://www.apache.org/licenses/LICENSE-2.0 | ||
9 | * | ||
10 | * Unless required by applicable law or agreed to in writing, software | ||
11 | * distributed under the License is distributed on an "AS IS" BASIS, | ||
12 | * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied. | ||
13 | * See the License for the specific language governing permissions and | ||
14 | * limitations under the License. | ||
15 | */ | ||
16 | |||
17 | #ifndef _NETUTILS_IFC_H_ | ||
18 | #define _NETUTILS_IFC_H_ | ||
19 | |||
20 | #include <sys/cdefs.h> | ||
21 | #include <arpa/inet.h> | ||
22 | |||
23 | __BEGIN_DECLS | ||
24 | |||
25 | extern int ifc_init(void); | ||
26 | extern void ifc_close(void); | ||
27 | |||
28 | extern int ifc_get_ifindex(const char *name, int *if_indexp); | ||
29 | extern int ifc_get_hwaddr(const char *name, void *ptr); | ||
30 | |||
31 | extern int ifc_up(const char *name); | ||
32 | extern int ifc_down(const char *name); | ||
33 | |||
34 | extern int ifc_enable(const char *ifname); | ||
35 | extern int ifc_disable(const char *ifname); | ||
36 | |||
37 | #define RESET_IPV4_ADDRESSES 0x01 | ||
38 | #define RESET_IPV6_ADDRESSES 0x02 | ||
39 | #define RESET_IGNORE_INTERFACE_ADDRESS 0x04 | ||
40 | #define RESET_ALL_ADDRESSES (RESET_IPV4_ADDRESSES | RESET_IPV6_ADDRESSES) | ||
41 | extern int ifc_reset_connections(const char *ifname, const int reset_mask); | ||
42 | |||
43 | extern int ifc_get_addr(const char *name, in_addr_t *addr); | ||
44 | extern int ifc_set_addr(const char *name, in_addr_t addr); | ||
45 | extern int ifc_add_address(const char *name, const char *address, | ||
46 | int prefixlen); | ||
47 | extern int ifc_del_address(const char *name, const char *address, | ||
48 | int prefixlen); | ||
49 | extern int ifc_set_prefixLength(const char *name, int prefixLength); | ||
50 | extern int ifc_set_hwaddr(const char *name, const void *ptr); | ||
51 | extern int ifc_clear_addresses(const char *name); | ||
52 | |||
53 | extern int ifc_create_default_route(const char *name, in_addr_t addr); | ||
54 | extern int ifc_remove_default_route(const char *ifname); | ||
55 | extern int ifc_get_info(const char *name, in_addr_t *addr, int *prefixLength, | ||
56 | unsigned *flags); | ||
57 | |||
58 | extern int ifc_configure(const char *ifname, in_addr_t address, | ||
59 | uint32_t prefixLength, in_addr_t gateway, | ||
60 | in_addr_t dns1, in_addr_t dns2); | ||
61 | |||
62 | extern in_addr_t prefixLengthToIpv4Netmask(int prefix_length); | ||
63 | |||
64 | __END_DECLS | ||
65 | |||
66 | #endif /* _NETUTILS_IFC_H_ */ | ||