diff options
Diffstat (limited to 'libsparse/include/sparse/sparse.h')
-rw-r--r-- | libsparse/include/sparse/sparse.h | 3 |
1 files changed, 2 insertions, 1 deletions
diff --git a/libsparse/include/sparse/sparse.h b/libsparse/include/sparse/sparse.h index 8b757d22a..42d4adb87 100644 --- a/libsparse/include/sparse/sparse.h +++ b/libsparse/include/sparse/sparse.h | |||
@@ -234,6 +234,7 @@ struct sparse_file *sparse_file_import(int fd, bool verbose, bool crc); | |||
234 | * | 234 | * |
235 | * @fd - file descriptor to read from | 235 | * @fd - file descriptor to read from |
236 | * @crc - verify the crc of a file in the Android sparse file format | 236 | * @crc - verify the crc of a file in the Android sparse file format |
237 | * @verbose - whether to use verbose logging | ||
237 | * | 238 | * |
238 | * Reads an existing sparse or normal file into a sparse file cookie. | 239 | * Reads an existing sparse or normal file into a sparse file cookie. |
239 | * Attempts to determine if the file is sparse or not by looking for the sparse | 240 | * Attempts to determine if the file is sparse or not by looking for the sparse |
@@ -243,7 +244,7 @@ struct sparse_file *sparse_file_import(int fd, bool verbose, bool crc); | |||
243 | * | 244 | * |
244 | * Returns a new sparse file cookie on success, NULL on error. | 245 | * Returns a new sparse file cookie on success, NULL on error. |
245 | */ | 246 | */ |
246 | struct sparse_file *sparse_file_import_auto(int fd, bool crc); | 247 | struct sparse_file *sparse_file_import_auto(int fd, bool crc, bool verbose); |
247 | 248 | ||
248 | /** sparse_file_resparse - rechunk an existing sparse file into smaller files | 249 | /** sparse_file_resparse - rechunk an existing sparse file into smaller files |
249 | * | 250 | * |