summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
Diffstat (limited to 'libunwindstack/include/unwindstack/MapInfo.h')
-rw-r--r--libunwindstack/include/unwindstack/MapInfo.h49
1 files changed, 49 insertions, 0 deletions
diff --git a/libunwindstack/include/unwindstack/MapInfo.h b/libunwindstack/include/unwindstack/MapInfo.h
new file mode 100644
index 000000000..2a97dde09
--- /dev/null
+++ b/libunwindstack/include/unwindstack/MapInfo.h
@@ -0,0 +1,49 @@
1/*
2 * Copyright (C) 2016 The Android Open Source Project
3 *
4 * Licensed under the Apache License, Version 2.0 (the "License");
5 * you may not use this file except in compliance with the License.
6 * You may obtain a copy of the License at
7 *
8 * http://www.apache.org/licenses/LICENSE-2.0
9 *
10 * Unless required by applicable law or agreed to in writing, software
11 * distributed under the License is distributed on an "AS IS" BASIS,
12 * WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 * See the License for the specific language governing permissions and
14 * limitations under the License.
15 */
16
17#ifndef _LIBUNWINDSTACK_MAP_INFO_H
18#define _LIBUNWINDSTACK_MAP_INFO_H
19
20#include <stdint.h>
21
22#include <string>
23
24namespace unwindstack {
25
26// Forward declarations.
27class Elf;
28class Memory;
29
30struct MapInfo {
31 uint64_t start;
32 uint64_t end;
33 uint64_t offset;
34 uint16_t flags;
35 std::string name;
36 Elf* elf = nullptr;
37 // This value is only non-zero if the offset is non-zero but there is
38 // no elf signature found at that offset. This indicates that the
39 // entire file is represented by the Memory object returned by CreateMemory,
40 // instead of a portion of the file.
41 uint64_t elf_offset;
42
43 Memory* CreateMemory(pid_t pid);
44 Elf* GetElf(pid_t pid, bool init_gnu_debugdata = false);
45};
46
47} // namespace unwindstack
48
49#endif // _LIBUNWINDSTACK_MAP_INFO_H