diff options
Diffstat (limited to 'qemu_pipe/include/qemu_pipe.h')
-rw-r--r-- | qemu_pipe/include/qemu_pipe.h | 6 |
1 files changed, 4 insertions, 2 deletions
diff --git a/qemu_pipe/include/qemu_pipe.h b/qemu_pipe/include/qemu_pipe.h index 16486c087..098749899 100644 --- a/qemu_pipe/include/qemu_pipe.h +++ b/qemu_pipe/include/qemu_pipe.h | |||
@@ -28,8 +28,10 @@ extern "C" { | |||
28 | // This file descriptor can be used as a standard pipe/socket descriptor. | 28 | // This file descriptor can be used as a standard pipe/socket descriptor. |
29 | // | 29 | // |
30 | // 'pipeName' is the name of the emulator service you want to connect to, | 30 | // 'pipeName' is the name of the emulator service you want to connect to, |
31 | // and must begin with 'pipe:' (e.g. 'pipe:camera' or 'pipe:opengles'). | 31 | // and should begin with 'pipe:' (e.g. 'pipe:camera' or 'pipe:opengles'). |
32 | // | 32 | // For backward compatibility, the 'pipe:' prefix can be omitted, and in |
33 | // that case, qemu_pipe_open will add it for you. | ||
34 | |||
33 | // On success, return a valid file descriptor, or -1/errno on failure. E.g.: | 35 | // On success, return a valid file descriptor, or -1/errno on failure. E.g.: |
34 | // | 36 | // |
35 | // EINVAL -> unknown/unsupported pipeName | 37 | // EINVAL -> unknown/unsupported pipeName |