diff options
Diffstat (limited to 'rootdir/init.rc')
-rw-r--r-- | rootdir/init.rc | 7 |
1 files changed, 6 insertions, 1 deletions
diff --git a/rootdir/init.rc b/rootdir/init.rc index be74f6fc2..86e124f15 100644 --- a/rootdir/init.rc +++ b/rootdir/init.rc | |||
@@ -61,7 +61,8 @@ loglevel 3 | |||
61 | 61 | ||
62 | # See storage config details at http://source.android.com/tech/storage/ | 62 | # See storage config details at http://source.android.com/tech/storage/ |
63 | mkdir /mnt/shell 0700 shell shell | 63 | mkdir /mnt/shell 0700 shell shell |
64 | mkdir /storage 0050 root sdcard_r | 64 | mkdir /mnt/media_rw 0700 media_rw media_rw |
65 | mkdir /storage 0751 root sdcard_r | ||
65 | 66 | ||
66 | # Directory for putting things only root should see. | 67 | # Directory for putting things only root should see. |
67 | mkdir /mnt/secure 0700 root root | 68 | mkdir /mnt/secure 0700 root root |
@@ -133,6 +134,10 @@ loglevel 3 | |||
133 | # This is needed by any process that uses socket tagging. | 134 | # This is needed by any process that uses socket tagging. |
134 | chmod 0644 /dev/xt_qtaguid | 135 | chmod 0644 /dev/xt_qtaguid |
135 | 136 | ||
137 | # Create location for fs_mgr to store abbreviated output from filesystem | ||
138 | # checker programs. | ||
139 | mkdir /dev/fscklogs 0770 root system | ||
140 | |||
136 | on post-fs | 141 | on post-fs |
137 | # once everything is setup, no need to modify / | 142 | # once everything is setup, no need to modify / |
138 | mount rootfs rootfs / ro remount | 143 | mount rootfs rootfs / ro remount |